Sort by
Introduction to TTL and CMOS Logic Gate Circuits24 November 2025
Electronic circuits that implement basic and common logic operations are called logic gate circuits. TTL and CMOS logic gate circuits are 2 typical types. Read this to learn their structure and features.
What are Varactor Diodes?24 November 2025
Varactor Diodes, also known as "variable reactance diodes", are made using the characteristic that the junction capacitance varies with the applied voltage when the PN junction is reverse biased. When the reverse bias voltage increases, the junction capacitance decreases, on the contrary, the junction capacitance increases.
Circuit Breaker: Working Principle, Types and Structure21 November 2025
Circuit breaker is a switching device capable of closing, carrying and breaking the current under normal and abnormal circuit conditions within a specified time. So what's its structure and how many types are there? How does it work? Read this.
Introduction to Electrochemical Sensors19 November 2025
Electrochemical sensors are made on the basis of ion conduction. According to the formation of their electrical characteristics, electrochemical sensors can be divided into potential sensors, conductivity sensors, electricity sensors, polarographic sensors, and electrolytic sensors.
Classification of Current Sensors18 November 2025
A current sensor is a detection device that can detect the information of the measured current, and can transform the detected information into electrical signals that meet certain standards or other required forms of information output according to certain rules to meet information transmission, processing, storage, display, recording, and control requirements.
What are Types and Application of Gas Sensors?18 November 2025
The gas sensor is the core of the gas detection system and is usually installed in the detection head. Essentially, a gas sensor is a converter that converts a certain gas volume fraction into a corresponding electrical signal. The probe uses the gas sensor to adjust the gas sample, which usually includes filtering out impurities and interfering gases, drying or refrigeration treatment, sample pump, and even chemical treatment of the sample, so that the chemical sensor can make faster measurements. In the following, we’ll mainly discuss the properties, typical types and application fields of gas sensors.
Humidity Sensor: Classification, Package and Application13 November 2025
Human survival and social activities are closely related to humidity. With the development of modernization, it is difficult to find an area that has nothing to do with humidity. Due to different application fields, the technical requirements for humidity sensors are also different. From a manufacturing point of view, humidity sensors with different materials and structures, and processes have different performance and technical indicators (such as accuracy), and the price also varies.
Basic Introduction to Hall Effect Sensors13 November 2025
The Hall effect sensor is a magnetic field sensor made according to the Hall effect. The Hall effect is a type of magnetoelectric effect. This phenomenon was discovered by Hall (A.H. Hall, 1855-1938) in 1879 when he studied the conductive mechanism of metals.
Lithium-ion Battery: Structure, Working Principle and Package08 November 2025
Hello everyone, I am Rose. Welcome to the new post today. Lithium battery is a kind of battery with lithium metal or lithium alloy as positive/negative material and non-aqueous electrolyte solution.
What is RF Power Amplifier?08 November 2025
Hello everyone, I am Rose. Today I will introduce RF Power Amplifier to you. The radio frequency power amplifier (RF PA) is a critical component of many wireless transmitters, and its significance is self-evident.
What is Amplifier?08 November 2025
Hello everyone, I am Rose. Today I want to introduce amplifier to you. An amplifier is a device that can amplify the voltage or power of an input signal, and is composed of tubes or transistors, power transformers and other electrical components. Used in communication, broadcasting, radar, television, automatic control and other devices.
Introduction to DC Amplifier07 November 2025
An amplifier that can amplify DC signals is called a DC amplifier. A DC amplifier amplifies a DC signal or an alternating signal that changes very slowly with time.


Product
Brand
Articles
Tools