web counter

What is a Cascode Amplifier?

Published: 03 March 2021 | Last Updated: 27 March 202516060
An analog circuit's output is increased by using a cascode amplifier. The use of cascode is a common approach that can be extended to both transistor and vacuum tube applications. In the year 1939, the tern cascode was included in an article written by Roger Wayne Hickman and Frederick Vinton Hunt.
In this video, what is Cascode Amplifier, and the small-signal analysis of the Cascode Amplifier is explained in detail. Using the small-signal analysis, the expression of output impedance and the intrinsic gain of the Cascode Amplifier is found. At the later part of the video, the effect of load on the voltage gain of the cascode amplifier is explained by taking the example of the passive-resistive load, the active PMOS current source as a load, and the cascode current source as a load.   Timestamps : 0:00 What is Cascode Amplifier? 1:22 Why Cascode Amplifier is used in integrated circuits? 2:36 Output Impedance of Cascode Amplifier (Small signal analysis) 8:00 Intrinsic Gain of Cascode Amplifier (Small signal analysis) 16:02 Effect of various load on the voltage gain of the cascode amplifier 19:49 Cascode amplifier with Cascode current source as a load   What is Cascode Amplifier? The Cascode Amplifier is the combination of the Common Source and the Common gate stages.  In this configuration, the input is applied to the Common Source Stage and the output of the Common Source Stage is fed to the Common Gate stage.    The Cascode Amplifier provides 1) High Input Impedance 2) High Output Impedance 3) High Intrinsic Gain 4) Large Bandwidth   In this video, through a small-signal analysis, the equation of the output resistance and the Intrinsic gain of the cascode amplifier is derived. And the effect of various loads on the voltage gain of the cascode amplifier is discussed.  The link for the other useful videos related to MOSFET:  1) MOSFET Biasing: Enhancement Type MOSFET Biasing Explained https://youtu.be/Ae8L9-WOiVE  2) MOSFET Channel Length Modulation https://youtu.be/qFbdsLm5mvI  3) MOSFET Small Signal Model: https://youtu.be/utBRWK4GmmE  4) MOSFET Common Source Amplifier (Voltage Divider Bias) https://youtu.be/T-0X1N9N5V8  5) MOSFET Common Gate Amplifier https://youtu.be/2zr5ykXpyXY  6) MOSFET Amplifier with Active Load: https://youtu.be/IOCK41RNpGs  This video is helpful to all the students of science and engineering for understanding what is cascode amplifier and the small-signal analysis of cascode amplifier.  #ALLABOUTELECTRONICS #MOSFET #CascodeAmplifier #MOSFETAmplifier #CascodeCurrentSource  -------------------------------------------------------------------------------------------------- Follow my second channel: https://www.youtube.com/channel/UCGA2...  Follow me on Facebook: https://www.facebook.com/ALLABOUTELEC...  Follow me on Instagram: https://www.instagram.com/all_about.e... -------------------------------------------------------------------------------------------------- Music Credit: http://www.bensound.com

Cascode Amplifier using MOSFET Explained (Cascode Amplifier with Cascode Current Source)

Catalog

I. General Introduction1. Cascode Amplifier Circuit 
2. Folded Cascode Amplifier
II. Features1. Frequency Response
2. Stability
3. Advantages and Disadvantages

 

An analog circuit's output is increased by using a cascode amplifier. The use of cascode is a common approach that can be extended to both transistor and vacuum tube applications. In the year 1939, the tern cascode was included in an article written by Roger Wayne Hickman and Frederick Vinton Hunt. The subject at hand is the use of voltage stabilizers. They constructed a cascode for two triodes, with the first using a common cathode configuration and the second using a common grid as a pentode substitution. As a consequence, the name can be translated as a reduction of cascaded triodes with pentode-like characteristics.

I. General Introduction of Cascode Amplifier

The cascode amplifier is split into two stages: a CE (common-emitter) stage and a CB (common-base) stage, with the CE feeding the CB. As opposed to a single stage of an amplifier, the mixture of both will have multiple properties such as high input/output separation, high i/p impedance, high o/p impedance, and high bandwidth.

This amplifier is commonly used in current circuits by using two transistors, either BJTs or FETs. One transistor acts as a CE, or common source, while the others act as a CB, or common gate. Since there is no direct coupling from the o/p to the i/p, this amplifier increases i/o separation, eliminates the miller effect, and hence provides high bandwidth.

1. Cascode Amplifier Circuit

The input step of a field-effect transistor is a FET CS amplifier, and Vin voltage is applied to the transistor's gate terminal. The output phase, on the other hand, is the FET CG amplifier that is powered by the input phase. Rd is the drain resistance for the output step, and Vout is the output voltage collected from Q2. Since Q2 is grounded in the circuit, the drain voltage in FET Q1 and the source voltage in FET Q2 are kept constant. This means that FET Q2 has the lowest input resistance for FET Q1. Low input resistance for Q1 decreases gain and Miller effect values, resulting in an increase in bandwidth level indirectly.

The reduction in FET Q1 gain has little effect on the circuit's total gain because FET Q2 compensates for it. Since discharge and charges from the drain terminal to the source stray capacitance are conducted via the Rd, the Miller effect has little effect on FET Q2, and the frequency response and load values are only disrupted for elevated frequency ranges. The output values of the cascode amplifier are totally isolated from the input values in the circuit architecture. Q1 has fixed voltage levels at the source and drain terminals, while Q2 has fixed voltage levels at the gate and source terminals. The following is a circuit diagram for a FET-operated cascode amplifier:

 

The FET-based Cascode amplifier circuit is shown below. The Vin (input voltage) is attached to the gate terminal of this amplifier's input stage, which is a typical source of FET. This amplifier's output stage is a typical gate FET with an ambitious input step. The o/p stage's drain resistance is Rd, and the Vout (output voltage) can be calculated at the drain terminal of the secondary transistor.

Since the gate terminal of the Q2 transistor is grounded, the source and drain voltages of the transistors are kept unchanged. That is, the higher Q2 transistor has a low i/p resistance in the direction of the lower Q1 transistor. As a result, the lower transistor's gain is diminished, and the Miller effect is reduced as well. The bandwidth of SO would increase.

The lower transistor's gain loss has little effect on the overall gain since the upper transistor compensates for it. The Miller effect would not affect the upper transistor since the drain resistor should be used to charge and discharge the drain to source drift capacitance. For high frequencies, both the frequency response and the load were affected.

The output of this circuit can be separated from the input. The lower transistor has an approximately stable voltage at its source and drain terminals, while the higher transistor has nearly stable voltage at both terminals. There is practically no input from the o/p to the i/p. As a consequence, the two terminals are well separated using a secure voltage middle relation.

2. Folded Cascode Amplifier

This is a single-stage amplifier in which the typical source transistor is cas0ded with the reverse polarity CB transistor. In this circuit, the input segment is a variable pair that serves as a CS stage for the cascode. The two transistor drains are attached to CG transistors with reverse polarity. The CG transistors are then connected to the complex current source, and the circuit is complete.

Gain increment in a multi-stage amplifier can be accomplished due to the constructional nature of this amplifier. By folding the cascode into reverse polarity transistors, the circuit size can be held to a minimum while retaining circuit output and requiring reduced supply voltage. The output resistance value of the circuits can be improved using cascode transistors, which increases the amplifier signal gain. This is the folded cascode amplifier's key benefit.

II. Features of Cascode Amplifier

1. Frequency Response of Cascode Amplifier

The output responses are inverted in correspondence with the input in the cascode amplifier frequency response. They deliver improved amplitude outputs by implementing either cascode or common-emitter amplifiers. The cascode amplifier signal is three times greater than the predicted range as compared to a CE signal.

2. Stability of Cascode Amplifier

Another noteworthy characteristic of the cascode amplifier that must be addressed is its reliability. The cascode constructional architecture is a safe arrangement in and of itself. The lower transistor has a nearly constant voltage level at the source and drain terminals, so there isn't anything to create gate feedback. The upper transistor, on the other hand, retains a steady voltage level at the source and gate terminals. As a consequence, the only nodes with matching voltage levels are the output and reference nodes.

3. Advantages and Disadvantages of Cascode Amplifier

Advantages

  • Increased gain, reliability, better impedance ratios, more bandwidth levels, and slew rate are all characteristics of the cascode circuit.

  • The circuit's construction is incredibly basic.

  • In superheterodyne receivers, the cascode amplifier is implemented as a multiplication mixer. The oscillator signal is fed to the upper gate, while the RF signal is fed to the lower gate. So all of these signals are compounded, and the IF is used as the mixer-upper amplifier's drain.

Disadvantages

Two transistors with a high voltage supply are necessary for this amplifier. Two transistors should be biased by ample VDS in the process for the two-transistor cascode, setting a lower limit on the voltage supply.

References

  1. Pass Labs. (n.d.). Cascode Amp Design. https://www.passlabs.com/technical_article/cascode-amp-design/

  2. Piercarlo. (2007, February 16). Cascode and phaseshift relation. diyAudio. https://www.diyaudio.com/community/threads/cascode-and-phaseshift-relation.96437/

  3. YIC Electronics. (2024, July 29). Decoding the Cascode Amplifier Concept. https://www.yic-electronics.com/blog/Decoding-the-Cascode-Amplifier-Concept.html

  4. Cadence. (2023, October 11). Cascode Amplifier Configuration: Advantages and Disadvantages. https://resources.pcb.cadence.com/blog/2023-cascode-amplifier-configuration-advantages-and-disadvantages

  5. LimpAirport2223. (2024, October 11). Stability issues in a cascode LNA configuration. Reddit. https://www.reddit.com/r/rfelectronics/comments/1g1629f/stability_issues_in_a_cascode_lna_configuration/

  6. WaElectronics. (2020, June 30). Cascode Amplifier: Circuit, Advantages, Disadvantages and Applications. https://www.watelectronics.com/what-is-cascode-amplifier-circuit-its-working/

  7. Allen, P. E. (2016). Lecture 24 – Cascode Op Amps. CMOS Analog Circuit Design. https://aicdesign.org/wp-content/uploads/2018/08/lecture24-170907.pdf

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

What is cascode amplifier?

The cascode is a two-stage amplifier that consists of a common-emitter stage feeding into a common-base stage. In modern circuits, the cascode is often constructed from two transistors (BJTs or FETs), with one operating as a common emitter or common source and the other as a common base or common gate.

Why is cascode amplifier used?

The cascode amplifier, with its variations, is a key element in the circuit designer's tool kit of useful circuits. It has advantages for increasing bandwidth and for high-voltage amplifier applications. A cascode amplifier has a high gain, moderately high input impedance, a high output impedance, and a high bandwidth.

What is the difference between Cascade and cascode amplifier?

From a transistor perspective, a cascade is typically when the amplifier load(s) are connected in a left-to right horizontal chain configuration, whereas a cascode has the load(s) stacked vertically. An amplifier consisting of a common emitter input stage that drives a common base output stage.

What do you mean by cascading?

Cascading corresponds that the output of one stage is connected as an input to the next stage.

What is the difference between cascode and cascade?

In the cascade condition, the amplifier loads are in the horizontal configuration, whereas in cascode the loads are in a vertical configuration.

What do you mean by feedback in an amplifier?

Reducing the Miller effect and showing many advantages, a cascode amplifier is implemented in many of the modern circuits and various industries. With the enhancement of integrated circuits and technology improvements, cascode amplifiers gain more prominence and even as a modulator, amplification devices and, others. The other device from this classification is a bimos cascode amplifier. The other question that arises in this concept is what is biasing condition in cascode amplifier?

What is cascode mirror?

One way to add emitter resistance without using actual resistors or generating a large voltage drop is to stack one current mirror on top of another, as shown to the left. This arrangement is known as a cascode current mirror.
Related Articles

  • Introduction to MD8002A Audio Amplifier
    Introduction to MD8002A Audio Amplifier
    UTMEL27 March 20259942

    The MD8002A is an audio power amplifier that uses a 5V DC power supply to provide 2.0 watts of continuous power to a BTL load with less than 10% distortion. It was created with the aim of providing high-quality o/p control with fewer components. It doesn't use any output coupling capacitors or bootstrap capacitors.

    Read More
  • Understanding the Low Noise Amplifier (LNA)
    Understanding the Low Noise Amplifier (LNA)
    UTMEL20 March 202526652

    A low noise amplifier is an amplifier with a very low noise figure. It is generally used as a high-frequency or intermediate-frequency preamplifier for various types of radio receivers, as well as amplifying circuits for high-sensitivity electronic detection equipment.

    Read More
  • Introduction to Optical Amplifier
    Introduction to Optical Amplifier
    UTMEL27 March 202510520

    An optical amplifier is a subsystem product that can amplify optical signals in optical fiber communication systems. The principle of the optical amplifier is basically based on the stimulated radiation of the laser, which realizes the amplification effect by converting the energy of the pump light into the energy of the signal light.

    Read More
  • What is an Inverting Amplifier?
    What is an Inverting Amplifier?
    UTMEL25 April 202512483

    An inverting amplifier is a fundamental configuration of operational amplifiers where the output signal has opposite polarity to the input signal. This configuration uses an operational amplifier with its inverting input terminal receiving the input signal, while the non-inverting terminal is typically connected to ground. The primary function of this circuit is to amplify the input signal while inverting its phase by 180 degrees.

    Read More
  • Low-Power Design of Operational Amplifiers
    Low-Power Design of Operational Amplifiers
    UTMEL27 March 20257804

    Hello, this is Candy. With the rise in popularity of battery-powered electronics in recent years, analog circuit designers have been increasingly concerned about power usage. This article will cover how to use low-power op amps in system design, as well as low-power op amps with low supply voltage capabilities and their applications, as well as how to read and understand op amp data sheets appropriately. Circuit design with energy-saving technologies for more efficient device choices.

    Read More

Subscribe to Utmel !

Featured Parts More