Basic Introduction to Photocell

What is a Photocell?
Catalog

Ⅰ What is a Photocell?
Photocells, also known as photoresistors or LDRs, are a type of light-sensitive resistor, but the term can also include photovoltaic cells that generate electricity from light. Elprocus (2019)
A photocell can be described as a module that is light-sensitive. In a wide variety of uses, such as sunset to sunrise illumination, this may be used by connecting to an electrical or electronic circuit that mechanically turns on when light intensity is low. These are also found in other applications, such as automatic doors and intrusion detectors.

photocell
Photocells are lightweight, cheap, low-power, user-friendly, and do not wear out. They also feature dolls, gadgets, and appliances for that purpose. CdS cells (made of Cadmium-Sulfide), light-dependent resistors (LDR), and photoresistors are commonly referred to.
For most light-sensitive applications such as "is it bright or dark out," "is there anything in front of the sensor (that will block light)," "is there anything interrupting a laser beam" (break-beam sensors), or "which is the most light entering it from various sensors," photocells would be a strong option!
One type of sensor is the photocell, which can be used to help you to detect light. These are very thin, low-power, economical, very easy to use, and are the key features of photo-cells. For these purposes, they are widely found in gadgets, games, and appliances. Cadmium-Sulfide (CdS) cells are often referred to as these sensors. Photoresistors and LDRs are made up of these.
These sensors are ideal for devices that are light-sensitive, such as light that would otherwise blackout. If the block light is in front of the sensor if there is something that disturbs a laser light, sensors that touch much of the light.
Ⅱ Working of Photocells
An evacuated glass tube that contains two electrodes such as the collector and emitter can be used to create a Photocell. The shape of the terminal of the emitter will take the form of a semi-hollow cylinder. At a negative potential, it is still planned. The outline of the terminal of the collector can be in the form of a metal that can be arranged at the partly cylindrical emitter axis. This can be maintained consistently at a positive terminal. It is possible to patch the evacuated glass tube over a non-metallic base & pins are provided for external attachment at the base.

photocell’s internal structure
A photocell's working theory will depend on the phenomenon of electrical resistance & the photoelectric effect. This can be used to transform electrical energy into light energy.
The positive (+ve) terminal of a battery is connected while the emitter terminal is connected to the negative (-ve) terminal & collector terminal. The frequency of radiation in the emitter will be higher than the threshold frequency of the material, and so photo ton leakage will occur. The photon electrons are engaged in the collector's path. Here, with respect to the emitter terminal, the collector terminal is the positive terminal. The movement of current inside the circuit would therefore be there. If the strength of radiation is improved, then the photoelectric current is increased.
The photoelectric effect occurs when photons strike a semiconductor, freeing electrons to flow, reducing resistance and converting light energy into electrical energy. For example, in a photoresistor, resistance can drop from several megaohms in the dark to a few hundred ohms in bright light, as noted in scientific literature. ScienceDirect (n.d.) for detailed explanations, "A photocell is a light-to-electrical transducer, with resistance decreasing as light intensity increases, sensitive to wavelengths 400-700 nm, similar to the human eye."
Ⅲ Circuit Diagram of Photocells
The photocell used in the circuit is otherwise called the transistor switched circuit as a dark sensing circuit. Breadboard, jumper wires, battery-9V, transistor 2N222A, photocell, resistors-22 kilo-ohm, 47 ohms, and LEDs are the necessary components to construct the circuit.
This circuit uses the photocell to detect darkness, triggering the transistor to switch on the LED, useful for automatic night lights. In light, the photocell’s low resistance keeps the LED off.

In two conditions, such as when there is light and when it is dark, the above photocell circuit runs.
The photocell resistance is smaller in the first example, and then there will be a current flow into the second resistor, such as 22Kilo Ohms & photocell. The transistor 2N222A here acts as an insulator. The lane that contains the LED1, R1 & transistor would also be off.
The resistance of the photocell is high in the second example, and then the circuit lane will change. So the low resistance to the base of the transistor or through the photocell would be there.
Whenever the transistor's base terminal gets power, then the transistor 2N222A works like a conductor. ON will be the lane including the Lead, R1 & 2N222A resistor, and the LED will blink. But, if the transistor's base terminal gets power, then the transistor would behave like a conductor, then the LED will turn on.
Ⅳ Types of Photocells
The main types of photocells are Photoemissive, Photovoltaic, and Photoconductive. Specialized devices like CCDs (used in scientific imagery), Golay Cells (for IR sensing), and Photomultipliers (highly sensitive, multiplying light by 100 million) are advanced variants.
| Type | Description |
|---|---|
| Photoemissive Cell | Emits electrons when illuminated. It is applied in phototubes and operates based on the photoelectric effect. |
| Photovoltaic Cell | Transforms solar energy into electrical energy. For instance, solar cells function through the photovoltaic effect. |
| Photoconductive Cell | Its resistance varies according to the light intensity. Light - Dependent Resistors (LDRs) are examples, and it is utilized in light - sensing devices. |
| CCD (Charge - Coupled Device) | A photosensor that captures photons. It is employed in scientific imaging and converts photons into electrical charges. |
| Golay Cell | An infrared - sensing apparatus. It is not as common and is used for specialized applications. |
| Photomultiplier | Exhibits high sensitivity and can amplify light by a factor of 100 million. It is mainly used in physics research. |
Ⅴ Applications of Photocells
Photocells have extensive applications across various fields. In automatic lighting systems, they detect darkness to activate lights at night, such as streetlights automatically turning on at sunset in "dusk-to-dawn" systems. In sporting events, they function as timers to measure runners' speeds. For traffic monitoring, photocells count vehicles on roads by sensing shadows or interruptions. They're also used in measuring instruments like light meters to determine light intensity, and in security systems as components of burglar alarms. In robotics, photocells enable robots to hide in darkness, follow light beacons, or track paths by detecting contrast differences. In photography and cinematography, photocells are applied in exposure meters to determine optimal settings, while also assisting with sound reproduction in film audio systems. Compared to variable resistors and photovoltaic cells, photocells serve uniquely as both switches and sensors, offering distinct advantages in these applications.
| Application | Example |
|---|---|
| Automatic Lighting | Streetlights turning on at dusk, e.g., dusk-to-dawn lights. |
| Security Systems | Burglar alarms detecting intrusions via light changes. |
| Robotics | Line-following robots using photocells for navigation. |
| Scientific Instruments | Lux meters measuring light intensity for research. |
| Cinematography | Exposure meters ensuring correct film exposure. |
| Energy Generation | Solar cells powering remote sensors, e.g., weather stations. |
Reference
Elprocus. (2019). Photocell: Circuit Diagram, Working, Types and Its Applications. Retrieved from https://www.elprocus.com/photocell-working-and-its-applications/
Vedantu. (2023). Overview of Photocells: Learn Important Terms and Concepts. Retrieved from https://www.vedantu.com/evs/overview-of-photocells
ScienceDirect Topics. (n.d.). Photocell: An Overview. Retrieved from https://www.sciencedirect.com/topics/engineering/photocell
Wikipedia contributors. (2024). Photoresistor: Definition and Working Principle. In Wikipedia. Retrieved from https://en.wikipedia.org/wiki/Photoresistor
1.What is a photocell used for?
Photocells and motion sensors are electronic devices you can use to manage indoor or outdoor lighting. These sensors improve the security and safety of your home, automatically turning on lights when it gets dark or they detect motion. They also save energy by turning themselves off when extra light is unnecessary.
2.Do photocells go bad?
What is a normal lifespan for this photocell? If your light burns continuously, then the photocell has gone bad, and the entire unit should be replaced. The life span depends on how often and long it is turned on, but mine usually will last upwards of 10 years or more.
3.What causes a photocell to go bad?
One common problem that affects photocell functioning is incorrect or loose wiring between the photocell and the main circuitry of the lighting system. The wire that connects the photocell to the lighting circuit needs to have a solid, soldered connection. In addition, the system needs to have proper electrical power.
4.Do LED lights work with photocells?
Yes, but first you need to make sure that the photocell you're using is compatible with the LEDs. The best option is to go with an all-in-one solution, which combines lights, fixtures, and the photocell.
5.Which metal is used in photocell?
Caesium Caesium (Cesium) is widely and commonly used in photoelectric cells because it can easily convert sunlight into electricity.
6.What is a photocell in physics?
Photoelectric cell, also called Electric Eye, Photocell, or Phototube, an electron tube with a photosensitive cathode that emits electrons when illuminated and an anode for collecting the emitted electrons. The tubes are also used in photometry and in spectroscopy.
7.Do LED lights need a special photocell?
Standard photocells require a small current to operate during the daytime when the light is off. Because LEDs run at such a low voltage, this small current causes interference, flickering, and premature degradation. Therefore, LEDs require a different type of photocell than conventional bulbs.
8. How does a photocell differ from a photodiode?
Photocells are bidirectional, photodiode unidirectional
9.What are limitations in high-speed applications?
Photocells have slower response times, e.g., tens of milliseconds, per ScienceDirect
Current Shunt Resistor Pulse Rating Selection: Sizing for Inrush Energy, TCR Drift, and Kelvin ConnectionsUTMEL12 September 2026445This guide explains how to size low-ohmic current shunt resistors by separating steady-state thermal design from transient pulse survivability. It covers adiabatic inrush energy calculations, manufacturer pulse curves, terminal-temperature derating, composite TCR errors from copper terminations, 4-terminal Kelvin layouts, thermal EMF suppression, ESL-induced spikes, and a dual-checklist verification workflow.
Read More
What are the Differences Between Pull up and Pull down Resistors?UTMEL22 October 202540194Pull up is to clamp an uncertain signal to a high level with a resistor, and the resistor also acts as a current limiter. In the same way, pull down means to clamp the uncertain signal to a low level through a resistor. To pull up is to input current to the device, and the pull-down is to output the current.
Read More
Rheostat Basics: Types, Principle and FunctionsUTMEL25 December 202519746A rheostat is a device that can adjust the size of the resistance and can be connected to the circuit to adjust the size of the current. A general rheostat is composed of a wire with a larger resistance and a device that can change the contact point to adjust the effective length of the resistance wire. Rheostat can limit the current and protect the circuit, and change the voltage distribution in the circuit.
Read More
Basic Introduction to Metal Film ResistorUTMEL28 August 202014461Metal film resistors are a kind of film resistors. Metal film resistors are resistors in which special metals or alloys are used as resistor materials, and the resistor film layer is basically formed on ceramic or glass by vacuum evaporation or sputtering.
Read More
Varistor: Definition, Function, Working and TestingUTMEL03 April 202585803A varistor is a device with a non-linear volt-ampere characteristic. When the voltage applied to the varistor is lower than its threshold value, the current flowing through it is extremely small, which is equivalent to a resistor with infinite resistance, vice versa. The most common varistor is a metal oxide varistor (MOV).
Read More
Subscribe to Utmel !
AD9364BBCZAnalog Devices Inc.
SE2537L-RSkyworks Solutions Inc.
CYBL10162-56LQXICypress Semiconductor Corp
ALT6702RM45Q7Skyworks Solutions Inc.
CSR8510A06-ICXR-RQualcomm
BLUENRG-232STMicroelectronics
ADF7025BCPZAnalog Devices Inc.
ENW-89847A3KFPanasonic Electronic Components
CYBLE-202007-01Cypress Semiconductor Corp
CYBT-353027-02Cypress Semiconductor Corp


Product
Brand
Articles
Tools