In Circuit Design, What are the Differences Between the 6 Types of Grounding?

Published: 07 February 2022 | Last Updated: 25 March 20244957
Hello, everyone. I am Rose. Today I will introduce the definition, types, function, and meaning of ground wires to you. In an electrical system or electronic equipment, the ground wire is a wire that connects to the ground, the casing, or the reference potential zero. The ground wire is connected to the outer casing in most electrical appliances to prevent electric shock accidents caused by the destruction of the outer casing's inner insulation.
In this video, we’re going to discuss the commonly used, but often misunderstood term, Ground.

Electrical Grounding Explained | Basic Concepts

Topics covered in this article:
Ⅰ. What are ground wires?
Ⅱ. Types and functions of ground wires
Ⅲ. The meaning of subdividing the GND ground wire


Ⅰ. What are ground wires?

In an electrical system or electronic equipment, the ground wire is a wire that connects to the ground, the casing, or the reference potential zero. The ground wire is connected to the outer casing in most electrical appliances to prevent electric shock accidents caused by the destruction of the outer casing's inner insulation. For a grounding device, the ground cable is too short. Working ground and safety ground are two types of ground wire. A type of safety grounding wire is used to prevent electric shock accidents when people use electronic equipment such as home appliances and office equipment.


Ⅱ. Types and functions of ground wires

1. Analog ground  wire AGND

The analog ground wire AGND is mostly used in analog circuit parts such as the analog sensor's ADC acquisition circuit, the operational amplification ratio circuit, and so on. 

Because the signal in these analog circuits is analog and weak, it is easily affected by the huge current in other circuits. If the huge current is not distinguished, it will create a large voltage drop in the analog circuit, distorting the analog signal and, in extreme situations, causing the analog circuit to fail.

 

2. Digital ground  wire DGND 

The digital ground wire DGND.  which is obviously different from the analog ground wire AGND, is primarily used in the digital circuit part, such as the button detection circuit, USB communication circuit, single-chip circuit, and so on. The reason for this is that digital circuits all have the same feature: they are all discrete open light signals with only the digital "0" and "1" distinguishable.

(Digital signal) The voltage changes when leaping from a digital "0" voltage to a digital "1" voltage, or when jumping from a digital "1" voltage to a digital "0" value. The change, according to Maxwell's electromagnetic theory, Around the current, a magnetic field will be produced, causing EMC  radiation to nearby circuits.

No way, a separate digital ground wire DGND  must be used to effectively isolate other circuits in order to limit the circuit's EMC  radiation effect.

 

3. Power ground  wire PGND 

A low-power circuit is either the analog ground wire AGND or the digital ground wire DGND,  A distinct reference ground wire, known as the power ground wire PGND.  is used in high-power circuits such as motor drive circuits, solenoid valve drive circuits, and so on.

High-power circuits are those that have relatively large currents, as the name implies. A significant current, of course, can easily result in ground offset across separate functional circuits.

(This is known as the Earth Offset Phenomenon.)

When a circuit has a ground offset, the initial 5V voltage may become 4V instead of 5V.

Because the 5V voltage relates to the 0V voltage on the GND ground wire, if the ground offset causes the GND ground wire to rise from 0V to 1V, the prior 5V (5V-0V=5V) voltage becomes the present 4V (5V-1V=4V) voltage.

 

4. Power ground GND 

The DC ground GND includes the analog ground AGND, the digital ground DGND, and the power ground PGND, the 0V reference ground wire for the entire circuit is made up of all of these different sorts of ground wires. The power ground wire GND  is the name given to this ground line.

All circuits get their energy from the power supply. The power supply provides the voltage and current required for all circuit operations. As a result, the power supply's ground line GND  serves as the 0V voltage reference point for all circuits.

This is why other ground wires, such as an analog ground wire AGND, a digital ground wire DGND.  or a power ground wire PGND, must eventually be connected to the power ground wire GND

 

5. AC ground wire CGND 

The ground wire in an AC system CGND is commonly seen in circuit projects that use AC power, such as AC-DC power supply circuits.

There are two elements to the AC -DC power circuit. The circuit's front stage is the AC component, and the circuit's backstage is the DC component, which is forced to produce two ground wires, one for the AC and one for the DC

The AC ground wire serves as the AC  circuit part's 0V reference point, while the DC ground wire serves as the DC circuit part's 0V reference point. Engineers usually use a coupling capacitor or inductor to connect the   AC  ground wire to the DC ground wire in order to unify the ground wire GND in the circuit.

 

6. Earth ground wire  EGND 

The human body's safe voltage is less than 36 volts. The human body will be damaged if a voltage greater than 36 volts is applied to it. Engineers in the development and design of circuit projects have a shared sense of safety.

Engineers commonly employ the ground wire  EGND in high-voltage and high-current projects, such as household appliances, electric fans, refrigerators, televisions, and other circuits, to improve the circuit's safety factor.

(socket with EGND protection function for earth ground wire)

Why are there three terminals on a household appliance's socket? Only two wires are required for 220V AC: live and neutral. So, why are there three terminals on the sockets?

The socket's three terminals, two of which are the live and neutral wires for 220V, and one of which is the earth ground wire EGND for protection.

It's vital to note that the earth ground wire EGND, which is simply connected to our earth, serves as a high-voltage protection wire, does not participate in the project circuit function, and has no bearing on it.

As a result, the earth ground wire EGND and other types of ground wires GND have quite different circuit meanings.

 

Ⅲ. The meaning of subdividing the GND ground wire

Engineers may wonder how there can be so many differences between a ground wire  GND and how a basic circuit problem can be so difficult. Why do you need to introduce so many  GND ground functions that are subdivided?

Engineers commonly refer to this type of GND ground wire as GND and do not differentiate it in the schematic design process, making it difficult to distinguish between the GND ground wires of different circuit functions during PCB wiring. All GND ground wires should be connected together.

While this is easy to do, it leads to a number of problems:


Problem 1: Signal Crosstalk

If the ground wires GND of separate functions are connected directly, the high-power circuit will flow through the ground wire GND. A  ffecting the low-power circuit's 0V reference point GND. Resulting in crosstalk between circuit signals.

 

Problem 2: Signal Accuracy

The correctness of the signal is the primary criterion for evaluating analog circuits. Analog circuits lose their original functional purpose when they are not precise.

Because the  AC power supply's ground wire CGND  is a sine wave, it varies up and down on a regular basis, and its voltage fluctuates as well, not always remaining at 0V like the DC  ground wire GND

Connect the ground wires GND of various circuits together, and the periodically changing  AC ground wire CGND  will cause the ground wire AGND of the analog circuit to change, affecting the analog signal's voltage accuracy.

 

Problem 3: EMC  Experiment

The external electromagnetic radiation EMC is weaker when the signal is faint; the external electromagnetic radiation EMC is stronger when the signal is strong.

When the ground lines GND of various circuits are coupled together, the strong signal circuit's ground line GND directly interferes with the weak signal circuit's ground line  GND,  As a result, a signal source with mild external electromagnetic radiation has become a signal source with significant external electromagnetic radiation, increasing the difficulty of circuit processing EMC  studies.

 

Problem 4: Circuit Reliability

The circuit's ability to operate independently is greater when there are fewer parts of the signal connection; the circuit's ability to operate independently is weaker when there are more parts of the signal connection.

Consider this: if the two circuit systems A and B do not intersect, the function of circuit A cannot impact the regular operation of circuit B, and the function of circuit B cannot affect circuit A. of normal work.

The girl's emotional fluctuations will not affect the boy's mood, just as they will not affect the mood of a pair of strangers before they become lovers, because they do not have any intersection.

Connecting the ground wires of circuits with various purposes together in a circuit system is equal to increasing a link of interference between circuits, lowering


UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1. Is GND a kind of earthing in the circuit?

GND is short for the ground end of a wire, which stands for ground or 0 wire. GND means the common terminal, it can also be said to be the ground, but this ground is not the ground in the real sense, it is a ground assumed for the application, for the power supply, it is the negative pole of a power supply.

2. What is the difference between digital ground and analog ground in wiring?

Just two lines, walk apart and keep a little distance. No difference.

3. Can the AC ground wire and the DC ground wire be shared?

The AC ground wire and the DC ground wire can be shared. The reasons and points to note are as follows: Both DC grounding and AC grounding are theoretically grounded. Under normal circumstances, the current entering the AC ground is relatively large, and the grounding also has a certain grounding resistance. In actual use, the grounding of the two should be separated, and the entry points should be separated by a certain distance (about 1.3 meters), so that the AC signal will not break into the DC circuit. If it is really inseparable, connect it at the entry point as much as possible, and connect more decoupling capacitors on the DC power line to reduce the effect of AC coupling.
Related Articles

  • Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap Devices
    Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap Devices
    Saumitra Jagdale15 March 20242545

    For a long era, silicon has stood out as the primary material for fabricating electronic devices due to its affordability, moderate efficiency, and performance capabilities. Despite its widespread use, silicon faces several limitations that render it unsuitable for applications involving high power and elevated temperatures. As technological advancements continue and the industry demands enhanced efficiency from devices, these limitations become increasingly vivid. In the quest for electronic devices that are more potent, efficient, and compact, wide bandgap materials are emerging as a dominant player. Their superiority over silicon in crucial aspects such as efficiency, higher junction temperatures, power density, thinner drift regions, and faster switching speeds positions them as the preferred materials for the future of power electronics.

    Read More
  • A Comprehensive Guide to FPGA Development Boards
    A Comprehensive Guide to FPGA Development Boards
    UTMEL11 September 202517523

    This comprehensive guide will take you on a journey through the fascinating world of FPGA development boards. We’ll explore what they are, how they differ from microcontrollers, and most importantly, how to choose the perfect board for your needs. Whether you’re a seasoned engineer or a curious hobbyist, prepare to unlock new possibilities in hardware design and accelerate your projects. We’ll cover everything from budget-friendly options to specialized boards for image processing, delve into popular learning paths, and even provide insights into essential software like Vivado. By the end of this article, you’ll have a clear roadmap to navigate the FPGA landscape and make informed decisions for your next groundbreaking endeavor.

    Read More
  • Applications of FPGAs in Artificial Intelligence: A Comprehensive Guide
    Applications of FPGAs in Artificial Intelligence: A Comprehensive Guide
    UTMEL29 August 20254127

    This comprehensive guide explores FPGAs as powerful AI accelerators that offer distinct advantages over traditional GPUs and CPUs. FPGAs provide reconfigurable hardware that can be customized for specific AI workloads, delivering superior energy efficiency, ultra-low latency, and deterministic performance—particularly valuable for edge AI applications. While GPUs excel at parallel processing for training, FPGAs shine in inference tasks through their adaptability and power optimization. The document covers practical implementation challenges, including development complexity and resource constraints, while highlighting solutions like High-Level Synthesis tools and vendor-specific AI development suites from Intel and AMD/Xilinx. Real-world applications span telecommunications, healthcare, autonomous vehicles, and financial services, demonstrating FPGAs' versatility in mission-critical systems requiring real-time processing and minimal power consumption.

    Read More
  • 800G Optical Transceivers: The Guide for AI Data Centers
    800G Optical Transceivers: The Guide for AI Data Centers
    UTMEL24 December 20255913

    The complete guide to 800G Optical Transceiver standards (QSFP-DD vs. OSFP). Overcome supply shortages and scale your AI data center with Utmel Electronic.

    Read More
  • The 2026 Engineer’s Guide: Choosing the Right MCU for Your Next IoT & New Energy Project
    The 2026 Engineer’s Guide: Choosing the Right MCU for Your Next IoT & New Energy Project
    UTMEL30 April 2026447

    A comprehensive comparison of 2026's leading MCUs from ST, NXP, and Microchip across power efficiency, processing performance, connectivity, and ecosystems to help engineers select the optimal chip for next-gen IoT and new energy projects.

    Read More