Introduction to Graphics Processing Unit (GPU)

Graphics Processing Unit (GPU)
Catalog
Ⅰ Definition
A Graphics Processing Unit (GPU) is a chip or electronic circuit that can render graphics on an electronic computer for display. In 1999, the GPU was introduced to the broader market and is best known for providing the smooth graphics that customers demand in modern videos and games.
The central processing unit (CPU) conducted these measurements in the early days of computing. However, as more graphics-intensive apps were made, their specifications imposed a burden on the CPU and decreased performance. As a way to offload these tasks from CPUs and to improve the rendering of 3D graphics, GPUs were developed. GPUs operate by using a technique called parallel processing, where different parts of the same job are performed by many processors.
In PC (personal computer) games, GPUs are well known, allowing for smooth, high-quality graphics rendering. Developers have also been using GPUs to speed up workloads in fields such as artificial intelligence (AI).
Ⅱ History of GPUs
Since the dawn of video games in the 1970s, advanced chips for rendering graphics have existed. As part of a video card, a discrete dedicated circuit board, silicon chip, and required cooling that provides 2D, 3D, and often even general-purpose graphics processing (GPGPU) calculations for a computer, graphics capabilities were added early on. GPUs are usually called modern cards with optimized calculations for triangle configuration, transition, and lighting features for 3D applications. Higher-end GPUs, once uncommon, are now commonplace and often mixed into CPUs themselves.
In the late 1990s, graphics processing units were added to high-performance business computers, and in 1999, Nvidia released the first personal computer GPU, the GeForce 256.
Over time, for other resource-intensive tasks not connected to graphics, the computing power of GPUs made the chips a common option. Early implementations included scientific simulations and modeling; machine learning and AI software were both powered by GPU computing by the mid-2010s.
A virtualized GPU was launched by Nvidia in 2012, which discharges graphics processing power from the server CPU into a virtual desktop infrastructure (VDI). Traditionally, graphics efficiency has been one of the most common concerns among virtual desktop and device users, and virtualized GPUs are aimed at solving that problem.
Ⅲ How does a graphics processing unit function?
It is possible to see a GPU combined with a CPU on the same electronic circuit, on a graphics card, or on a personal computer or server motherboard. In construction, GPUs and CPUs are somewhat comparable. GPUs, however, are primarily designed for more complicated mathematical and geometric calculations to be done. To render graphics, these calculations are required. More transistors than a CPU can be used in GPUs.
Parallel processing can be used by GPUs, where several processors perform different pieces of the same job. To save data on the images it processes, a GPU may also have its own RAM (random access memory). There is information stored about each pixel, including its position on the monitor. The RAM is attached to a digital-to-analog converter (DAC) which converts the image into an analog signal so that it can be viewed by the monitor. Usually, video RAM can run at high speeds.
In two ways, GPUs will come: integrated and discrete. In addition to the GPU, integrated GPUs come embedded, while discrete GPUs can be placed on a separate circuit board.
It could be a reasonable idea to get GPUs fixed in the cloud for businesses that need strong processing resources, or deal with deep learning or 3D visualizations. Google's Cloud GPUs, which deliver Google Cloud high-performance GPUs, is an example of this. The advantages of freeing up local energy, saving time, expense, and scalability would be to host GPUs in the cloud. Users can select from a number of types of GPU while gaining customizable performance depending on their specifications.
Ⅳ What are GPUs used for?
While GPUs in top-quality video games are most commonly associated with life-like graphics, they can also be found in other industries.
In rendering 3D models, business applications such as AutoCAD, for example, benefit from GPUs. The PC on which it is made has to be able to handle the pressure of the editing process due to this form of the program requiring continuous adjustments in a brief amount of time. The GPU supports the re-rendering of the 3D models in this case.
In video editing, another common use of GPUs is particularly when dealing with massive amounts of high-resolution images, such as 4K or 360-degree videos. For most regular CPUs, editing these types of files may be difficult, which is why a high-end GPU is extremely helpful in being able to transcode video files at a fair cost.
GPUs will also make it easy to process machine learning functions and build neural networks, which is another job that can be daunting for a CPU because of the vast swaths of data involved in the process.
It is important to remember, though, that not all GPUs are made equal. It is advised that you select a GPU with additional in-depth support if you are looking for a customized, business type of processor that is intended for particular types of applications. These are made by giants of the semiconductor industry such as AMD and Nvidia, known for selling high-level chips to some of the largest software firms, from Facebook and Google to Microsoft and Lenovo.
Ⅴ How to select GPU?
You now know the fundamentals of what a GPU does and the many kinds out there. So, how do you know which one is necessary for you? You need a graphics card if you're playing games on a laptop, and there's a whole world of feedback out there to help you pick the right one.

Generally, make sure to choose a graphics card that is perfect for the size of your display, such as 1080p, 1440p, or 4K. The features of video games are continually advancing and require new hardware. This means that graphics cards appear to become easier than other elements to become redundant. Anything published in the last two or three years should be purchased by desktop owners.
Be very, very patient when gaming on a laptop. There are multiple gaming laptops with standalone GPUs that are up to two decades old and cost almost as much (or almost as much) as a newer GPU laptop.
A powerful CPU is more important if you are concentrating on video editing enthusiasts, but a discrete graphics card is also needed.
Integrated graphics will do it for everybody else. For video streaming, basic online sports, or even basic picture editing, there is no need to get a graphics card. Only make sure that there is currently an optimized GPU on your CPU. Otherwise, when you start to boot up this new desktop build, you may be in for a disappointing surprise.
Ⅵ What's the Difference between GPU and CPU?
GPUs are similar to CPU architectures quite a bit. CPUs are, however, used to respond to and process the simple instructions driving a device, while GPUs are primarily designed to make high-resolution images and video rapidly. Basically, CPUs are responsible for translating much of the commands of a machine, whereas graphics processing is the focus of GPUs.
In general, a GPU is designed for data parallelism and for several data objects implementing the same instruction (SIMD). For task-parallelism and doing numerous operations, a CPU is built.
The number of cores also differentiates them. The processor inside the processor is actually the heart. Most CPU cores, though some have up to 32 cores, are numbered between four and eight. Each center can process tasks or threads of its own. As some processors have multithreading capability-in which the core is virtually separated, causing two threads to be processed by a single core-the number of threads can be much greater than the number of cores. In video editing and transcoding, this may be helpful. Two threads (independent instructions) per core can be executed on CPUs (the independent processor unit). There can be four to 10 threads per core on a GPU core.
Due to its parallel-processing architecture, a GPU can render images more efficiently than a CPU, which enables it to run several calculations at the same time. While multi-core processors can conduct calculations in parallel by combining more than one CPU on the same chip, a single CPU does not have this capability.
A CPU often has a higher clock speed, which ensures that it can perform an actual computation quicker than a GPU, meaning that simple computing operations are much best suited to handle.
1.What is GPU how is it useful?
The GPU, or Graphics Processing Unit, is a specialized circuit that focuses on generating images for a device to display. Every modern mobile device has some form of a GPU to aid in generating images and computer graphics and is an essential part of every modern mobile device.
2.Is a GPU a graphics card?
GPU stands for the graphics processing unit. You'll also see GPUs commonly referred to as graphics cards or video cards. Every PC uses a GPU to render images, video, and 2D or 3D animations for display. A GPU performs quick math calculations and frees up the CPU to do other things.
3.What is the difference between GPU and CPU?
The main difference between CPU and GPU architecture is that a CPU is designed to handle a wide range of tasks quickly (as measured by CPU clock speed), but is limited in the concurrency of tasks that can be running. A GPU is designed to quickly render high-resolution images and video concurrently.
4.How much faster is a GPU than a CPU?
It has been observed that the GPU runs faster than the CPU in all tests performed. In some cases, GPU is 4-5 times faster than CPU, according to the tests performed on GPU server and CPU server. These values can be further increased by using a GPU server with more features.
5.Can you turn on a PC without a graphics card?
Yes. You will need a CPU with an iGPU and motherboard with a display output to see POST and the BIOS though. If you don't have that, things may turn on, but not all boards will boot without a display output.
6.Does a graphics card make your computer faster?
If the computer's built-in graphics card shares the computer's memory, installing a graphics card will free up that memory for the computer to use in other tasks. Additionally, the memory built-in to a graphics card is usually faster than the memory the computer uses, which can also contribute to a performance boost.
Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap DevicesSaumitra Jagdale15 March 20242975For a long era, silicon has stood out as the primary material for fabricating electronic devices due to its affordability, moderate efficiency, and performance capabilities. Despite its widespread use, silicon faces several limitations that render it unsuitable for applications involving high power and elevated temperatures. As technological advancements continue and the industry demands enhanced efficiency from devices, these limitations become increasingly vivid. In the quest for electronic devices that are more potent, efficient, and compact, wide bandgap materials are emerging as a dominant player. Their superiority over silicon in crucial aspects such as efficiency, higher junction temperatures, power density, thinner drift regions, and faster switching speeds positions them as the preferred materials for the future of power electronics.
Read More
Applications of FPGAs in Artificial Intelligence: A Comprehensive GuideUTMEL29 August 20255834This comprehensive guide explores FPGAs as powerful AI accelerators that offer distinct advantages over traditional GPUs and CPUs. FPGAs provide reconfigurable hardware that can be customized for specific AI workloads, delivering superior energy efficiency, ultra-low latency, and deterministic performance—particularly valuable for edge AI applications. While GPUs excel at parallel processing for training, FPGAs shine in inference tasks through their adaptability and power optimization. The document covers practical implementation challenges, including development complexity and resource constraints, while highlighting solutions like High-Level Synthesis tools and vendor-specific AI development suites from Intel and AMD/Xilinx. Real-world applications span telecommunications, healthcare, autonomous vehicles, and financial services, demonstrating FPGAs' versatility in mission-critical systems requiring real-time processing and minimal power consumption.
Read More
The 2026 Engineer’s Guide: Choosing the Right MCU for Your Next IoT & New Energy ProjectUTMEL30 April 20262324A comprehensive comparison of 2026's leading MCUs from ST, NXP, and Microchip across power efficiency, processing performance, connectivity, and ecosystems to help engineers select the optimal chip for next-gen IoT and new energy projects.
Read More
AI Server Components: Engineering Next-Gen Data Center Hardware for 100kW RacksUTMEL15 May 20261232The transition from traditional enterprise IT to AI-driven workloads has rendered legacy data center hardware obsolete, forcing infrastructure planners to re-engineer server components for extreme thermal environments.
Read More
The Practical Engineer’s Guide to the NE555N Timer: Pinout, Setup, and TroubleshootingUTMEL29 May 20261088This comprehensive guide explores the NE555N timer, detailing its 8-pin layout, internal architecture, and key datasheet specifications. It compares the bipolar IC to CMOS variants and details setup configurations for astable, monostable, and bistable modes. Additionally, the guide offers practical troubleshooting advice to prevent common breadboard failures, such as floating reset pins and electrical noise issues.
Read More
Subscribe to Utmel !
MOC3010SMON Semiconductor
ADATE320-1KCPZAnalog Devices Inc.
AT88SC0104CA-SUMicrochip Technology
MOC3162MON Semiconductor
80HCPS1848CBLGIRenesas Electronics America Inc.
HCS500-I/PMicrochip Technology
AD8190ACPZ-R7Analog Devices Inc.
ATA663231-GBQWMicrochip Technology
AD9942BBCZAnalog Devices Inc.
ATAES132A-SHEQ-BMicrochip Technology


Product
Brand
Articles
Tools