web counter

VRAM (Video RAM) Explained

Published: 03 June 2021 | Last Updated: 03 June 202110598
VRAM (video RAM), also known as a frame buffer, is used to store the rendering data processed or about to be extracted by the graphics chip. Like computer memory, VRAM is a component used to store graphics information to be processed.
This video tells you how many gigabytes of graphics memory (VRAM) do you REALLY need.

How much VRAM do you need?

Catalog

Ⅰ Overview
Ⅱ Working principle of VRAM
Ⅲ VRAM parameters1.Memory capacity
2.Data bits
3.VRAM bit width
4.VRAM bandwidth
5.VRAM frequency
6.VRAM package
7.Clock cycle


Ⅰ Overview

The VRAM (video RAM) is a component used to store graphics information to be processed. The picture we see on the display is composed of individual pixels, and each pixel uses 4-32 or even 64-bit data to control its brightness and color. These data must be saved through the VRAM, and then deployed by the display chip and CPU, and finally, the calculation results are converted into graphics and output to the display. The VRAM, like the motherboard memory, performs the storage function, but the object it stores is the information of each pixel output by the graphics card to the display. After the display chip processes the data, it saves the data to the VRAM, and then the RAMDAC (digital-to-analog converter) reads the data from the VRAM and converts the digital signal into an analog signal. Finally, it is displayed on the screen.

Video memory or VRAM.jpeg

In advanced graphics accelerator cards, the VRAM is not only used to store graphics data but also used by the display chip to perform 3D function operations. In advanced display chips such as nVIDIA, a "GPU" (graphics processing unit) parallel to the CPU has been developed. Due to the role played by the graphics card, obviously, the speed and bandwidth of the graphics memory directly affect the overall speed of the graphics card. As a memory, VRAM has gone through multiple stages of development just like motherboard memory. It can even be said that the development of VRAM is more active than motherboard memory and has more varieties and types. The widely used VRAM types are SDRAM and SGRAM. DDR memory with better performance was first applied to graphics cards.

The graphics card is a BGA-packaged chipset on the motherboard, similar to the CPU (Central Processing Unit), called GPU (Graphics Processing Unit) in the industry. There are mainly two vendors, nVIDIA and AMD, on the market. The graphics chip is equivalent to the CPU of the graphics card, but its main task is to process display information. In the process of processing information, it will generate a large amount of temporary data (unprocessed, processing, processed), which requires a special place to store these temporary data, that is, VRAM. It may also be a chip or just a part of the chip, depending on the hardware design (dedicated graphics and integrated graphics).

Ⅱ Working principle of VRAM

Before the graphics card starts to work (graphic rendering modeling), the required material and texture data are transferred to the VRAM. At the beginning of modeling and rendering, these data are transmitted through the AGP bus, and the display chip will extract the data stored in the VRAM through the AGP bus. In addition to the modeling and rendering data, there is a large amount of vertex data and work instruction streams that need to be exchanged. These data are converted into analog signals through RAMDAC and output to the display end, which is the image we see in the end. The performance of the display chip is increasing day by day, and its data processing ability is getting stronger and stronger, making the VRAM data transmission volume and transmission rate also higher and higher, and the requirements for the VRAM of the graphics card are also higher. The size of the VRAM exchange and the speed of the speed are crucial to the performance of the graphics card core, and how to effectively improve the performance of the VRAM has become the key to improving the performance of the entire graphics card.

Ⅲ VRAM parameters

1.Memory capacity

8gb GDDR5 VRAM.jpg

8gb GDDR5 VRAM

VRAM capacity is the capacity of local VRAM on the graphics card, which is one of the key parameters for choosing a graphics card. The size of the VRAM capacity determines the ability of the VRAM to temporarily store data, and to a certain extent also affects the performance of the graphics card. The VRAM capacity is also gradually increasing with the development of graphics cards. The VRAM capacity has grown from the extremely small capacities of 512KB, 1MB, 2MB in the early days to 64MB, 128MB, 256MB, 512MB, 768MB, and up to the current mainstream 2GB, 4GB, 6GB and high-end graphics cards such as 8GB, 16GB, 32GB. Some professional graphics cards It even has 48GB of VRAM.

2.Data bits

The data bits refer to the number of bits that can be transmitted in one clock cycle. It is an important factor in determining the VRAM bandwidth and is closely related to the performance of the graphics card. When the type of VRAM is the same and the operating frequency is the same, the larger the number of data bits, the higher its performance. The calculation method of the VRAM bandwidth is: operating frequency×data bandwidth/8. Taking the current GeForce3 graphics card as an example, its VRAM system bandwidth = 230MHz × 2 (because DDR VRAM is used, it is multiplied by 2) × 128/8=7.36GB.

3.VRAM bit width

The VRAM bit width is the number of bits of data that can be transmitted in one clock cycle of the VRAM. The larger the number of bits, the greater the amount of data that can be transmitted in an instant. This is one of the important parameters of VRAM. There are currently three types of VRAM widths on the market: 64-bit, 128-bit, and 256-bit. The 64-bit, 128-bit, and 256-bit graphics cards that people are accustomed to calling refer to their corresponding VRAM widths. The higher the VRAM bit width, the better the performance, the higher the price. Therefore, 256-bit wide VRAM is more used in high-end graphics cards, and mainstream graphics cards basically use 128-bit VRAM. Everyone knows that the VRAM bandwidth = the VRAM frequency X the VRAM bit width/8, so when the VRAM frequency is equivalent, the VRAM bit width will determine the size of the VRAM bandwidth. For example, 128-bit and 256-bit VRAM with the same VRAM frequency of 500MHz, then their VRAM bandwidth will be: 128-bit=500MHz*128∕8=8GB/s, and 256-bit=500MHz*256∕8= 16GB/ s, is 2 times of 128 bits, which shows the importance of VRAM bit width in VRAM data.

4.VRAM bandwidth

The VRAM bandwidth is the bridge between the display chip and the VRAM. The larger the bandwidth, the faster the communication between the display chip and the VRAM. In order to indicate this width, the unit of VRAM bandwidth is bytes/second. The bandwidth of the VRAM is related to the bit width of the VRAM and the speed of the VRAM (that is, the operating frequency). Finally draw a conclusion: VRAM bandwidth = VRAM bit width × VRAM frequency/8. The speed of the VRAM is generally in ns, and the common VRAM is 6ns, 5.5ns, 5ns, 4ns, 3.8ns, up to 1.8ns. The corresponding operating frequencies are 143MHz, 166MHz, 183MHz, 200MHz, 250MHz, up to 550MHz. The calculation method of operating frequency is very simple-the reciprocal of the VRAM speed is the rated operating frequency of the VRAM. For example, if the clock cycle of the VRAM is 4ns, the operating frequency of the VRAM is 1/4ns=250MHz.

5.VRAM frequency

The VRAM frequency refers to the frequency at which the VRAM is working on the graphics card by default, in MHz (megahertz). The VRAM frequency reflects the speed of the VRAM to a certain extent. The VRAM frequency varies with the type and performance of the VRAM. SDRAM VRAM generally works at a lower frequency, generally 133MHz and 166MHz. The VRAM frequency is mainly used on low-end graphics cards. The VRAM frequencies that different VRAM can provide are also very different, mainly 400MHz, 500MHz, 600MHz, 650MHz, etc., and there are 800MHz, 1200MHz, 1600MHz, and even higher in high-end products.

6.VRAM package

VRAM package refers to the type of packaging technology used by the VRAM particles. The package is to wrap the VRAM chip to prevent the chip from contacting the outside world. Impurities and undesirable gases in the air, and even water vapor, will corrode the precision circuits on the chip, thereby causing the electrical performance to decline. Different packaging technologies have great differences in manufacturing processes and processes, and the performance of the memory chip itself after packaging also plays a vital role. VRAM package forms mainly include QFP, TSOP-II, MBGA, etc., among which TSOP-II and MBGA are more common. Many early SDRAM and DDR VRAM used TSOP-II, but now with the improvement of VRAM speed, more and more VRAM uses MBGA package, especially DDR2 and DDR3 VRAM, all use MBGA package. In addition, many manufacturers also refer to the DDR2 and DDR3 memory packages as FBGA, which emphasizes the naming of the pin arrangement, which is actually the same package form. Although MBGA and TSOP-II can achieve higher VRAM frequency, it cannot be simply assumed that MBGA packaged VRAM must be better overclocked, because whether it is easy to overclock or not depends more on the default frequency set by the manufacturer and the actual VRAM. The gap between the frequencies that can be reached includes the design and manufacture of the graphics card. Simply put, the MBGA package can achieve higher frequencies, but the default frequency is also higher.

7.Clock cycle

The VRAM clock cycle is the repetition period of the VRAM clock pulse, which is an important indicator to measure the speed of the VRAM. The faster the VRAM speed, the greater the amount of data exchanged per unit time, and the performance of the graphics card will be significantly improved under the same conditions. The clock cycle of the VRAM is generally in ns (nanoseconds), and the operating frequency is in MHz. The relationship between the VRAM clock cycle and the working frequency: working frequency=1÷clock cycle×1000. Then the memory frequency is 166MHz, then its clock cycle is 1÷166×1000=6ns. For DDR SDRAM or DDR2, DDR3 VRAM, the equivalent output frequency is used when describing its operating frequency. Because data can be transmitted on both the rising and falling edges of the clock cycle, the VRAM bandwidth is twice that of SDRAM when the operating frequency and data bit width are the same. In other words, under the same VRAM clock cycle, the equivalent output frequency of DDR SDRAM VRAM is twice that of SDRAM VRAM. For example, the operating frequency of 5ns SDRAM VRAM is 200MHz, while the equivalent operating frequency of 5ns DDR SDRAM or DDR2, DDR3 VRAM is 400MHz. Common VRAM clock cycles are 5ns, 4ns, 3.8ns, 3.6ns, 3.3ns, 2.8ns, 2.0ns, 1.6ns, 1.1ns, or even lower.

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1.What is meant by VRAM?

VRAM is memory on a video card and in some cases on the motherboard, that's accessible by the video and computer processor. With more VRAM, the video card and computer are capable of handling more complex graphics at a faster rate.

2.Is VRAM the same as RAM?

RAM is the memory your processor uses to store data on which it is currently doing some computation. VRAM is the video RAM on which the graphic processor store data on which it is doing computation. They are different on PCs which have discrete graphics.

3.What is a good VRAM?

If modern games should run smoothly, you'll require a discrete graphics card with dedicated memory. While 128 or 256 MB VRAM no longer suffice graphically demanding titles, mid-range graphics cards should feature a minimum of 512 MB and high-end graphics cards at least 1024 MB VRAM.

4.What is the purpose of VRAM?

Stands for "Video Random Access Memory" and is pronounced "V-RAM." System RAM is great for loading and running programs, but when you need graphics power, VRAM is where it's at. This is the memory used to store image data that the computer displays; it acts as a buffer between the CPU and the video card.

5.Can you allocate RAM to VRAM?

You can never turn RAM into VRAM. They are two different animals. But I presume you mean you want to use some of your system memory for VRAM. That happens automatically if needed by the gfx card.
Related Articles

  • High-Capacity HDDs in the AI Era: Sourcing Massive Storage for Cold Data
    High-Capacity HDDs in the AI Era: Sourcing Massive Storage for Cold Data
    UTMEL04 July 2026697

    As generative AI and LLMs drive an explosion of unstructured data, high-capacity enterprise HDDs remain the most cost-effective solution for cold storage. Despite rising prices and supply chain bottlenecks, mechanical drives offer a massive cost-per-gigabyte advantage over SSDs. Technologies like HAMR and SMR enable capacities beyond 24TB, though deploying these drives requires robust RAID 6 strategies and secured IC supply chains to mitigate rebuilding and procurement risks.

    Read More
  • LPDDR5 Memory 2026: Lead Times, HBM Impact, and Procurement Strategies
    LPDDR5 Memory 2026: Lead Times, HBM Impact, and Procurement Strategies
    UTMEL17 July 20264574

    Global semiconductor fabrication facility managing advanced memory production. In Q2 2026, contract prices for 12GB LPDDR5X modules surged 89% quarter-over-quarter, jumping from $77.10 to $145.90, while lead times for advanced memory components stretched to 40–58 weeks. A vehicle platform designed in 2023 with specific memory requirements must ship in 2026, regardless of spot market conditions.

    Read More
  • 2026 DRAM and the 3-to-1 HBM Rule: Market Supply Analysis and B2B Procurement Guide
    2026 DRAM and the 3-to-1 HBM Rule: Market Supply Analysis and B2B Procurement Guide
    UTMEL23 July 20265857

    This technical report explains how the physical "3-to-1 wafer penalty" of High Bandwidth Memory (HBM) production has cannibalized standard DRAM capacity, causing severe shortages of DDR4 and DDR5 in 2026. As major hardware OEMs pass these soaring component costs directly to enterprise buyers, procurement teams must abandon Just-in-Time models in favor of rolling safety stocks and strategic long-term distributor agreements to protect budgets.

    Read More
  • Automotive vs. Industrial Memory: How to Verify Grade Codes Before Sourcing In this guide
    Automotive vs. Industrial Memory: How to Verify Grade Codes Before Sourcing In this guide
    UTMEL06 August 2026485

    Memory ordering codes can look almost identical while representing different temperature limits, packages, revisions, qualification evidence, or lifecycle commitments. For automotive and long-life industrial designs, the safe purchasing unit is the complete manufacturer ordering code, not a base part number plus a familiar-looking suffix.

    Read More
  • How to Use an External Hard Drive?
    How to Use an External Hard Drive?
    UTMEL24 June 20219469

    The external hard drive is a compact and portable hard drive storage which can be plugged in or unplugged at any time. It mainly uses USB or IEEE1394 interfaces. It can transmit data with the system at a higher speed. The IEEE 1394 interface transfer rate is 50-100 MB/s.

    Read More

Subscribe to Utmel !

Featured Parts More