What is a Baseband Processor?

Published: 11 November 2021 | Last Updated: 11 November 20217940
A baseband processor is used to synthesize the baseband signal to be transmitted or to decode the received baseband signal. Specifically, when transmitting, the audio signal is compiled into the baseband code used to transmit. When receiving a signal, the received baseband code is decoded into the audio signal. It is also responsible for compiling address information (cell phone number, website address), text information (SMS text, website text), and picture information.


Catalog

Ⅰ Overview

Ⅱ Baseband processor components

Ⅲ Baseband processor SOC architecture

Ⅳ Baseband processor ARM architecture

Ⅴ Baseband processors used in today's cell phones

Ⅵ Conclusion


Ⅰ Overview

The baseband processor synthesizes the baseband signal that is about to be transmitted and decodes the received baseband signal. When transmitting a baseband signal, it compiles the audio signal into a baseband code; when receiving a signal, it decodes the baseband code into an audio signal. At the same time, the baseband processor is also responsible for compiling address information, text information, picture information, etc.

A baseband processor is a kind of SOC with complex integration. Mainstream baseband processors support multiple network standards, i.e., all mobile and wireless network standards are supported on one baseband processor, including 2G, 3G, 4G, and WiFi, etc. Multi-mode mobile terminals can realize seamless roaming between multiple mobiles and wireless networks around the world. The basic structure of most current baseband processors is a microprocessor and a digital signal processor. The microprocessor is the control center of the entire chip, mostly using ARM cores, while the DSP subsystem is responsible for baseband processing.

baseband processor.jpg

baseband processor

The baseband processor present in a smartphone can be understood as a complex SoC chip with a variety of functions, and the normal operation of each function is configured and coordinated through the microprocessor. This complex chip is centered on the ARM microprocessor, which controls and configures each peripheral function module around the ARM microprocessor through the ARM microprocessor's dedicated bus (AHB bus), which mainly includes GSM, WiFi, GPS, Bluetooth, DSP, and memory, etc... Each function module has its own memory and address space. Their functions are independent of each other. The baseband processor itself has a power management chip.

Ⅱ Baseband processor components

baseband processor structure diagram.jpg

Figure: baseband processor structure diagram

The baseband processor can be divided into five sub-blocks: CPU processor, channel coder, digital signal processor, modem, and interface module.

CPU processor: control and management of the whole mobile station, including timing control, digital system control, RF control, power saving control, and human-machine interface control. If frequency hopping is used, it should also include the control of frequency hopping. At the same time, the CPU processor performs all software functions of the GSM terminal, i.e. layer1 (physical layer), layer2 (data link layer), layer3 (network layer), MMI (human-machine interface), and application layer software of the GSM communication protocol.

Channel coder: mainly completes the channel coding and encryption of service and control information, including convolutional coding, FIRE code, parity check code, interleaving, burst pulse formatting.

Digital signal processor: mainly completes the channel equalization using Viterbi algorithm and the voice coding/decoding based on the regular pulse excitation-long-term prediction technique (RPE-LPC).

Modem: mainly completes the Gaussian Minimum Shift Keying (GMSK) modulation/demodulation required by the GSM system.

Interface module: including three sub-blocks: analog interface, digital interface, and human-machine interface.

What network standard the mobile terminal supports is determined by the baseband processor mode, while what frequency band it supports is determined by the antenna and RF module. The baseband processor completes the access function of the mobile terminal. The current baseband processor is a highly complex system-on-chip (SoC), which not only supports several communication standards (including GSM, CDMA 1x, CDMA2000, WCDMA, HSPA, LTE, etc.), but also provides multimedia functions and interfaces related to multimedia displays, image sensors, and audio devices. To further simplify the design, the power management circuits required for these compiled circuits are increasingly integrated into them.

Ⅲ Baseband processor SOC architecture

Baseband digital processing functions and the basic peripheral functions of cell phones are concentrated in a single system on chip (SOC), whose basic architecture uses a microprocessor + digital signal processor (DSP) structure, and the processing power of the microprocessor and DSP has been enhanced.

1. The microprocessor is the control center of the whole chip and will run a real-time embedded operating system (such as Nucleus PLUS).

2. The DSP subsystem is the focus of the baseband processing, which contains many hardware gas pedals and baseband-specific processing modules that perform all physical layer functions.

With the development of real-time digital signal processing technology, ARM microprocessor (different micro-series will be used, 3G chips mostly use ARM9), DSP, and FPGA architecture become the main way of mobile terminal baseband processors.

Ⅳ Baseband processor ARM architecture

In the field of chip architecture, X86 and ARM can be said to have been competing for decades and have occupied an unshakable position in their respective fields. Among them, X86 dominates the PC chip market, while ARM dominates the mobile terminal chip market. Because of the low cost, low power consumption, and high efficiency, the ARM architecture has catered to the development trend of many mobile terminal devices including smartphones.

The following figure shows the logic architecture of a typical ARM-based baseband processor, where 3G/4G Baseband Logic refers to the DSP computing subsystem.

baseband processor framework on a typical ARM architecture.jpg

Figure: baseband processor framework on a typical ARM architecture

1 The microprocessor completes multitasking scheduling, inter-task communication, peripheral drivers, and communication between the microprocessor and the DSP subsystem and other modules, etc. through the real-time operating system RTOS (e.g. Nucleus PLUS).

Functions also include:

(1) control and management of the entire mobile station, including timing control, digital system control, RF control, power saving control, etc.;

(2) complete all software functions, i.e., communication between the physical layer and protocol stack of wireless communication protocols, high-level protocol stack (TCP/IP, etc.), and if used in a functional machine, it will also include MMI (human-computer interaction interface) and application software.

2 The DSP subsystem is used for processing all algorithms of the physical layer, including channel coding, encryption, channel equalization, voice coding/decoding, modulation, and demodulation, etc. The means of data communication between the DSP subsystem and the microprocessor subsystem include dual-port random read memory (RAM), multi-bus shared resources (some vendors use AMBA's multi-layer bus protocol), etc. The multimode multi-frequency baseband processor may contain multiple DSPs.

3 In terms of memory organization, both the microprocessor and DSP subsystem may have their own independent cache with shared on-chip SRAM and shared external expansion memory. The extended memory commonly supports synchronous dynamic random memory (SDRAM) and NAND-type Flash RAM, etc.

FLASH ROM can be used to store Boot Rom and CP Rom for linking OS and user applications. ROM interface is mainly used to connect FLASH ROM for storing programs, and RAM interface is mainly used to connect static RAM (SRAM) for storing temporary data. On-chip embedded large-capacity static random read memory (SRAM) has become very common, which is conducive to reducing power consumption and reducing system costs.

4 In terms of peripherals and interfaces, the baseband processor often supports a variety of interfaces to facilitate communication with the application processor and the addition of other modules such as Wifi, GPS. Interfaces include UART, multimedia interface (MMI), universal serial bus (USB), SPI, etc..

MCU communication with external interfaces can be done through DMA, and if the baseband processor does not integrate RF, there is also a dedicated RF interface.

Ⅴ Baseband processors used in today's cell phones

The baseband processors used in today's popular cell phones are as follows.

Chip maker: Qualcomm

Baseband processors: Snapdragon 888, Snapdragon 865, Snapdragon 855, Snapdragon 660, Snapdragon 653, Snapdragon 626, Snapdragon 435, Snapdragon 430, Snapdragon 427, ETC

Cell phone products: Xiaomi 10, Samsung S20, One Plus 9, Nubia Z12, LeEco, Redmi Note, Huawei G series, etc.

Chip manufacturer: Huawei Hisilicon

Baseband processors: Kirin 9000, Kirin 990, Kirin 985, Kirin 970, Kirin 965, Kirin 660

Cell phone products: Mate 40, P50 Pro, P40, mate 30, Nova 9, etc.

Chip maker: Samsung

Baseband processors: Exynos 8895, Exynos Modem 5100

Cell phone products: Samsung S8, Samsung Note 8, Meizu PRO 7 series

Chip maker: MediaTek

Baseband processors: Helio M70, Helio X30/X35, Helio X23/X27, Helio P30/P35, Helio P20/P25

Cell phone products: Meizu MX7, Meilan X2, Redmi Note4, Samsung C9 Pro, Vivo X9

Chip maker: Spreadtrum

Baseband processor: Spreadtrum SC6815, Spreadtrum SC7701B, Spreadtrum SC7730S

Cell phone products: Samsung Galaxy Star 2 (G130E), Samsung Galaxy Star 2 Plus (G350E), etc.

Ⅵ Conclusion

We generally think that the performance of the cell phone CPU is reflected in its processing speed and power consumption. In fact, in the era of smartphones, there is a layer of the most basic and critical needs - cell phone signal quality. This communication function determined by the baseband processor will directly affect the quality of cell phone calls and Internet speed.

With the advent of the 5G network and 5G cell phones, the rapid capture of the 5G baseband processor market share will help the chip giants to improve financial revenue in order to gain a head start in the 6G network and form a virtuous circle.

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1.What is the function of a smartphones baseband processor?

A chip in a smartphone or tablet that handles the cellular transmission. The baseband processor converts the data to a signal that can be used to modulate the carrier frequency for transmission and vice versa. That signal is handed off to the RF processor, which may also be part of the baseband chip.

2.What is 5G baseband?

The baseband is the chip in a device that connects to mobile networks to deliver that always-on connected experience. Those chips will also need to meet the standards required of the network, in order to deliver the improvements in connectivity, reliability, and bandwidth that 5G brings.
Related Articles

  • Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap Devices
    Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap Devices
    Saumitra Jagdale15 March 20242452

    For a long era, silicon has stood out as the primary material for fabricating electronic devices due to its affordability, moderate efficiency, and performance capabilities. Despite its widespread use, silicon faces several limitations that render it unsuitable for applications involving high power and elevated temperatures. As technological advancements continue and the industry demands enhanced efficiency from devices, these limitations become increasingly vivid. In the quest for electronic devices that are more potent, efficient, and compact, wide bandgap materials are emerging as a dominant player. Their superiority over silicon in crucial aspects such as efficiency, higher junction temperatures, power density, thinner drift regions, and faster switching speeds positions them as the preferred materials for the future of power electronics.

    Read More
  • A Comprehensive Guide to FPGA Development Boards
    A Comprehensive Guide to FPGA Development Boards
    UTMEL11 September 202513943

    This comprehensive guide will take you on a journey through the fascinating world of FPGA development boards. We’ll explore what they are, how they differ from microcontrollers, and most importantly, how to choose the perfect board for your needs. Whether you’re a seasoned engineer or a curious hobbyist, prepare to unlock new possibilities in hardware design and accelerate your projects. We’ll cover everything from budget-friendly options to specialized boards for image processing, delve into popular learning paths, and even provide insights into essential software like Vivado. By the end of this article, you’ll have a clear roadmap to navigate the FPGA landscape and make informed decisions for your next groundbreaking endeavor.

    Read More
  • Applications of FPGAs in Artificial Intelligence: A Comprehensive Guide
    Applications of FPGAs in Artificial Intelligence: A Comprehensive Guide
    UTMEL29 August 20253465

    This comprehensive guide explores FPGAs as powerful AI accelerators that offer distinct advantages over traditional GPUs and CPUs. FPGAs provide reconfigurable hardware that can be customized for specific AI workloads, delivering superior energy efficiency, ultra-low latency, and deterministic performance—particularly valuable for edge AI applications. While GPUs excel at parallel processing for training, FPGAs shine in inference tasks through their adaptability and power optimization. The document covers practical implementation challenges, including development complexity and resource constraints, while highlighting solutions like High-Level Synthesis tools and vendor-specific AI development suites from Intel and AMD/Xilinx. Real-world applications span telecommunications, healthcare, autonomous vehicles, and financial services, demonstrating FPGAs' versatility in mission-critical systems requiring real-time processing and minimal power consumption.

    Read More
  • 800G Optical Transceivers: The Guide for AI Data Centers
    800G Optical Transceivers: The Guide for AI Data Centers
    UTMEL24 December 20253457

    The complete guide to 800G Optical Transceiver standards (QSFP-DD vs. OSFP). Overcome supply shortages and scale your AI data center with Utmel Electronic.

    Read More
  • Xilinx FPGAs: From Getting Started to Advanced Application Development
    Xilinx FPGAs: From Getting Started to Advanced Application Development
    UTMEL09 September 20254186

    This guide is your comprehensive roadmap to understanding and mastering the world of Xilinx FPGA technology. From selecting your first board to deploying advanced AI applications, we'll cover everything you need to know to unlock the potential of these remarkable devices. The global FPGA market is on a significant growth trajectory, expected to expand from USD 8.37 billion in 2025 to USD 17.53 billion by 2035. This surge is fueled by the relentless demand for high-performance, adaptable computing in everything from 5G networks and data centers to autonomous vehicles and the Internet of Things (IoT). This guide will walk you through the key concepts, tools, and products in the Xilinx ecosystem, ensuring you're well-equipped to be a part of this technological revolution.

    Read More