Solar Inverter: Definition, Types and Costs

Published: 01 February 2021 | Last Updated: 01 February 20216006
The solar inverter's main function is to transform or "invert" the solar energy produced by your solar panels from DC to AC so that it can be used by your home and utility grid.
In this video Solar Power Inverters have been discussed.  There are a wide variety of Inverters on the market. They are classified by their power output and voltage input.

All you need to know about Solar Inverters

Catalog

Ⅰ What does a solar inverter do?

Ⅱ Types of solar inverters

Ⅲ How much does a solar inverter cost?

 

Ⅰ What does a solar inverter do?

As an interpreter, think about your solar inverter and DC and AC as two separate languages. As do your equipment and your power system, all the electrical wires flowing across your home bear or 'talk' AC. Your solar panels, though, 'talk' DC. So, there's a contact barrier, in nature. Without any support, the solar energy system can't transmit electricity to either your house or the electric grid.

solar inverter

What offers the assist is an inverter. The solar inverter's main function is to transform or "invert" the solar energy produced by your solar panels from DC to AC so that it can be used by your home and utility grid. But that's the first and most important service it delivers. But your inverter has another essential function, in addition to inverting energy from one medium to another: online networking.

Solar inverters help you to link your solar energy device to the internet, enabling you to access your system details in turn. This is extremely beneficial when you want to measure your output of solar energy against your use of household energy (the energy expressed in your utility bill) or to ensure that your system is working properly.

Ⅱ Types of solar inverters

There are a handful of different suppliers of inverters out there, but most businesses rely on one of the forms of inverters listed below. Starting with styles that have the fewest features to types with the most features, we have put them in order.

The inverter you get is dependent on a variety of considerations, such as: which company you employ, how much shade your home has, how you want to use your solar inverter, and/or the residential solar utility specifications in your location.

1.Straight String Inverter

A string inverter was the only available alternative for several years. Owing to its lower general upfront costs and minimal long-term maintenance needs, one of the key reasons for this was (since there is only one point of failure).

As an example of how a string inverter operates, consider that a swimmer is caught in an ocean riptide to create a human chain on the beach to save him from drowning (like the Panama City Beach rescue in July 2017). Each entity in the chain represents a solar panel, and it directly impacts the output of the rest of the chain whether one of them is poor or injured.

It is how the inverter of a string works. Solar panels are related in sequence, and if one of the panels in that series is shaded or dirty because the string can only work at the level of the least efficient panel, it impacts the output of the rest of the string. A straight string inverter may not be the best option for you if you have a home with many roof planes. However, if you live anywhere that is normally sunny and your house has a roof facing south, then a straight string inverter could be a perfect choice for you because it will help you keep a little coin in your wallet and you will gain the repair advantages that come with ease.

2.Optimized String Inverter

Except that it has power optimizers mounted underneath each solar panel on the roof, the optimized string inverter is identical to the regular string inverter. The power optimizer transforms the solar panel into a "smart panel" and, by tracking and then communicating the performance of each solar panel independently, maximizes performance. This helps you to pull the most electricity out of your system.

A straight string device will normally outperform programmed string inverters. One business dominates the residential industry when it comes to offering a solution of power optimizers: SolarEdge. Over the past five years, SolarEdge's power-optimized approach has evolved steadily and accounted for nearly 60 percent of all residential solar installations in the US as of December 2019.

3.Microinverter

A microinverter is mounted under each solar panel on the roof, rather than having a larger inverter on the side of the tower (similar to the way power optimizers are installed). Giving each panel its own microinverter gives designs more versatility (technically, a person could install a system with one microinverter, and then add on later as needs arise). The microinverter also converts DC to AC right on the roof, while DC energy is passed to the string inverter by the optimizer, which then converts DC to AC.

4.Hybrid Inverter

The "New Kid on the Block" for inverter technologies is hybrid Inverters. A mixture of a PV (photovoltaic) inverter and a battery inverter is a hybrid inverter and is available in straight string and optimized string options. For homeowners interested in energy backup choices (even if the homeowner is not yet ready to mount a battery), this is becoming a common alternative because it makes installing a battery much less costly.

The option to wire an electric vehicle (EV) charger to the converter is an added feature (now provided by SolarEdge). This way, as he/she is ready to go electric, a homeowner will have the option to install an EV charger without the potential to pay extra costs for the main panel update.

A hybrid inverter, as you can see, has all the characteristics you expect from a PV inverter, but also makes upgrades to please the most die-hard energy enthusiasts.

Ⅲ How much does a solar inverter cost?

Inverters don't slip into a "one size fits all" category when it comes to cost, comparable to rooftop solar panels. Inverters are so important to a solar energy system that the cost of an inverter is included in the average price of a solar energy system for certain solar firms (including Vivint Solar), which may make it difficult to identify the precise price of an inverter. Standalone inverters can be found to buy online, but costs vary wildly (between $1,500 and $20,000 anywhere) because there are a number of cost considerations that can include items like:

1.Where you buy the inverter: The cost price will generally fluctuate depending on where you buy the inverter due to factors such as tariffs, packaging, supply, etc. Since the expense of the inverter is included in the overall cost of the device for many solar firms, your buying choices would be limited to third-party suppliers selling solar equipment to those on the market to install the solar power system on their own.

2.The size of your solar energy system: In general, the bigger the solar system you have, the more expensive your solar inverter would need to work. The greatest thing to keep in mind is that you're going to want something that lasts, so be cost selective, but not so selective that you sacrifice consistency.

3.The sort of solar agreement you have chosen: the solar agreement will decide how you want to pay for your solar energy which is based on your area's agreement choices. The cost of the facilities would generally be included in the total cost of the device. Otherwise, from a third party, you would actually buy the inverter and pay for the cost of the other solar devices.

4.Some inverters come with built-in special characteristics, such as revenue-grade meters (which are often needed by state incentive programs and are more detailed in terms of energy production), safe power supplies (such as the SMA Sunnyboy), and smart inverter settings/functionality (which are required in select jurisdictions).

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1.How much does a solar inverter cost?

A 3kW solar inverter will cost around $800 (retail) for a budget brand such as Sungrow, and up to $1,500 for a premium model from Fronius or SMA. 5kW solar inverter costs start at $1,000 for budget, single-phase models and up to $2,000 for the premium single-phase models.

2.Which solar inverter is best?

top 5 Solar inverters - Residential  Fronius  SolarEdge  SMA  Sungrow  FIMER (ABB)

3.Are solar inverters dangerous?

No, inverters are not harmful to our health and adhere to the FCC rules Part 15 Class B, which regulate what electronic devices emit, called "radiating" energy.

4.Will a 5kW solar system run a house?

This 5kW microinverter-based kit is a serious residential solar system. This could produce an estimated 350 to 850-kilowatt hours (kWh) of alternating current (AC) power per month, assuming at least 5 sun hours per day with the solar array facing South.

5.Do solar inverters turn off at night?

Solar inverters are connected to solar panels, and solar panels only function in response to sunlight, they will turn off when night falls. This happens if there is not enough sunlight for the panels to generate electricity.
Related Articles