web counter

Memory Chip: The Key to Smart Connectivity

Published: 03 November 2021 | Last Updated: 03 November 20213132
In today's post, we talk about memory chips, especially their emerging applications in the AIoT smart interconnect space.
From laptops to mobile phones to connected cars and homes, memory and storage are helping change how the world works, plays, communicates and connects.

Making Memory Chips – Process Steps


Catalog

Edge Computing and memory chips

New storage technology for IoT and AIoT

Security of AIoT memory chip

Summary

 

Edge Computing and memory chips

The most important factors driving the development of artificial intelligence are computing power, algorithms, and data, respectively. That is changes in computing technology, innovation in theoretical algorithms, and the generation and accumulation of massive amounts of data. No matter how advanced the algorithm progresses, or how powerful the arithmetic power improves, in the final analysis, it is necessary to calculate, carry and store a large amount of data.

Especially with the continuous rise and development of autonomous driving, 5G, smart home, and other such IoT-related technologies, coupled with the dramatically increasing demand for remote communication and collaboration brought about by the global epidemic, so there will be more and more data generated continuously. Some have also compared data to oil in the age of artificial intelligence. This also places more stringent demands on both the performance and efficiency of data processing.

Usually, the data center is the main battlefield for processing these data, where there are thousands of servers and massive hardware resources for data computation transmission and storage. But as the volume of data grows rapidly, it puts great pressure and challenges on the computing power of the chips, the bandwidth of the network, and the capacity of the storage in the data center.

edge computing and IoT applications.jpg

edge computing and IoT applications

It is slowly becoming impossible to transfer all the data to the data center, process it, and then send it out. In fact, less than 1% of the data generated by the aforementioned sources is processed efficiently. So people consider whether they can process the data directly where it is generated so that they can largely reduce the bandwidth of transmission, storage space, and computational pressure. This is the main background of the rise of edge computing, that is, computing at the edge of the data processing network.

One of the important application scenarios of edge computing is IoT applications. For IoT, it is initially just some sensors, data sending and receiving devices, and some simple controller MCUs and so on. But as the amount of data increases, the demand for the computing power of these IoT devices is getting bigger and bigger, but this is only one side.

Another important aspect is that these IoT devices also have very strict limitations on cost and power consumption. For example, for wearable devices, we not only want it to be able to run various applications smoothly, collect and sense various data of our movement and physiology but also to be power-saving enough, preferably to be charged once a week or once a month.

Therefore, for IoT hardware devices, high energy efficiency, low power consumption, and small size will be the future development direction of such devices and chips. It is worth noting that the chip here includes not only the processor, but also those data transmission modules, sensor modules, and, very importantly, the storage unit, especially the system RAM memory.

New storage technology for IoT and AIoT

For processors, many MCUs have been able to achieve a good balance between power consumption and performance, but the technological progress of storage units is not so obvious.

memory chip.jpg

memory chip

The most common SDRAM was released around 1994 when the semiconductor process node was still at 800nm. pSRAM was born around 2005, corresponding to the 90nm process node, and then the low-power SDRAM was released in 2007 when the process node was 65nm. Then it seems that the definition of standards regarding DRAM stagnated. As you can see, there is a relatively large gap and the chasm between the standards and processes of the two types of chips, mobile device processors and memory.

In order to keep filling this gap, the industry introduced a technology called HyperBus in 2014 and made an update in 2019. HyperBus is essentially an interface technology, and the most important feature of HyperBus is the small number of pins compared to other memory's transmission control interfaces, which allows for a cleaner and smaller area when designing the circuit.

The HyperBus technology-based memory chip is called HyperRAM, which has only 13 pins compared to traditional RAM products that have 3 to 40 pins. This greatly simplifies the PCB design on the one hand, and also allows more flexibility in MCU selection. For example, we can use the extra pins on the MCU for other things, or we can simply choose an MCU with fewer pins, thus reducing costs.

HyperRAM.jpg

HyperRAM

Another benefit of the reduced pin count of HyperRAM is the ability to use smaller package sizes, such as consumer-oriented HyperRAM packages up to wafer-level chip packages, with some package options shown below.

  • For automotive and industrial applications: 24-ball 8mm x 6mm TFBGA

  • For consumer products: 49-ball 4mm x 4mm WFBGA

  • For lean size requirements such as IoT: 15-ball wafer-level chip package (WLCSP)

  • Good bare wafer (KGD)

Using smaller packages can further reduce PCB size, which is very important for wearable consumer devices such as smart watches, smart bracelets, etc...

In addition to the area, power consumption is also critical for IoT devices. For example, many IoT devices are battery-powered. Many devices are even very difficult to change the battery, such as those deployed in mines, oil and gas fields, chemical plants, and other dangerous environments. So the power consumption of these IoT devices directly determines their working life.

Security of AIoT memory chip

We may be familiar with the hacking of personal computers or data centers, but what most people may not know is that IoT devices are also very vulnerable to cyber-attacks. In 2019, for example, the number of cyberattacks launched against IoT devices in the United States jumped 300 percent year-over-year.

To make matters worse, about 57% of IoT devices have difficulty resisting these attacks. For example, a significant number of attacks are targeting devices like smart meters and smart gas meters to modify the readings of these meters so that they can underpay or not pay for their energy usage. There are also many attacks on medical devices and wearable areas to illegally access and collect users' private information, etc. It is important to understand that the damage caused by these attacks is huge. Some data show that the average cost of each attack is $9 million.

From the hardware point of view, the main places where these security vulnerabilities exist are the processing unit itself and the external flash memory that stores critical program code or data. In the case of simpler wearable products or IoT products, security issues mainly arise in the control chip, such as the lack of complex cryptographic algorithms, differential power analysis, key encryption storage, and so on.

As these IoT devices continue to evolve, the control chip becomes more and more complex, with more and more programs to run, and moving towards a chipless memory process. At this point, embedded memory is not enough or even exists and external flash memory must be used to store program code. However, if such external flash memory lacks the necessary security features, it can become a major security vulnerability for the system.

To address such security issues, a common practice is to replace external NOR Flash in IoT devices with Secure Flash, which, by its very nature, provides secure storage space with basic encrypted authentication, thus allowing only authorized hosts to perform read and write operations.

In fact, in addition to secure authentication, other hardware protection features are required to better defend against many types of cyberattacks.

For example, the system recovery feature detects potential attacks and automatically reboots the device after an attack has occurred, and executes known security codes. And the secure channel feature enables remote firmware updates so that even if the control unit is compromised, the memory can upgrade the bootloader code to a secure version without the control unit's intervention. This allows the host to be forced into a clean boot mode using a known security code.

It is also worth noting that secure flash memory is typically packaged in the same size and pin locations as standard flash memory and is controlled through the standard SPI NOR Flash command set, which further facilitates the use of secure flash memory.

Summary

In the current era of data blowout, memory chips are of increasing importance. Especially in edge computing and IoT applications, the performance, power consumption, and size of the memory chip are all critical evaluation and consideration factors.

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1.What are memory used in IoT devices?

Traditional External Flash Memory: Many consumer products use this type of memory, because it is inexpensive, reliable, and flexible, offering a high degree of density and the ability to execute in place without using too much power. Flash memory falls into two categories: NOR Flash and NAND Flash.

2.What is chip in IoT?

IoT modules or chips are technically identified as electronic devices that are embedded in machines, objects, and things, capable of connecting to wireless networks and sending and receiving data. These devices operate on different protocols, such as NB-IoT, LTE, and BLE 5.0, among others.
Related Articles

  • High-Capacity HDDs in the AI Era: Sourcing Massive Storage for Cold Data
    High-Capacity HDDs in the AI Era: Sourcing Massive Storage for Cold Data
    UTMEL04 July 2026579

    As generative AI and LLMs drive an explosion of unstructured data, high-capacity enterprise HDDs remain the most cost-effective solution for cold storage. Despite rising prices and supply chain bottlenecks, mechanical drives offer a massive cost-per-gigabyte advantage over SSDs. Technologies like HAMR and SMR enable capacities beyond 24TB, though deploying these drives requires robust RAID 6 strategies and secured IC supply chains to mitigate rebuilding and procurement risks.

    Read More
  • LPDDR5 Memory 2026: Lead Times, HBM Impact, and Procurement Strategies
    LPDDR5 Memory 2026: Lead Times, HBM Impact, and Procurement Strategies
    UTMEL17 July 20263581

    Global semiconductor fabrication facility managing advanced memory production. In Q2 2026, contract prices for 12GB LPDDR5X modules surged 89% quarter-over-quarter, jumping from $77.10 to $145.90, while lead times for advanced memory components stretched to 40–58 weeks. A vehicle platform designed in 2023 with specific memory requirements must ship in 2026, regardless of spot market conditions.

    Read More
  • 2026 DRAM and the 3-to-1 HBM Rule: Market Supply Analysis and B2B Procurement Guide
    2026 DRAM and the 3-to-1 HBM Rule: Market Supply Analysis and B2B Procurement Guide
    UTMEL23 July 20264344

    This technical report explains how the physical "3-to-1 wafer penalty" of High Bandwidth Memory (HBM) production has cannibalized standard DRAM capacity, causing severe shortages of DDR4 and DDR5 in 2026. As major hardware OEMs pass these soaring component costs directly to enterprise buyers, procurement teams must abandon Just-in-Time models in favor of rolling safety stocks and strategic long-term distributor agreements to protect budgets.

    Read More
  • Automotive vs. Industrial Memory: How to Verify Grade Codes Before Sourcing In this guide
    Automotive vs. Industrial Memory: How to Verify Grade Codes Before Sourcing In this guide
    UTMEL06 August 2026349

    Memory ordering codes can look almost identical while representing different temperature limits, packages, revisions, qualification evidence, or lifecycle commitments. For automotive and long-life industrial designs, the safe purchasing unit is the complete manufacturer ordering code, not a base part number plus a familiar-looking suffix.

    Read More
  • How to Use an External Hard Drive?
    How to Use an External Hard Drive?
    UTMEL24 June 20219377

    The external hard drive is a compact and portable hard drive storage which can be plugged in or unplugged at any time. It mainly uses USB or IEEE1394 interfaces. It can transmit data with the system at a higher speed. The IEEE 1394 interface transfer rate is 50-100 MB/s.

    Read More

Subscribe to Utmel !

Featured Parts More