web counter

Results: ( 69,708 )

Filters

Filters definition

Utmel Electronics, one of the most electrical parts distributors, provides you with a wide range of filters, including filter accessories, EMI Filters(electromagnetic interference filters), Wix Filters, Air Filters, Water Filters, Ceramic Filters, Helical Filters, RF Filters, SAW Filters and more. The below will give you some explanation about Filters, such as Filters definition, Filters types and How Do Filter work.

What is Filter in Electrical?

Electronic Filters are one type of electrical circuits, which is used to process signal filter. And as one of the common electronic components, Filters have a wide range of practical applications, such as radio communications, Audio electronics, DC Power Supplies, Analog-to-Digital conversion and more.

Types of Filers in Electrical

There are 4 main filters types available in marketplace: the high-pass filter, the notch filters, the low-pass filter and the band-pass filter. The following passage will list some other popular types of filters, including Ferrite Beads, Power Line Filter, EMI/RFI Filters, SAW Filters and RF Filters, etc.

What are Ferrite Beads

Ferrite beads, are also called as Ferrites, Ferrite Chokes, Ferrite Blocks, Ferrite Rings, Ferrite Cores. And a ferrite bead is a kind of choke types, which is used to suppress high-frequency electronic noise in electronic circuits.

RF Filters

RF Filter, short for Radio Frequency Filter, is a special types of electrical circuits that allows the right signals to pass. So it can prevent or allow the selected frequencies or signals so as to pass through of unwanted signals or eliminate noise. And there are 4 RF filters types, including high pass filters, low pass filers, bandpass filers and band reject. Meanwhile, RF filters, generally are used in wireless communications, television and broadcast radio.

SAW Filters

SAW Filter, short for Surface Acoustic Wave Filter, is a passive semiconductor component, which can filter out desired frequencies. And SAW Filters widely are  applied to filter IF and RF frequencies in mobile telecommunications & Communications, Radar, Medical and Aerospace & Military Communications.

Related to the manufacturers

Recommended Manufacturers

ABB Embedded PowerAbracon LLC.Acme ElectricAlpha and Omega Semiconductor, Inc.Altran Magnetics, Inc.American Technical Ceramics
Frequently Asked Questions

How do filters work?

Firstly, the huge interior surface area traps sediments and pollutants physically. Secondly, as water travels through, activated carbon serves as a magnet for substances like lead and volatile chemical compounds. Last, chemical processes within the filter decrease chemicals such as chlorine when they come into touch with it.

What is DC EMI filter?

DC EMI Filters with High Performance and High Voltage DC EMI Filters let DC and low-frequency currents flow through while preventing high-frequency currents that are hazardous. This helps a gadget to function properly by redirecting unwanted sounds.

How does a DC filter work?

The DC filter namely is a device that enables the load's DC component to pass while blocking the rectifier's ac component. As a result, the filter circuit's output will be a constant dc voltage. Components such as inductors, resistors and capacitors can be used to create the filter circuit.

What is AC EMI filter?

By suppressing undesirable high-frequency signals/noise, EMI filters, also known as EMI suppression filters, reduce electromagnetic noise. These filters prevent line noise from entering equipment when they are installed at the point of power entrance.

What is the Difference between DC and AC EMI filter?

The AC side harmonic filters' job is to stop harmonic currents from flowing into the associated AC networks. The DC side harmonic filters generally are used to prevent telephone interference by restricting the passage of harmonic currents in the DC pole and electrode lines.