LR41 Battery, LR41 Battery Equivalent, LR41 and SR41 Cell Battery [FAQ]
ALKALINE MANGANESE BATTERIES
LR41 battery is a small, button/coin cell battery often used in digital thermometers, wristwatches, toys, small LED flashlights, wearable electronics, remote controls, and similar devices. This article is going to introduce detailed information about the LR41 battery.

How to Digital Thermometer Battery replacement LR41 how to use alternative 317 377 376
What is the LR41 battery?
The LR41 battery is an alkaline button cell battery. The LR41 battery has a standard voltage of 1.5V and a size of 7.9mm in diameter by 3.6mm in height. LR41's have an operating temperature ranging from 0°C- 60°C, while the optimal temperature for an LR41 battery is 20°C.
The LR41 battery can be utilized in many devices such as watches, electronic toys, remote controls, thermometers, and calculators. The most common use for the LR41 batteries is for use as thermometer batteries and thermometer battery replacements.
LR41 battery equivalents are also referred to as SR41, G3, LR4192, LR736, A63, AG3, SR41SW, 325, 384, SR736, SB-A1/D1, 280-18, V384, D384, 247, GP192, GP384, S736E, SR736PW, SR736SW, TR41SW, SR41W, V392, Seiko SB-B1, Seiko SB-A1, Citizen 280-13, Citizen 280-18, and the Timex K. These sizes are possible LR41 battery replacements.
Main Specs of LR41 Battery

LR41 Discharge Curve
Chemistry: Alkaline
Diameter: 7.9mm
Height: 3.6mm
Voltage: 1.5V
Capacity: 25-32 mAh
LR41 Battery Features
It has an excellent cost performance. It can achieve this because of the use of manganese dioxide as a cathode material.
It has excellent leakage resistance.
It has a stable voltage output during high drain pulse discharge, allowing it has a regular discharge and an excellent pulse discharge characteristic.
Specifications
- TypeParameter
- Factory Lead Time12 Weeks
- Voltage Rated
RATED voltage is the voltage on the nameplate - the "design point" for maximum power throughput and safe thermal operation.
1.5V - Size / Dimension
In electronic components, the parameter "Size / Dimension" refers to the physical dimensions of the component, such as its length, width, and height. These dimensions are crucial for determining how the component will fit into a circuit or system, as well as for ensuring compatibility with other components and the overall design requirements. The size of a component can also impact its performance characteristics, thermal properties, and overall functionality within a given application. Engineers and designers must carefully consider the size and dimensions of electronic components to ensure proper integration and functionality within their designs.
0.31Dia x 0.14 H 7.9mmx3.6mm - Part Status
Parts can have many statuses as they progress through the configuration, analysis, review, and approval stages.
Active - Moisture Sensitivity Level (MSL)
Moisture Sensitivity Level (MSL) is a standardized rating that indicates the susceptibility of electronic components, particularly semiconductors, to moisture-induced damage during storage and the soldering process, defining the allowable exposure time to ambient conditions before they require special handling or baking to prevent failures
Not Applicable - Reach Compliance Code
Reach Compliance Code refers to a designation indicating that electronic components meet the requirements set by the Registration, Evaluation, Authorization, and Restriction of Chemicals (REACH) regulation in the European Union. It signifies that the manufacturer has assessed and managed the chemical substances within the components to ensure safety and environmental protection. This code is vital for compliance with regulations aimed at minimizing risks associated with hazardous substances in electronic products.
compliant - Termination Style
"Termination style" in electronic components refers to the method used to connect the component to a circuit board or other electronic devices. It determines how the component's leads or terminals are designed for soldering or mounting onto the circuit board. Common termination styles include through-hole, surface mount, and wire lead terminations.Through-hole components have leads that are inserted through holes in the circuit board and soldered on the other side. Surface mount components have flat terminals that are soldered directly onto the surface of the circuit board. Wire lead terminations involve attaching wires to the component for connection.The choice of termination style depends on factors such as the type of component, the manufacturing process, and the space available on the circuit board. Different termination styles offer various advantages in terms of ease of assembly, reliability, and space efficiency in electronic designs.
Requires Holder - Storage/Refrigeration Temperature
The parameter "Storage/Refrigeration Temperature" in electronic components refers to the recommended temperature range at which the components should be stored to maintain their integrity and functionality. This parameter indicates the temperature limits within which the components can be safely stored without risking damage or degradation. Storage temperature is crucial for preserving the performance and reliability of electronic components over time, especially for sensitive components such as integrated circuits and semiconductors. Refrigeration temperature may be specified for certain components that require lower temperatures to prevent degradation or prolong shelf life. It is important to adhere to the recommended storage/refrigeration temperature guidelines to ensure the longevity and proper functioning of electronic components.
50°F~77°F 10°C~25°C - Battery Chemistry
A battery is a device that stores chemical energy, and converts it to electricity. This is known as electrochemistry and the system that underpins a battery is called an electrochemical cell. A battery can be made up of one or several (like in Volta's original pile) electrochemical cells.
Alkaline Manganese Dioxide - Battery Cell Size
The most common lithium-ion cell is the 18650 (the numbers define the physical dimensions and shape as follows: 18mm in diameter, 65mm long and the 0 means it has a round cross-section) which is due to its widespread use in laptop battery packs.
Coin 7.9mm - Capacity
In electronic components, "Capacity" typically refers to the maximum amount of electrical charge that a component can store. It is measured in units called farads (F). Capacitors are the most common components that have a capacity rating. The capacity of a capacitor determines how much energy it can store and release when connected in a circuit. Higher capacity capacitors can store more charge and are often used in applications requiring larger energy storage or filtering capabilities. It is important to select a capacitor with the appropriate capacity to ensure proper functioning of the circuit.
45mAh - Battery Type
Battery type refers to the specific chemistry and design of a battery that determines its characteristics, performance, and applications. Common battery types include alkaline, lithium-ion, nickel-metal hydride, and lead-acid, each with unique properties such as voltage, capacity, energy density, and discharge rates. The choice of battery type affects factors such as longevity, rechargeability, and suitability for various electronic devices and systems. Understanding battery type is crucial for selecting the appropriate power source for specific electronic components and applications.
PRIMARY - RoHS Status
RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.
Non-RoHS Compliant
LR41 Battery Equivalent
LR41 batteries can be interchanged with AG3, SR41, 392A, 392, 384, 192, 92A, GP192, G3, V3GA, V36, V36A, LR736, CX42, and SR41SW batteries.
| Battery | Chemistry | Nominal and Cutoff Voltages | Capacity | Operating Temperature | Annual Self-Discharge Rate | Discharge Current |
| Duracell 312 | Zinc Air | 1.45V, 1.1V | 185 mAh 1k5Ω down to 1.1V @21°C | 0°C to +50°C | 4 years unactivated @21°C | - |
| Duracell D384/D392 | Silver Oxide | 1.55V, 1.2V | 45 mAh 22kΩ down to 1.2V @20°C | 0°C to +60°C | <10% @20°C | 70.6μA @1.55V 22kΩ @20°C |
| Energizer 312 | Zinc Air | 1.4V, 1.05V | 181 mAh down to 1.05V, 10/2 mA @21°C | - | - | - |
| Energizer 392/384 | Silver Oxide | 1.55V, 1.2V | 44 mAh 22kΩ down to 1.2V @21°C | - | ~2% @20°C | 68μA @1.50V 22kΩ @21°C |
| muRata LR41 | Alkaline | 1.5V, 0.9V | 45 mAh | -10°C to +60°C | - | - |
| Murata SR41 | Silver Oxide | 1.55V, 1.2V | 45 mAh 22kΩ down to 1.2V @23°C | -10°C to +60°C | - | 70μA @1.55V 22kΩ @23°C |
| Rayovac 312 | Zinc Air | 1.45V, 1.05V | (test dependent) | -10°C to +50°C | 4 years unactivated @21°C | |
| Varta SR736W | Silver Oxide | 1.55V, 1.2V | 40 mAh 13kΩ down to 1.2V @20°C | 0°C to +60°C | - | - |
LR41 Battery Applications
The LR41 battery is a common choice for applications that require a small, reliable battery, The following are some instances of LR41 applications.
Calculator
Laser Pen
Flashlight
Digital Thermometer
Security System Panel
Wrist Watches
Medical Devices and Instruments
Memory Backup
Battery Pack Application
LR41 and SR41 Cell Battery
SR41 and LR41 batteries are button/coin cell batteries that are commonly found in digital thermometers, wristwatches, toys, small LED flashlights, wearable electronics, remote controls, and other similar products.
These batteries come in a variety of chemistries with similar, but not identical, discharge characteristics, and are frequently labeled differently by their makers, causing some user confusion.
The SR41 and LR41 batteries have the same physical dimensions (D x H) of 7.9 x 3.6 mm (0.311 x 0.142 inches), with the following shared features:
| Chemistry | Alkaline | Silver-Oxide | Zinc Air |
| Nominal Voltage | 1.5V | 1.55V | 1.4 - 1.45V |
| Cutoff Voltage | 1.0V | 1.2V | 1.1V |
| Notes | Voltage drops over time | Very constant voltage | Slightly lower voltage, large capacity; mostly used as hearing aid batteries |
| Typical Labels | LR41, LR736, AG3 | SR41 , SR736, SR736PW, SR736SW, SG3, AG3, 192, 384, 392 | 312, ZA312, Brown Tab, PR41, 7002ZD |
| Typical Capacity | 25-32 (45) mAh | 38-45 mAh | ~180 mAh |
LR41 Battery Dimensions

LR41 Battery Dimensions
LR41 Battery Manufacturer
Murata is a global leader in the design, manufacture, and supply of advanced electronic materials, leading-edge electronic components, and multi-functional, high-density modules. Murata innovations can be found in a wide range of applications from mobile phones to home appliances, and automotive applications to energy management systems and healthcare devices.
Datasheet PDF
- Datasheets :
- Environmental Information :
Is LR41 same as LR44?
LR41 is also known as AG3 384 392 192 LR736 L736 GP192 and V36A button battery. LR44 is also known as AG13 357 L1154 A76 PX76A 303 D303 and D357 button battery.
What battery can replace LR41?
Direct replacements for LR41 would be 192, 92A, LR736, and AG3. These batteries are exact equivalents for the LR41 battery, the only difference being the name.
Can I use 377 instead of LR41?
A 377 battery is a Silver Oxide type. They will both fit the application, but the Silver Oxide type will last longer.
What are LR41 batteries for?
LR41 batteries are most commonly used in thermometers, as well as other common electronic devices including laser pointers and some watches.
What are LR41 batteries for?
I checked reference guides and found that the lr41 is equivalent to 392, and lr44 is equivalent to the 357 button batteries.
A Comprehensive Guide to GOLDELOX Microcontroller by 4D Systems Pty Ltd07 March 2024303
A Comprehensive Guide to LTC6992CS6-4#TRPBF Programmable Timer and Oscillator06 March 2024292
A Comprehensive Guide to the 5962-8770203RX Digital to Analog Converter (DAC)06 March 2024169
MCP3424 A/D Converter: Datasheet, Pinout and Schematic13 August 20214576
PT2399 Delay Echo Processor IC: Datasheet, Schematic and Circuit04 November 202134436
FQP27P06 QFET MOSFET: Datasheet, Pinout, Test Circuit07 October 20215261
Kioxia America THGBMJG6C1LBAU7 Memory Overview28 August 20251428
TIP117 PNP Power Transistor: Datasheet pdf, STM Darlington transistor21 December 20213073
Antenna: Principles, Performance Parameters and Classification15 November 20218619
What is Chiplet?17 November 20214298
Intel Launches First-of-its-Kind Semiconductor Technician Certificate Program to Address Workforce Shortage28 September 20233601
How to Address IoT Eco-security in the Era of Digital Transformation?22 April 2022603
How Electric Fuses Work: Types, Ratings, and Selection Guide14 July 202617775
Organic Semiconductor Market Set to Reach USD 843.62 Billion by 2032, Driven by Rising Demand for Flexible Electronics05 October 20232539
Power of Dual and Isomorphic Principles in Power Electronics24 July 20233036
Introduction to Lead Acid Battery: Construction, Working Principle and Types04 March 202110548
Murata Electronics
In Stock: 7450
United States
China
Canada
Japan
Russia
Germany
United Kingdom
Singapore
Italy
Hong Kong(China)
Taiwan(China)
France
Korea
Mexico
Netherlands
Malaysia
Austria
Spain
Switzerland
Poland
Thailand
Vietnam
India
United Arab Emirates
Afghanistan
Åland Islands
Albania
Algeria
American Samoa
Andorra
Angola
Anguilla
Antigua & Barbuda
Argentina
Armenia
Aruba
Australia
Azerbaijan
Bahamas
Bahrain
Bangladesh
Barbados
Belarus
Belgium
Belize
Benin
Bermuda
Bhutan
Bolivia
Bonaire, Sint Eustatius and Saba
Bosnia & Herzegovina
Botswana
Brazil
British Indian Ocean Territory
British Virgin Islands
Brunei
Bulgaria
Burkina Faso
Burundi
Cabo Verde
Cambodia
Cameroon
Cayman Islands
Central African Republic
Chad
Chile
Christmas Island
Cocos (Keeling) Islands
Colombia
Comoros
Congo
Congo (DRC)
Cook Islands
Costa Rica
Côte d’Ivoire
Croatia
Cuba
Curaçao
Cyprus
Czechia
Denmark
Djibouti
Dominica
Dominican Republic
Ecuador
Egypt
El Salvador
Equatorial Guinea
Eritrea
Estonia
Eswatini
Ethiopia
Falkland Islands
Faroe Islands
Fiji
Finland
French Guiana
French Polynesia
Gabon
Gambia
Georgia
Ghana
Gibraltar
Greece
Greenland
Grenada
Guadeloupe
Guam
Guatemala
Guernsey
Guinea
Guinea-Bissau
Guyana
Haiti
Honduras
Hungary
Iceland
Indonesia
Iran
Iraq
Ireland
Isle of Man
Israel
Jamaica
Jersey
Jordan
Kazakhstan
Kenya
Kiribati
Kosovo
Kuwait
Kyrgyzstan
Laos
Latvia
Lebanon
Lesotho
Liberia
Libya
Liechtenstein
Lithuania
Luxembourg
Macao(China)
Madagascar
Malawi
Maldives
Mali
Malta
Marshall Islands
Martinique
Mauritania
Mauritius
Mayotte
Micronesia
Moldova
Monaco
Mongolia
Montenegro
Montserrat
Morocco
Mozambique
Myanmar
Namibia
Nauru
Nepal
New Caledonia
New Zealand
Nicaragua
Niger
Nigeria
Niue
Norfolk Island
North Korea
North Macedonia
Northern Mariana Islands
Norway
Oman
Pakistan
Palau
Palestinian Authority
Panama
Papua New Guinea
Paraguay
Peru
Philippines
Pitcairn Islands
Portugal
Puerto Rico
Qatar
Réunion
Romania
Rwanda
Samoa
San Marino
São Tomé & Príncipe
Saudi Arabia
Senegal
Serbia
Seychelles
Sierra Leone
Sint Maarten
Slovakia
Slovenia
Solomon Islands
Somalia
South Africa
South Sudan
Sri Lanka
St Helena, Ascension, Tristan da Cunha
St. Barthélemy
St. Kitts & Nevis
St. Lucia
St. Martin
St. Pierre & Miquelon
St. Vincent & Grenadines
Sudan
Suriname
Svalbard & Jan Mayen
Sweden
Syria
Tajikistan
Tanzania
Timor-Leste
Togo
Tokelau
Tonga
Trinidad & Tobago
Tunisia
Turkey
Turkmenistan
Turks & Caicos Islands
Tuvalu
U.S. Outlying Islands
U.S. Virgin Islands
Uganda
Ukraine
Uruguay
Uzbekistan
Vanuatu
Vatican City
Venezuela
Wallis & Futuna
Yemen
Zambia
Zimbabwe


Product
Brand
Articles
Tools