Which works better, LR41 or SR41?
ALKALINE MANGANESE BATTERIES
Just like other batteries, LR41 and SR41 are button batteries that seem very similar in many respects. By comparing the LR41 and SR41, we’ll see if the two are interchangeable, and what their differences are.

How to Digital Thermometer Battery replacement LR41 how to use alternative 317 377 376 COVID19
Introduction
Batteries are an item that every family requires. Depending on the specs of your gadget, these batteries, such as the LR41 and SR41, can be used to power it. The quality of these two varieties is comparable but differs in several aspects, so learning more about them before selecting one or both is beneficial.
The fundamental distinction between LR41 and SR41 batteries is that the LR41 has a nominal voltage of 1.5v, while the SR41 has a slightly higher nominal voltage of 1.55V. In addition, the LR41 is an alkaline battery, whereas the SR41 is constructed of silver oxide.
What does LR/SR mean?
Silver Oxide is abbreviated as SR, and SR batteries are silver oxide batteries. For various purposes, experts frequently compare this type of battery to lithium-ion batteries or alkaline batteries.
An SR battery is also referred to as an LR Button Battery. The discharge curve of this battery is flatter than that of an alkaline battery, and it has a longer run time than a lithium-ion battery. This battery has no flammability issues. And you don't even need a thermal runaway!
The LR41 batteries, on the other hand, are alkaline zinc manganese batteries. The ideal temperature is 20°C. LR is an abbreviation for a round alkaline battery. Because of its performance and precision, it is widely used all over the world.
LR41 VS SR41: Physical Dimension
The SR41 button battery size is the same regardless of type or manufacturer. It is a similarity of the same kind. The diameters are constantly 0.311inches and the height is 7.9mm. However, there will be some height discrepancies.

LR41 batteries, on the other hand, are cylindrical. It has the shape of a disc. The average diameter is 7.9mm, while the height of these batteries is 3.6mm.

LR41 VS SR41: Substantial Features
This time, allow us to focus on the LR41 batteries first. This type of battery has some notable features. These are as follows:
It provides a stable performance consistently
The inclusion of manganese dioxide as the cathode material ensures resistance to leakage
Comprises a tremendous pulse discharge technology
Regular discharge output despite under high drain conditions results in proper maintenance of electric voltage
It can be a cost-effective solution
On the contrary, the SR41 battery features some fantastic things comparatively. Would you mind watching the points below?
Comprises a high energy density
Extended storage characteristics
Maintains constant voltage output
Resists leakage carefully
LR41 VS SR41: Applications
The uses of the LR41 Battery
The LR41 is an alkaline magnesium battery that is used in a variety of small electronic devices that require little power.
You can employ this in precision devices such as –
Digital watches
Bike computers
Digital keyboard pianos
Label printers
Cash registers
Electronic dictionaries
Calculators
Laser points
Kids’ toys
Cameras
Heart rate monitors for athletes
Hearing aids
The SR41 is a silver oxide battery model that is befitting for any quartz device. The SR41 lasts longer than most of its counterparts and is very often used for small electronic devices. The SR41 is mainly used in the following application and devices.
Wristwatches
Laser pointers
Digital voice recorders
Clocks
Children’s toys
Glucometers
Interactive children’s books
Thermometers
Digital voice recorders
Cholesterol testers
LR41 VS SR41: Equivalence
LR41 battery equivalent
G3, B-A1/D1, D384, LR4192, LR736, A63, SR41SW, SR41W, V392, 325, 384, S280-18, V384, 247, GP192, GP384, AG3, S736E, SR736PW, SR736SW, TR41SW, SR736, Seiko SB-B1, Seiko SB-A1, Citizen 280-13, Citizen 280-18, and the Timex K.
SR41 battery equivalent
SR41, G3, SR736SW, LR4192, A63, S736E, SR736PW, 325, 384, 392, LR41, LR736, SR736, SB-A1/D1, 280-18, V384, D384, 247, AG3, SR41SW, GP192, TR41SW and SR41W.
LR41 VS SR41: Voltage and Capacity
The nominal voltage of LR41 is 1.5 volt. However, you would be glad to know that a brand new battery LR41 can carry up to 1.55 volts. Overall, its capacity ranges from 25 mAh to 32 mAh. Just one drawback concerning this, its voltage drops over time.
On the opposite, SR41 batteries come up with a nominal voltage of 1.55 volts. And its nominal capacity range is between 38 to 45 mAh. It provides you with a very constant voltage.
LR41 VS SR41: Operating Temperature
The working temperature of SR41 batteries is -10°C to 60°C, while that of LR41 batteries is 0°C to 60°C.
LR41 VS SR41: Durability
The shelf life of the SR41 batteries is 3 years. Since it is for precision electronic devices, this lifespan suffices for many. On the opposition, the LR41 batteries last for around 2 to 3 years.
How to install LR41/SR41?
The installation procedure is essentially the same. The first and most important task is to determine the positive and negative ends of the battery. In general, the flat side of an alkaline battery is the positive side. A "+" sign appears on the positive side.
And the negative side is usually the opposing side with a round protrusion. In other terms, the rounded side is the negative side with the "-" symbol.
Is LR41 same as LR44?
LR41 is also known as AG3 384 392 192 LR736 L736 GP192 and V36A button battery. LR44 is also known as AG13 357 L1154 A76 PX76A 303 D303 and D357 button battery.
What battery can replace LR41?
Direct replacements for LR41 would be 192, 92A, LR736, and AG3. These batteries are exact equivalents for the LR41 battery, the only difference being the name.
Are LR43 and LR44 batteries interchangeable?
The 43 and 44 batteries are different sizes. It's not advisable to interchange them.
Is there a difference between LR and SR batteries?
Physically, LR44 and SR44 are the same sizes. The SR version, on the other hand, has a little higher terminal voltage (1.55v -v- 1.5v) and a slightly greater capacity. There are a plethora of gadgets intended to work with the LR44 battery on the market.
What are LR41 batteries used for?
LR41 batteries are most commonly used in thermometers, as well as other common electronic devices including laser pointers and some watches.
ADC0809CCN ADC: Feature, Specification, Datasheet20 May 20218489
A Comprehensive Guide to LTC6995CS6-2#TRPBF Programmable Timer and Oscillator06 March 2024444
BAV199 Low Leakage Diode: 85V 140MA SOT323, BAV199 Dual Surface Mount and Datasheet19 January 20223395
MCP73831T-2ACI/OT IC Controller Lithium Ion 4.2V: Datasheet, Pinout,and Equivalents22 February 20225718
NC7SZ125P5X: Overview, Features, and Applications19 December 20231278
AP1509 PWM DC-DC Converter: Pinout, Equivalent and Datasheet30 March 20224946
EPM240T100C5 Altera: Specifications, Features and Applications10 April 2025859
AS3935 Lightning Sensor: AS3935 Arduino, Pinout, Datasheet07 July 20213768
Japanese Companies Increase Investment in Power Semiconductors17 March 20225442
Inductor Basics: Structure, Parameters, and Measurement24 October 202517434
What is Regulated Power Supply?08 January 202115598
What is VCSEL?28 October 202112563
What is a Knock Sensor?08 January 202621353
Oregon's Semiconductor Boost: Governor Announces $240 Million Investment06 October 20233455
What is a Fiber Optic Sensor?31 October 202510959
Optical Gates for High-Speed Optical Processing Using Semiconductor-Based Amplifiers30 December 20222199
Murata Electronics
In Stock
United States
China
Canada
Japan
Russia
Germany
United Kingdom
Singapore
Italy
Hong Kong(China)
Taiwan(China)
France
Korea
Mexico
Netherlands
Malaysia
Austria
Spain
Switzerland
Poland
Thailand
Vietnam
India
United Arab Emirates
Afghanistan
Åland Islands
Albania
Algeria
American Samoa
Andorra
Angola
Anguilla
Antigua & Barbuda
Argentina
Armenia
Aruba
Australia
Azerbaijan
Bahamas
Bahrain
Bangladesh
Barbados
Belarus
Belgium
Belize
Benin
Bermuda
Bhutan
Bolivia
Bonaire, Sint Eustatius and Saba
Bosnia & Herzegovina
Botswana
Brazil
British Indian Ocean Territory
British Virgin Islands
Brunei
Bulgaria
Burkina Faso
Burundi
Cabo Verde
Cambodia
Cameroon
Cayman Islands
Central African Republic
Chad
Chile
Christmas Island
Cocos (Keeling) Islands
Colombia
Comoros
Congo
Congo (DRC)
Cook Islands
Costa Rica
Côte d’Ivoire
Croatia
Cuba
Curaçao
Cyprus
Czechia
Denmark
Djibouti
Dominica
Dominican Republic
Ecuador
Egypt
El Salvador
Equatorial Guinea
Eritrea
Estonia
Eswatini
Ethiopia
Falkland Islands
Faroe Islands
Fiji
Finland
French Guiana
French Polynesia
Gabon
Gambia
Georgia
Ghana
Gibraltar
Greece
Greenland
Grenada
Guadeloupe
Guam
Guatemala
Guernsey
Guinea
Guinea-Bissau
Guyana
Haiti
Honduras
Hungary
Iceland
Indonesia
Iran
Iraq
Ireland
Isle of Man
Israel
Jamaica
Jersey
Jordan
Kazakhstan
Kenya
Kiribati
Kosovo
Kuwait
Kyrgyzstan
Laos
Latvia
Lebanon
Lesotho
Liberia
Libya
Liechtenstein
Lithuania
Luxembourg
Macao(China)
Madagascar
Malawi
Maldives
Mali
Malta
Marshall Islands
Martinique
Mauritania
Mauritius
Mayotte
Micronesia
Moldova
Monaco
Mongolia
Montenegro
Montserrat
Morocco
Mozambique
Myanmar
Namibia
Nauru
Nepal
New Caledonia
New Zealand
Nicaragua
Niger
Nigeria
Niue
Norfolk Island
North Korea
North Macedonia
Northern Mariana Islands
Norway
Oman
Pakistan
Palau
Palestinian Authority
Panama
Papua New Guinea
Paraguay
Peru
Philippines
Pitcairn Islands
Portugal
Puerto Rico
Qatar
Réunion
Romania
Rwanda
Samoa
San Marino
São Tomé & Príncipe
Saudi Arabia
Senegal
Serbia
Seychelles
Sierra Leone
Sint Maarten
Slovakia
Slovenia
Solomon Islands
Somalia
South Africa
South Sudan
Sri Lanka
St Helena, Ascension, Tristan da Cunha
St. Barthélemy
St. Kitts & Nevis
St. Lucia
St. Martin
St. Pierre & Miquelon
St. Vincent & Grenadines
Sudan
Suriname
Svalbard & Jan Mayen
Sweden
Syria
Tajikistan
Tanzania
Timor-Leste
Togo
Tokelau
Tonga
Trinidad & Tobago
Tunisia
Turkey
Turkmenistan
Turks & Caicos Islands
Tuvalu
U.S. Outlying Islands
U.S. Virgin Islands
Uganda
Ukraine
Uruguay
Uzbekistan
Vanuatu
Vatican City
Venezuela
Wallis & Futuna
Yemen
Zambia
Zimbabwe


Product
Brand
Articles
Tools