LR43 VS LR44 VS LR41: Can I Use LR43 or LR41 Instead of LR44?
ALKALINE MANGANESE BATTERIES
The LR41, LR43, and LR44 batteries are alkaline batteries. They are manufactured by the same factory, but they are not the totally same. Do you know what and how they are applied to in daily life? This article is going to explain the differences among these three batteries and translate why they can't replace each other.

Review & Save Money LR44 AG13 1.5V Alkaline Button Cell Batteries
- A guide to LR43
- A guide to LR44
- A guide to LR41
- LR43 VS LR44 VS LR41: Specifications
- LR43 VS LR44 VS LR41: Features
- LR43 VS LR44 VS LR41: Applications
- LR43 VS LR44 VS LR41: Equivalents
- LR43 VS LR44 VS LR41: Dimensions
- Are LR43 and LR44 and LR41 batteries interchangeable?
- What to look when purchasing alkaline batteries?
- LR43 VS LR44: Manufacturer
A guide to LR43
The LR43 battery is an alkaline button cell battery. LR43 batteries are 1.5 volts and can operate at temperatures ranging from 0 to 60 degrees Celsius, with 20 degrees Celsius being the ideal range. These batteries are known for their long lifespan, large capacity, high energy density, and dependability. They contribute to consistent performance, great efficiency, and long service life.
A guide to LR44
The LR44 Battery is a 1.5-volt alkaline button cell battery that can be used for a variety of applications. The LR44 1.5V Battery is required by watches, calculators, and medical devices. A button cell battery is a small, spherical battery with a diameter of 11.6mm and a thickness of 5.4mm with a diameter of 11.6mm and a thickness of 5.4mm (0.21 inch).
A guide to LR41
The LR41 battery is a button cell alkaline battery. The LR41 battery has a standard voltage of 1.5V and a diameter of 7.9mm by a height of 3.6mm. The operating temperature of an LR41 battery ranges from 0°C to 60°C, with 20°C being the ideal temperature.
LR43 VS LR44 VS LR41: Specifications
| LR41 | LR43 | LR44 | |
| Battery Nominal Voltage | 1.50 Volts | 1.5V | 1.5V |
| Battery Capacity | ≈ 25-32mAh | 110mAh | 150mAh |
| Battery Operating Temperature | 0°C – 60°C | -10℃ to 60℃ | -10°C to 60°C |
| Battery Diameter | 7.9mm | 11.6mm | 11.6mm |
| Battery Height | 3.6mm | 4.2mm | 5.4mm |
| Battery Chemistry | Alkaline (similarly sized variants in silver oxide) | Alkaline | Alkaline |
| Battery Weight | 0.57g | 1.6g | 2.0g |
LR43 VS LR44 VS LR41: Features
LR43 Battery Features :
Excellent cost performance
High-cost performance has been achieved owing to the use of manganese dioxide as a cathode material.
Excellent stable discharge and high-drain pulse discharge characteristics
Stable voltage output is available during the high-drain pulse discharge.
Excellent leakage resistance
Murata-unique sealing structure, coupled with special sealing-material treatment, has helped accomplish excellent leakage resistance.
RoHS Directive / European Directives
This product does not contain Mercury (Hg), Cadmium (Cd), nor Lead(Pb), and conforms to EC regulation values. (Directive 2006/66/EC, 2013/56/EU)
The battery pack is excluded from the RoHS directive.
LR44 Battery Features :
High-drain discharge characteristics: Large current and high voltage about 3 times that of conventional types can be maintained for long periods.
High safety: The use of patented mercury-free technology ensures safe and secure batteries that are ideal for medical use.
High quality and reliability: 100% made in Japan with over 40 years of manufacturing experience.
LR41 Battery Features :
LR41 battery features a nominal voltage of 1.5 volts and a nominal capacity of 25-32 mAh. Some brands claim a much larger capacity of their LR41 batteries, but such batteries are often drained using ultra-low currents, with their actual capacities being often within the 25-32 mAh range.
LR43 VS LR44 VS LR41: Applications
LR43 Works in:
LR43 Battery is ideal for watches, alarm transmitters, children's books, calculators. sugar level detectors, and many other toys and small electronics.
LR44 Works in:
Medical devices, stopwatches, calorie counters, pedometers, sporting goods, LED lights, pet collars, door chimes, games, toys, garage door openers, electronic organizers, PDAs, hearing aid industries, consumer electronics, keyless entry, Car alarms, Digital thermometers, computer motherboards, Laser pointers, Calculators, and watches.
LR41 Works in:
LR41 batteries are a common choice for applications that require a compact but reliable battery. An LR41 battery is mostly used as a thermometer battery. The LR41 battery is small and provides a consistent, stable discharge, making it perfect for use as a thermometer or digital thermometer battery, The LR41 is an excellent thermometer battery substitute. The following are some more applications for LR41 batteries.
Digital Thermometer
Calculator
Laser Pen
Flashlight
Security System Panel
Wrist Watches
Medical Devices and Instruments
Memory Backup
Battery Pack Application
LR43 VS LR44 VS LR41: Equivalents
LR43 Battery Equivalents:
LR43 battery equivalents are also referred to as SR43, AG12, LR1142, 386, 301, and 186.
LR44 Battery Equivalents:
The LR44 battery is of the alkaline type category, with equivalent batteries being A76, AG13, G13, LR1154, L1154, 154, etc. Silver-oxide batteries can replace these alkaline batteries, with equivalent batteries being SR44, SR44SW, SR44W, SB-B9, 303, 357, etc.
LR41 Battery Equivalents:
192, 92A, LR736, and AG3 are direct replacements for LR41. The 384, SR41, and 392 silver oxide batteries are the same size and dimensions as the LR41 battery, but they are not perfect counterparts or direct replacements because they are made of various chemistries that function differently in different applications. Despite the fact that these batteries have the same size as an LR41 battery, they are not the same.
LR43 VS LR44 VS LR41: Dimensions
LR43 Dimensions

LR44 Dimensions

LR41 Dimensions

Are LR43 and LR44 and LR41 batteries interchangeable?
LR43, LR41, and LR44 batteries are different in size, voltage, and weight. Therefore, they are not interchangeable totally.
LR43 batteries are slimmer than LR44 batteries. If you can put the batteries into the battery compartment (same number, polarity, etc.) and make excellent contact, your gadget should operate. With LR43. the gadget will last less time than with LR44.
The LR41 is much smaller than the LR44 and has a much lower energy capacity, LR41 is equivalent to 392, and LR44 is equivalent to the 357 button batteries.
What to look when purchasing alkaline batteries?
Alkaline batteries are identified by the letters Alkaline. When purchasing a product, there are a few things to keep in mind to ensure that the battery lasts as long as feasible. First and foremost, the expiration date must be considered. Reserves should not be purchased because they have a limited validity duration. The package must be undamaged and all words must be legible; otherwise, it is a forgery. When purchasing batteries, it is important to consider the manufacturer. It is preferable to buy things from well-known firms because they will last longer.
LR43 VS LR44: Manufacturer
Murata is a global leader in the design, manufacture, and supply of advanced electronic materials, leading-edge electronic components, and multi-functional, high-density modules. Murata innovations can be found in a wide range of applications from mobile phones to home appliances, and automotive applications to energy management systems and healthcare devices.
Recommended articles:
CR2450 vs. CR2032: Are they interchangeable?
What does LR stand for when it comes to batteries?
LR denotes a round alkaline battery, whereas CR denotes around lithium battery. The first letter indicates the battery’s kind, while the second indicates its form (R meaning round).
Are LR43 and LR44 batteries interchangeable?
The 43 and 44 batteries are different sizes. It's not advisable to interchange them.
Is there a difference between LR and SR batteries?
Physically, LR44 and SR44 are the same sizes. The SR version, on the other hand, has a little higher terminal voltage (1.55v -v- 1.5v) and a slightly greater capacity. There are a plethora of gadgets intended to work with the LR44 battery on the market.
Is 357 battery same as LR41?
The lr41 is equivalent to 392, and lr44 is equivalent to the 357 button batteries.
Is this interchangeable with an LR 44 Battery?
LR43 is the same voltage, same diameter, lower mA-hr, and most of all, thinner by 1.2mm than LR44.
Are the LR41 and LR44 the same?
The LR41 is much smaller than the LR44 and has a much lower energy capacity.
What are LR41 batteries used for?
LR41 batteries are most commonly used in thermometers, as well as other common electronic devices including laser pointers and some watches.
TL082CP Operational Amplifier: Pinout, Datasheet, and Typical Applications20 July 202111512
LSM6DSRXTR Motion Sensor: STM LSM6DSRXTR, Datasheet, Application Hint09 April 2022972
PSoC® CY8C27143/CY8C27243/CY8C27443/CY8C27543/CY8C27643: Unleashing the Programmable System-on-Chip29 February 2024193
How to Utilize the TLP250 Isolated MOSFET Driver?10 March 202222392
Audio Amplifier IC LM386:Where/How to use?05 May 202212345
A Comprehensive Guide to LTC7880IUKG#TRPBF DC/DC Switching Controller06 March 2024361
LM43603PWPR:Step-Down, DC-DC Converter, 42V18 February 2022685
PIC24FJ128GB204 Microcontroller Datasheet Overview29 February 2024182
What is Bluetooth Low Energy (BLE) Audio Technology?26 April 20227359
Real-time Cloud Analytics in Semiconductor Manufacturing01 November 20222854
Japan's Three-Stage Strategy to Revive the Semiconductor Industry01 April 20228532
A Simple Method to Build a Programmable Oscillator27 May 20227738
A Hybrid SiC and GaN-Based DC-DC Converter for EVs20 September 20243097
What is Chip: Definition, Classification and Design Process17 January 20267776
Microcontroller (MCU) Market Analysis09 February 20226560
An Overview of Thermal Overload Relays12 October 202013843
Murata Electronics
In Stock
United States
China
Canada
Japan
Russia
Germany
United Kingdom
Singapore
Italy
Hong Kong(China)
Taiwan(China)
France
Korea
Mexico
Netherlands
Malaysia
Austria
Spain
Switzerland
Poland
Thailand
Vietnam
India
United Arab Emirates
Afghanistan
Åland Islands
Albania
Algeria
American Samoa
Andorra
Angola
Anguilla
Antigua & Barbuda
Argentina
Armenia
Aruba
Australia
Azerbaijan
Bahamas
Bahrain
Bangladesh
Barbados
Belarus
Belgium
Belize
Benin
Bermuda
Bhutan
Bolivia
Bonaire, Sint Eustatius and Saba
Bosnia & Herzegovina
Botswana
Brazil
British Indian Ocean Territory
British Virgin Islands
Brunei
Bulgaria
Burkina Faso
Burundi
Cabo Verde
Cambodia
Cameroon
Cayman Islands
Central African Republic
Chad
Chile
Christmas Island
Cocos (Keeling) Islands
Colombia
Comoros
Congo
Congo (DRC)
Cook Islands
Costa Rica
Côte d’Ivoire
Croatia
Cuba
Curaçao
Cyprus
Czechia
Denmark
Djibouti
Dominica
Dominican Republic
Ecuador
Egypt
El Salvador
Equatorial Guinea
Eritrea
Estonia
Eswatini
Ethiopia
Falkland Islands
Faroe Islands
Fiji
Finland
French Guiana
French Polynesia
Gabon
Gambia
Georgia
Ghana
Gibraltar
Greece
Greenland
Grenada
Guadeloupe
Guam
Guatemala
Guernsey
Guinea
Guinea-Bissau
Guyana
Haiti
Honduras
Hungary
Iceland
Indonesia
Iran
Iraq
Ireland
Isle of Man
Israel
Jamaica
Jersey
Jordan
Kazakhstan
Kenya
Kiribati
Kosovo
Kuwait
Kyrgyzstan
Laos
Latvia
Lebanon
Lesotho
Liberia
Libya
Liechtenstein
Lithuania
Luxembourg
Macao(China)
Madagascar
Malawi
Maldives
Mali
Malta
Marshall Islands
Martinique
Mauritania
Mauritius
Mayotte
Micronesia
Moldova
Monaco
Mongolia
Montenegro
Montserrat
Morocco
Mozambique
Myanmar
Namibia
Nauru
Nepal
New Caledonia
New Zealand
Nicaragua
Niger
Nigeria
Niue
Norfolk Island
North Korea
North Macedonia
Northern Mariana Islands
Norway
Oman
Pakistan
Palau
Palestinian Authority
Panama
Papua New Guinea
Paraguay
Peru
Philippines
Pitcairn Islands
Portugal
Puerto Rico
Qatar
Réunion
Romania
Rwanda
Samoa
San Marino
São Tomé & Príncipe
Saudi Arabia
Senegal
Serbia
Seychelles
Sierra Leone
Sint Maarten
Slovakia
Slovenia
Solomon Islands
Somalia
South Africa
South Sudan
Sri Lanka
St Helena, Ascension, Tristan da Cunha
St. Barthélemy
St. Kitts & Nevis
St. Lucia
St. Martin
St. Pierre & Miquelon
St. Vincent & Grenadines
Sudan
Suriname
Svalbard & Jan Mayen
Sweden
Syria
Tajikistan
Tanzania
Timor-Leste
Togo
Tokelau
Tonga
Trinidad & Tobago
Tunisia
Turkey
Turkmenistan
Turks & Caicos Islands
Tuvalu
U.S. Outlying Islands
U.S. Virgin Islands
Uganda
Ukraine
Uruguay
Uzbekistan
Vanuatu
Vatican City
Venezuela
Wallis & Futuna
Yemen
Zambia
Zimbabwe


Product
Brand
Articles
Tools