AG10 Battery, AG10 Battery Equivalents and AG10 VS LR44
SINGLE O/P, DC-HV DC PCB MOUNT,
The AG10 Battery is a button shape alkaline battery with a nominal voltage of 1.5 that is used for small electronic devices. It is a popular alkaline button cell battery commonly used in cameras, calculators, toys, and watches. This article is going to explain guide details about ag10 battery.

G10-A battery, 1.5V Button Cell (AG10, SG10, LR54, SR54, LR1130, SR1130)
The guide to AG10 Battery
LR1130/AG10 batteries are alkaline 11.6 x 3.1 mm coin-cell batteries. The AG10's alkaline chemistry is similar to that of a non-rechargeable primary cell. It works by causing a reaction between the two electrodes of the cell: zinc and manganese dioxide (MnO2).
The AG10 is used for small electronic devices. It is a popular alkaline button cell battery commonly used in cameras, calculators, toys, and watches.

The Introduction to AG Alkaline Batteries
AG coded button cell batteries are alkaline batteries and we normally do not stock these however we have listed below our equivalent silver oxide batteries, Silver oxide batteries are slightly more potent than alkaline batteries and usually last a little longer.
AG10 Specifications
| Part: | AG10 |
| Voltage: | 1.5 Volt |
| Capacity: | 50 mAh |
| Type: | Alkaline |
| Height: | 3.05 mm |
| Diameter: | 11.6 mm |
| Shipping Weight: | 0.01Lbs (0.16 oz) |
| Warranty: | 60 Day Return |
| Composition | Zinc/ Manganese dioxide alkaline chemistry |
| Appearance | Tablet disc-shaped button cell |
| Weight | 1gram |
| Resistance | 15KΩ |
| Discharge | Continuous |
| Optimum Temperature | 21 degrees celsius |
| Analogues | LR54, LR1130, L1131, V389, D390, GP89A |
AG10 Features and Benefits
AG10 Batteries Are Non-Rechargeable
AG10 Batteries Are Stable
Alkaline Button AG10 Batteries Have a Long Lifespan
The AG10 Is Small and Portable
Where to use AG10?
The AG10 Battery is a compact electronic device alkaline battery in the shape of a button with a nominal voltage of 1.5. It's a typical alkaline button cell battery that's found in cameras, calculators, toys. and wristwatches.
AG10 Battery Equivalents
SR1130W, SR54, SR1130, SB-BU, 280-15, M, V389, D389, 626, S1131E, GP389, AG10, AG-10, 389, 189, L1131, G10, V10GA, LR1130, GP189, LR54, SG10, A389, L1131. L1131 C, L1131 D RW89. LR1130 S, LR1131, L1131/D, LR1130 H, 389A, 389E, 389X, L1133, SR1131, LL1131, LL1131F, L1131F, L1131H, LR1130X, L-1131, SR1130PW, L1130, LH1130, E389
AG10 VS LR44
Despite the fact that they have the same diameter, AG10 is thinner (about 3.1 mm vs. about 5.4 mm for the LR44. As a result, the LR44 has slightly more capacity than the AG10.
If you're having trouble figuring out which one you have, consider the following: The AG10 is roughly the thickness of two US/Canadian pennies or Euro cents; the LR44 is roughly the thickness of three US quarters or Canadian toonies, slightly thicker than three Euro cents, or slightly smaller than the diameter of a pencil.
An AG10 may fit in an LR44 device, but it will most likely not establish good contact. If it fits, it will work, but only for a short while. It's unlikely that an LR44 will fit into a gadget. An LR44 is unlikely to fit in a device designed for an AG10.
Why the AG10 is non-chargeable?
The AG10's alkaline chemistry is similar to that of a non-rechargeable primary cell, It works by causing a reaction between the two electrodes of the cell: zinc and manganese dioxide (MnO2).
The electrolyte is formed of potassium hydroxide, a metal salt.
So, what's the deal with it not being rechargeable?
It all boils down to the chemistry of the chemical reaction. The chemical reactions in a battery cell must be totally reversible in order for it to be recharged.
That is, the reaction's product must be broken down into the same substances that it was made of.
If A+B =C, then C must break down in the reverse reaction to create A and B.
However, the zinc/manganese dioxide process that generates the cell's chemical energy can only be reversed when it reaches 40% discharge with this sort of alkaline battery,
The process grows more difficult beyond the first 40% and is irreversible. This is because the hydrogen ions (H+) produced will combine with the manganese oxide (MnO2) to form groutite, a non-reversible chemical (MnOOH).
There is no method to restore the charge of the alkaline battery since groutite cannot be broken down into MnO2 even after the hydrogen ions have been removed.
If you try to recharge it, the cells may explode due to the gas that has accumulated inside the seal.
Are LR54 and AG10 the same?
These batteries are also known as 189, AG10 or V10GA batteries. This LR54 battery measures 11.6mm in diameter and 3.1mm in height with 44-68mAh capacity.
Is AG10 the same as LR1130?
LR1130 is same as LR54 or AG10. L means it is an alkaline battery, R means it is round, 11 means it us 11.8mm in diameter and 30 means it is 3.0mm in height
Is an AG10 button cell battery the same as a VG10A alkaline button battery?
AG10 and VG10A is one and the same thing. The two designations are used for alkaline batteries used in small gadgets like watches and toys. The size dimensions and specifications on both are the same. So, you can use the two names interchangeably.
What battery replaces AG10?
389 Battery is a direct replacement for SR1130W, SR54, SR1130, SB-BU, 280-15, M, V389, D389, 626, S1131E, GP389, AG10, AG-10, 389, 189, L1131, G10, V10GA, LR1130, GP189, LR54, SG10, A389, L1131, L1131C, L1131D RW89.
Can I use AG13 instead of AG10?
No, AG13 and AG10 are different batteries.
What is an AG10 Battery used for?
The AG10 Battery is a button shape alkaline battery with a nominal voltage of 1.5 that is used for small electronic devices. It is a popular alkaline button cell battery commonly used in cameras, calculators, toys, and watches
What is the voltage of AG10 button cell?
1.5 Volts
M16C/26A Group: Single-Chip 16-Bit CMOS Microcomputer Overview28 February 2024261
NE556 Timer: Datasheet, Pinout and Circuit20 July 20215934
A Comprehensive Guide to OP97EN8#PBF Linear Amplifier06 March 2024207
LTM9011IY-14#PBF Analog to Digital Converter: A Comprehensive Product Overview06 March 2024329
STM32L151RDT7 Microcontroller: Thorough Technical Analysis29 February 2024195
Which works better, LR41 or SR41?21 July 202235121
TL431AIDBZR IC: Features, Applications and Datasheet31 October 2023670
Renesas MCF5235CVM100 Microcontroller: Comprehensive Technical Overview29 February 2024210
Arduino Based Gas Leakage Detection29 August 202310984
What are Quantum Sensors?27 October 20212713
This New Material Promises to Be the Best Semiconductor25 July 20222570
16 Q&A About the Secrets of Operational Amplifiers27 March 20256857
Introduction to Potential Transformers21 September 202011822
Radiation Robustness of Gallium Nitride Power Devices16 January 20243107
What is NAND Flash?04 November 202112861
What is a Multimeter?20 December 20217152
XP Power
In Stock
United States
China
Canada
Japan
Russia
Germany
United Kingdom
Singapore
Italy
Hong Kong(China)
Taiwan(China)
France
Korea
Mexico
Netherlands
Malaysia
Austria
Spain
Switzerland
Poland
Thailand
Vietnam
India
United Arab Emirates
Afghanistan
Åland Islands
Albania
Algeria
American Samoa
Andorra
Angola
Anguilla
Antigua & Barbuda
Argentina
Armenia
Aruba
Australia
Azerbaijan
Bahamas
Bahrain
Bangladesh
Barbados
Belarus
Belgium
Belize
Benin
Bermuda
Bhutan
Bolivia
Bonaire, Sint Eustatius and Saba
Bosnia & Herzegovina
Botswana
Brazil
British Indian Ocean Territory
British Virgin Islands
Brunei
Bulgaria
Burkina Faso
Burundi
Cabo Verde
Cambodia
Cameroon
Cayman Islands
Central African Republic
Chad
Chile
Christmas Island
Cocos (Keeling) Islands
Colombia
Comoros
Congo
Congo (DRC)
Cook Islands
Costa Rica
Côte d’Ivoire
Croatia
Cuba
Curaçao
Cyprus
Czechia
Denmark
Djibouti
Dominica
Dominican Republic
Ecuador
Egypt
El Salvador
Equatorial Guinea
Eritrea
Estonia
Eswatini
Ethiopia
Falkland Islands
Faroe Islands
Fiji
Finland
French Guiana
French Polynesia
Gabon
Gambia
Georgia
Ghana
Gibraltar
Greece
Greenland
Grenada
Guadeloupe
Guam
Guatemala
Guernsey
Guinea
Guinea-Bissau
Guyana
Haiti
Honduras
Hungary
Iceland
Indonesia
Iran
Iraq
Ireland
Isle of Man
Israel
Jamaica
Jersey
Jordan
Kazakhstan
Kenya
Kiribati
Kosovo
Kuwait
Kyrgyzstan
Laos
Latvia
Lebanon
Lesotho
Liberia
Libya
Liechtenstein
Lithuania
Luxembourg
Macao(China)
Madagascar
Malawi
Maldives
Mali
Malta
Marshall Islands
Martinique
Mauritania
Mauritius
Mayotte
Micronesia
Moldova
Monaco
Mongolia
Montenegro
Montserrat
Morocco
Mozambique
Myanmar
Namibia
Nauru
Nepal
New Caledonia
New Zealand
Nicaragua
Niger
Nigeria
Niue
Norfolk Island
North Korea
North Macedonia
Northern Mariana Islands
Norway
Oman
Pakistan
Palau
Palestinian Authority
Panama
Papua New Guinea
Paraguay
Peru
Philippines
Pitcairn Islands
Portugal
Puerto Rico
Qatar
Réunion
Romania
Rwanda
Samoa
San Marino
São Tomé & Príncipe
Saudi Arabia
Senegal
Serbia
Seychelles
Sierra Leone
Sint Maarten
Slovakia
Slovenia
Solomon Islands
Somalia
South Africa
South Sudan
Sri Lanka
St Helena, Ascension, Tristan da Cunha
St. Barthélemy
St. Kitts & Nevis
St. Lucia
St. Martin
St. Pierre & Miquelon
St. Vincent & Grenadines
Sudan
Suriname
Svalbard & Jan Mayen
Sweden
Syria
Tajikistan
Tanzania
Timor-Leste
Togo
Tokelau
Tonga
Trinidad & Tobago
Tunisia
Turkey
Turkmenistan
Turks & Caicos Islands
Tuvalu
U.S. Outlying Islands
U.S. Virgin Islands
Uganda
Ukraine
Uruguay
Uzbekistan
Vanuatu
Vatican City
Venezuela
Wallis & Futuna
Yemen
Zambia
Zimbabwe


Product
Brand
Articles
Tools