web counter

MAX30100 Heart-Rate Sensor IC : Specification, Pinout and Datasheet

Sophie

Published: 18 September 2021 | Last Updated: 18 September 2021

10711

datasheet pdf and product details from stock available at Utmel

Purchase Guide

Hi, fellas. Welcome back to the new post today. MAX30100 is a Pulse Oximeter and Heart-Rate Sensor IC which is used to check the health of a person with any condition that affects blood oxygen levels. This article mainly introduces specification, pinout, datasheet, and other detailed information about Maxim Integrated MAX30100.

In this video, we will make a device that can measure Blood Oxygen Concentration & Heart Rate using MAX30100 Pulse Oximeter & Arduino.

Blood Oxygen & Heart Rate Measurement with MAX30100/02 Pulse Oximeter & Arduino

MAX30100 Description

MAX30100 is a Pulse Oximeter and Heart-Rate Sensor IC which is used to check the health of a person with any condition that affects blood oxygen levels, such as Heart Attack, Heart failure, Lungs Cancer Asthma, etc. 


The MAX30100 operates from 1.8V and 3.3V power supplies and can be powered down through software with negligible standby current, permitting the power supply to remain connected at all times. 


The sensor comprises two Light Emitting Diodes, a photodetector, and a series of low noise signal processing devices to detect heart rate and to perform pulse oximetry.


MAX30100 Pinout

MAX30100 PINOUT.jpg

MAX30100 Pinout

Pin NumberPin NameDescription
1,7,8,14N.C.No Connection. Connect to PCB Pad for Mechanical Stability.
2SCLI2C Clock Input
3SDAI2C Clock Data, Bidirectional (Open-Drain)
4PGNDPower Ground of the LED Driver Blocks
5IR_DRVIR LED Cathode and LED Driver Connection Point. Leave floating in the circuit.
6R_DRVRed LED Cathode and LED Driver Connection Point. Leave floating in the circuit.
9R_LED+Power Supply (Anode Connection) for Red LED. Bypass to PGND for best performance.  Connected to IR_LED+ internally.
10IR_LED+Power Supply (Anode Connection) for IR LED. Bypass to PGND for best performance. Connected to R_LED+ internally
11VDDAnalog Power Supply Input. Bypass to GND for best performance.
12GNDAnalog Ground
13INTActive-Low Interrupt (Open-Drain)

MAX30100 Pin Description

MAX30100 Features

●Operating Voltage - 1.8V to 3.3V

●Input Current - 20mA

●Integrated Ambient Light Cancellation

●High Sample Rate Capability

●Fast Data Output Capability


Specifications

technical specifications, attributes, parameters and parts with similar specifications to .
  • Type
    Parameter
0 Similar Products Remaining

MAX30100 Functional Diagram

Functional Diagram.png

MAX30100 Functional Diagram

MAX30100 System Block Diagram

System Block Diagram.png

System Block Diagram

As the system block diagram is shown, there should be a small distance between the sensor and finger.


MAX30100 Advantages

● Complete Pulse Oximeter and Heart-Rate Sensor Solution Simplifies Design

• Integrated LEDs, Photo Sensor, and High-Performance Analog Front -End

• Tiny 5.6mm x 2.8mm x 1.2mm 14-Pin Optically Enhanced System-in-Package

● Ultra-Low-Power Operation Increases Battery Life for Wearable Devices

• Programmable Sample Rate and LED Current for Power Savings

• Ultra-Low Shutdown Current (0.7µA, typ)

● Advanced Functionality Improves Measurement Performance

• High SNR Provides Robust Motion Artifact Resilience

• Integrated Ambient Light Cancellation

• High Sample Rate Capability

• Fast Data Output Capability


MAX30100 Disadvantages

1. If the fingers are not placed properly, incorrect readings may be produced. Ambient light falling on the sensor will affect the final reading. When using the Max30100 oximeter, make sure that your fingers are not moving, as this may cause incorrect readings.

2. Do not press the sensor forcefully, as this will affect blood flow and cause incorrect readings. Place your fingers as gently as possible and make sure that they do not move, so that you can get the most accurate readings.


MAX30100 Arduino

MAX30100 Arduino.png

Interfacing Max30100 Pulse Oximeter Sensor with Arduino Circuit Diagram

First, let's start with a very basic circuit diagram. As you can see the VIN and GND pins of the Max30100 sensor are connected with the Arduino’s 3.3v and GND pins. The SCL pin is connected with the Analog pin A5, SDA pin is connected with the Analog pin A4. While the INT pin is not connected.


max30100 arduino 2.png

Interfacing Max30100 Pulse Oximeter Sensor and 16×2 LCD with Arduino Circuit Diagram

This is the modified circuit diagram. The max30100 pulse Oximeter sensor connection with the Arduino remains the same. This time I added a 16×2 LCD. As you can see, pin number 1 and pin number 16 are connected with the Arduino’s ground. Pin number 2 and pin number 15 are connected with the Arduino’s 5 volts. Pin number 3 is the contrast pin and is connected with the middle leg of the potentiometer this is used for the LCD contrast adjustment.

The RS pin of the LCD is connected with the Arduino’s pin number 9, the R/W pin is connected with the ground, Enable pin is connected with the Arduino’s pin number 8. Pins D4 to D7 of the 16X2 LCD is connected with the Arduino’s pins 7, 6, 5, and 4.



MAX30100 Equivalent

MAX30102


MAX30100 Applications

-Used in medical oxygen measurement devices

-Used in wearable devices

-Used in fitness assistant systems


MAX30100 Manufacturer

Maxim Integrated, a subsidiary of Analog Devices, designs, manufactures and sells analog and mixed-signal integrated circuits for the automotive, industrial, communications, consumer, and computing markets. Maxim's product portfolio includes power and battery management ICs, sensors, analog ICs, interface ICs, communication solutions, digital ICs, embedded security, and microcontrollers. The company is headquartered in San Jose, California, with design centers, manufacturing facilities, and sales offices around the world.


Frequently Asked Questions

1.How to connect the MAX30100 chip to the MCU?

You only need to connect to the I2C interface, if the microcontroller does not have an I2C interface, you can use IO to simulate an I2C.

2.What electronic component is MX30100?

MAX30100 is a sensor chip that can collect heart rate, blood oxygen temperature, and the communication serial port uses I2C.
MAX30100 is a sensor that can read heart rate and blood oxygen. The communication method is through IIC.
Its working principle is to get the ADC value of heart rate through infrared LED light.

3.Will the red LED light up when the MAX30100 is powered on?

It is not appropriate to use 12V voltage to directly bring 4 red LED lights. It is easy to cause damage to one or several of the four LED lights, so it will not light up.
Because the forward voltage drop of a general red LED light-emitting tube is only about 2.2V 

In Stock

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe