DL2032 vs. CR2032: Is there a difference between them?
BATTERY LITHIUM 3V COIN 20MM
Batteries are essential in our daily lives. For all the credits taken by the devices, they work invisibly behind the curtain, under the scene. When it comes to DL2032 and CR2032, the titles, sizes, and voltages of DL and CR are the most significant differences. This article is going to explain the differences between DL2032 and CR2032 batteries. Furthermore, there is huge in stock on our website. Welcome your RFQ!

Can Amazon Basics CR2032 Battery Beat Energizer or Duracell? I Have The Answer!
Why Compare?
The sizes and voltages are the most significant differences between DL2032 and CR2032. Aside from that, the dot fact is the manufacturing source. CR, like AA and AAA, is essentially a generic designation. Almost all battery manufacturers use it. The DL mark, on the other hand, is reserved for Duracell, a battery manufacturer.
Overview of DL2032
Duracell DL2032 special application batteries deliver the same dependable, long-lasting power that Duracell is known for. Duracell is the #1 trusted brand of pharmacists, doctors & office workers, so you can be sure it's a battery you can rely on. Security gadgets, fitness devices, calculators, medical equipment, watches, key fobs, and other devices can all benefit from the Duracell 2032 coin cell battery.

DL2032
Main Features of DL2032
The particular uses of DL2032 batteries provide dependable service throughout their 10-year life span. It has a higher energy density and rate of discharge than the CR2032. It maintains a constant supply of power under the intermittent or continuous drain, well surpassing the limitations of CRs.
Limitations of DL2032
Once replaced and it collapses
One of the most common complaints from consumers is that once the DR2032 has been changed by another, it does not appear to work as well as before. You can utilize it just fine, but if you expect it to be a long-term service provider, you may be disappointed.
Non-reusable
As previously stated, non-rechargeable and non-reusable batteries require additional money out of your wallet, which we do not approve of.
Overview of CR2032
The CR2032 battery is a three-volt lithium-ion battery in the shape of a coin. With some minor modifications, this class of batteries has a diameter of 20 mm and a thickness of 3.1 mm. CR2032 battery units, often known as CMOS batteries or coin batteries, are commonly used in low-power applications like powering a computer's BIOS or a quiescent device's real-time clock.

CR2032
Main Features of CR2032
The most widely used batteries of all time are Panasonic Lithium coin CR batteries. They are well-known for their long battery life. That means one purchase is followed by a long period of not purchasing anything else. These are dependable power sources that can be used in a variety of applications. Toys, calculators, electronic devices, such as watches, key fobs, and cameras, are just a few examples. It's important not to be swayed by the size of this outstanding power transmitter. Despite its modest size, the CR2032 has been tested and true by many users.
Limitations of CR2032
Non-reusable
One of the biggest disadvantages of CRs is that the batteries are not rechargeable. It implies you have no choice but to buy a new one if it becomes damaged. Without the reusable quality of the CR2032, no matter how many dives, it must be replaced, which adds to the cost, time, and effort.
Low current draw capability
Low current draw capability means that, while it is suitable for a variety of electronic applications, it is unlikely to draw a substantial amount of current. It is ideal for use with small objects such as toys and watches, but not for handling a device larger and more powerful than that with a significant purpose.
Needs a special holder
It's difficult for CR2032 to be useful in any area because of the unique holder. The positioning of CR2032 is not possible in every compartment. And without the right fit and current flow where the current streams may intersect, the battery is as useless as the gadget without it.
DL2032 vs. CR2032: Battery Maker
The manufacturer is the key distinction between these two batteries. Any Li-MnO2 coin battery that begins with the letter CR is a general IEC prefix. This is a technique that most manufacturers now employ. Duracell, on the other hand, makes a battery that starts with the letter DL.
DL2032 vs. CR2032: Battery Capacity
In comparison to the CR2032, the DL2032 battery has a substantially higher capacity. A CR2032 battery has a capacity of 220 mAh, whereas a DL2032 has a capacity of 240 mAh. This prolongs the life of the Duracell battery and reduces the frequency with which it must be replaced.
DL2032 vs. CR2032: Features and Specifications
| DL2032 | CR2032 |
| Power Preserve technology, which allows them to retain their charge even after sitting for 10 years | 8-year leak-free shelf life, ideal for watches, calculators, key fobs, Apple TV remotes, and other small electronics |
| General-purpose battery with many applications. | Panasonic Lithium coin with long-lasting reliable power. |
| Chemistry: Lithium, high-power, non-rechargeable. | Chemistry: Lithium, high-power, non-rechargeable. |
| 3V power and 225mAh capacity; offers reliable performance | 3V power and 225mAh capacity; offers reliable performance |
| Weight: 8g | Typical Weight: 3.0g. |
| Dimension: 19mm x 19mm x 3mm | Dimension: 20mm diameter, 3.2 height. |
| Battery Type: Coin Cell. | Battery Type: Lithium Coin Cell. |
| Reusability Single-Use | Reusability Single-Use |
| Typical Application: Electronics. | Operating temp: 30C-60C, used in a various range of products. |
DL vs. CR Batteries
The only distinction between CR and DL batteries is the manufacturer. CR, like AA and AAA, is essentially a generic designation. Almost all battery manufacturers use it. Duracell, on the other hand, uses the DL designation for their batteries.
The most likely reason for switching from a generic to a unique designation is to distinguish their product from what is currently available. Duracell may seek to set them apart from the competition since their product has a bigger capacity and they want their good name to propagate. It's not simple when the batteries in this category are used in low-power devices and are expected to last months, if not years.
This modification causes some confusion because people often look for a battery that is an identical match to the one they have. The DL and CR batteries can be interchanged as long as the numbers after they are the same. A DL2032 battery can be used to replace a CR2032 battery in the example above, and vice versa.
Summary
With almost every component covered, from the interior to the exterior, both batteries have the same set of advantages and disadvantages that are nearly equal. The only difference between DL and CR in non-reusable batteries is their manufacturer. So it's reasonable to state that one can choose between the CR2032 and the DL2032, both of which have the Duracell brand on them.
Is there a difference between DL2032 and CR2032?
Answer- As far as the number is concerned, with the similar number code there is not much of a contrast between these two. The only dissimilarity worth mentioning is that DL2032 is made by the battery company Duracell and CRs by someone else.
Are DL2032 and CR2032 interchangeable?
They are indeed replaceable with the same number code. For example, you can definitely place DL2031 instead of CR2032 and vice versa. With the standard size of 2omm diameter and 3.2 mm thickness, yes, they are interchangeable.
Is CR2032 and DL2032 battery the same?
No difference, totally interchangeable. DL2032 is made by Duracell; all other manufacturers call it CR2032.
What battery can replace a DL2032 battery?
It is okay to replace a DL2032 battery with a CR2032 battery as these have the same voltage, same performance, and 3 times cheaper price. But you may find that a CR2032 battery doesn’t last as long as a DL2032 battery does.
STUSB4500 USB PD Controller: Pinout, Features and Datasheet06 January 202212838
TL06xx Series (TL064) 200µA Low-Power JFET Op-Amp: Specs, Pinout, and Design Analysis28 February 2026119
L6203 Bridge Driver: Circuit, Pinout, and Datasheet22 October 20216064
STM32MP157CAA3 Development: From Setup and Configuration to Advanced Features Implementation07 June 20251406
D882 Transistor: NPN Medium Power Transistor, Pinout, Equivalent, Uses13 January 202255227
MMBT3904 NPN Transistor: Pinout, Datasheet and Applications08 July 20213625
PCF8574T I/O Expander[FAQ+Video]: Datasheet, Alternatives, and Circuit23 April 20226473
OnSemi MBR0540T1G Schottky Diode: 40V 500mA Fast Switching Review27 August 2025411
What Are Buck-Boost Converters?07 June 20251188
How does a Resettable Fuse Work?26 August 202037575
China to Inject $40 Billion into Semiconductor Sector with New State Fund07 September 20232798
Global Semiconductor Sales Experience a 2.3% Surge in July 202309 September 20233876
What is Amplifier?08 November 20258078
What is a Gyroscope Sensor?11 September 202018164
Introduction to Potential Transformers21 September 202011440
Best 1N4007 diode alternatives to use in 202525 August 20259099
Panasonic - BSG
In Stock
United States
China
Canada
Japan
Russia
Germany
United Kingdom
Singapore
Italy
Hong Kong(China)
Taiwan(China)
France
Korea
Mexico
Netherlands
Malaysia
Austria
Spain
Switzerland
Poland
Thailand
Vietnam
India
United Arab Emirates
Afghanistan
Åland Islands
Albania
Algeria
American Samoa
Andorra
Angola
Anguilla
Antigua & Barbuda
Argentina
Armenia
Aruba
Australia
Azerbaijan
Bahamas
Bahrain
Bangladesh
Barbados
Belarus
Belgium
Belize
Benin
Bermuda
Bhutan
Bolivia
Bonaire, Sint Eustatius and Saba
Bosnia & Herzegovina
Botswana
Brazil
British Indian Ocean Territory
British Virgin Islands
Brunei
Bulgaria
Burkina Faso
Burundi
Cabo Verde
Cambodia
Cameroon
Cayman Islands
Central African Republic
Chad
Chile
Christmas Island
Cocos (Keeling) Islands
Colombia
Comoros
Congo
Congo (DRC)
Cook Islands
Costa Rica
Côte d’Ivoire
Croatia
Cuba
Curaçao
Cyprus
Czechia
Denmark
Djibouti
Dominica
Dominican Republic
Ecuador
Egypt
El Salvador
Equatorial Guinea
Eritrea
Estonia
Eswatini
Ethiopia
Falkland Islands
Faroe Islands
Fiji
Finland
French Guiana
French Polynesia
Gabon
Gambia
Georgia
Ghana
Gibraltar
Greece
Greenland
Grenada
Guadeloupe
Guam
Guatemala
Guernsey
Guinea
Guinea-Bissau
Guyana
Haiti
Honduras
Hungary
Iceland
Indonesia
Iran
Iraq
Ireland
Isle of Man
Israel
Jamaica
Jersey
Jordan
Kazakhstan
Kenya
Kiribati
Kosovo
Kuwait
Kyrgyzstan
Laos
Latvia
Lebanon
Lesotho
Liberia
Libya
Liechtenstein
Lithuania
Luxembourg
Macao(China)
Madagascar
Malawi
Maldives
Mali
Malta
Marshall Islands
Martinique
Mauritania
Mauritius
Mayotte
Micronesia
Moldova
Monaco
Mongolia
Montenegro
Montserrat
Morocco
Mozambique
Myanmar
Namibia
Nauru
Nepal
New Caledonia
New Zealand
Nicaragua
Niger
Nigeria
Niue
Norfolk Island
North Korea
North Macedonia
Northern Mariana Islands
Norway
Oman
Pakistan
Palau
Palestinian Authority
Panama
Papua New Guinea
Paraguay
Peru
Philippines
Pitcairn Islands
Portugal
Puerto Rico
Qatar
Réunion
Romania
Rwanda
Samoa
San Marino
São Tomé & Príncipe
Saudi Arabia
Senegal
Serbia
Seychelles
Sierra Leone
Sint Maarten
Slovakia
Slovenia
Solomon Islands
Somalia
South Africa
South Sudan
Sri Lanka
St Helena, Ascension, Tristan da Cunha
St. Barthélemy
St. Kitts & Nevis
St. Lucia
St. Martin
St. Pierre & Miquelon
St. Vincent & Grenadines
Sudan
Suriname
Svalbard & Jan Mayen
Sweden
Syria
Tajikistan
Tanzania
Timor-Leste
Togo
Tokelau
Tonga
Trinidad & Tobago
Tunisia
Turkey
Turkmenistan
Turks & Caicos Islands
Tuvalu
U.S. Outlying Islands
U.S. Virgin Islands
Uganda
Ukraine
Uruguay
Uzbekistan
Vanuatu
Vatican City
Venezuela
Wallis & Futuna
Yemen
Zambia
Zimbabwe


Product
Brand
Articles
Tools