IRF540N N-Channel Power MOSFET: Circuits, Equivalent, and IRF540N vs IRF540

Sophie

Published: 19 August 2021 | Last Updated: 19 August 2021

32810

IRF540N

IRF540N

VBsemi Elec

IRF540N datasheet pdf and Unclassified product details from VBsemi Elec stock available at Utmel

Purchase Guide

The IRF540N is an N-channel power MOSFET in the TO-220AB package.

The IRF540N is an advanced HEXFET N-channel power MOSFET.

Voltage controller circuit with ampere using IRF540N? Electronics

IRF540N Description

The IRF540N is an N-channel power MOSFET in the TO-220AB package. The IRF540N utilizes advanced processing techniques to achieve extremely low on-resistance per silicon area. This benefit, combined with the fast switching speed and ruggedized device design that HEXFET Power MOSFETs are well known for, provides the designer with an extremely efficient and reliable device for use in a wide variety of applications.

The TO-220 package is universally preferred for all commercial-industrial applications at power dissipation levels to approximately 50 watts. The low thermal resistance and low package cost of the TO-220 contribute to its wide acceptance throughout the industry.


IRF540N Pinout

IRF540N Pinout.jpg


IRF540N CAD Model

Symbol

IRF540N Symbol.png


Footprint


IRF540N Footprint.png


3D Model


IRF540N 3D Model.jpg


IRF540N Features

  • Package Type: TO-220AB

  • Transistor Type: N Channel

  • Max Drain to Source Voltage: 100 V

  • Max Drain to Gate Voltage: 100 V

  • Max Gate to Source Voltage: ±20 V

  • Max Continuous Drain Current: 45 A (Different manufacturers might have different ratings, for Fairchild Semiconductor it is 33 A)

  • Max Power Dissipation: 127 W (For Fairchild Semiconductor it is 120 W)

  • Typical Drain to Source On Resistance: 0.032 Ω

  • Max Drain to Source On Resistance: 0.065 Ω (For Fairchild Semiconductor it is 0.04 Ω)

  • Storage & Operating temperature: -55 to +175 Celsius


IRF540N Advantages

  • Cutting-Edge Process Technology

  • Ultra-Low On-Resistance

  • Dynamic dv/dt Rating

  • Fast Switching

  • Fully Avalanche Rated

  • Capable of Being Wave-soldered


Specifications

VBsemi Elec IRF540N technical specifications, attributes, parameters and parts with similar specifications to VBsemi Elec IRF540N.
  • Type
    Parameter
  • Package / Case

    refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.

    TO-220AB
  • Packaging

    Semiconductor package is a carrier / shell used to contain and cover one or more semiconductor components or integrated circuits. The material of the shell can be metal, plastic, glass or ceramic.

    Tube-packed
  • RoHS Status

    RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.

    RoHS Compliant
0 Similar Products Remaining

IRF540N Test Circuits and Waveforms

IRF540N Unclamped Energy Test Circuit and Waveform.png

IRF540N Unclamped Energy Test Circuit and Waveform

 

 IRF540N Gate Charge Test Circuit and Waveform.png

IRF540N Gate Charge Test Circuit and Waveform

 

 IRF540N Switching Time Test Circuit and Waveform.png

IRF540N Switching Time Test Circuit and Waveform


IRF540N Functional Alternatives

IRF540N Functional Alternatives.png


IRF540N Equivalents

RFP30N06, IRFZ44, 2N3055, IRF3205, IRF1310N, IRF3415, IRF3710, IRF3710Z, IRF3710ZG, IRF8010, IRFB260N, IRFB4110, IRFB4110G, IRFB4115, IRFB4115G, IRFB4127, IRFB4227, IRFB4233, IRFB4310, IRFB4310G, IRFB4310Z, IRFB4310ZG, IRFB4321, IRFB4321G, IRFB4332, IRFB4410, IRFB4410Z, IRFB4410ZG, IRFB4510, IRFB4510G, IRFB4610, IRFB4615, IRFB4710, IRFB52N15D, IRFB5615, IRFB59N10D, IRFB61N15D

Please check the pin configuration before replacing them in your circuit.


Where to use IRF540N

The IRF540N is an N-Channel power MOSFET that's best suited for high power DC switching applications, such as in high current SMPS power supplies, compact ferrite inverter circuits, iron core inverter circuits, buck and boost converters, power amplifiers, motor sped controllers, robotics, etc. It can also be used with Arduino and other microcontrollers for logic switching.


How to use IRF540N

As a voltage-controlled device, MOSFET can be turned on/off by supplying the required gate threshold voltage (VGS). The IRF540N is an N-channel MOSFET, so the Drain and Source pins will be left open when there is no voltage applied to the Gate pin. When a voltage is applied to the Gate, the Drain and Source pins will close.

This circuit shows how this MOSFET behaves when there is a Gate voltage (5V) and there is not (0V). Since this is an N-Channel MOSFET, the load to be switched (in this case a motor) should always be connected above the drain pin.

How to use IRF540N.png

When you turn on a MOSFET by supplying the required voltage to the gate pin, it will remain on unless you supply 0V to the gate. To avoid this problem we should always use a pull-down resistor (R1), here I have used a value of 10k. In applications like controlling the speed of the motor or dimming light, we would use a PWM signal for fast switching, during this scenario the MOSFET's gate capacitance will create a reverse current due to the parasitic effect. To tackle this problem we should use a current limiting capacitor, I have used a value of 470 here.


How to Connect IRF540N

1. Connect the source to the ground or the negative line of the supply.

2. Connect the drain to the positive terminal of the supply via the load which needs to be operated by the device.

3. Connect the gate, which is the trigger lead of the device, to the trigger point of the circuit. This trigger input should be preferably a +5V supply from a CMOS logic source. If the trigger input is not a logic source make sure the gate is permanently connected to the ground via a high-value resistor.

4. When the device is being used for switching inductive loads like a transformer or a motor, a flyback diode should be connected across the load, with the cathode of the diode connected to the positive side of the load.

5. Because the IRF540N has a built-in avalanche protective diode, there is no need for an external diode. But you can use one if you want to provide extra safety to the device.


IRF540N vs IRF540

The IRF540N and IRF540 are both N-channel MOSFETs. The IRF540 is made with trench technology, with a small wafer area and relatively lower cost. The IRF540N, however, is made with planar technology, with a large wafer area and high current-carrying capability. The IRF540N also has a lower maximum on-resistance which is 0.044 Ω, while the IRF540 is 0.077 Ω.

The difference in some important parameters (Note: different manufacturers might have different parameters):

IRF540: 23 A, 100 V, 0.077 Ohm; IRF540N: 33 A, 100 V, 0.044 Ohm. They both come in the TO-220 package and their pins are the same, the main difference is their current-carrying capability, if you are fine with it, then the two are totally interchangeable.


IRF540N Applications

  • Switching high power devices

  • Control speed of motors

  • LED dimmers or flashers

  • High-speed switching applications

  • Converters or inverter circuits

  • Microcontroller logic switching


IRF540N Package

IRF540N Package.png

IRF540N Package Outline

 

 IRF540N Mechanical Data.png

IRF540N Mechanical Data


IRF540N Manufacturer

Founded in 2003, VBsemi Co., Ltd. is a national high-tech enterprise specializing in the production of high-quality VBsemi MOSFET and other related products. We are a terminal manufacturer serving the mid to high-end market and are committed to providing your company with high-quality MOSFET to make your company a success in today's highly competitive market. VBsemi factory is headquartered in Taiwan China, We take VBsemi brand series products as the core, actively developing our product line, and strictly implements ISO9001 international quality standards.


Trend Analysis

Frequently Asked Questions

1.What is IRF540N?

The IRF540N is an advanced HEXFET N-channel power MOSFET. The device is extremely versatile with its current, voltage switching capabilities, and thus becomes ideal for numerous electronic applications.

2.How to use IRF540N?

Unlike transistors, MOSFETs are voltage-controlled devices. Meaning, they can be turned on or turned off by supplying the required Gate threshold voltage (VGS). IRF540N is an N-channel MOSFET, so the Drain and Source pins will be left open when there is no voltage applied to the gate pin.

3.Is IRF540N a logic level MOSFET?

The IRF540N is an N-Channel MOSFET. This MOSFET can drive loads up to 23A and can support peak current up to 110A. It also has a threshold voltage of 4V, which means it can easily be driven by low voltages like 5V. Hence it is mostly used with Arduino and other microcontrollers for logic switching.

4.Which region MOSFET works as an amplifier?

The saturation region. When used as a switching device, only triode and cut-off regions are used, whereas, when it is used as an amplifier, the MOSFET must operate in the saturation region, which corresponds to the active region in the BJT. The device operates in the cut-off region (off-state) when vGS < VTh, resulting in no induced channel.
IRF540N

VBsemi Elec

In Stock

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe