CR123A 3V Lithium Battery, CR123 VS CR123A, CR123A Equivalents
BATTERY LITHIUM 3V CR123A RETAIL
CR123A is a high-power lithium-based battery used extensively in security alarm systems. CR123A battery is a very popular cylindrical lithium battery, commonly used in various devices like photo cameras, flashlights, security devices, military equipment, etc. This article is going to introduce details about the CR123A battery. Welcome your RFQ!

CR123 Lithium Battery Information
What is CR123A?
The CR123A battery is a tiny high-voltage battery. The CR123A is often utilized for high-performance LED torches and digital cameras, as well as other small gadgets that require a lot of power. CR123A is approximately 33.4 mm long, 17 mm in diameter, and weighs around 17 grams. Most CR123A batteries have a continuous power of 2,000 mAh and a pulse current of around 3,000 mAh. The rating indicates that, like the CR123, they can power a 100 mA device for 30 hours.
CR123A Features and Benefits
Operating temperature range between -40° C to +-70° C
High current pulse discharge capability
Stable voltage level during discharge
High safety and reliability
Specifications
- TypeParameter
- Factory Lead Time12 Weeks
- Weight17g
- Voltage Rated
RATED voltage is the voltage on the nameplate - the "design point" for maximum power throughput and safe thermal operation.
3V - Usage LevelCommercial grade
- Series
In electronic components, the "Series" refers to a group of products that share similar characteristics, designs, or functionalities, often produced by the same manufacturer. These components within a series typically have common specifications but may vary in terms of voltage, power, or packaging to meet different application needs. The series name helps identify and differentiate between various product lines within a manufacturer's catalog.
CR123A - Published2002
- Size / Dimension
In electronic components, the parameter "Size / Dimension" refers to the physical dimensions of the component, such as its length, width, and height. These dimensions are crucial for determining how the component will fit into a circuit or system, as well as for ensuring compatibility with other components and the overall design requirements. The size of a component can also impact its performance characteristics, thermal properties, and overall functionality within a given application. Engineers and designers must carefully consider the size and dimensions of electronic components to ensure proper integration and functionality within their designs.
0.67Dia x 1.36 H 17.0mmx34.5mm - Part Status
Parts can have many statuses as they progress through the configuration, analysis, review, and approval stages.
Active - Moisture Sensitivity Level (MSL)
Moisture Sensitivity Level (MSL) is a standardized rating that indicates the susceptibility of electronic components, particularly semiconductors, to moisture-induced damage during storage and the soldering process, defining the allowable exposure time to ambient conditions before they require special handling or baking to prevent failures
Not Applicable - Voltage - Rated DC
Voltage - Rated DC is a parameter that specifies the maximum direct current (DC) voltage that an electronic component can safely handle without being damaged. This rating is crucial for ensuring the proper functioning and longevity of the component in a circuit. Exceeding the rated DC voltage can lead to overheating, breakdown, or even permanent damage to the component. It is important to carefully consider this parameter when designing or selecting components for a circuit to prevent any potential issues related to voltage overload.
3V - Termination Style
"Termination style" in electronic components refers to the method used to connect the component to a circuit board or other electronic devices. It determines how the component's leads or terminals are designed for soldering or mounting onto the circuit board. Common termination styles include through-hole, surface mount, and wire lead terminations.Through-hole components have leads that are inserted through holes in the circuit board and soldered on the other side. Surface mount components have flat terminals that are soldered directly onto the surface of the circuit board. Wire lead terminations involve attaching wires to the component for connection.The choice of termination style depends on factors such as the type of component, the manufacturing process, and the space available on the circuit board. Different termination styles offer various advantages in terms of ease of assembly, reliability, and space efficiency in electronic designs.
Button Top (Extending) - Battery Chemistry
A battery is a device that stores chemical energy, and converts it to electricity. This is known as electrochemistry and the system that underpins a battery is called an electrochemical cell. A battery can be made up of one or several (like in Volta's original pile) electrochemical cells.
Lithium Manganese Dioxide - Battery Cell Size
The most common lithium-ion cell is the 18650 (the numbers define the physical dimensions and shape as follows: 18mm in diameter, 65mm long and the 0 means it has a round cross-section) which is due to its widespread use in laptop battery packs.
CR123A - Capacity
In electronic components, "Capacity" typically refers to the maximum amount of electrical charge that a component can store. It is measured in units called farads (F). Capacitors are the most common components that have a capacity rating. The capacity of a capacitor determines how much energy it can store and release when connected in a circuit. Higher capacity capacitors can store more charge and are often used in applications requiring larger energy storage or filtering capabilities. It is important to select a capacitor with the appropriate capacity to ensure proper functioning of the circuit.
1.55Ah - Discharge Rate
The "Discharge Rate" in electronic components refers to the rate at which a component can release stored energy or power. This parameter is particularly important in devices that use batteries or capacitors, as it determines how quickly these components can discharge their stored energy. A high discharge rate means that the component can release energy quickly, while a low discharge rate indicates a slower release of energy. Understanding the discharge rate of electronic components is crucial for designing circuits and systems that require specific power delivery characteristics.
20mA - Diameter
In electronic components, the parameter "Diameter" typically refers to the measurement of the width of a circular component, such as a resistor, capacitor, or inductor. It is a crucial dimension that helps determine the physical size and fit of the component within a circuit or on a circuit board. The diameter is usually measured in millimeters (mm) or inches (in) and is important for ensuring proper placement and soldering of the component during assembly. Understanding the diameter of electronic components is essential for selecting the right size for a specific application and ensuring compatibility with other components and the overall design of the circuit.
17mm - Height19.05mm
- Length107.95mm
- Width88.9mm
- RoHS Status
RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.
Non-RoHS Compliant - Lead Free
Lead Free is a term used to describe electronic components that do not contain lead as part of their composition. Lead is a toxic material that can have harmful effects on human health and the environment, so the electronics industry has been moving towards lead-free components to reduce these risks. Lead-free components are typically made using alternative materials such as silver, copper, and tin. Manufacturers must comply with regulations such as the Restriction of Hazardous Substances (RoHS) directive to ensure that their products are lead-free and environmentally friendly.
Lead Free
CR123A Applications
The CR123A is often utilized for high-performance LED torches and digital cameras, as well as other small gadgets that require a lot of power.
CR123A Equivalents
123, 123A, 2/3A, 5018LC, BR2/3A, CR123, CR123A. CR17335 , CR17345 , CR23, DL123A, EL123A, K123LA, L123A, SF123A, VL123A
Differences between CR123 and CR123A
Comparison in Size:
Both the CR123 and the CR123A batteries are small and powerful. Because of their modest size in relation to the power they provide, they are both excellent choices for compact devices that consume a lot of power, such as high-output LED lights.
In general, 123s are longer and thinner than 123As. However, the difference in either direction is less than 0.55 mm. Each manufacturer's measurements are frequently somewhat different, making it difficult to distinguish between the two.
Comparison in Voltage :
The nominal voltage of both conventional 123s and 123As is 3 volts. Their standard loaded voltage is between 2 and 2.5 volts.
In basic terms, considering their compact size, both cells have a tremendous ability to push electric current through the device.
The voltage difference between the two battery types is usually insignificant.
Comparison in Life Span:
When stored at temperatures below 60°C, both batteries have a shelf life of up to 10 years before being used.
They are both long-lasting when used in your gadgets. The actual lifespan is determined by the device and its maker. In an alarm system, for example, they can last up to five years.
Comparison in Safety:
Lithium is a hazardous substance to come into touch with, especially if it comes into contact with the skin. Furthermore, excessive voltage may cause gadget damage.
PTC (Pressure, Temperature, Current) protection is built into both the 123s and 123As, and it disconnects the circuit if the current becomes too high.
Comparison in Chemistry:
With a Lithium and Manganese dioxide (LiMnO2) chemical system, both types of batteries use a lithium-based salt as an electrolyte. On both types of cells, the cathode (positive terminal) is made of heat-treated manganese dioxide.
The chemical system functions in the same way, resulting in a high energy density per mass (280 Wh/kg) and volume (580 Wh/litre).
In conclusion, the letter A is the only significant distinction between the two. When it comes to functionality, performance, longevity, and chemistry, the two are practically identical.
Both batteries can power high-performance equipment, such as digital cameras with flashes and high-tech LED torches, which require high-power discharges on occasion.
Parts with Similar Specs
- ImagePart NumberManufacturerRoHS StatusLead FreeShipping InfoPart StatusMax Operating TemperatureMoisture Sensitivity Level (MSL)CapacityBattery TypeView Compare
CR-123APA/1B
Not applicable
Lead Free
Due to restrictions, only ground shipment is allowed.
Active
-
Not Applicable
1.55Ah
-
Not applicable
Lead Free
Due to restrictions, only ground shipment is allowed.
Active
85 °C
Not Applicable
1.2Ah
PRIMARY
Not applicable
Lead Free
Due to restrictions, only ground shipment is allowed.
Active
85 °C
Not Applicable
1.2Ah
PRIMARY
Not applicable
Lead Free
Due to restrictions, only ground shipment is allowed.
Active
85 °C
1 (Unlimited)
1.2Ah
PRIMARY
CR123A Dimensions

CR123A Dimensions
CR123A Manufacturer
Panasonic Industrial Devices Sales Company of America is the industrial components and electronic devices division of Panasonic Corporation of North America. Panasonic Industrial Devices Sales Company of America provides key components that power the home appliances, consumer electronics, computers, communications, and commercial and healthcare products used by millions of people each day. Our wide offering of high-quality industrial products, global manufacturing, and advanced research and development facilities as well as our commitment to customer service make us a preferred vendor to the world's most famous original equipment manufacturers of high-tech electronic products.
Trend Analysis
Datasheet PDF
- MSDS Material Safety Datasheet :
- Datasheets :
Why is it called a CR123A?
Like many batteries, the name of a CR123A cell holds a lot of information about the chemistry and size. The CR indicates the chemistry of the battery, a prefix the IEC uses to denote the use of lithium chemistry, specifically LiMnO2. The 23A refers to the size of the battery, which in this case means the CR123A is 2/3, the length of a standard A-size battery.
Can I use 2 x CR123A batteries instead of an 18650 battery?
Some 18650 battery-powered flashlights and devices have long, spring-loaded interiors to account for varied battery length, allowing 2 x CR123A batteries to squeeze in. 18650s are slightly thicker than CR123As, so you may need a battery sleeve for a secure connection.
Are All CR 123A Batteries the Same?
In terms of their specs, all 123As have the same basic capabilities. However, each manufacturer may add different features and aesthetics to differentiate their products. For most tried and tested brands like Panasonic, Duracell, or Energizer, you shouldn’t be able to tell the difference. But if the battery is not made in the USA, it may differ from standard 123, so make sure to check manufacturer information.
Can I Use Rechargeable and Non-Rechargeable CR123A Batteries Interchangeably?
It won’t damage your device if you do; however, rechargeable and the non-rechargeable battery may have different voltages and capacities. Also, the dimensions may be slightly different. Some devices will only work properly with either one of the two, so check the specifications on your device first before switching out.
Can I use CR123 instead of CR123A?
There are no differences between CR123 and CR123a batteries. They have the same size, only their names are different because CR123A is the most common name.
LM3914V Driver:Alternatives, Pinout, Datasheet05 August 20213272
RF101 Diode: Datasheet, Features, Dimensions21 July 2021956
A Comprehensive Guide to LTC6952IUKG#TRPBF Clock Generator by Linear Technology/Analog Devices06 March 2024384
The LM2596S-5.0 Voltage Regulator: Pinout, Datasheet, Equivalent29 July 202124053
SG3525A PWM Controller: Pinout, Equivalent and Datasheet25 October 202115737
onsemi MMBFJ201 JFET setup, wiring, and tips for audio20 August 20251829
LM338 Regulator: Circuit, Price and Pinout31 August 20215684
MMBT2907A PNP Transistor: 60V 0.8A, SOT-23 MMBT2907A Bipolar Transistor and Datasheet pdf20 January 20222787
ADC Selection Guide: Architectures, Resolution, Sample Rate, and Digital Interfaces18 August 2026371
Smartphone RF Chips Availability Forecast 2026: Lead-Time Risks and Alternatives14 July 2026583
What is ToF Technology?22 January 20213768
SR44 vs LR44 Which Battery Should You Use21 August 20253242
The Complete Guide to DC-DC Converters24 May 20252951
What is a Ground Fault Circuit Interrupter?27 March 20255940
Nexperia Enters the Analog Chip Market23 March 20221177
Understanding the Basics of I2C Interface Controllers11 June 20251980
Panasonic - BSG
In Stock
United States
China
Canada
Japan
Russia
Germany
United Kingdom
Singapore
Italy
Hong Kong(China)
Taiwan(China)
France
Korea
Mexico
Netherlands
Malaysia
Austria
Spain
Switzerland
Poland
Thailand
Vietnam
India
United Arab Emirates
Afghanistan
Åland Islands
Albania
Algeria
American Samoa
Andorra
Angola
Anguilla
Antigua & Barbuda
Argentina
Armenia
Aruba
Australia
Azerbaijan
Bahamas
Bahrain
Bangladesh
Barbados
Belarus
Belgium
Belize
Benin
Bermuda
Bhutan
Bolivia
Bonaire, Sint Eustatius and Saba
Bosnia & Herzegovina
Botswana
Brazil
British Indian Ocean Territory
British Virgin Islands
Brunei
Bulgaria
Burkina Faso
Burundi
Cabo Verde
Cambodia
Cameroon
Cayman Islands
Central African Republic
Chad
Chile
Christmas Island
Cocos (Keeling) Islands
Colombia
Comoros
Congo
Congo (DRC)
Cook Islands
Costa Rica
Côte d’Ivoire
Croatia
Cuba
Curaçao
Cyprus
Czechia
Denmark
Djibouti
Dominica
Dominican Republic
Ecuador
Egypt
El Salvador
Equatorial Guinea
Eritrea
Estonia
Eswatini
Ethiopia
Falkland Islands
Faroe Islands
Fiji
Finland
French Guiana
French Polynesia
Gabon
Gambia
Georgia
Ghana
Gibraltar
Greece
Greenland
Grenada
Guadeloupe
Guam
Guatemala
Guernsey
Guinea
Guinea-Bissau
Guyana
Haiti
Honduras
Hungary
Iceland
Indonesia
Iran
Iraq
Ireland
Isle of Man
Israel
Jamaica
Jersey
Jordan
Kazakhstan
Kenya
Kiribati
Kosovo
Kuwait
Kyrgyzstan
Laos
Latvia
Lebanon
Lesotho
Liberia
Libya
Liechtenstein
Lithuania
Luxembourg
Macao(China)
Madagascar
Malawi
Maldives
Mali
Malta
Marshall Islands
Martinique
Mauritania
Mauritius
Mayotte
Micronesia
Moldova
Monaco
Mongolia
Montenegro
Montserrat
Morocco
Mozambique
Myanmar
Namibia
Nauru
Nepal
New Caledonia
New Zealand
Nicaragua
Niger
Nigeria
Niue
Norfolk Island
North Korea
North Macedonia
Northern Mariana Islands
Norway
Oman
Pakistan
Palau
Palestinian Authority
Panama
Papua New Guinea
Paraguay
Peru
Philippines
Pitcairn Islands
Portugal
Puerto Rico
Qatar
Réunion
Romania
Rwanda
Samoa
San Marino
São Tomé & Príncipe
Saudi Arabia
Senegal
Serbia
Seychelles
Sierra Leone
Sint Maarten
Slovakia
Slovenia
Solomon Islands
Somalia
South Africa
South Sudan
Sri Lanka
St Helena, Ascension, Tristan da Cunha
St. Barthélemy
St. Kitts & Nevis
St. Lucia
St. Martin
St. Pierre & Miquelon
St. Vincent & Grenadines
Sudan
Suriname
Svalbard & Jan Mayen
Sweden
Syria
Tajikistan
Tanzania
Timor-Leste
Togo
Tokelau
Tonga
Trinidad & Tobago
Tunisia
Turkey
Turkmenistan
Turks & Caicos Islands
Tuvalu
U.S. Outlying Islands
U.S. Virgin Islands
Uganda
Ukraine
Uruguay
Uzbekistan
Vanuatu
Vatican City
Venezuela
Wallis & Futuna
Yemen
Zambia
Zimbabwe


Product
Brand
Articles
Tools