LR44 VS SR44: Interchangeable?

Sophie

Published: 26 April 2022 | Last Updated: 26 April 2022

61445

LR44

LR44

Murata Electronics

ALKALINE MANGANESE BATTERIES

Purchase Guide

ALKALINE MANGANESE BATTERIES

LR44/LR1154 (alkaline) or SR44/SR1154 (silver-oxide) batteries are button/coin cell batteries 11.6 mm in diameter and 5.4 mm in height. Their capacity depends on the used chemistry, but also on the cut-off voltage of the used device. Their names are similar, and their appearances are alike. Are they interchangeable? What’s the difference between them? This passage will tell you these.

 This video will cover the difference between the SR44 vs LR44 and the issue with use in digital calipers.

Shop Talk - Digital Calipers and SR44 vs LR44 Batteries!

What is LR44?

The IR44 battery is an Alkaline Zinc Manganese button cell battery. The IR44 battery is typically a 1.5 Volt with an operating temperature ranging from 0°C to 60°C, while the optimal temperature is 20°C. The IR44 battery can be utilized in many devices such as watches, motherboards, and a variety of medical devices like thermometers.

LR44 dimension.jpg

LR44 Dimensions


What is SR44?

The SR44 battery is a silver oxide button cell featured in several well-known brand-name timepieces. The SR44 battery can also be used to power handheld calculators and other small devices. LR44, AG13, SG13, 357, and a few other cells are direct SR44 battery counterparts. This SR44 design is one of the largest the most common watch batteries, with a case that measures 11.6mm in diameter by 5.4mm in thickness. The output voltage is 1.55V, and the typical capacity ranges from 170 to 200mAh.

sr44 dimensions.jpg

SR44 Dimensions

LR44 VS SR44: Price

Alkaline LR batteries are less expensive than silver-oxide batteries. However, in terms of life expectancy, silver-oxide batteries outperform alkaline batteries.


LR44 VS SR44: Longevity

    Despite being expensive, silver oxide batteries are better than alkaline. Because Silver oxide batteries have longer shelf life compared to alkaline. For example, silver-oxide batteries provide services up to five years easily, whereas alkaline have two to five years of shelf life. 


LR44 VS SR44: Usage

When you are using batteries for toys and similar general use applications, LR44 is a better option. Yet, while using batteries for significant applications and devices, such as marine and similar applications, go for SR44 batteries.  


LR44 VS SR44: Voltage

Moreover, silver-oxide batteries have a slightly higher voltage than alkaline batteries. Besides, they have higher cut-off voltage. On the other hand, SR44 batteries have a more stable output voltage. And have a larger capacity in comparison to LR44 batteries. In this regard, you must choose SR44 batteries.  


LR44 VS SR44: Equivalents

LR44:

LR44 battery equivalents are also referred to as A76, AG13, L1154, LR1154, and 157. These sizes are possible LR44 battery replacements.

There are other batteries that are similar to the LR44 battery but are different in composition chemistry. The LR44 battery is identical in size, but different in chemistry to silver oxide button cells such as SR44, SR44SW, 303, 357.

Although batteries can fit into each other's devices fairly easily, it is important to choose the recommended battery type for your device to avoid over/under discharge. Please be sure to double-check the size and voltage of the battery you need, to avoid any issues that can damage your device.

 

SR44:

LR44, CR44, SR44, 357, SR44W, AG13, G13, A76, A-76, PX76, 675, 1166a, LR44H, V13GA, GP76A, L1154, RW82B, EPX76, SR44SW, 303, SR44, S303, S357, SP303, SR44SW


Which One is Better Between SR44 and LR44

It's difficult to choose between SR44 and LR44. However, in other circumstances, silver oxide outperforms alkaline. In this way, SR44 may be preferable. Furthermore, silver oxide has a capacity that is 50% to 100% greater than alkaline.

 

Furthermore, SR44 has a longer lifespan than LR44. Because of its higher capacity, the silver oxide battery's falling voltage is also very slow. LR batteries, on the other hand, are preferable for general applications because of their cheaper cost.


Silver Oxide Batteries vs Alkaline Batteries

For several of our battery sizes, we carry both Silver Oxide and Alkaline chemistry batteries. So what's the difference between the two (outside of price)? Well, Silver Oxide batteries often have a higher energy density and have the ability to put out a high current for their size. These batteries typically last longer than their alkaline counterparts. These should never be used on a battery charger.

 

As for alkaline batteries, they are often used for most kinds of batteries and watch batteries are no exception. They have a shorter shelf life compared to silver oxide batteries, but they still last pretty long regardless. They are cheaper to make (hence the smaller cost), the only problem with alkaline watch cells would be that they could potentially leak and could cause corrosion and damage to your watch (or other devices that use these batteries.


LR44 VS SR44: Interchangeability

LR44 and SR44 are the same physical size. However, the terminal voltage of the SR version is a tad higher (1.55v -v- 1.5v) and its capacity is also higher. There are plenty of devices around that are designed to work with the LR44 battery. Some may work with the SR44 but there is no way to know for sure and trying it is not a good idea.

The LR44 battery is identical in size, but different in chemistry to silver oxide button cells such as SR44, SR44SW, 303, 357. Although batteries can fit into each other's devices fairly easily, it is important to choose the recommended battery type for your device to avoid over/under discharge. Please be sure to double-check the size and voltage of the battery you need, to avoid any issues that can damage your device.


Frequently Asked Questions

What is an LR44 battery?

The LR44 battery is an alkaline button cell defined by its unique dimensions (11.6mm diameter x 5.4mm thickness). They typically feature up to 240mAh capacities, have a 1.5V voltage, and are primary (non-rechargeable) due to their alkaline chemistry. LR44 batteries are often used in small devices like watches, alarm clocks, motherboards, medical devices, and more.

Are LR44s the same as an SR44 or 357 battery?

While they are the same size, SR44 '357' batteries use a silver oxide chemistry to produce a more stable voltage (1.55V) and a lower self-discharge rate for an increased lifespan. This makes SR44 batteries more ideal for devices like watches and glucometers. However, LR44 cells are more widely available and usually cost less.

Are LR44s the same as a CR2032 battery?

No, CR2032 batteries use lithium chemistry and are wider and flatter (like a coin). You cannot replace CR2032s with an LR44 battery.

Which of the Two Is Better, SR44 or LR44?

LR44 is the cheaper of the two and enjoys a specialty with toys and general use applications. Conversely, SR44 batteries’ specialty is in marine functions in electronic devices. 
This is because LR44 batteries quickly drop below the 1.4V threshold, while the silver-oxide SR44 maintains at 1.55V virtually all the time. That said, it is easier to replace an LR44 with an SR44 than vice versa. Duracell Button alkaline batteries are the most common in the market. They exist in LR43, LR44, LR54, and 625A sizes, with a 5-year guarantee in storage.

What’s LR44 Advantage?

The LR44 alkaline battery is a powerful, long-lasting button cell. Apart from its compact shape, this alkaline battery has economic value and a nominal voltage of 1.5V. It works efficiently in both high and cold temperatures and is powered by the reaction between manganese dioxide and zinc, which in turn powers your devices. LR44 batteries are more affordable than silver oxide batteries, while still providing high capacity and long service life. Such cells are used in products like calculators, electronics toys, small radios, cameras, and portable electronics. 
LR44

Murata Electronics

In Stock

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe

Related Parts More