What are the Commonly Used Anti-Jamming Technologies for Sensors?
| Topics covered in this article: |
| Ⅰ. Shielding technology |
| Ⅱ. Grounding technology |
| Ⅲ. Isolation measures |
| Ⅳ. Filtering technology |
Ⅰ. Shielding technology
Including electrostatic shielding, electromagnetic shielding, low-frequency magnetic shielding, thermal shielding, etc.
1. Electrostatic shielding: Electrostatic shielding is to make a closed metal container with a material with good conductivity such as copper or aluminum, and connect it to the ground wire, and put the circuit that needs to be shielded in it so that the electric field of the external interference electric field is Affect the internal circuit, and conversely, the power line generated by the internal circuit cannot escape affecting the external circuit. Electrostatic shielding can not only prevent electrostatic interference but also prevent the interference of alternating electric fields. Therefore, the housings of many instruments are made of conductive materials and grounded. Although more and more instruments are made of engineering plastic (ABS), when you open the case, you will still see a layer of grounded metal film pasted on the inner wall of the case, which acts like a metal case. The electrostatic shielding effect.
2. Low-frequency magnetic shielding: Low-frequency magnetic shielding is an effective measure to isolate the coupling interference of low-frequency magnetic fields and fixed magnetic fields. There is a magnetic field around any wire or coil that passes current, and there is a magnetic field objectively, which may cause magnetic field coupling interference to the signal line of the detection instrument or the instrument. In order to prevent magnetic field coupling interference, high-permeability materials must be used as the shielding layer to allow low-frequency interference magnetic lines of force to pass through the magnetic shielding layer with small magnetic resistance so that the circuits inside the low-frequency magnetic shielding layer are protected from low-frequency magnetic field coupling interference. For example, the iron shell of the instrument acts as a low-frequency magnetic shield. If the shell is further grounded, it will also act as an electrostatic shield.
3. Electromagnetic shielding: Electromagnetic shielding also uses good conductive metal materials to make shields, shielding boxes and other different shapes, which enclose the protected circuit. The interference object it shields is not an electric field, but a high-frequency (above 40KHz) magnetic field. When the high-frequency magnetic field generated by the interference source encounters an electromagnetic shielding layer with good conductivity, it induces an eddy current of the same frequency on its outer surface, thereby consuming the energy of high-frequency interference. Secondly, the eddy current will also generate a new magnetic field. According to Lenz's law, its direction is exactly opposite to the direction of the interference source to offset a part of the energy of the interference magnetic field, so that the circuit inside the electromagnetic shielding layer is protected from high-frequency interference magnetic field. Impact.
Since the nature of radio broadcasting is electromagnetic waves, electromagnetic shielding can also absorb their energy. This is why we cannot receive radio in a car (steel body, but not grounded), and we must pull the radio antenna out of the car. reason.
If the electromagnetic shielding layer is grounded, it can also have an electrostatic shielding effect at the same time, and the shielding effect of electromagnetic waves will be better. The copper mesh shielded cable usually used as a transmission line can play the role of electromagnetic shielding and electrostatic shielding at the same time when it is grounded.
Ⅱ. Grounding technology
Grounding includes safety grounding, signal grounding, signal source grounding, load grounding, etc.
Grounding is a method to ensure the safety and anti-interference of people and equipment. Reasonable selection of grounding methods is an important measure to suppress capacitive coupling, inductive coupling, and resistance coupling, and to reduce or weaken interference.
The detection system is usually composed of a sensor (primary instrument) and a secondary instrument. In the actual industrial site, because the two are far apart and the signal transmission line is longer, the measured data will jump and cause the error to become larger. To solve this kind of problem, we must follow the one-point grounding principle. The so-called one-point grounding means that if multiple points of grounding are used in the circuit, the potential of each grounding point may be different, which may cause interference signals in the circuit. Therefore, one point of grounding should be achieved in the circuit as much as possible. If one point of grounding cannot be achieved, try your best to Widen the grounding wire so that the potentials of the grounding points are similar, so as not to form a source of signal interference.
Ⅲ. Isolation measures
Isolation includes transformer isolation, photoelectric coupler isolation, etc.
Isolation is a technical measure to destroy the interference path and cut off the coupling channel, so as to suppress the interference.
Transformer isolation is mainly used in transmission channels that transmit alternating signals.
Optocoupler isolation is widely used in digital interface circuits. At present, more and more photocouplers are used in automatic detection systems to improve the system's ability to resist common-mode interference. The photoelectric coupler is a kind of electric photoelectric coupling device, its input is an electric current, the output is also an electric current, but the input and output are electrically insulated. Ensure the electrical isolation of the input circuit and output circuit.
The main features of photocouplers are: high insulation resistance of input and output circuits (greater than 1010Ω), withstand voltage exceeding 1KV; because the transmission of light is one-way, the output signal will not feedback and affect the input end; the input and output circuits are in It is electrically isolated completely, which can solve the isolation and transmission contradiction between different potentials and different logic circuits.
Ⅳ. Filtering technology
Filtering technology is to uses a corresponding form of filter to filter out various interference signals so that the interference signals in the signal transmission process do not enter the detection system. It is one of the most effective measures to suppress interference. Filtering technology is a widely used measure especially for suppressing the interference coupled to the circuit via wires. Connect the filter of the corresponding frequency band to the signal transmission channel to filter or attenuate the interference signal as much as possible to achieve the purpose of improving the signal-to-noise ratio and suppressing interference.
Various filters are one of the effective measures to suppress differential mode interference. The filters commonly used in automatic detection systems are:
1. RC filter. When the signal source is a sensor with slow signal changes such as thermocouples and strain gauges, the use of a small, low-cost passive RC low-pass filter will have a better suppression effect on serial mode interference.
2. AC power filter. The power network absorbs various high and low-frequency noises. For this, LC filters are often used to suppress the noise mixed into the power supply. After inserting the AC power filter between the power supply and the load, the electromagnetic interference in the range of several kilohertz to tens of megahertz can be attenuated by more than tens of times. It is best to connect AC power filters in series with the power supplies of computers, sensors, secondary meters, and other electrical equipment that work in interference environments. The main considerations when choosing an AC power filter are: first, the rated current of the filter must be greater than the working current of the electrical equipment; second, in the foreseeable frequency range, the attenuation coefficient for interference must meet the requirements. When in use, you can choose a power filter that contains one-stage LC or two-stage or even three-stage LC inside according to your needs. It must be well-grounded when in use.
3. DC power supply filter. DC power supply is often shared by several circuits. In order to avoid mutual interference between several circuits caused by the internal resistance of the power supply, RC or LC decoupling filtering should be added to the DC power supply of each circuit. Device. Corresponding measures can also be adopted for other interferences such as thermal interference, temperature interference, and light interference. Thermal interference can be solved by thermal shielding; for temperature interference, temperature compensation can be used to adapt to temperature changes at the worksite. . In addition, in the design process, when selecting electrical components and sensors, devices with stable performance parameters, high reliability, and adaptable to specific working site conditions must be selected to ensure the reliability and safety of the system after it is composed.
1. What anti-interference measures are usually used in sensor signal transmission?
Sensor signal interference sources mainly include electrostatic interference, high-frequency interference and electromagnetic interference. On-site interference may be one of them, or multiple interferences may coexist, which need to be eliminated one by one according to the actual situation. Electrostatic interference can be eliminated or reduced by proper grounding; high-frequency interference should be removed in time, and if it cannot be removed, effective hardware measures (such as signal isolation) or software measures (such as filtering technology) should be taken to reduce the impact of interference; There are many electromagnetic interference protection measures, and measures such as grounding, signal isolation or filtering can all reduce the harm of electromagnetic interference.
2. Why take anti-interference measures to the sensor measurement circuit?
There are many types of sensors (force sensors, temperature sensors, etc.). Generally speaking, the sensor converts a certain physical quantity into an electrical signal at the first time, so that the control purpose can be achieved through the control circuit. If the electrical signal provided by the sensor is unstable or inaccurate, then the control circuit will not be able to achieve correct control and may even cause disasters. Therefore, the sensor must do its best to shield irrelevant interference information, such as the use of anti-interference circuits and the use of metal shells ( Grounding) to cover the sensor, etc.
3. Why capacitive sensors are susceptible to interference?
Sensors based on the electrical signal principle are susceptible to electromagnetic interference. Capacitance is related to voltage. Voltage is related to charge. The charge will be affected by the magnetic field and electric field.
The Key Role of Electronic Components in IoT DevicesUTMEL01 September 20236233The article discusses the pivotal role of electronic components in Internet of Things (IoT) devices. IoT devices work by capturing real-world data using sensors, processing it through a microcontroller, and then sending it to the cloud for further analysis.
Read More
Accelerometer Sensors Guide: Working Principle, Circuit Design, Specifications, and ApplicationsUTMEL25 June 20261028A practical accelerometer sensor guide covering working principles, MEMS and piezoelectric types, datasheet specifications, circuit design, mounting, applications, and selection.
Read More
2026 ADAS Sensors: Supply Outlook and Alternative SourcingUTMEL18 July 20261165Automotive cleanroom assembly integrating advanced driver assistance systems. The automotive industry faces a structural semiconductor deficit in 2026, driven not by pandemic-era demand shocks but by AI data centers absorbing global foundry capacity on legacy nodes (40nm-90nm) where 95% of automotive-grade components are manufactured. Video demonstrations of these systems show a "machine view" overlay with red crosshairs tracking pedestrian movement and sudden cut-ins before traditional collision thresholds are triggered.
Read More
Magnetic Sensors for Position Detection: Hall Effect vs. AMR vs. TMR Engineering GuideUTMEL21 August 2026575This guide compares Hall effect, AMR, and TMR magnetic sensors for position detection in motor control and robotics. It explains their physical principles, key performance metrics, and selection criteria. Hall effect suits low-cost commutation, AMR offers high-speed angle sensing, and TMR provides maximum precision and low power, with practical integration advice.
Read More
Temperature Sensor Types Comparison: Thermocouple, RTD, and Semiconductor IC Selection GuideUTMEL17 August 2026493This comprehensive selection guide compares thermocouples, platinum RTDs, and semiconductor ICs across measurement range, accuracy limits, and signal conditioning complexity. It covers fundamental operating physics, mathematical transfer functions, lead-wire compensation topologies, and power budgets. Engineers will find practical design checklists, benchtop multimeter diagnostic techniques, and an architectural decision workflow to optimize system performance and bill-of-materials cost.
Read More
Subscribe to Utmel !


Product
Brand
Articles
Tools