Photocoupler Basis: Description, Applications and Working Principle

How Optocouplers work - opto-isolator solid state relays phototransistor
| Topics covered in this article: |
| Ⅰ. What is Photocoupler? |
| Ⅱ. The classification of Photocoupler |
| Ⅲ.What’s the advantage of Photocoupler? |
| Ⅳ.What’s the working principle of Photocoupler? |
Ⅰ. What is Photocoupler?

PC817 Photocoupler
Photocoupler is also known as optocoupler. To communicate electrical impulses, optocouplers employ light as a channel. It is frequently utilized in many circuits because it provides an excellent isolation effect on input and output electrical signals. It has evolved into one of the most diversified and adaptable optoelectronic devices available today. Light emission, light reception, and signal amplification are the three main components of an optical coupler. The input electrical signal causes the light-emitting diode (LED) to emit light of a specific wavelength, which is detected by the photodetector and converted into a photocurrent, which is then output after amplification. This completes the electrical-optical-electrical conversion, acting as input, output, and isolation at the same time. The optocoupler offers good electrical insulation and anti-interference characteristics since its input and output are isolated from each other and the electrical signal transmission is unidirectional.
Ⅱ. The classification of Photocoupler
Because there are so many different types and varieties of photoelectric couplers, the optoelectronics DATA handbook has over a thousand models, which can usually be categorized using the following methods:
(1) It can be classified as an external optical path photoelectric coupler (also known as a photoelectric interruption detector) or an interior optical path photoelectric coupler, depending on the optical path. The transmission type and reflection type photoelectric couplers are the two types of external optical path photoelectric couplers.
(2) It may be classified into two types based on the output form:
a. Photosensitive device output type, which includes photodiode output type, phototransistor output type, photocell output type, and light thyristor output type, among others.
b. Type of NPN triode output, such as AC input, DC input, complementary output, and so on.
c. Darlington transistor output type, which includes both AC and DC inputs.
d. The type of logic gate circuit output, such as gate circuit output, Schmitt trigger output, tri-state gate circuit output, and so on.
e. Output type with low conduction (output low-level millivolts).
f. Type of optical switch output (on resistance less than ten).
g. Type of power output (IGBT/MOSFET, etc.)
(3) Coaxial type, dual in-line type, TO package type, flat package type, chip package type, and optical fiber transmission type are the different package types.
(4) Digital photocouplers (OC gate output type, totem pole output type, tri-state gate circuit output type, etc.) and linear photocouplers can be classified based on the transmission signal (can be divided into low drift type, high linearity Type, broadband type, single power supply type, dual power supply type, etc.).
(5) Photoelectric couplers can be classified as low-speed (phototransistor, photocell, etc. output type) or high-speed (phototransistor, photocell, etc. output type) (photodiode with signal processing circuit or photosensitive integrated circuit output type).
(6) It can be classified as a single channel, dual channel, or multi-channel photocoupler based on the channel.
(7) It may be separated into regular isolation optocouplers (usually, optical glue potting is less than 5000V, and the empty seal is less than 2000V) and high-voltage isolation optocouplers based on isolation properties (can be divided into 10kV, 20kV, 30kV, etc.).
(8) It can be classified as a low power supply voltage type photoelectric coupler (usually 515V) or a high power supply voltage type photoelectric coupler based on the working voltage (generally greater than 30V).
Ⅲ.What’s the advantage of Photocoupler?
(1) It effectively suppresses ground loop noise, eliminates ground interference, and electrically isolates the signal field from the main control terminal, preventing unintentional main control system damage.
(2) It has the ability to transport electrical signals between different potentials and impedances, as well as functionalities like as signal amplification and shaping, substantially simplifying the real circuit construction.
(3) The switching speed is quick, and the high-speed photoelectric coupler's response time is on the order of ns, substantially expanding the photoelectric coupler's applicability in digital signal processing.
(4) Compact size; most devices use dual-in-line packaging, which comes in single-channel, dual-channel, and up to eight-channel configurations and are very easy to operate.
(5) It can be used in place of transformer isolation, produces no peak noise owing to contact bounce, and is anti-vibration and impact resistant.
(6) In addition to power monitoring, high-linearity photocouplers are utilized in medical devices that can efficiently protect patients' lives.
Ⅳ.What’s the working principle of Photocoupler?

Working Principle of Photocoupler
The photocoupler's principle is to supply an electrical signal to the photocoupler's input to cause the light-emitting source to emit light. The magnitude of the excitation current determines the light intensity. The photoelectric effect generates a photocurrent once this light is irradiated on the packed light receiver. Is led out of the light receiver's output end, completing the electric-optical-electric conversion. The optocoupler's idea is that an electrical signal drives a light-emitting diode (LED) to emit a specific wavelength of light, which is detected by a photodetector, which generates a photocurrent, which is then amplified and output. This completes the electrical-optical-electrical conversion, acting as input, output, and isolation at the same time. The optocoupler offers good electrical insulation and anti-interference characteristics since its input and output are isolated from each other and the electrical signal transmission is unidirectional. Furthermore, because the optocoupler's input end is a low-resistance element that operates in current mode, it has a high common-mode rejection capability. As a result, as a terminal isolation element in long-line information transmission, it can considerably increase the signal-to-noise ratio. It may considerably improve the dependability of computer operations as a signal isolation interface device in computer digital communication and real-time control.
Ⅴ.Where can Photocoupler be used?
Optocouplers have a wide range of applications due to their distinctive architectures, unique advantages, and wide range of uses, primarily in the following situations:
(1) Logic circuit application
Optocouplers can be used to create a variety of logic circuits. Because optocouplers have stronger anti-interference and isolation properties than transistors, the logic circuits they generate are more trustworthy.
(2) For use as a solid switch
In the switch circuit, good electrical isolation between the control circuit and the switch is frequently required, which is difficult to achieve with standard electronic switches but relatively simple with a photocoupler.
(3) Use in the trigger circuit
Because the light-emitting diodes can be linked in series to the two emitter loops, the photoelectric coupler is employed in the bistable output circuit to effectively handle the problem of output and load isolation.
(4) Pulse amplifier circuit application
In digital circuits, photocouplers are used to amplify pulse signals.
(5) Linear circuit application
Linear photocouplers are employed in linear circuits because of their strong linearity and electrical isolation.
(6) Use in specific circumstances
Photocouplers can also be utilized for high-voltage control, transformer replacement, contact relay replacement, A/D circuits, and other applications.
1.What is the difference between optocoupler and opto-isolator?
The place of use is different. The photoelectric coupler converts the optical signal into the electrical signal and transmits it. Although the photoelectric isolator also has similar functions, its more important function is to play a protective role, such as the one on your device. The interface itself does not have photoelectric protection, so it needs an optoelectronic isolator. Once a surge occurs, the isolator will be burned directly without harming your equipment.
2.How to determine the input end of the photocoupler?
The closest to the coupling port is the input.
3.What is the selection principle of optocoupler?
The photocoupler in the common ATX power supply (hereinafter referred to as "optocoupler") is usually 4 pins and is a dual in-line type. How to measure whether it is good or bad is as follows: 1. If the naked eye can see the light If the coupling has burst, cracked, or has burnt marks, it must be unusable and damaged. 2. For the 2 columns of pins of the optocoupler, find a pointer meter (take MF47 type) as an example, use a multimeter to set the ohms position X1K position, short the test leads, adjust the zero, and measure the positive of each column of the optocoupler. Reverse resistance, the normal optocoupler is only open in one direction (the resistance is generally about 30 to 100 kohms (you can find a normal comparison), this column is the resistance of the forward diode of the optocoupler, remember this column first What is the test lead connected to the forward resistance of the 2 pins in order to determine the preparation for the next step; if the 2 columns of pins fail to find that the one-way resistance is on, the optocoupler must be broken. 3. Prepare another pointer meter. , Also set the gear to X1K, first measure the second point above, and then use the prepared pointer meter to measure another column. A good optocoupler is connected in the forward and reverse directions, and the resistance is relatively small. Thousands of ohms; a bad optocoupler fails or has a large resistance.
Optical Transceiver Guide: How It Works, Types, Form Factors, and SelectionUTMEL24 June 2026695An optical transceiver is the replaceable interface between electronic network equipment and an optical fiber link. It converts electrical data from a switch, router, server, storage system, or transport platform into modulated light, then converts received light back into electrical data.
Read More
Transceivers Shortage Outlook 2026: Supply, Lead Times, and Sourcing OptionsUTMEL09 July 20262370The 2026 transceiver market is defined not by a broad, systemic silicon crisis, but by a highly targeted, structural constraint driven by AI data center build-outs. Figure 3: Power connectors on server racks designed for intense workloads.
Read More
The Introduction to Common Tools and Using Methods of Fiber OpticUTMEL07 January 20227506The building and maintenance of optical cables in the intelligent industry has gradually expanded with the rapid expansion of the Internet of Things and 5G technologies, resulting in an increase in demand for various optical fiber tools. Cutting shears, for example, come in a variety of shapes and sizes, and each tool serves a different purpose. Do you have any experience with them? When should you utilize certain fiber optic tools?
Read More
What are Fiber Optic Patch Cables?UTMEL11 February 20228498Hello everyone, I am Rose. Today I will introduce fiber optic patch cables to you. Optical fiber communication, as an emerging technology, has become one of the main pillars of modern communication and plays a critical role in modern telecommunication networks, thanks to the rapid growth of traffic data.
Read More
Basis of Fiber Optic and Fiber Optic CommunicationUTMEL22 October 20215475Hello everyone, I am Rose. Today I will introduce fiber optic to you. Fiber Optic is a type of glass or plastic fiber that can be utilized to transmit light. It is mostly used for communication. This article will show you the basic knowledge of fiber optic and fiber optic communication.
Read More
Subscribe to Utmel !
SME2470-021Honeywell Sensing and Productivity Solutions
HFBR-2521Broadcom Limited
APL3015SGC-F01Kingbright
12-21C/BHC-ANQ/2CEverlight Electronics Co Ltd
IR25-21C/TR8Everlight Electronics Co Ltd
HLMP-6400-F0021Broadcom Limited
HSMM-A430-X90M2Broadcom Limited
PLR135/T10Everlight Electronics Co Ltd
SFH 4053OSRAM Opto Semiconductors Inc.
19-213/R6C-AP1Q2B/3TEverlight Electronics Co Ltd


Product
Brand
Articles
Tools