What is a Transmitter?

Transmitter Explained | Types of Transmitters
Topics covered in this post: |
What is a transmitter?
The transmitter and sensor together constitute a monitoring signal source for automatic control. The transmitter is to convert the output signal of the sensor into a signal that can be recognized by the controller, or convert the non-electricity input from the sensor into an electrical signal and amplify it at the same time, and uniformly convert it into a standard signal source (such as 4-20mA DC power supply). It can be used for remote measurement and control. Therefore, the transmitter is not only a conversion medium but also a medium.
The process in automatic control is: signal source --> sensor --> transmitter --> arithmetic controller --> actuator --> control output.
In the industrial field, sometimes the transmitter and the sensor are common because the output signal of most modern sensors is already a signal that the general controller can receive, and this signal can be directly recognized by the controller without the conversion of the transmitter.
Similar to sensors, transmitters are generally divided into temperature/humidity transmitters, pressure transmitters, differential pressure transmitters, liquid level transmitters, current transmitters, power transmitters, and flow transmitters, Weight transmitters, etc.

transmitters
Principle of Transmitter
The transmitter works based on the principle of negative feedback, and it is mainly composed of a measuring part, an amplifier, and a feedback part.
The measurement part is used to detect the measured variable x and convert it into an input signal Zi (signal such as voltage, current, displacement, force, or torque) that can be accepted by the amplifier. The feedback part converts the output signal y of the transmitter into a feedback signal Zf, and then sends it back to the input terminal. The algebraic sum of Zi and the zeroing signal Zo is compared with the feedback signal Zf. And the difference ε is sent to the amplifier for amplification and converted into the standard output signal y.
Transformation- refers to the process of transforming various physical quantities from sensors into electrical signals. For example: using thermocouples to convert temperature into electric potential; using current transformers to convert large currents into small currents. Since electrical signals are the easiest to process, modern transmitters convert various physical signals into electrical signals.
Transmission- refers to the transformation of various electrical signals. In order to facilitate the reception and transmission of other instruments or control devices, once again through electronic circuits to unify the electrical signals from the sensors (such as 4-20MA). The method is achieved through multiple operational amplifiers.
For example, SST3-AD is a current transformer that converts the output current of a current transformer into a standard 4-20MA current transmitter; another example: SST4-LD, which can convert the weight signal from a weight sensor into a standard 4 -20MA weight transmitter.
Classification of Transmitter
1. According to the output signal type, the transmitter can be divided into two types: current output type and voltage output type.
(1) The voltage output transmitter has the nature of a constant voltage source. The impedance of the voltage input terminal of the PLC analog input module is very high. If the transmission distance is long, the small interference signal current will produce a higher interference voltage on the input impedance of the module. So the anti-interference ability of the remotely transmitted analog voltage signal is poor. But it is suitable for sending the same signal to multiple instruments in parallel, and the installation is simple. Disassembly and assembly of one of the instruments will not affect the work of other instruments, and the withstand voltage requirements of the output stage is reduced, thereby improving the reliability of the instrument. The voltage signal ranges from 1 to 5 V, 0 to 10 V, and -10 to 10 V, and firstly, it is 1 to 5 V and 0 to 10 V.

Differential pressure level transmitter
(2) The current output transmitter has the properties of a constant current source, and the internal resistance of the constant current source is very large. When the input of the PLC analog input module is current, the input impedance is low. The interference voltage generated by the interference signal on the line is very low on the module, so the analog current signal is suitable for remote transmission and can be reached hundreds of meters when using shielded cable signal lines. The standard of the current signal is 0~10 mA, 0~20 mA, 4~20 mA, and the first choice is 4~20 mA. 0 mA is usually used as a circuit failure or power failure indication signal.
Current signal transmission and voltage signal transmission have their own characteristics. The current signal is suitable for long-distance transmission, and the voltage signal enables the meter to be connected in a "parallel system". Therefore, in the control meter system, the transmission signal in and out of the control room adopts the current signal, and the communication between the instruments in the control room adopts the voltage signal, that is, the connection method is the method of current transmission and parallel reception of the voltage signal.
The transmitter is divided into a two-wire system and a four-wire system. The four-wire transmitter has two power lines and two signal lines, and there is no strict requirement on the power consumption of the fractional component of the current signal. Two-wire transmitters have only two external wirings. They are both power lines and signal lines. The lower limit of the current signal cannot be zero. However, the two-wire transmitters have fewer wirings and long transmission distances, which are the most widely used in industry.
2. Depending on the energy used, the transmitter is divided into two types: pneumatic transmitter and electric transmitter.
(1) Pneumatic transmitter
The pneumatic transmitter uses dry and clean compressed air as an energy source. It can transform various measured parameters (such as temperature, pressure, flow rate, and liquid level) into a pressure signal of 0.02~0.1IMPa for transmission to the regulator, display, and other units combined instruments for indication, recording or adjustment. The structure of the pneumatic transmitter is relatively simple. The anti-interference ability against the electromagnetic field, radiation, temperature, humidity, and other environmental influences is strong. It can be fireproof and explosion-proof, and the price is relatively cheap. The disadvantage is that the response speed is slow and the transmission distance is relatively low. Due to restrictions, it is difficult to connect to a computer.
(2) Electric transmitter
The electric transmitter uses electricity as an energy source, and the connection between signals is convenient, suitable for long-distance transmission, and easy to connect with electronic computers. In recent years, it can also be explosion-proof to facilitate safe use. The disadvantage is that the investment is generally high, and it is greatly affected by the interference of temperature, humidity, electromagnetic field, and radiation: the electric transmitter can transform various measured parameters into 0~10V or 4~20mA (uniform standard signal of direct current) to transmit to other units in the automatic control system.
Transmitter protection functions
1. Input overload protection;
2. Output overcurrent limit protection;
3. Long-term short circuit protection of output current;
4. Two-wire port transient induced lightning and surge current TVS suppression protection;
5. Overvoltage limit protection of working power supply≤35V;
6. Reverse connection protection of working power supply.
Common malfunctions
1. When installing, make the pressure-sensitive part of the transmitter perpendicular to the direction of gravity.
If the installation conditions are limited, the zero position of the transmitter should be adjusted to the standard value after installation and fixation.
2. The remaining pressure cannot be released, so the zero position of the sensor cannot be lowered. The best way to eliminate this is to remove the sensor and directly check whether the zero position is normal. If it is normal, replace the sealing ring and try again.
3. The output of the pressure transmitter does not change, and the output of the pressure transmitter changes suddenly, and the zero position of the pressure relief transmitter cannot be returned. The reason for this phenomenon is most likely caused by the pressure sensor sealing ring.
4. Whether it meets the power supply requirements; whether there are wiring errors between the power supply and the transmitter and load equipment. If there is no voltage on the transmitter terminal or the polarity is reversed, it can cause the transmitter to have no voltage signal output.
5. The shells of pressure sensors and transmitters generally need to be grounded, signal cables must not be mixed with power cables, and strong electromagnetic interference should be avoided around the sensors and transmitters. Sensors and transmitters should be periodically verified in accordance with industry regulations.
6. When selecting pressure sensors and transmitters, users should fully understand the working conditions of the pressure measurement system and make reasonable selections according to their needs to make the system work in the best state and reduce the project cost.
7. The filling liquid in the spacer and the element are transferred to both sides of the measuring diaphragm. The electrodes on the measuring diaphragm and the insulating plates on both sides each form a capacitor.
8. The pressure transmitter is required to be inspected once a week and once a month. The main purpose is to remove the dust in the instrument. Check the electrical components carefully, and check the output current value frequently. The pressure transmitter has a weak current inside. It must be separated from the external strong electricity.
1.What is the function of the transmitter?
As its name implies, the general purpose of a transmitter is to transmit signals. These signals contain information, which can be audio, video, or data. In essence, a transmitter launches signals into the air via a transmitting antenna.
2.What is a transmitter in data communication?
Transmitter: A device that encodes the data to be transmitted in such a way as to create electromagnetic signals that can be transmitted across some kind of transmission system.
The Key Role of Electronic Components in IoT DevicesUTMEL01 September 20236478The article discusses the pivotal role of electronic components in Internet of Things (IoT) devices. IoT devices work by capturing real-world data using sensors, processing it through a microcontroller, and then sending it to the cloud for further analysis.
Read More
Accelerometer Sensors Guide: Working Principle, Circuit Design, Specifications, and ApplicationsUTMEL25 June 20261449A practical accelerometer sensor guide covering working principles, MEMS and piezoelectric types, datasheet specifications, circuit design, mounting, applications, and selection.
Read More
2026 ADAS Sensors: Supply Outlook and Alternative SourcingUTMEL18 July 20261560Automotive cleanroom assembly integrating advanced driver assistance systems. The automotive industry faces a structural semiconductor deficit in 2026, driven not by pandemic-era demand shocks but by AI data centers absorbing global foundry capacity on legacy nodes (40nm-90nm) where 95% of automotive-grade components are manufactured. Video demonstrations of these systems show a "machine view" overlay with red crosshairs tracking pedestrian movement and sudden cut-ins before traditional collision thresholds are triggered.
Read More
Magnetic Sensors for Position Detection: Hall Effect vs. AMR vs. TMR Engineering GuideUTMEL21 August 2026911This guide compares Hall effect, AMR, and TMR magnetic sensors for position detection in motor control and robotics. It explains their physical principles, key performance metrics, and selection criteria. Hall effect suits low-cost commutation, AMR offers high-speed angle sensing, and TMR provides maximum precision and low power, with practical integration advice.
Read More
Temperature Sensor Types Comparison: Thermocouple, RTD, and Semiconductor IC Selection GuideUTMEL17 August 2026767This comprehensive selection guide compares thermocouples, platinum RTDs, and semiconductor ICs across measurement range, accuracy limits, and signal conditioning complexity. It covers fundamental operating physics, mathematical transfer functions, lead-wire compensation topologies, and power budgets. Engineers will find practical design checklists, benchtop multimeter diagnostic techniques, and an architectural decision workflow to optimize system performance and bill-of-materials cost.
Read More
Subscribe to Utmel !


Product
Brand
Articles
Tools