What’s the relationship between CR1616 and CR1632?

Sophie

Published: 31 May 2022 | Last Updated: 31 May 2022

29889

CR1616

CR1616

Murata Electronics

CR STANDARD

Purchase Guide

CR STANDARD

Just like other batteries in the CR series, CR1616 and CR1632 are button batteries that seem very similar in many respects. By comparing the CR1616 and CR1632, we’ll see if the two are interchangeable, and what their differences are. Here we will compare the main specs, voltage, thickness, applications, and other features of CR1616 and CR1632 batteries.

This video is about how to replace the 3V  lithium (CR1616) battery in the car remote.

Honda Key Remote 3V Battery (CR1616) Replacement

CR1616 Description

Lithium CR1616 is a button /coin cell battery, featuring a 16 mm (0.63 inches) diameter and 1.6 mm height  (0.06 inches) - hence the '1616' as a common part of most labels. Common CR1616 battery weighs in the 1.1 and 1.3 grams range. The CR1616 batteries can be used for laser pointers, insulin pumps, heart rate monitors, toys, watches, cameras, calculators, car security alarms, keyless car remotes, organizers, and computer equipment. They also work in extreme temperatures and hold power for up to eight years in storage.

The following is the 2D-Model of CR1616.

cr1616 2D-model.jpg

CR1632 Description

The CR1632 battery provides a consistent voltage supply while remaining lightweight enough for travel and storage. These batteries were designed with performance in mind, providing you with the long-lasting power you need to keep all of your gadgets running. These batteries can be found in a variety of gadgets, including calculators, cameras, heart rate monitors, and even toys, and can operate in a wide range of temperatures. The CR1632 battery has a long shelf life and a large storage capacity, making it a reliable power source for your tiny electrical gadgets.

The following is the 2D-Model of CR1632.

cr1632.jpg

CR1616 VS CR1632: Features

CR1616 Features

  • The high energy density  (3V) with a flat and low self-discharge.

  • Design, safety, manufacturing, and qualification follow Procell’s stringent battery standards, which incorporate parts of the ANSI and IEC battery standards.

  • Economically packaged.

  • Child secure packaging: tamper-proof pack with a double blister so that it is impossible for a child  to open without scissors 

  • Operating temperatures  from -20℃~+70℃

  • Good pulse capability

  • High discharge  characteristics

  • Stable voltage level  during discharge 

  • Long-term reliability 


CR1632 Features

  • Non-Rechargeable Lithium coin cell Battery

  • Nominal Voltage: 3V

  • Battery Capacity: 130mAh

  • Continuous drain current: 0.19mA

  • Peak drain current: 6.8mA

  • Weight: 1.8 grams


CR1616 VS CR1632: Specification Comparision


CR1616CR1632
Nominal Capacity50mAh140 mAh
Nominal Voltage3V3V
Weight1.2g1.8g
Operating Temperature-20℃~+70℃-30°C ~ +60°C
Diameter16mm16mm
Height1.6mm3.2mm
storage humidity range40%~75% not more than 60%
storage temperature range0℃~30℃-30°C ~ 60°C


CR1616 VS CR1632: Nominal Voltage

According to the specifications, the two batteries have the same nominal voltage, which is 3V

CR1616 VS CR1632: Height

A CR1616 battery is 1.6mm high, whereas a CR1632 battery is 3.2mm high. Remember, in respect of various works, the height of a battery also matters. It’s a crucial part of cell composition.

CR1616 VS CR1632: Applications

You may have heard of the use of CR1616 in Honda and Lexus key fobs. Aside from these, it can also be used in other car brands. The CR1616 is a reliable battery that can be used in a variety of electrical gadgets. These are as follows: 

  • Glucometers

  • Heart rate monitors

  • Toys

  • Computer backup equipment


On the contrary, CR1632 batteries are ideal for different helpful stuff. 

  • Small PDA devices

  • Wireless doorbell for house

  • Electronic Toys

  • Portable electronics

  • Digital thermometers

  • Digital altimeter

  • Cyclocomputers

  • Heart rate monitors


CR1616 VS CR1632: Durability

You won’t see any expiration date of a 1616 battery. However, it has an average lifespan. Generally, this type of battery lasts for approximately 5-10 years.  

On the contrary, a battery CR1632 usually lasts for around 7 to 10 years.


CR1616 VS CR1632: Compatibility

A single battery has several variations, each with its own label. Anyway, here are some popular CR1616 comparable battery labels:

  • DL1616

  • BR1616

  • ECR1616

  • 280-209

  • GPCR1616

  • LiR1616

  • KCR1616

  • 5021LC  


Now let us see the common labels for CR1632 equivalent batteries! Here they are:

DL1632, ECR1632


CR1616 VS CR1632: Interchangeability

Same diameters

CR1616: 16mm 

CR1632: 16mm


Different thickness

CR1616: 1.6mm

CR1632:  3.2mm


Obviously, they are not the same size. CR1616 is 1.6mm in thickness while CR1632 is 3.2mm in thickness. And the thickness of TWO pieces of CR1616 equals ONE CR1632. Can I use 2 pieces of CR1616 to replace ONE CR1632? No. The two batteries are added together to form a series. Consequently, the current-voltage is 3+3=6V. 6V is bigger than 3V. If forcibly used, electronic products will be destroyed.


CR1616 VS CR1632: Datasheet

Product Manufacturer

Murata is a global leader in the design, manufacture, and supply of advanced electronic materials, leading-edge electronic components, and multi-functional, high-density modules. Murata innovations can be found in a wide range of applications from mobile phones to home appliances, and automotive applications to energy management systems and healthcare devices.





Recommended articles:

CR1616 Lithium Battery-Dimensions, Equivalence, Datasheet

CR1616 vs CR2025[Video+FAQ]: Differences and Similarities

Can a 1616 battery be replaced by 1620?


Frequently Asked Questions

Are CR1616 and CR1632 rechargeable?

Both the CR1616 and CR1632 batteries are non-rechargeable. That implies you'll have to acquire fresh batteries for your devices.

Are CR1620 and CR1632 interchangeable?

Depending on what you're using the battery for, there's no harm in replacing a CR1632 with a CR1620; you'll just get less utilization out of the CR1620 than the CR1632. It is permissible to use it to replace the battery in a car key remote.

Can I Use CR2016 Instead of CR1632?

No, it probably won't physically fit in the battery socket. This is because a CR2016 is wider than a CR1620. (The CR2016 is also thinner too.)

What Are 1632 Batteries Used For?

The CR1632 batteries are often used in car key remotes, watches, toys and other electronic appliances. The Panasonic Lithium coin batteries provide long-lasting reliable power.

Are CR2016 and CR2032 Interchangeable?

Electrically speaking they have the same voltage so they will drive a circuit the same. However, they are different physical sizes so they are not physically interchangeable.
CR1616

Murata Electronics

In Stock