TMC2100 Stepper Motor Driver[Video]: TMC2100 VS TMC2130 VS TMC2208, Pinout, and Datasheet
SILENTSTEPSTICK TMC2100 STEPPER
TRINAMIC's most autonomous driving IC is the TMC2100. With only seven pins to set up, this tiny and sophisticated standalone driver for two-phase stepper motors offers market-leading functionality. It is not necessary to interface with the CPU. Step and Direction signals are used to control the motor. This article is going to talk about the features, pinout, and more detailed information about the TMC2100.

TMC2100 guide - Stepper driver upgrades part 1 / How to set VREF & firmware
Overview of TMC2100
For 3D printing, cameras, scanners, and other automated equipment applications, the TMC2100 delivers an integrated motor driver solution. The device is designed to operate a bipolar stepper motor and includes an integrated microstepping indexer as well as the entirely noiseless current control mode StealthChopTM. To drive the motor windings, the output driver block consists of low RDSon N-Channel power MOSFETs configured as full H-bridges. Each of the TMC2100's outputs may drive up to 2.5A of current (with proper heatsinking). The TMC2100 is designed to work with a 546V supply voltage. The gadget features a step and direction interface and digital pins that can be adjusted.
TMC2100 Features
Hardware compatible with StepStick and Pololu A4988 Stepper Driver
Components on the bottom PCB side for better heat emission
Automatic standby current reduction
StealthChop - for quiet operation and smooth motion
SpreadCycle - highly dynamic motor control chopper
Drive capability up to 1.2A (RMS) continuous coil current
Step/Dir interface with micro-step interpolation (up to 256 micro steps)
Configuration via CFG pins
TMC2100 Specifications
| Model | TMC2100 |
| Interface | Step/Dir |
| Configuration | CFG Pins |
| Native Micro steps | up to 1 ⁄ 16 |
| microPlyer Micro steps | 1 ⁄ 256 |
| Logic Supply Voltage (VIO) | 3 - 5V |
| Motor Supply Voltage (VM) | 5.5 - 46V |
| Motor Phase Current max | 1.2A RMS, 2.5A Peak |
| Internal V- Regulator | enabled |
| RDSon | >=0.5 Ohm |
| stealthChop (quiet) | yes |
| spreadCycle | yes |
| coolStep | no |
| stallGuard | no |
| dcStep | no |
TMC2100 Pinout

TMC2100 Pinout
Pin Descriptions
| Pin | Function |
| Power Supply | |
| GND | Ground |
| VM | Motor Supply Voltage |
| VIO | Logic Supply Voltage |
| Motor Outputs | |
| M1A | Motor Coil 1 |
| M1B | Motor Coil 1 |
| M2A | Motor Coil 2 |
| M2B | Motor Coil 2 |
| Control Inputs | |
| STEP | Step-Signal Input |
| DIR | Direction-Signal Input |
| TMC2100 | |
| EN | Enable Motor Outputs: GND=on, VIO=off, OPEN=Auto-Power-Down |
| CFG0 | Chopper Off Time TOFF: GND=140tclk, VIO=236tclk, OPEN=332tclk |
| CFG1 | Step-Configuration |
| CFG2 | Step-Configuration |
| CFG3 | Current Setting: GND=int, VIO=int, OPEN=ext |
| CFG4 | Chopper Hysteresis HEND: GND=5, VIO=9, OPEN=13 |
| CFG5 | Chopper Blank Time TBL: GND=16, VIO=24, OPEN=36 |
| DIAG0 | Diagnostics Output 0 |
| DIAG1 | Diagnostics Output 1 |
| VREF | Analog Reference Voltage |
TMC2100 Wiring Diagram

TMC2100 Wiring Diagram
TMC2100 Motor Current Setting

Measuring the voltage on the Vref pin (0...2.5V) and adjusting the voltage with the potentiometer is the best technique to set the motor current. The greatest motor current that can be set is 1.77A RMS (0.11Ohm sensing resistors), while the SilentStepSticks can only handle 1.2A RMS.
TMC2100 Applications
3D-Printing
Cameras
Scanners
Other automated equipment applications
TMC2100 VS TMC2130 VS TMC2208

Conclusion of TMC2100 VS TMC2130 VS TMC2208
SpreadCycle and StealthChop are two of the TMC2100's operation modes. The TMC2130 is similar to the TMC2130, however, it has more operation modes and stall detection. The TMC2208 is identical to the TMC2100, but it has a UART interface and a StealthChop 2 operation mode. This chip is also less difficult to install, and it can be utilized without any firmware updates! Additionally, the major differences between the TMC2100, TMC2130, and TMC2208 are their driver current. The driver current of TMC2100 is up to 1.7A, while the driver current of TMC2130 and TMC2208 is up to 2A.
TMC2100 VS TMC2130 VS TMC2208 Datasheet
TMC2100 Manufacturer
Watterott electronic GmbH specializes in open-hardware, DIY (do-it-yourself), and development components. Stephan Watterott founded the company in Hausen (Thuringia, Germany) in March 2008 to offer unique microcontroller boards and specialty hard-to-find development components. In the early days, a 20 m2 room was enough space for an office, manufacturing, warehouse, and shipping departments, but as the product range and shipping volumes increased, the original space became too small. In 2010, the company renovated and moved into a new location in Leinefelde. Since then, the product range has continued to grow and the in-house production is constantly expanded.
Popularity by Region
What is the TMC2100?
TRINAMIC's most autonomous driving IC is the TMC2100. With only seven pins to set up, this tiny and sophisticated standalone driver for two-phase stepper motors offers market-leading functionality. It is not necessary to interface with the CPU. Step and Direction signals are used to control the motor.
What are the differences between the TMC2100 VS TMC2130 VS TMC2208?
Two of the TMC2100's operation modes are SpreadCycle and StealthChop. The TMC2130 is identical to the TMC2130, however, it includes more modes of operation and stall detection. The TMC2208 is identical to the TMC2100 except for the addition of a UART interface and the StealthChop 2 operation mode. This chip is much easier to install and use, and it doesn't require any firmware upgrades! Furthermore, the driving current of the TMC2100, TMC2130, and TMC2208 differs significantly. TMC2100 has a driver current of up to 1.7A, whereas TMC2130 and TMC2208 have driver currents of up to 2A.
What’s the logical voltage of TMC2100?
3-5V.
What’s the input voltage of TMC2100?
4.75-46V DC.
What’s the relationship between CR2032 and CR2016?16 June 202212661
LM258 Op-Amp IC : Uses, Pinout and Datasheet26 August 20216766
LIS3DH Accelerometer: Datasheet, Pinout, Functionality, and Block Diagram08 July 20219382
LTC6930MPMS8-8.19#PBF Programmable Timer and Oscillator: Product Overview and Applications06 March 2024289
74HC595 Shift Register IC : Pinout, Advantage and Datasheet13 September 202110844
OPT3001DNPT: Light Sensor, Pinout, Circuit26 March 2022770
A Practical Guide to STM32F429IIT6 in Embedded Systems24 July 2025263
H6 vs H7 Battery: Which One Do You Like Better?01 April 202250639
Challenges and Control Approaches for Current Sharing in DC Microgrids07 June 20235287
Basic Introduction to Power Amplifier09 January 202610796
3 Semiconductor Stocks to Watch in 202426 December 20234231
Top 10 Technology Trends in the Global Semiconductor Industry in 202208 January 20229349
How do We Select Automotive Relays?30 September 202010739
An Overview of Top Semiconductor Companies17 October 202525587
Optimizing Energy Exchange with Vehicle-to-Grid Technology25 April 20233293
European Chipmakers Experience Decline Following SMIC's Profit Slump20 November 20233326
Watterott Electronic GmbH
In Stock
United States
China
Canada
Japan
Russia
Germany
United Kingdom
Singapore
Italy
Hong Kong(China)
Taiwan(China)
France
Korea
Mexico
Netherlands
Malaysia
Austria
Spain
Switzerland
Poland
Thailand
Vietnam
India
United Arab Emirates
Afghanistan
Åland Islands
Albania
Algeria
American Samoa
Andorra
Angola
Anguilla
Antigua & Barbuda
Argentina
Armenia
Aruba
Australia
Azerbaijan
Bahamas
Bahrain
Bangladesh
Barbados
Belarus
Belgium
Belize
Benin
Bermuda
Bhutan
Bolivia
Bonaire, Sint Eustatius and Saba
Bosnia & Herzegovina
Botswana
Brazil
British Indian Ocean Territory
British Virgin Islands
Brunei
Bulgaria
Burkina Faso
Burundi
Cabo Verde
Cambodia
Cameroon
Cayman Islands
Central African Republic
Chad
Chile
Christmas Island
Cocos (Keeling) Islands
Colombia
Comoros
Congo
Congo (DRC)
Cook Islands
Costa Rica
Côte d’Ivoire
Croatia
Cuba
Curaçao
Cyprus
Czechia
Denmark
Djibouti
Dominica
Dominican Republic
Ecuador
Egypt
El Salvador
Equatorial Guinea
Eritrea
Estonia
Eswatini
Ethiopia
Falkland Islands
Faroe Islands
Fiji
Finland
French Guiana
French Polynesia
Gabon
Gambia
Georgia
Ghana
Gibraltar
Greece
Greenland
Grenada
Guadeloupe
Guam
Guatemala
Guernsey
Guinea
Guinea-Bissau
Guyana
Haiti
Honduras
Hungary
Iceland
Indonesia
Iran
Iraq
Ireland
Isle of Man
Israel
Jamaica
Jersey
Jordan
Kazakhstan
Kenya
Kiribati
Kosovo
Kuwait
Kyrgyzstan
Laos
Latvia
Lebanon
Lesotho
Liberia
Libya
Liechtenstein
Lithuania
Luxembourg
Macao(China)
Madagascar
Malawi
Maldives
Mali
Malta
Marshall Islands
Martinique
Mauritania
Mauritius
Mayotte
Micronesia
Moldova
Monaco
Mongolia
Montenegro
Montserrat
Morocco
Mozambique
Myanmar
Namibia
Nauru
Nepal
New Caledonia
New Zealand
Nicaragua
Niger
Nigeria
Niue
Norfolk Island
North Korea
North Macedonia
Northern Mariana Islands
Norway
Oman
Pakistan
Palau
Palestinian Authority
Panama
Papua New Guinea
Paraguay
Peru
Philippines
Pitcairn Islands
Portugal
Puerto Rico
Qatar
Réunion
Romania
Rwanda
Samoa
San Marino
São Tomé & Príncipe
Saudi Arabia
Senegal
Serbia
Seychelles
Sierra Leone
Sint Maarten
Slovakia
Slovenia
Solomon Islands
Somalia
South Africa
South Sudan
Sri Lanka
St Helena, Ascension, Tristan da Cunha
St. Barthélemy
St. Kitts & Nevis
St. Lucia
St. Martin
St. Pierre & Miquelon
St. Vincent & Grenadines
Sudan
Suriname
Svalbard & Jan Mayen
Sweden
Syria
Tajikistan
Tanzania
Timor-Leste
Togo
Tokelau
Tonga
Trinidad & Tobago
Tunisia
Turkey
Turkmenistan
Turks & Caicos Islands
Tuvalu
U.S. Outlying Islands
U.S. Virgin Islands
Uganda
Ukraine
Uruguay
Uzbekistan
Vanuatu
Vatican City
Venezuela
Wallis & Futuna
Yemen
Zambia
Zimbabwe


Product
Brand
Articles
Tools