The Guide to OV5647 Fisheye Camera Module for Raspberry Pi
RASPBERRY PI WIDE ANGLE CAMERA M
Unit Price: $22.880958
Ext Price: $22.88









RASPBERRY PI WIDE ANGLE CAMERA M
The OV5647 is OmniVision's first 5-megapixel CMOS image sensor built on proprietary 1.4-micron OmniBSI™ backside illumination pixel architecture. This article is going to explain details about OV5647.

How to use Arducam OV5647 Camera Module for Raspberry Pi
What is OV5647?
The OV5647 Camera Module is a Raspberry Pi add-on that was specially designed. One of the two little connections on the board's upper surface connects it to the Raspberry Pi. This interface employs the CSI interface, which was created specifically for connecting to cameras. The CSI bus can handle exceptionally high data rates and is only used to transport pixel data.
The camera is connected to the Pi's BCM2835 processor through the CSI bus, a higher-bandwidth link that sends pixel data back to the processor. This bus follows the ribbon cable that connects the camera board to the Raspberry Pi, The camera is compatible with Raspbian, Raspberry Pi's chosen operating system.
OV5647 Pad Diagram

OV5647 Pad Diagram
OV5647 Specifications
| Model No | CMT-5MP-RP-OV5647-X010 |
| Sensor | 1/4’’ Omnivision OV4647 |
| Pixel | 5 Mega Pixels |
| Most effective pixels | 2592 x 1944 |
| Pixel Size | 1.4 um x 1.4 um |
| Focus type | Fixed focus |
| FOV | 62° |
| Image format | VGA |
| Color | 24-Bit True color |
| Lens construction | 4G+IR650 |
| Aperture | F2.4 |
| Operating temperature | - 20 ° C to 70 ° C |
| Dimension | 25mm x24mm |
| Power consumption | 90Wm/30uW |
| Voltage | 1.7V-3.0V |
| Pin Number | 15 Pin |
| Output signal | YCBCR4:2:2, RGB565, RAWRGB |
| Frame rate | 30fps |
OV5647 Block Diagram

OV5647 Block Diagram
OV5647 Features
Raspberry Pi Camera, supports all revisions of the Pi
Fisheye Lens, offers a wider field of view
5-megapixel OV5647 sensor
Adjustable focus distance
Camera specifications
CCD size: 1/4inch
Aperture (F) : 2.35
Focal Length: 3.15mm
The angle of view (diagonal): 160 degrees (while other normal cameras are typically 72 degrees)
Sensor best resolution : 1080p
4 screw holes
Used for attachment
Provides 3.3V power output
Supports connecting fill flash LED
Dimension: 25mm x 24mm
OV5647 Applications
Mobile Phones
Digital Still Cameras
PC Multimedia
Cellular PDAs,Toys
Other battery-powered products
Can be used on all Raspberry Pi platforms
How does OV5647 work?
A small ribbon connection links the OV5647 to the Raspberry Pi. The camera is connected to the Pi's BCM2835 processor through the CSI bus, a higher-bandwidth link that sends pixel data back to the processor. This bus follows the ribbon cable that connects the camera board to the Raspberry Pi,1.
OV5647 Package Information
1 * RPi Night Vision Camera
1 * 15 cm 15 pin FFC adapter
1 * 50 cm 15 pin FFC adapter

OV5647 Package Information
OV5647 Manufacturer
Seeed is the IoT hardware enabler providing open source products and services that empower developers to swiftly realize IoT projects. By partnering with world-famous IoT ecosystem companies from hardware to cloud, Seeed offers a wide range of hardware platforms and sensor modules ready to be integrated with existing IoT platforms. It was founded in 2008 in Shenzhen - the world capital of electronics - and specialized in hardware innovation for makers to grow inspirations into differentiating products.
Specifications
- TypeParameter
- Factory Lead Time9 Weeks
- Part Status
Parts can have many statuses as they progress through the configuration, analysis, review, and approval stages.
Active - Moisture Sensitivity Level (MSL)
Moisture Sensitivity Level (MSL) is a standardized rating that indicates the susceptibility of electronic components, particularly semiconductors, to moisture-induced damage during storage and the soldering process, defining the allowable exposure time to ambient conditions before they require special handling or baking to prevent failures
1 (Unlimited) - TypeSensor
- Function
The parameter "Function" in electronic components refers to the specific role or purpose that the component serves within an electronic circuit. It defines how the component interacts with other elements, influences the flow of electrical signals, and contributes to the overall behavior of the system. Functions can include amplification, signal processing, switching, filtering, and energy storage, among others. Understanding the function of each component is essential for designing effective and efficient electronic systems.
Camera - Utilized IC / Part
Utilized IC / Part is a parameter that refers to the extent to which an integrated circuit (IC) or electronic component is being used or consumed within a system or application. It typically indicates the percentage or ratio of the component's capabilities that are being utilized in a given scenario. This parameter is important for assessing the efficiency and performance of the component, as well as for determining if the component is being underutilized or overburdened in a particular application. Monitoring and optimizing the utilization of ICs and electronic parts can help improve overall system reliability, efficiency, and cost-effectiveness.
OV5647 - ContentsBoard(s), Cable(s)
- Platform
In the context of electronic components, the parameter "Platform" typically refers to the specific hardware or software environment on which the component is designed to operate. This could include the type of operating system, processor architecture, communication protocols, or other technical specifications that the component is compatible with. Understanding the platform requirements of electronic components is crucial for ensuring proper functionality and integration within a larger system. Manufacturers often provide detailed information about the supported platforms to help users select the right components for their applications.
Raspberry Pi - RoHS Status
RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.
RoHS Compliant
What is the use of OV5647?
5MP OV5647 cameras, namely the V1 camera series, are used a lot on Raspberry Pi camera applications.
How does OV5647 work?
A small ribbon connection links the OV5647 to the Raspberry Pi. The camera is connected to the Pi's BCM2835 processor through the CSI bus, a higher-bandwidth link that sends pixel data back to the processor. This bus follows the ribbon cable that connects the camera board to the Raspberry Pi. 1
What interface does the OV5647 Camera Module use?
CSI
What is the CSI bus only used to transport?
pixel data
What cable connects the camera board to the Raspberry Pi?
ribbon cable
LM2575 Replacement & Datasheet: A Cost-Effective Selection Guide31 January 2026220
CC2541 MCU: Pinout, Circuit, Application14 August 20214428
STM32F072C8T6 Microcontroller: 48MHz, 48-LQFP, Pinout and Datasheet21 January 20226084
SI5347 Clock Generator: Features, Pinout and Datasheet18 April 20221097
ESP-01 Wi-Fi Module: ESP-01 Pinout, Programming and ESP-01 VS ESP8266 [FAQ]14 December 202162508
TOP224YN: Features, Applications, and Datasheet26 October 20231658
Intel EPCS4SI8N What You Need to Know30 August 2025287
What is a CL10B104KB8NNNC Multilayer Ceramic Capacitor?25 April 20221171
The U.S. Semiconductor Sector Faces Workforce Challenges Amidst Surging Demand27 November 20233792
What is Digital Counter?01 September 202012884
What causes the Noise of Electronic Equipment when it is Running?01 August 20222789
Introduction to DC Amplifier07 November 202518810
Kyoto University Successfully Demonstrates That SiC Can Also Work at 350°C26 March 2022752
2 Semiconductor Stocks to Buy Hand Over Fist in 2024 and 1 to Avoid Like the Plague18 December 20234354
Exploring the Strengths and Hurdles of Wide Bandgap Devices in Alternating Current Electric Drives19 January 20243631
An Overview of Digital Signal Processor31 October 202510886
Seeed Technology Co., Ltd
In Stock: 309
Minimum: 1 Multiples: 1
Qty
Unit Price
Ext Price
1
$22.880958
$22.88
10
$21.585809
$215.86
100
$20.363971
$2,036.40
500
$19.211294
$9,605.65
1000
$18.123862
$18,123.86
Not the price you want? Send RFQ Now and we'll contact you ASAP.
Inquire for More Quantity


Product
Brand
Articles
Tools