NXP MPX5500DP Differential Pressure Sensor: High-Accuracy Industrial Solution Guide
MPX5500 Series Differential Pressure Sensor Analog Voltage -40°C~125°C 72.52PSI (500kPa) Barbed ±2.5% 0.2 V ~ 4.7 V 4.75V~5.25V









MPX5500 Series Differential Pressure Sensor Analog Voltage -40°C~125°C 72.52PSI (500kPa) Barbed ±2.5% 0.2 V ~ 4.7 V 4.75V~5.25V
NXP MPX5500DP is a differential pressure sensor offering high accuracy, robust design, and analog output for reliable measurement in demanding applications.
Product Introduction
A differential pressure sensor measures the difference in pressure between two points. In a busy factory, workers rely on accurate pressure readings to keep machines running smoothly and safely. The nxp mpx5500dp stands out as a top choice for these tasks. This sensor uses advanced technology to deliver reliable results. Many industries trust it because about 42% of automation systems and nearly half of industrial equipment depend on sensors like this for monitoring and control. The nxp mpx5500dp helps users track pressure changes quickly and with confidence.
Differential Pressure Sensor Basics
How It Works
A differential pressure sensor measures the difference in pressure between two points. The sensor uses a thin diaphragm placed between two ports. When pressure is applied to each port, the diaphragm bends. This bending changes either the resistance or the capacitance inside the sensor. The sensor then converts this change into an electrical signal. Some sensors use piezoresistive materials, while others use capacitive or inductive methods. For example, a capacitive sensor has a flexible diaphragm between two metal plates. When the diaphragm moves, the capacitance changes, and the sensor sends out a signal. This process allows the sensor to give accurate pressure readings. The design of the diaphragm ensures both flexibility and strength, so the sensor can work for a long time without wearing out.
Note: The sensor’s ability to turn small mechanical changes into electrical signals makes it very useful for many types of equipment.
Key Uses
People use differential pressure sensors in many industries. These sensors help monitor and control systems by tracking pressure changes. The table below shows some common types of sensors and how they work:
| Sensor Type | How It Works | Main Features |
|---|---|---|
| Capacitive | Diaphragm movement changes capacitance | High sensitivity, low power use |
| Strain Gauge | Pressure changes resistance in a material | High accuracy, reliable |
| Inductive | Core movement changes inductance | Good for harsh environments |
| Piezoelectric | Pressure creates an electric charge in special materials | Accurate, used in fast-changing environments |
| Bourdon Tube | Pressure straightens a curved tube | Simple, mechanical, reliable |
| Manometer | Pressure moves liquid in a U-shaped tube | Accurate for low ranges, slow response |
Industries such as HVAC, automotive, and healthcare rely on these sensors. In HVAC systems, sensors monitor airflow and check for clogged filters. In cars, they help control air intake and manage exhaust systems. Medical devices use them to keep track of airway pressure in ventilators. These uses show how important accurate pressure measurement is for safety and efficiency.
NXP MPX5500DP Overview
Main Features
The nxp mpx5500dp stands out as a high-range differential pressure sensor. It uses dual ports to measure the difference in pressure between two points. This sensor provides an analog output, which makes it easy to connect to many types of equipment. The device uses advanced piezoresistive technology. This technology relies on a silicon strain gauge that changes resistance when pressure is applied. The monolithic silicon design means the sensor element and signal processing sit on a single chip. This design improves durability and helps the sensor deliver accurate readings over a wide temperature range.
The monolithic silicon structure also allows for built-in temperature compensation and calibration. This feature ensures the sensor remains reliable even when the environment changes. The nxp mpx5500dp works well in many fields, such as industrial automation, automotive systems, and medical devices.
A quick look at what sets this sensor apart:
| Feature | Description |
|---|---|
| Sensing Technology | Differential piezoresistive |
| Mounting Type | Through-hole mounting |
| Package / Case | 6-SIP module (unibody-6) |
| Pressure Measurement | Up to 72.52 PSI (500 kPa) |
| Accuracy | ±2.5% |
| Output Voltage Range | 0.20 V to 4.70 V (analog output) |
| Temperature Compensation | Yes |
| Port Style | Male barbed dual tube port |
| Operating Temperature | -40°C to 125°C |
| Maximum Pressure | 406.11 PSI (2800 kPa) |
| Sensitivity & Noise | High sensitivity, low noise |
| Applications | Industrial, commercial, military, aerospace, automotive, medical, HVAC, power generation, industrial automation |
The nxp mpx5500dp combines a wide pressure range, robust packaging, and precise analog output. These features make it a trusted choice for demanding applications.
Technical Specs
The technical specifications of the nxp mpx5500dp show why it is so popular. The sensor can measure pressure up to 72.52 PSI (500 kPa) and can handle a maximum pressure of 406.11 PSI (2800 kPa). It offers an accuracy of ±2.5%, which means users can trust its readings. The analog output ranges from 0.2 V to 4.7 V, making it easy to connect to analog-to-digital converters in microcontroller systems. The supply voltage should stay between 4.75 V and 5.25 V for best performance. The sensor responds quickly, with a response time of just 1 millisecond.
| Specification | Value |
|---|---|
| Operating Pressure | 72.52 PSI (500 kPa) |
| Maximum Pressure | 406.11 PSI (2800 kPa) |
| Accuracy | ±2.5% |
| Output Voltage Range | 0.2 V to 4.7 V |
| Supply Voltage | 4.75 V to 5.25 V |
| Output Type | Analog Voltage |
| Response Time | 1 ms (1000 µs) |
The analog output of this sensor allows for flexible integration. Users can connect it to many types of microcontrollers, but they need an external analog-to-digital converter to read the signal. While some digital sensors offer higher resolution and direct digital output, the nxp mpx5500dp provides a simple and reliable solution for many projects.
The piezoresistive technology and monolithic silicon design give the sensor high accuracy and stability. The sensor uses a patented silicon shear stress strain gauge, which helps it keep a maximum error of only 2.5% across a wide temperature range. The integration of the sensor element and signal conditioning on a single chip improves durability and ensures the sensor can handle tough environments. This makes the nxp mpx5500dp a strong choice for anyone needing precise pressure measurement.
MPX5500DP Applications
Common Uses
The MPX5500DP finds its place in many real-world systems. Engineers often select this sensor for its ability to measure pressure differences with high accuracy. Many industries rely on it to keep their equipment running safely and efficiently. Some of the most common uses include:
Environmental control systems: These systems use the sensor to monitor air flow and maintain proper ventilation.
Pneumatic control systems: The sensor helps regulate air pressure in machines that use compressed air.
Appliances: Manufacturers use the sensor in devices like washing machines and dishwashers to track water or air pressure.
Automotive performance controls: The sensor measures pressure in fuel and air systems, helping vehicles run smoothly.
Medical instrumentation: Hospitals use the sensor in devices that monitor patient breathing or blood pressure.
Industrial controls: Factories depend on the sensor to keep track of pressure in pipes and tanks.
The MPX5500DP works well in both simple and complex setups. Its wide pressure range and reliable readings make it a favorite for engineers who need dependable results.
User Feedback
Users often praise the MPX5500DP for its strong performance. Many highlight its high sensitivity and accuracy, which help deliver reliable pressure readings with very little error. The sensor’s wide pressure range, from 0 to 500 kPa, allows it to fit many different applications. Its compact design makes it easy to add to new or existing systems.
A table below shows what users like most about this sensor:
| Advantage | Description |
|---|---|
| High sensitivity and accuracy | Reliable pressure readings with minimal error |
| Wide pressure range | Suitable for many uses |
| Compact design | Fits easily into various systems |
| Durable construction | Works well in harsh environments |
| Low power consumption | Supports energy-efficient projects |
| Stable output | Accurate even with temperature changes or vibrations |
Users also note that the sensor remains stable and accurate even when temperatures or vibrations change. Many appreciate its versatility in automotive, industrial, medical, and consumer electronics fields. No major disadvantages appear in user reviews, which shows strong satisfaction with the MPX5500DP.
Why Choose NXP MPX5500DP
Advantages
The NXP MPX5500DP offers several strong advantages that make it a top choice for many users. This sensor delivers high sensitivity and accuracy, which helps engineers and hobbyists get reliable readings in important projects. The wide pressure range, from 0 to 500 kPa, allows the sensor to work in both low and high-pressure situations. Its compact design and through-hole mounting make it easy to add to different systems. Many users find this helpful when building new devices or upgrading old ones.
High sensitivity and accuracy support precise measurements.
Wide pressure range fits many uses, from small gadgets to large machines.
Compact size and simple mounting help with quick installation.
Low power use supports energy-saving designs.
The sensor works well in harsh environments, such as factories or outdoor equipment.
The MPX5500DP also connects easily to microcontrollers. This feature lets students, hobbyists, and professionals use the sensor in custom projects. Many people use it in cars, HVAC systems, medical devices, and even consumer electronics. The sensor’s popularity comes from its ability to meet the needs of both experts and beginners.
Tip: The MPX5500DP is available from many distributors. Users can find samples, get support, and enjoy warranty services, which makes it easy to start new projects.
Reliability
Reliability stands out as one of the main reasons people choose the MPX5500DP. The sensor uses a strong monolithic silicon design, which helps it last a long time. It keeps working even when temperatures change or when there are vibrations. This durability is important for industrial systems that run all day.
A table below shows what makes the MPX5500DP reliable:
| Reliability Feature | Benefit |
|---|---|
| Monolithic silicon design | Long-lasting and stable performance |
| Built-in temperature compensation | Accurate readings in changing conditions |
| Robust construction | Handles tough environments |
| Stable analog output | Consistent data for control systems |
| Active product support | Easy access to help and replacement |
Many engineers trust the MPX5500DP for critical tasks. The sensor’s stable output helps keep machines safe and efficient. Hobbyists also like the sensor because it works well in small projects and does not need much power. The combination of strong performance, easy integration, and lasting reliability explains why the MPX5500DP remains popular in so many fields.
The NXP MPX5500DP gives users true differential pressure measurement with its dual-port design and linear analog output. Its high accuracy, built-in temperature compensation, and robust construction support reliable results in many fields. When choosing a sensor, users should consider factors like pressure range, accuracy, and environmental conditions.
Sensor type and range
Accuracy for the application
Durability in harsh settings
The global differential pressure sensor market is expected to grow at a CAGR of 7.08% from 2024 to 2031, reaching $29.25 billion. As technology advances, sensors like the MPX5500DP will play an even bigger role in future innovations.
| Market Segment | CAGR (%) | Forecast Period | Market Size Projection (USD Billion) |
|---|---|---|---|
| Global Differential Pressure Sensor | 7.08% | 2024-2031 | 29.25 (by 2031) from 17.05 (2023) |
FAQ
What is the main function of the NXP MPX5500DP sensor?
The NXP MPX5500DP measures the difference in pressure between two points. It helps users monitor and control systems in many fields, such as automotive, industrial, and medical applications.
Can the MPX5500DP connect to microcontrollers?
Yes, the MPX5500DP provides an analog voltage output. Users can connect it to most microcontrollers by using an analog-to-digital converter (ADC) to read the sensor’s signal.
How accurate is the MPX5500DP?
The MPX5500DP offers an accuracy of ±2.5%. This level of precision makes it suitable for tasks that require reliable and repeatable pressure measurements.
What environments can the MPX5500DP handle?
The MPX5500DP works in temperatures from -40°C to 125°C. Its strong construction allows it to perform well in harsh environments, including factories, vehicles, and outdoor equipment.
Specifications
- TypeParameter
- Factory Lead Time12 Weeks
- Package / Case
refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.
6-SIP Module - Surface Mount
having leads that are designed to be soldered on the side of a circuit board that the body of the component is mounted on.
NO - Mounting Feature
a process by which the operating system makes files and directories on a storage device (such as hard drive, CD-ROM, or network share) available for users to access via the computer's file system.
THROUGH HOLE MOUNT - Operating Temperature
The operating temperature is the range of ambient temperature within which a power supply, or any other electrical equipment, operate in. This ranges from a minimum operating temperature, to a peak or maximum operating temperature, outside which, the power supply may fail.
-40°C~125°C - Series
In electronic components, the "Series" refers to a group of products that share similar characteristics, designs, or functionalities, often produced by the same manufacturer. These components within a series typically have common specifications but may vary in terms of voltage, power, or packaging to meet different application needs. The series name helps identify and differentiate between various product lines within a manufacturer's catalog.
MPX5500 - Published1998
- Part Status
Parts can have many statuses as they progress through the configuration, analysis, review, and approval stages.
Active - Moisture Sensitivity Level (MSL)
Moisture Sensitivity Level (MSL) is a standardized rating that indicates the susceptibility of electronic components, particularly semiconductors, to moisture-induced damage during storage and the soldering process, defining the allowable exposure time to ambient conditions before they require special handling or baking to prevent failures
Not Applicable - ECCN Code
An ECCN (Export Control Classification Number) is an alphanumeric code used by the U.S. Bureau of Industry and Security to identify and categorize electronic components and other dual-use items that may require an export license based on their technical characteristics and potential for military use.
EAR99 - Applications
The parameter "Applications" in electronic components refers to the specific uses or functions for which a component is designed. It encompasses various fields such as consumer electronics, industrial automation, telecommunications, automotive, and medical devices. Understanding the applications helps in selecting the right components for a particular design based on performance, reliability, and compatibility requirements. This parameter also guides manufacturers in targeting their products to relevant markets and customer needs.
Board Mount - HTS Code
HTS (Harmonized Tariff Schedule) codes are product classification codes between 8-1 digits. The first six digits are an HS code, and the countries of import assign the subsequent digits to provide additional classification. U.S. HTS codes are 1 digits and are administered by the U.S. International Trade Commission.
8542.39.00.01 - Voltage - Supply
Voltage - Supply refers to the range of voltage levels that an electronic component or circuit is designed to operate with. It indicates the minimum and maximum supply voltage that can be applied for the device to function properly. Providing supply voltages outside this range can lead to malfunction, damage, or reduced performance. This parameter is critical for ensuring compatibility between different components in a circuit.
4.75V~5.25V - Output
In electronic components, the parameter "Output" typically refers to the signal or data that is produced by the component and sent to another part of the circuit or system. The output can be in the form of voltage, current, frequency, or any other measurable quantity depending on the specific component. The output of a component is often crucial in determining its functionality and how it interacts with other components in the circuit. Understanding the output characteristics of electronic components is essential for designing and troubleshooting electronic circuits effectively.
0.2 V ~ 4.7 V - Termination Style
"Termination style" in electronic components refers to the method used to connect the component to a circuit board or other electronic devices. It determines how the component's leads or terminals are designed for soldering or mounting onto the circuit board. Common termination styles include through-hole, surface mount, and wire lead terminations.Through-hole components have leads that are inserted through holes in the circuit board and soldered on the other side. Surface mount components have flat terminals that are soldered directly onto the surface of the circuit board. Wire lead terminations involve attaching wires to the component for connection.The choice of termination style depends on factors such as the type of component, the manufacturing process, and the space available on the circuit board. Different termination styles offer various advantages in terms of ease of assembly, reliability, and space efficiency in electronic designs.
PC Pin - Body Length or Diameter
Body length or diameter in electronic components refers to the physical dimensions of a component's housing, typically measured in millimeters or inches. It indicates the size of the component that affects its fit within a circuit board or system. This parameter is crucial for ensuring compatibility with the design and mounting of electronic devices. It can impact heat dissipation, electrical performance, and overall assembly efficiency. Accurate measurement of body length or diameter is essential for proper component selection and placement in electronic applications.
29.46mm - Body Breadth
Body breadth in electronic components refers to the width of the physical body of a component, such as a resistor, capacitor, or integrated circuit. This measurement is crucial for ensuring proper fit within a circuit board or enclosure. It can affect the component's thermal performance, mechanical stability, and overall compatibility with other components in a design. Body breadth is typically specified in millimeters or inches and is an important factor in the selection and design of electronic assemblies.
10.67 mm - Output Type
The "Output Type" parameter in electronic components refers to the type of signal or data that is produced by the component as an output. This parameter specifies the nature of the output signal, such as analog or digital, and can also include details about the voltage levels, current levels, frequency, and other characteristics of the output signal. Understanding the output type of a component is crucial for ensuring compatibility with other components in a circuit or system, as well as for determining how the output signal can be utilized or processed further. In summary, the output type parameter provides essential information about the nature of the signal that is generated by the electronic component as its output.
Analog Voltage - Accuracy
Accuracy in electronic components refers to the degree to which a measured value agrees with the true or accepted value. It evaluates the precision of a component in providing correct output or measurement under specified conditions. High accuracy indicates minimal deviation from the actual value, while low accuracy shows significant error in measurement. This parameter is crucial in applications where precise data is essential for reliable performance and decision-making.
±2.5% - Response Time
the time taken for a circuit or measuring device, when subjected to a change in input signal, to change its state by a specified fraction of its total response to that change.
1000 µs - Operating Pressure
An operating pressure is the amount of internal force applied to the walls of some type of pressure vessel during normal conditions.
72.52PSI (500kPa) - Pressure Type
Pressure Type in electronic components refers to the type of pressure that the component can withstand without being damaged or malfunctioning. This parameter is important in applications where the component may be exposed to varying levels of pressure, such as in industrial or automotive settings. The pressure type specification typically includes information on the maximum pressure the component can handle, whether it is positive or negative pressure, and any specific conditions under which the component can operate safely. It is crucial to consider the pressure type rating when selecting electronic components for use in environments where pressure variations are a concern.
Differential - Port Style
Port style in electronic components refers to the physical and electrical characteristics of a connection point on a device or circuit. It encompasses the design and configuration of ports used for input and output, including their shape, size, and pin arrangement. Different port styles are used to ensure compatibility and facilitate connections between various electronic devices and systems. This parameter is crucial for defining how components interface with one another in electronic design and integration.
Barbed - Port Size
In electronic components, the parameter "Port Size" typically refers to the physical dimensions of the ports or connectors on the component. This measurement is important for determining compatibility with other components or devices that need to be connected. Port size can include the diameter, length, and shape of the ports, as well as the spacing between multiple ports on the same component. Understanding the port size is crucial for ensuring proper fit and connection between components in an electronic system. It is often specified in datasheets or product specifications to help users select the appropriate components for their needs.
Male - 0.19 4.93mm Tube Dual - Linearity
In electronic components, linearity refers to the relationship between the input and output signals of the component. A component is said to be linear if its output is directly proportional to its input over a specified range. In other words, when the input signal changes, the output signal changes in a consistent and predictable manner without introducing distortion or non-linear effects.Linearity is an important parameter in electronic components such as amplifiers, filters, and sensors, as it determines the accuracy and fidelity of signal processing. Non-linearities in components can lead to signal distortion, harmonic generation, and other undesirable effects that can degrade the performance of electronic systems.Engineers often characterize the linearity of components by measuring parameters such as gain error, harmonic distortion, and intermodulation distortion. By ensuring that components exhibit good linearity characteristics, designers can create electronic systems that accurately process signals and faithfully reproduce the desired output.
2.5 % - Maximum Pressure
The parameter "Maximum Pressure" in electronic components refers to the maximum amount of pressure or force that the component can withstand without being damaged or failing. This specification is important for components that may be exposed to external pressure, such as in high-pressure environments or applications where physical pressure may be applied. Exceeding the maximum pressure rating of a component can lead to deformation, cracking, or complete failure of the component, potentially causing system malfunctions or safety hazards. It is crucial to adhere to the specified maximum pressure limits to ensure the reliable operation and longevity of electronic components in various applications.
406.11PSI (2800kPa) - Sensors/Transducers Type
In electronic components, the parameter "Sensors/Transducers Type" refers to the specific type of sensor or transducer that is integrated into the component. Sensors are devices that detect changes in physical properties and convert them into electrical signals, while transducers are devices that convert one form of energy into another. The type of sensor or transducer used in an electronic component can vary widely depending on the intended application, such as temperature sensors, pressure sensors, proximity sensors, accelerometers, and more. Understanding the Sensors/Transducers Type parameter is crucial for selecting the right component for a particular electronic system or device, as different types of sensors/transducers have different functionalities and performance characteristics.
PRESSURE SENSOR,PEIZORESISTIVE - Housing
Housing in electronic components refers to the physical enclosure that protects the internal circuitry and components from environmental factors such as dust, moisture, and mechanical damage. It provides structural support and electrical insulation while facilitating heat dissipation. The design and materials used for housing are crucial for the reliability and performance of the electronic device, as they impact factors like thermal management, electromagnetic interference, and overall aesthetics.
PLASTIC - Pressure Range-Max
Pressure Range-Max in electronic components refers to the maximum amount of pressure that the component can withstand without being damaged or malfunctioning. This parameter is crucial in applications where the component may be exposed to varying levels of pressure, such as in industrial or automotive settings. It is typically specified in units such as pounds per square inch (psi) or pascals (Pa). Ensuring that electronic components are rated for the appropriate pressure range is essential to prevent failures and maintain the reliability of the overall system.
72.51 Psi - Offset-Nom
Offset-Nom is a parameter commonly found in electronic components, particularly in operational amplifiers and other analog circuits. It refers to the nominal value of the input offset voltage, which is the voltage difference required between the two input terminals of the component to bring the output voltage to zero. In other words, it represents the inherent voltage offset present in the component that can affect the accuracy of the output signal. The Offset-Nom value is specified by the manufacturer and is important to consider when designing circuits that require precise voltage levels or when high accuracy is needed.
0.20V - Features
In the context of electronic components, the term "Features" typically refers to the specific characteristics or functionalities that a particular component offers. These features can vary depending on the type of component and its intended use. For example, a microcontroller may have features such as built-in memory, analog-to-digital converters, and communication interfaces like UART or SPI.When evaluating electronic components, understanding their features is crucial in determining whether they meet the requirements of a particular project or application. Engineers and designers often look at features such as operating voltage, speed, power consumption, and communication protocols to ensure compatibility and optimal performance.In summary, the "Features" parameter in electronic components describes the unique attributes and capabilities that differentiate one component from another, helping users make informed decisions when selecting components for their electronic designs.
Temperature Compensated - Sensitivity (mV/V)
The parameter "Sensitivity (mV/V)" in electronic components refers to the ratio of the output voltage change to the input voltage change, typically expressed in millivolts per volt (mV/V). It indicates how responsive the component is to changes in the input voltage, providing a measure of its ability to convert input signals into output signals. A higher sensitivity value means that the component will produce a larger output voltage change for a given input voltage change, making it more responsive and accurate in its operation. Sensitivity is an important characteristic in various electronic devices such as sensors, transducers, and amplifiers, as it directly impacts the precision and reliability of the system's performance.
9 mV/V - Body Height
In electronic components, "Body Height" refers to the vertical dimension of the component's physical body or package. It is the measurement from the bottom of the component to the top, excluding any leads or terminals. Body Height is an important parameter to consider when designing circuit boards or enclosures to ensure proper fit and clearance. It is typically specified in datasheets or technical drawings provided by the component manufacturer. Understanding the Body Height of electronic components is crucial for proper placement and integration within a circuit or system.
17.78mm - RoHS Status
RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.
ROHS3 Compliant
Parts with Similar Specs
- ImagePart NumberManufacturerPackage / CaseAccuracyPort StyleRoHS StatusOffset-NomFactory Lead TimeLinearityView Compare
MPX5500DP
6-SIP Module
±2.5%
Barbed
ROHS3 Compliant
0.20V
12 Weeks
2.5 %
6-SIP Module
±2.5%
Barbed
ROHS3 Compliant
0.20V
12 Weeks
2.5 %
6-SIP Module
±2.5%
Barbed
ROHS3 Compliant
0.20V
12 Weeks
2.5 %
6-SIP Module
±2.5%
Barbed
ROHS3 Compliant
0.20V
12 Weeks
2.5 %
Datasheet PDF
- PCN Packaging :
- Datasheets :
- Environmental Information :
LTC4054 Single-cell Lithium-ion Battery: Circuits, Pinout, and Datasheet [Video]04 January 202216499
AD780 3 ppm/°C Voltage Reference: Datasheet, Specs, and Design Analysis11 April 2026200
MOC3021 Optoisolators: Pinout, Circuit and Equivalent06 August 202117396
FT230X USB To Basic UART IC14 August 20217536
DS1307N Real-Time Clock: Circuit, Pinout, and Datasheet17 April 20251570
MPU6000 Sensor: Comparison, Pinout, and Datasheet10 December 202119818
ULN2003A Seven Darlington Array: Pinout, Features and Datasheet18 May 202122523
A Comprehensive Guide to LTC6947IUFD#TRPBF PLL Frequency Synthesizer06 March 2024458
Understanding Power Management Units (PMUs)06 June 20252686
Electronic components distributor UTMEL Stands Out at electronica china 202409 July 20244950
Understanding Electronic Speed Controllers (ESCs): Working Principles, Key Specifications, and Sourcing Guide15 June 2026885
All You Need to Know about Ultrasonic Sensors25 October 202513030
Hot Swap Controllers:Semiconductors That Provide In-circuit Protection and Control Functions22 February 20234926
How Can Memory Adapt and Influence the Smart Age of the Future?11 October 20222492
Random Access Memory: Definition, Types and Working29 August 202010758
What is Variable Frequency Driver(VFD)?20 October 20212896
NXP USA Inc.
In Stock
United States
China
Canada
Japan
Russia
Germany
United Kingdom
Singapore
Italy
Hong Kong(China)
Taiwan(China)
France
Korea
Mexico
Netherlands
Malaysia
Austria
Spain
Switzerland
Poland
Thailand
Vietnam
India
United Arab Emirates
Afghanistan
Åland Islands
Albania
Algeria
American Samoa
Andorra
Angola
Anguilla
Antigua & Barbuda
Argentina
Armenia
Aruba
Australia
Azerbaijan
Bahamas
Bahrain
Bangladesh
Barbados
Belarus
Belgium
Belize
Benin
Bermuda
Bhutan
Bolivia
Bonaire, Sint Eustatius and Saba
Bosnia & Herzegovina
Botswana
Brazil
British Indian Ocean Territory
British Virgin Islands
Brunei
Bulgaria
Burkina Faso
Burundi
Cabo Verde
Cambodia
Cameroon
Cayman Islands
Central African Republic
Chad
Chile
Christmas Island
Cocos (Keeling) Islands
Colombia
Comoros
Congo
Congo (DRC)
Cook Islands
Costa Rica
Côte d’Ivoire
Croatia
Cuba
Curaçao
Cyprus
Czechia
Denmark
Djibouti
Dominica
Dominican Republic
Ecuador
Egypt
El Salvador
Equatorial Guinea
Eritrea
Estonia
Eswatini
Ethiopia
Falkland Islands
Faroe Islands
Fiji
Finland
French Guiana
French Polynesia
Gabon
Gambia
Georgia
Ghana
Gibraltar
Greece
Greenland
Grenada
Guadeloupe
Guam
Guatemala
Guernsey
Guinea
Guinea-Bissau
Guyana
Haiti
Honduras
Hungary
Iceland
Indonesia
Iran
Iraq
Ireland
Isle of Man
Israel
Jamaica
Jersey
Jordan
Kazakhstan
Kenya
Kiribati
Kosovo
Kuwait
Kyrgyzstan
Laos
Latvia
Lebanon
Lesotho
Liberia
Libya
Liechtenstein
Lithuania
Luxembourg
Macao(China)
Madagascar
Malawi
Maldives
Mali
Malta
Marshall Islands
Martinique
Mauritania
Mauritius
Mayotte
Micronesia
Moldova
Monaco
Mongolia
Montenegro
Montserrat
Morocco
Mozambique
Myanmar
Namibia
Nauru
Nepal
New Caledonia
New Zealand
Nicaragua
Niger
Nigeria
Niue
Norfolk Island
North Korea
North Macedonia
Northern Mariana Islands
Norway
Oman
Pakistan
Palau
Palestinian Authority
Panama
Papua New Guinea
Paraguay
Peru
Philippines
Pitcairn Islands
Portugal
Puerto Rico
Qatar
Réunion
Romania
Rwanda
Samoa
San Marino
São Tomé & Príncipe
Saudi Arabia
Senegal
Serbia
Seychelles
Sierra Leone
Sint Maarten
Slovakia
Slovenia
Solomon Islands
Somalia
South Africa
South Sudan
Sri Lanka
St Helena, Ascension, Tristan da Cunha
St. Barthélemy
St. Kitts & Nevis
St. Lucia
St. Martin
St. Pierre & Miquelon
St. Vincent & Grenadines
Sudan
Suriname
Svalbard & Jan Mayen
Sweden
Syria
Tajikistan
Tanzania
Timor-Leste
Togo
Tokelau
Tonga
Trinidad & Tobago
Tunisia
Turkey
Turkmenistan
Turks & Caicos Islands
Tuvalu
U.S. Outlying Islands
U.S. Virgin Islands
Uganda
Ukraine
Uruguay
Uzbekistan
Vanuatu
Vatican City
Venezuela
Wallis & Futuna
Yemen
Zambia
Zimbabwe


Product
Brand
Articles
Tools