web counter

CR1616 vs CR2025[Video+FAQ]: Differences and Similarities

Sophie

Published: 21 April 2022 | Last Updated: 21 April 2022

13748

CR2025

CR2025

FDK America, Inc., a member of Fujitsu Group

BATTERY LITHIUM 3V COIN 20MM

Purchase Guide

BATTERY LITHIUM 3V COIN 20MM

Just like other batteries in the CR series, CR2025 and CR1616 are button batteries that seem very similar in many respects. By comparing the CR2025 vs CR1616, we’ll see if the two are interchangeable, and what their differences and similarity are.

This is a comparison video about CR1616 and CR2025.

CR1616 vs CR2025: The Difference Between CR1616 & CR2025 Tabbed Gameboy Save Batteries [Comparison]

What is CR1616?

cr1616.jpg

The CR1616 is a coin cell battery that works in many smaller electronic devices. It is able to power key fobs, glucometers, heart rate monitors, toys, computer backup equipment, and more. One of its most popular uses is in the Honda and Lexus key fobs, but it is also used in many other car brands and devices. Having a battery you can rely on gives you peace of mind. No one wants to run out of power for his or her important devices. With these batteries, you can easily store them long-term so that you always have the power that you need.

Also known as 1616, L28, BR1616, or DL1616 batteries, these coin cell batteries use lithium technology and offer high charge density for longer life.


What is CR2025?

CR2025.jpg

CR2025 is a coin cell battery. Coin cell batteries like CR2025 have many uses, they are usually used for small portable electronics devices such as:

  • wristwatches

  • pocket calculators

  • automobile keyless entry transmitter

  • hearing aids

They are generally of a compact size, 5-25mm in diameter and 1-6mm in height. The name defines the size of the battery as for CR2025, the first two digits are for the diameter and the second for the height or thickness of tenths of mm. Therefore, 20mm is the diameter of CR2025, and 2.5mm is the thickness.

Lithium button or coin cell batteries are a bit more expensive than alkaline, ones but last longer, weigh less, and have a wide operating temperature range.


CR1616 vs CR2025: Difference in Specifications


CR2025CR1616
Battery typeCoin Manganese Dioxide Lithium BatteriesCoin Manganese Dioxide Lithium Batteries
Nominal Voltage3.0V3.0V
Nominal Capacity160mAh55mAh
Standard Discharge Current0.2mA0.1mA
Operating Temperature Range-30℃ to 70℃-30℃ to 60℃
Diameter (mm)20mm16mm
Height (mm)2.5mm1.6mm
IEC (JIS)CR2025CR1616
Mass (oz)0.0917oz0.0388oz
Mass (g)2.6g1.1g


CR1616 vs CR2025: Difference in Dimensions

CR1616 Dimensions.jpg

CR1616 Dimensions

CR2025 Dimensions.jpg

CR2025 Dimensions

CR1616 vs CR2025: Difference in Applications

The 1616 battery is used for:

Heart Rate Monitors, Watches, Cameras, Calculators, Car Security Alarm, Keyless Car Remotes, Organizers, Glucometer, Computer Equipment (memory backup battery) CMOS, Toys, Communication Equipment, data pack for video cameras, and other devices that requires this battery size

 

CR2025 Works in Watches, computer motherboards, calculators, PDAs, electronic organizers, garage door openers, toys, games, door chimes, pet collars, LED lights, sporting goods, pedometers, calorie counters, stopwatches, medical devices, PCMCIA static RAM memory cards, Small PDA devices, Various electronic toys, Laser pointers, Digital thermometers, Digital altimeter, Cyclocomputers, Heart rate monitors


CR1616 vs CR2025: Difference in Equivalents

CR1616 Equivalent Batteries:

CR1616, DL1616, ECR1616, BR1616, 280-209, DL 1616B, CR1616-1W, LM1616, KCR1616, 5021LC, L11, L28

 

CR2025 Equivalent to: 

CR2025, DL2025, ECR2025, NA, BR2025, 208-205, DL20256B, BR2025-1W, CR2025-1W, KCR2025


CR1616 vs CR2025: Difference in Pros and Cons


CR2025CR1616
Pros1. Higher capacity, which will lead to a longer life.1. It takes less space, and you won’t worry   about damaging the battery when you put it in the device

2. Perfect for watches, heart monitor scans,   and hearing aids.2. It is best used for children’s toys and calculators.

3. Ideal size for replacing batteries in Pokemon, Zelda, and similar games that require a battery to save3. Small size is ideal for games that allow only a small physical space for the saved game battery
ConsTakes more space1. Less capacity


2. Shorter duration


CR1616 vs CR2025: Similarity in Features

  • Lightweight, High Voltage, and High Energy Density

The battery voltage is 3V, almost double that of normal alkaline or manganese batteries. This means that the number of batteries required for equipment can be halved for maximum space-saving and weight reduction.

  • Excellent Discharge Characteristics

Voltage characteristics remain stable even for a long period of discharge, greatly improving the reliability of equipment that uses the battery. Such equipment is also maintenance-free (battery replacement is seldom required).

  • Excellent Leakage Resistance

The newly developed battery construction and electrolyte ensure maximum leakage resistance over a long span of time.

  • Excellent Long-Term Reliability

Carefully selected active materials are used for the active material as well as for the electrolyte.

  • RoHS  Directive / European Directives

This product does not contain Mercury(Hg), Cadmium(Cd), nor Lead(Pb), and conforms to EC regulation values. (Directive 2006/66/EC, 2013/56/EU)

Battery packs are excluded from the RoHS directive (DIRECTIVE 2011/65/EU OF THE EUROPEAN PARLIAMENT AND OF THE COUNCIL of 8 June 2011 on the restriction of the use of certain hazardous substances in electrical and electronic equipment).


CR1616 vs CR2025: Similarity in Pros and Cons

pros

It comes with a lightweight coin-looking design

High voltage output

The energy density is very high compared to the size

Slow discharge increases the usable time

Great leakage resistance is included

Ensures long-term reliability

Cons

This battery is allowed for single-use

Non-rechargeable


Can I use a CR2025 battery instead of a CR1616?

Because CR1616 batteries and CR2025 batteries have the same voltage, they can be used interchangeably. However, because 2025s are a few millimeters thicker than the 1616s, they might not fit in cartridges that originally included 1616s.


Warning:

       Although CR1616 should NOT contain mercury or any other heavy metal like cadmium or similar, they are small and compact and even kids can swallow them.

     That is why most manufacturers package their CR1616 and similar batteries in 'child safe' packages which require some strength to be opened without tools of some kind. If these batteries are swallowed, induce vomiting right away and call emergency services and act according to their instructions!


Frequently Asked Questions

What does CR stand for in batteries?

CR is the generic designation that is used by the entire batteries maker but lithium batteries are also having chromium. All the batteries that have this chemical substance in their batteries can use this abbreviation CR. On the other DL is the short abbreviation of the battery-making company Duracell.

Is 2025 battery same as 2032?

2032 and 2025 are literally the dimensions of the battery. 2032 is 20mm in diameter, 3.2mm thick, and 2025 is slightly thinner, at 2.5mm thick. They usually both have the same voltage (3V) and assuming they fit in the case, they are interchangeable.

What battery is equivalent to CR2025?

Although there are no exact equivalent batteries to the CR2025, there are multiple batteries that may act as suitable substitutions. The CR2016 and CR2032 are exchangeable with the CR2025, but users must consider space limitations. The CR2016, CR2025, and CR2032 cell batteries all have the same voltage.

Can I use cr2025 instead of cr1616?

Technically they are cross-compatible if a CR2032 can fit into the spot for a CR1616, though this is very unlikely.

How do I know if my lithium ion battery is bad?

Without an analyzer, or running runtime test, etc, the easiest way to tell that a Li-Ion cell is nearing its EOL, is that it will not hold a charge well, and will not perform as well it used to and will get noticeably warmer when charging.
CR2025

FDK America, Inc., a member of Fujitsu Group

In Stock

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe

Related Parts More
  • CR12600SE
    CR12600SE

    FDK America, Inc., a member of Fujitsu Group

  • CR2430
    CR2430

    FDK America, Inc., a member of Fujitsu Group

  • CR17335E-R
    CR17335E-R

    FDK America, Inc., a member of Fujitsu Group

  • CR14250SE
    CR14250SE

    FDK America, Inc., a member of Fujitsu Group

  • LR03 G07 (2S)
    LR03 G07 (2S)

    FDK America, Inc., a member of Fujitsu Group

  • LR03RS
    LR03RS

    FDK America, Inc., a member of Fujitsu Group

  • LR6RS
    LR6RS

    FDK America, Inc., a member of Fujitsu Group

  • CR123A
    CR123A

    FDK America, Inc., a member of Fujitsu Group

  • CR17335SET-FT
    CR17335SET-FT

    FDK America, Inc., a member of Fujitsu Group

  • LR03 C (2S)
    LR03 C (2S)

    FDK America, Inc., a member of Fujitsu Group