SI4410DY: datasheet, package,pinout and applications
N-Channel 1V@250uA 13.5mΩ@10A,10V MOSFET
SI4410DY is 30v N-channel MOSFET in SOP8. This passage is going to introduce SI4410DY from the perspectives of datasheet, specifications, package, and CAD models.
SI4410DY Description
Utmei Electronics distributes the SI4410DY, which is manufactured by Onsemi. It falls under the Electronic Components ICs category.
It is used in a variety of fields, including automotive hybrid, electric, and powertrain systems. Communication devises Enterprise systems Datacenter & enterprise computing Datacom module
And the main parameters of this section are N-ch Mosfet 30V 10A 8-SOIC. It is also environmentally friendly and RoHS compliant (lead-free / RoHS compliant). This N-Channel Logic Level MOSFET is manufactured using Fairchild Semiconductor's advanced PowerTrench process, which is specifically designed to minimize on-state resistance while maintaining superior switching performance.
This device is ideal for low voltage and battery-powered applications that require low in-line power loss and fast switching.
SI4410DY Features
„ Low conduction losses due to low on-state resistance
„ Suitable for high-frequency applications due to fast switching
characteristics
SI4410DY Applications
Automotive
Advanced driver assistance systems (ADAS)/Body electronics & lighting/Hybrid, electric & powertrain systems/Infotainment & cluster
Communications equipment
Broadband fixed-line access/Datacom module/Wired networking/Wireless infrastructure
Enterprise systems
Datacenter & enterprise computing/Enterprise machine/Enterprise projectors
SI4410DY CAD Modals
Symbol

Footprint

3D Models

SI4410DY Manufacturer
Onsemi is an American semiconductor supplier company that was previously in the Fortune 500 but dropped to the Fortune 1000 (ranked 512) in 2020. Power and signal management, logic, discrete, and custom devices for automotive, communications, computing, consumer, industrial, LED lighting, medical, military/aerospace, and power applications are among the company's offerings. Onsemi operates a network of manufacturing facilities, sales offices, and design centers throughout North America, Europe, and the Asia Pacific. Onsemi, headquartered in Phoenix, Arizona, has $3.907 billion in revenue, ranking it among the top 20 semiconductor sales leaders in the world.
SI4410DY Package

SO-8

Package Dimensions
SI4410DY Alternatives
DMN3016LSS-13, which is produced by Diodes Incorporated is an ideal alternative to SI4410DY.
SI4410DY Pinning Information

| Pin | Symbol | Description |
| 1 | S | source |
| 2 | S | source |
| 3 | S | source |
| 4 | G | gate |
| 5 | D | drain |
| 6 | D | drain |
| 7 | D | drain |
| 8 | D | drain |
Specifications
- TypeParameter
- Package / Case
refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.
SOIC-8_150mil - Power Dissipation (Max)2.5W
- Current - Continuous Drain (Id) @ 25℃10A
- Packaging
Semiconductor package is a carrier / shell used to contain and cover one or more semiconductor components or integrated circuits. The material of the shell can be metal, plastic, glass or ceramic.
Tape & Reel (TR) - FET Type
"FET Type" refers to the type of Field-Effect Transistor (FET) being used in an electronic component. FETs are three-terminal semiconductor devices that can be classified into different types based on their construction and operation. The main types of FETs include Metal-Oxide-Semiconductor FETs (MOSFETs), Junction FETs (JFETs), and Insulated-Gate Bipolar Transistors (IGBTs).Each type of FET has its own unique characteristics and applications. MOSFETs are commonly used in digital circuits due to their high input impedance and low power consumption. JFETs are often used in low-noise amplifiers and switching circuits. IGBTs combine the high input impedance of MOSFETs with the high current-carrying capability of bipolar transistors, making them suitable for high-power applications like motor control and power inverters.When selecting an electronic component, understanding the FET type is crucial as it determines the device's performance and suitability for a specific application. It is important to consider factors such as voltage ratings, current handling capabilities, switching speeds, and power dissipation when choosing the right FET type for a particular circuit design.
N-Channel - Rds On (Max) @ Id, Vgs
Rds On (Max) @ Id, Vgs refers to the maximum on-resistance of a MOSFET or similar transistor when it is fully turned on or in the saturation region. It is specified at a given drain current (Id) and gate-source voltage (Vgs). This parameter indicates how much resistance the component will offer when conducting, impacting power loss and efficiency in a circuit. Lower Rds On values are preferred for better performance in switching applications.
13.5mΩ@10A,10V - Vgs(th) (Max) @ Id
The parameter "Vgs(th) (Max) @ Id" in electronic components refers to the maximum gate-source threshold voltage at a specified drain current (Id). This parameter is commonly found in field-effect transistors (FETs) and is used to define the minimum voltage required at the gate terminal to turn on the transistor and allow current to flow from the drain to the source. The maximum value indicates the upper limit of this threshold voltage under specified operating conditions. It is an important parameter for determining the proper biasing and operating conditions of the FET in a circuit to ensure proper functionality and performance.
1V@250uA - Drain to Source Voltage (Vdss)
The Drain to Source Voltage (Vdss) is a key parameter in electronic components, particularly in field-effect transistors (FETs) such as MOSFETs. It refers to the maximum voltage that can be applied between the drain and source terminals of the FET without causing damage to the component. Exceeding this voltage limit can lead to breakdown and potentially permanent damage to the device.Vdss is an important specification to consider when designing or selecting components for a circuit, as it determines the operating range and reliability of the FET. It is crucial to ensure that the Vdss rating of the component is higher than the maximum voltage expected in the circuit to prevent failures and ensure proper functionality.In summary, the Drain to Source Voltage (Vdss) is a critical parameter that defines the maximum voltage tolerance of a FET component and plays a significant role in determining the overall performance and reliability of electronic circuits.
30V - RoHS Status
RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.
RoHS Compliant
Trend Analysis
Parts with Similar Specs
What’s the advantages of OptiMOS™ 5 Power MOSFET 175°C in SuperSO8 package?
* Higher reliability: 175°C TJ_MAX provides longer service life at the same operating junction temperature * Higher operating temperature: 175°C TJ_MAX provides more power at higher operating junction temperatures * Highest system reliability * heat resistance
What’s the difference between LS and LSI?
The I in the SI suffix stands for an additional feature of OptiMOS™ products (Super Barrier Diode, Monolithic integrated Schottky like diode).
What’s the advantages of SI4410DY?
In line with the RoHS With the industry's advanced quality Low switching energy consumption Low on-state loss
Can SI4410DY be operated in the temperature of 100℃?
Yes, its operating temperature is suitable for -55-175℃.
What kind of package does SI4410D use?
SO-8
AD7794 Integration Notes: Resolving SPI Drops, Gain Errors, and ADC Replacement Constraints27 April 2026514
The Guide to MB10S Bridge Rectifier [FAQ]18 April 20226530
BMP085 Pressure Sensor: Datasheet, Pinout, BMP085 vs.BMP18001 November 20213319
ST2001FX Transistor: Datasheet, Pinout, Application09 August 20212080
CD4027 JK Flip-Flop IC:Pinout, Diagram and Datasheet12 August 20217939
S3K DIODE GEN PURP 800V 3A SMC: S3K Marking Information, Key parameters and Applications10 January 2022861
PIC16F1776ISS Microcontroller Datasheet Overview29 February 2024305
L293D Vs. L298N: What’s The Difference?20 December 202326489
What is Spectrum Analyzer?17 December 20215601
Beginner's Guide to Cache Memory26 February 20217330
Using Microcontrollers in the Internet of Things (IoT) Applications27 June 20236884
An Overview of Common Mode Chokes10 August 202015978
Ceramic Capacitors vs Film Capacitors: A Comprehensive Comparison Guide14 May 20257643
The U.S. Semiconductor Sector Faces Workforce Challenges Amidst Surging Demand27 November 20233981
Analysis and Solutions of Common Causes of Serial Port Lost Data15 August 20225572
Apple M1 Ultra -- The Technology Behind the Chip Interconnection12 March 20227415
Vishay Intertech
In Stock
United States
China
Canada
Japan
Russia
Germany
United Kingdom
Singapore
Italy
Hong Kong(China)
Taiwan(China)
France
Korea
Mexico
Netherlands
Malaysia
Austria
Spain
Switzerland
Poland
Thailand
Vietnam
India
United Arab Emirates
Afghanistan
Åland Islands
Albania
Algeria
American Samoa
Andorra
Angola
Anguilla
Antigua & Barbuda
Argentina
Armenia
Aruba
Australia
Azerbaijan
Bahamas
Bahrain
Bangladesh
Barbados
Belarus
Belgium
Belize
Benin
Bermuda
Bhutan
Bolivia
Bonaire, Sint Eustatius and Saba
Bosnia & Herzegovina
Botswana
Brazil
British Indian Ocean Territory
British Virgin Islands
Brunei
Bulgaria
Burkina Faso
Burundi
Cabo Verde
Cambodia
Cameroon
Cayman Islands
Central African Republic
Chad
Chile
Christmas Island
Cocos (Keeling) Islands
Colombia
Comoros
Congo
Congo (DRC)
Cook Islands
Costa Rica
Côte d’Ivoire
Croatia
Cuba
Curaçao
Cyprus
Czechia
Denmark
Djibouti
Dominica
Dominican Republic
Ecuador
Egypt
El Salvador
Equatorial Guinea
Eritrea
Estonia
Eswatini
Ethiopia
Falkland Islands
Faroe Islands
Fiji
Finland
French Guiana
French Polynesia
Gabon
Gambia
Georgia
Ghana
Gibraltar
Greece
Greenland
Grenada
Guadeloupe
Guam
Guatemala
Guernsey
Guinea
Guinea-Bissau
Guyana
Haiti
Honduras
Hungary
Iceland
Indonesia
Iran
Iraq
Ireland
Isle of Man
Israel
Jamaica
Jersey
Jordan
Kazakhstan
Kenya
Kiribati
Kosovo
Kuwait
Kyrgyzstan
Laos
Latvia
Lebanon
Lesotho
Liberia
Libya
Liechtenstein
Lithuania
Luxembourg
Macao(China)
Madagascar
Malawi
Maldives
Mali
Malta
Marshall Islands
Martinique
Mauritania
Mauritius
Mayotte
Micronesia
Moldova
Monaco
Mongolia
Montenegro
Montserrat
Morocco
Mozambique
Myanmar
Namibia
Nauru
Nepal
New Caledonia
New Zealand
Nicaragua
Niger
Nigeria
Niue
Norfolk Island
North Korea
North Macedonia
Northern Mariana Islands
Norway
Oman
Pakistan
Palau
Palestinian Authority
Panama
Papua New Guinea
Paraguay
Peru
Philippines
Pitcairn Islands
Portugal
Puerto Rico
Qatar
Réunion
Romania
Rwanda
Samoa
San Marino
São Tomé & Príncipe
Saudi Arabia
Senegal
Serbia
Seychelles
Sierra Leone
Sint Maarten
Slovakia
Slovenia
Solomon Islands
Somalia
South Africa
South Sudan
Sri Lanka
St Helena, Ascension, Tristan da Cunha
St. Barthélemy
St. Kitts & Nevis
St. Lucia
St. Martin
St. Pierre & Miquelon
St. Vincent & Grenadines
Sudan
Suriname
Svalbard & Jan Mayen
Sweden
Syria
Tajikistan
Tanzania
Timor-Leste
Togo
Tokelau
Tonga
Trinidad & Tobago
Tunisia
Turkey
Turkmenistan
Turks & Caicos Islands
Tuvalu
U.S. Outlying Islands
U.S. Virgin Islands
Uganda
Ukraine
Uruguay
Uzbekistan
Vanuatu
Vatican City
Venezuela
Wallis & Futuna
Yemen
Zambia
Zimbabwe


Product
Brand
Articles
Tools