Can a 1616 battery be replaced by a 1620?
BATTERY LITHIUM 3V COIN 16MM
The CR1616 and CR1620 batteries are the most important of all the CR batteries. You'll see that they're used all around the world. The CR1616 and CR1620 batteries are also Chinese-made. Today, we'll discuss whether CR1616 can be replaced by CR1620.

Can a 1616 battery be replaced by a 1620?
CR1616 Overview

The CR1616 is a 3V/50mAh coin cell Non-rechargeable Battery that features lithium technology. It is suitable for use with low drain devices and high-temperature applications. It features pressure contact terminals.
CR1620 Overview

The CR1620 is a 3V/70mAh coin cell Non-rechargeable Battery that features lithium technology. It is suitable for use with low drain devices and high-temperature applications. It features pressure contact terminals.
CR1616 vs CR1620: Specifications
| CR1616 | CR1620 | |
| Capacity | 55 mAh | 75 mAh |
| Chemistry | Lithium Manganese Dioxide | Lithium Manganese Dioxide |
| Mounting | Holder | Holder |
| Operating Temperature | -30 to 60 °C | -30 to 60 °C |
| Product Dimensions | 16 x 1.6 mm | 16 x 2 mm |
| Screening Level | Commercial | Commercial |
| Shape | Coin | Coin |
| Terminals | Pressure Contact | Pressure Contact |
| Weight | 1.2 g | 1.3g |
| Output Voltage | 3 V | 3 V |
| Voltage Rating | 3 V | 3 V |
| Height | 1.524 mm | 2mm |
CR1616 vs CR1620: Dimensions

CR1616 Dimensions

CR1620 Dimensions
CR1616 vs CR1620: Features and Benefits
CR1616
Good pulse capability
High discharge characteristics
Stable voltage level during discharge
Long-term reliability
CR1620
High Energy & Continuous Voltage Supply
Long shelf Life
Ideal Temperature Resistance
Superior Storage capacity
CR1616 vs CR1620: Applications
CR1616 battery is used for:
Heart Rate Monitor, Watches, Cameras, Calculators, Car Security Alarm, Keyless Car Remotes, Organizers, Glucometer, Computer Equipment (memory backup battery) CMOS, Toys, Communication Equipment, data pack for video cameras, and other devices that requires this battery size
CR1620 battery is used for:
car security (car alarm/keyfob batteries), organizer (backup battery for PDA such as Psion, etc), glucometer, camera, electric thermometer, calculator, computer equipment (memory backup battery), toys, communication equipment, electronic watches/clocks, card radios, data pack for a video camera, Watches, pagers, and other electronic devices.
CR1616 vs CR1620: Equivalents
CR1616 vs CR1620: Durability
A 1616 battery does not have an expiration date. It does, however, have an average lifespan. This sort of battery usually lasts between 5 and 10 years.
A CR1620 battery, on the other hand, typically lasts 7 to 10 years. These batteries, obviously, have a longer lifespan. As a result, you'll see it in heavy-duty professions like computer equipment, video cameras, and various communication devices.
Can I use CR1616 instead of CR1620?
CR1616 and CR1620 are both non-rechargeable manganese-dioxide lithium batteries that have the same diameter of 16.0 mm, but they differ in height and thus the capacity and other features like drain currents and similar:
- CR1616 battery: 16.0 x 1.6 mm, 50-55 mAh,
- CR1620 battery: 16.0 x 2.0 mm, 65-80 mAh.
While most battery compartments that can accept a CR1620 battery can also accept a CR1616 battery, it is not recommended to replace a CR1620 battery with a CR1616 battery due to the lower capacity and somewhat lower maximum drain/pulse currents that can cause the device to malfunction.
Using Warm
Like all similar small and shiny objects (another button/coin cell batteries included), CR1620 batteries can be swallowed by kids and pets - that is why these batteries come in so-called 'pets-safe' and 'kids-safe' packages.
Although CR1620 batteries don't contain mercury, cadmium, lead, or any other toxic heavy metals and similar pollutants, they are very dangerous when swallowed - if swallowed, they can cause chemical burns and physical damage to internal organs.
If CR1620 batteries (or any similar battery) get swallowed, immediately contact the nearest emergency center (or doctor), explain what happened, and act according to their instructions.
What uses CR1616 battery?
The CR1616 is a coin cell battery that works in many smaller electronic devices. It is able to power key fobs, glucometers, heart rate monitors, toys, computer backup equipment, and more. One of its most popular uses is in the Honda and Lexus key fobs, but it is also used in many other car brands and devices.
How long does a CR1616 battery last?
5-10 years
Is 1620 battery the same as 1616?
CR1616 and CR1620 are both non-rechargeable manganese-dioxide lithium batteries that have the same diameter of 16.0 mm, but they differ in height and thus the capacity and other features like drain currents and similar: – CR1616 battery: 16.0 x 1.6 mm, 50-55 mAh, – CR1620 battery: 16.0 x 2.0 mm, 65-80 mAh.
What battery can replace a CR1616?
Common labels for CR1616 equivalent batteries are DL1616, BR1616, ECR1616, 280-209, GPCR1616, LiR1616, KCR1616, 5021LC etc.
Can you use CR2025 instead of CR1616?
Exact same batteries are used by all GameBoy games. All GameBoy games that use battery back-ups use either CR2025 or CR1616 coin cell batteries. A CR2025 coin cell battery is 20mm wide while a CR1616 coin cell battery is 16mm wide. In order to open your game cartridges, you will need a security bit.
AD5241 Integration Notes: Addressing I2C Failures, Thermal Issues, and Dual-Supply Trade-offs25 April 2026323
2SC2625 NPN Power Transistor: Equivalent, Datasheet pdf and Pinout12 November 20219969
MC68HC705C8ACFNE: Trusted Sourcing Guide for Microcontroller Components07 June 2025424
STPS2045CT Rectifier: Circuit, Pinout, and Datasheet11 October 20218300
AT89S52-24PU Microcontroller: Diagram, Pinout, and Datasheet04 March 20229423
CR1220 Lithium Coin Battery: Datasheet, Equivalent and CR1220 vs BR122029 April 202210724
S9014 Transistor: Pinout, Datasheet and Circuit [Video&FAQ]28 September 202148215
A Comprehensive Guide to LTC7880IUKG#TRPBF DC/DC Switching Controller06 March 2024358
MCU with Built-in NPU: How to Pick an Edge AI Microcontroller in 202630 July 20261485
A Guide to Selecting the Ideal Microphone for Your Audio Needs15 May 20232248
Exploring SPI Communication for Faster Data Transfer20 June 20251711
Best 1N4007 diode alternatives to use in 202525 August 20259722
Classification and Application of UV Sensor20 October 20215708
How Many Smart Sensors Should a Car Be Equipped With?28 March 20224929
What is LCD? Working Principle, Features, and Future Trends05 January 202614248
What Size Wire for a 60 Amp Breaker? The Complete NEC Guide22 May 20267171
Panasonic - BSG
In Stock
United States
China
Canada
Japan
Russia
Germany
United Kingdom
Singapore
Italy
Hong Kong(China)
Taiwan(China)
France
Korea
Mexico
Netherlands
Malaysia
Austria
Spain
Switzerland
Poland
Thailand
Vietnam
India
United Arab Emirates
Afghanistan
Åland Islands
Albania
Algeria
American Samoa
Andorra
Angola
Anguilla
Antigua & Barbuda
Argentina
Armenia
Aruba
Australia
Azerbaijan
Bahamas
Bahrain
Bangladesh
Barbados
Belarus
Belgium
Belize
Benin
Bermuda
Bhutan
Bolivia
Bonaire, Sint Eustatius and Saba
Bosnia & Herzegovina
Botswana
Brazil
British Indian Ocean Territory
British Virgin Islands
Brunei
Bulgaria
Burkina Faso
Burundi
Cabo Verde
Cambodia
Cameroon
Cayman Islands
Central African Republic
Chad
Chile
Christmas Island
Cocos (Keeling) Islands
Colombia
Comoros
Congo
Congo (DRC)
Cook Islands
Costa Rica
Côte d’Ivoire
Croatia
Cuba
Curaçao
Cyprus
Czechia
Denmark
Djibouti
Dominica
Dominican Republic
Ecuador
Egypt
El Salvador
Equatorial Guinea
Eritrea
Estonia
Eswatini
Ethiopia
Falkland Islands
Faroe Islands
Fiji
Finland
French Guiana
French Polynesia
Gabon
Gambia
Georgia
Ghana
Gibraltar
Greece
Greenland
Grenada
Guadeloupe
Guam
Guatemala
Guernsey
Guinea
Guinea-Bissau
Guyana
Haiti
Honduras
Hungary
Iceland
Indonesia
Iran
Iraq
Ireland
Isle of Man
Israel
Jamaica
Jersey
Jordan
Kazakhstan
Kenya
Kiribati
Kosovo
Kuwait
Kyrgyzstan
Laos
Latvia
Lebanon
Lesotho
Liberia
Libya
Liechtenstein
Lithuania
Luxembourg
Macao(China)
Madagascar
Malawi
Maldives
Mali
Malta
Marshall Islands
Martinique
Mauritania
Mauritius
Mayotte
Micronesia
Moldova
Monaco
Mongolia
Montenegro
Montserrat
Morocco
Mozambique
Myanmar
Namibia
Nauru
Nepal
New Caledonia
New Zealand
Nicaragua
Niger
Nigeria
Niue
Norfolk Island
North Korea
North Macedonia
Northern Mariana Islands
Norway
Oman
Pakistan
Palau
Palestinian Authority
Panama
Papua New Guinea
Paraguay
Peru
Philippines
Pitcairn Islands
Portugal
Puerto Rico
Qatar
Réunion
Romania
Rwanda
Samoa
San Marino
São Tomé & Príncipe
Saudi Arabia
Senegal
Serbia
Seychelles
Sierra Leone
Sint Maarten
Slovakia
Slovenia
Solomon Islands
Somalia
South Africa
South Sudan
Sri Lanka
St Helena, Ascension, Tristan da Cunha
St. Barthélemy
St. Kitts & Nevis
St. Lucia
St. Martin
St. Pierre & Miquelon
St. Vincent & Grenadines
Sudan
Suriname
Svalbard & Jan Mayen
Sweden
Syria
Tajikistan
Tanzania
Timor-Leste
Togo
Tokelau
Tonga
Trinidad & Tobago
Tunisia
Turkey
Turkmenistan
Turks & Caicos Islands
Tuvalu
U.S. Outlying Islands
U.S. Virgin Islands
Uganda
Ukraine
Uruguay
Uzbekistan
Vanuatu
Vatican City
Venezuela
Wallis & Futuna
Yemen
Zambia
Zimbabwe


Product
Brand
Articles
Tools