Always charge the battery to 100%? Stop it!

20+ Tricks to Charge Phone Battery Faster and Safer
| Topics covered in this article: |
| Ⅰ. Key point |
| Ⅱ. The working principle of lithium-ion battery |
| Ⅲ. Why is my battery draining so fast? |
| Ⅳ. Regarding charging, are these statements reasonable? |
Ⅰ. Key point
★The best approach to charge your phone is to do a shallow charge and shallow discharge, which means charging when the battery is empty and pulling out when the charge is finished.
★When the phone is too hot or too cold, don't charge it.
★Keep your phone's battery at half when you are not using it for an extended period of time.

Source: Internet
Mobile phones are no longer just a means of communication; they are also playing an increasingly essential role in business, leisure, and social contact. The most concerning aspect of using a mobile phone is the low battery reminder.
When the battery level on their mobile phone dropped below 20%, 90% of participants felt "panic," according to a survey done by LG in 2016. Despite the fact that major manufacturers are working hard to increase the capacity of mobile phone batteries, most people have progressively switched from one-day charging to one-day charge, or even less, as the frequency and intensity of mobile phone use in daily life have increased. People will bring power banks with them when they go out in case of an emergency.
So, when we use our phones on a regular basis, what can we do to maximize the battery life of our phones?
Ⅱ. The working principle of lithium-ion battery
Currently, the majority of lithium-ion batteries used in mobile phones are Nobel Prize-winning inventions. Lithium-ion batteries offer a large capacity, small size, high voltage platform, and extended cycle life as compared to older batteries like nickel-metal hydride, zinc-manganese, and lead storage. Mobile phones can be utilized as a result of their advantages, such as their smaller size and longer battery life.
For the anode, LiCoO2 (lithium cobalt oxide), NCM, and NCA materials are commonly used in mobile phones; anode materials in mobile phones include artificial graphite, natural graphite, MCMB, SiO, and others. Lithium is removed from the positive electrode in the form of lithium ions and then implanted in the negative electrode through the movement of the electrolyte in the charging process, whereas the discharge process is the polar opposite. As a result, the charging and discharging process is a continuous cycle of insertion/de-intercalation and insertion/de-intercalation of lithium ions between the positive and negative electrodes, sometimes known as the "rocking chair battery."

Working Principle of lithium-ion batteries
Ⅲ. Why is my battery draining so fast?
The battery life of a newly purchased mobile phone is not bad at first, but it will become less and less durable after a period of use. For example, a fully charged new phone can last 36 to 48 hours, but more than half a year later, the same full power can only last 24 hours or less.
What is the rationale behind mobile phone batteries being "life-saving"? The following are the key reasons:
① Overcharge and over-discharge
Lithium ions must travel between the positive and negative electrodes for lithium-ion batteries to work. As a result, the quantity of lithium ions that a lithium-ion battery's positive and negative electrodes can contain is proportional to its capacity. When a lithium-ion battery is charged and drained repeatedly, the structure of the positive and negative materials may be destroyed, and the space available to accommodate lithium ions decreases, resulting in a reduction in battery capacity and life.

Before (a) after 50 times of deep charge and discharge (b) the result of electron microscopy of LiCoO2 cathode material
The LiCoO2 after deep charge and discharge has structural damage
The lithium-ion battery's capacity can be maintained at more than 80% of the number of charge and discharge cycles, which is how cycle life is commonly measured.
The national standard GB/T18287 stipulates that lithium-ion batteries in mobile phones must have a cycle life of at least 300 times. Is this to say that after 300 charges and discharges, our cellphone batteries will become less durable? No, the answer is no.
First, the attenuation of battery capacity during cycle life measurement is a gradual process, not a cliff or step; second, the lithium-ion battery is deeply charged and discharged, and during daily use, the battery is deeply charged and discharged; and third, the lithium-ion battery is deeply charged and discharged, and the battery is deeply charged and discharged. The management system has a battery protection function. When the battery is fully charged, it will automatically power off, and when the battery is low, it will immediately shut down, avoiding as much deep charging and discharging as possible. As a result, the battery of a mobile phone has a life span of more than 300 times.
However, we cannot rely solely on a superior battery management system. Leaving a phone on low or full power for an extended period of time might harm the battery and lower its capacity. As a result, the ideal approach to charge and discharge a mobile phone is to do so in short bursts. Maintaining 50% of the phone's power when it is not in use for an extended period of time will successfully extend its service life.

② Charging under too cold or too hot conditions
Lithium-ion batteries have greater temperature needs, with a usual working (discharge) temperature range of 0°C to 35°C. The electrolyte ion conductivity falls at low temperatures, the charge transfer resistance rises, and the performance of lithium-ion batteries degrades. The decrease in capacity is the intuitive experience. This capability loss, on the other hand, is reversible. The performance of the lithium-ion battery will revert to normal once the temperature returns to room temperature.
However, if the battery is charged at a low temperature, the polarization of the negative electrode may cause its potential to approach the lithium metal reduction potential, resulting in lithium metal deposition on the negative electrode's surface. As a result, battery capacity will be reduced. Lithium, on the other hand, is a substance. Dendrite creation has the potential to short circuit the battery, posing a threat.
Charging a lithium-ion battery at high temperatures changes the structure of the positive and negative electrodes, resulting in irreversible capacity loss. As a result, try to avoid charging the phone in extreme cold or heat, as this will help to extend its service life.

Too cold conditon
Ⅳ. Regarding charging, are these statements reasonable?
① Will charging all night affect the battery life of the mobile phone?
Overcharging and discharging the battery will shorten its life, however, charging overnight is not the same as overcharging. On the one hand, once the phone is fully charged, it will turn off automatically; on the other hand, many phones now employ a fast charging method that involves charging the battery to 80% capacity and then switching to a slower trickle charge. As a result, you are free to charge your phone as you sleep. Engineers have taken these concerns into account for everyone involved in the design.
② The summer weather is very hot, and the mobile phone will have a high temperature when charging. Is this normal, or does it mean that there is a problem with the battery of the mobile phone?
Complex processes such as chemical reactions and charge transfer accompany battery charging. Heat is typically generated as a result of these processes. As a result, it is typical for mobile phones to create heat when they are being charged. Poor heat dissipation and other factors, rather than problems with the battery, are to blame for the high temperature and hot phenomenon of mobile phones. Removing the protective cover when charging allows the phone to disperse heat more effectively, potentially extending the phone's service life.
③ Will the battery life of the mobile phone be affected by the power bank and car charger charging the mobile phone?
not going to happen. Using a power bank or a car charger to charge your phone will not damage the battery's service life as long as you use a charging method that meets national standards.
④ Plug the charging cable into the computer to charge the mobile phone and connect the charging plug to the power socket to charge the mobile phone. Is the charging efficiency the same?
The charging rate is only connected to the charging power supported by the charger and mobile phone, whether it is charged using a power bank, car charger, computer, or simply plugged into the power source. A 5W charger (5V=1A) charges at a faster rate than an 18W charger. The charger is sluggish (9V=2A).

Charging in car
⑤ Can the mobile phone be used while charging? What caused the previous case of "Electric death while calling while charging"?
When the phone is fully charged, it can be used. When charging the phone, the charger uses a transformer to convert 220V high-voltage AC power to low-voltage (often 5V) DC electricity to charge the battery. The cell phone is just attached to the low-voltage component. The human body's safe voltage is 36 volts in general. That is to say, even if the phone case leaks during regular charging, the low output voltage will not hurt the human body.
When it comes to important news on the Internet regarding "calling and being electrocuted while charging," the content is essentially reproduced. It's difficult to verify the original source of the information, and there's no report from any authority, such as the police, so judging the truth of the relevant news is difficult. sex. However, "the phone was electrocuted while charging" is alarmist when it comes to utilizing authorized charging equipment that fulfills national criteria to charge mobile phones. However, this serves as a reminder that when charging our phones, we must utilize chargers made by reputable manufacturers that comply with applicable national requirements.
Furthermore, do not disassemble the battery on your own while using your phone. When the battery becomes abnormal, such as bulging, cease using it immediately and have it replaced by the mobile phone maker to avoid any safety hazards caused by incorrect battery use.
1.Must the phone be fully charged?
Not really! It’s safest to keep your mobile phone at 30-80% of the battery. Too much "overcharge" will damage the phone, but start charging below 30% will cause the phone to "over-discharge", so the battery is too full or too full. The low state is hurting the battery.
2.Is it OK to charge the phone intermittently?
Not good, although in theory, the lithium battery has no memory function, intermittent charging is equivalent to repeated charging, which will shorten the battery life and lead to premature charging and dissatisfaction.
3.How long does it take to replace the battery of a mobile phone?
The service life of a mobile phone battery is about 2 years or more under normal use. The service life of the battery is related to the type of battery and the number of recharges. Lithium batteries can generally be recharged 350 to 700 times. If the following two situations occur, your phone battery needs to be replaced: 1. It cannot be used continuously for one day after being fully charged (the battery is aging); 2. The mobile phone will automatically turn off the power suddenly (the battery is broken);
Power Converter with Inbuilt Charging technology using WBG DevicesSaumitra Jagdale18 January 20242772Although plug-in electric vehicles (PEVs) have gained traction globally, reducing cost, weight, and volume, while enhancing power conversion efficiency in chargers remains crucial. PEVs, recognized by governments for curbing fossil fuel consumption and emissions, rely on sizable battery packs for substantial all-electric range coverage.
Read More
SR626SW Battery Equivalent: Technical Specs, Chemistries, and Selection GuideUTMEL26 May 20262053This comprehensive technical guide details the SR626SW battery, a widely used 1.55V silver oxide cell. It explains regional naming conventions, cross-referencing equivalents like the 377 and LR626, and highlights the performance differences between silver oxide and alkaline chemistries. Additionally, it offers product engineers and technicians essential handling best practices to avoid voltage drops and ensure device longevity.
Read More
How to Choose the Best Deep Cycle Battery in 2024 | Reviews and Buying GuideUTMEL21 July 20253070You will learn about deep-cycle batteries in this post, including their main characteristics, things to think about while selecting one, and more.
Read More
CR123A vs 123A Batteries Explained for 2025UTMEL27 May 20255923CR123A and 123A batteries differ in capacity, lifespan, and compatibility. Learn how these differences affect your device's performance and safety.
Read More
A Guide to the Best AG13 Battery SubstitutesUTMEL27 May 20253378Discover the top AG13 battery equivalents for 2025, including LR44, SR44, 357, and A76. Compare performance, compatibility, and cost for your devices.
Read More
Subscribe to Utmel !
45-1327G6Anderson Power Products, Inc.
SK2-076C040000-C70Anderson Power Products, Inc.
104G15Anderson Power Products, Inc.
45-6310G1Anderson Power Products, Inc.
114916P5Anderson Power Products, Inc.
SBS75GBLUAnderson Power Products, Inc.
G7924-17Glenair
52045-1545Molex
D3899922JFAmphenol Interconnect India
52807-1810Molex


Product
Brand
Articles
Tools