How much do you know about Button Battery?

How to Make a Coin Battery
Ⅰ. What is Button Battery?
A Button Battery is a battery that has the appearance of a button but is actually a lithium battery. Lithium batteries have the advantages of lightness, durability, high stability, and long-lasting power because lithium is the lightest metal. The downside is that the power is limited and the price is prohibitively high. As a result, precision instruments are the most common use.
There are two types of button batteries: rechargeable and non-rechargeable. 3.6V rechargeable lithium-ion button batteries (LIR series) and 3V rechargeable lithium-ion button batteries (ML or VL series) are among the rechargeable options; no 3V lithium manganese button batteries (CR series) and 1.5V alkaline zinc manganese button batteries are both rechargeable (LR and SR series).
AG3, AG10, and AG13 batteries are the most common button batteries found in toys and gifts. On the computer motherboard, the battery type is CR2032, which is the same as CR2025 in electronic dictionaries and CR2016 or SR44 and SR626 in electronic timepieces. The most popular and cheapest button batteries are carbon button batteries.
The type of battery is indicated by the English letter in front of the model name, the size is indicated by the number, the first two digits indicate the diameter, and the final two numbers indicate the thickness.
6F22 (9V), 4F22 (6V), 15F20 (22.5V), 10A (9V), 11A (6V), 23A (12V), 25A (9V), 26A (6V), 27A (12V), 476A (6V), 120H7D (8.4V), 2X625A (3V), and so on are common standard types.
Ⅱ. The characteristics of various types of Button Battery
Lithium battery
A lithium manganese battery (code C) with a nominal voltage of 3V is a typical disposable lithium battery.
A lithium-carbon fluoride battery (code B) with a nominal voltage of 3V is another less frequent form of disposable lithium battery.
In addition, the ML lithium battery (code-named ML) is a regularly used secondary lithium battery with a nominal voltage of 3V.
The new IEC numbering technique is typically used for lithium battery size numbers. The diameter (in mm) is the first two digits, and the thickness (in 0.1mm) is the last two digits, whichever is closest. The dimensions of CR2032, for example, are 20mm in diameter and 3.2mm in thickness.
Silver oxide
The button battery has extended service life, huge capacity, and a wide range of uses, with the largest application being the button battery. The positive pole is silver oxide, the negative pole is metal zinc powder, and the electrolyte is potassium hydroxide or sodium hydroxide. The chemical reaction between zinc and silver oxide produces electricity. The silver oxide button battery has five thickness (height) specifications: 5.4mm, 4.2mm, 3.6mm, 2.6mm, and 2.1mm, and four diameter specifications: 11.6mm, 9.5mm, 7.9mm, and 6.8mm. One of them should be chosen based on the size of the area.
Silver peroxide
The battery's construction is nearly identical to that of a silver oxide button battery. The key distinction is that the battery's anode (glen pole) is constructed of silver peroxide.
Basic Manganese
The battery has a huge capacity, outstanding low-temperature performance, inexpensive materials, and a low price, and it can handle continuous discharge at a high current. The drawback is that the energy density is insufficient, and the discharge voltage is unstable. Manganese dioxide serves as the positive pole, zinc serves as the negative pole, and potassium hydroxide serves as the electrolyte in alkaline manganese button batteries. 1.5V is the nominal voltage.
Mercury
It is also known as a mercury battery and has the ability to operate at high temperatures, as well as long-term storage, a constant discharge voltage, and superior mechanical features. However, it has poor low-temperature properties. The battery's positive electrode is mercury, the negative pole is zinc, and the electrolyte is either potassium or sodium hydroxide. It has a nominal voltage of 1.35 volts.
Lithium-ion
Lithium manganese disposable button batteries have a nominal voltage of 3V and a termination voltage of 2V.
Button Battery
0.1-0.2mA is the typical operating current. The cathode material is manganese dioxide, which has very stable chemical properties, and the anode material is lithium metal, which has a very high specific energy. The storage life is long, and the annual average capacity decline is less than 2%. The battery has a semi-sealed design and is completely safe to use. Disposable lithium-manganese button batteries have a wide temperature adaption range and can function normally in temperatures ranging from -20 to +60 degrees Celsius. It's commonly found in electronic dictionaries, motherboard CMOS batteries, and timepieces, among other things.
Secondary lithium
It's a secondary button battery and a rechargeable button battery with a nominal voltage of 3.7V and a charging voltage of 4.2V.
From the rear of the battery, you can see the appropriate mark.
LR---Alkaline--1.5V
SR---silver oxide--1.55V
CR---Lithium Battery--3V
ZA---Zinc Air--1.4V
LIR---secondary lithium battery--3.7V
Hammer
The battery offers a high energy density, excellent storage performance, low self-discharge, and long life. The internal resistance of the battery is relatively high, which is a negative. The battery's positive pole is made of raw materials such as manganese dioxide or iron disulfide, the negative pole is a hammer, and the electrolyte is organic matter. The Li/MnO hammer battery has a nominal voltage of 2.8V, whereas the Li(CF)n hammer battery has a nominal voltage of 3V.
Solder pin battery
In Taiwan and Hong Kong, a solder pin battery, also known as a pin battery or a pin battery, is referred to as a PIN battery.
In most cases, button batteries used to store power supplies for small devices, digital products, medical equipment, and other applications must be welded to a circuit board (PCBA). The battery slices are nickel-plated stainless steel strips with a hardness of steel strips. It is difficult to bend. Nickel plating adheres to electronic components and is difficult to remove. Soldering cannot link the battery and the steel strip directly, and the soldering is weak, prone to falling off, and has a narrow contact surface. Soldering is unprofessional for some antique crafts or tiny businesses that require it urgently.
Ⅲ. How to test a Button Battery with a multimeter?
1. Set up the multimeter and the battery to be checked, then plug in the red and black test lines.

2. To turn on the multimeter, press the "Power" button.

3. Select the voltage testing equipment.

4. The positive pole of the battery is linked to the red test wire, and the negative pole is connected to the black test wire.

5. Pay attention to the multimeter's display of power. If it reads 1.2V, the battery is fully charged. If the voltage reads 0V, the battery is dead.

Ⅳ. What happens if a Button Battery is swallowed?
When a coin-sized lithium battery becomes lodged in a child's throat, saliva causes an electric current to flow, causing a chemical reaction that badly burns the esophagus in just two hours. At this point, the youngster may cough, drool, or exhibit discomfort. Therefore, we need to keep the button batteries away from the children.
1.How to distinguish whether button batteries have electricity or not?
The button batteries can be used to measure the current to distinguish between electricity and electricity. You can use the multimeter's current gear to measure. The measurement result is much smaller than the rated current, that is, there is no electricity.
2.What's the hazards of button batteries?
Button batteries contain harmful substances such as mercury, lead, cadmium, acid, and alkali. If the metal on the outside of the battery is corroded, the substances inside will slowly leak out. Once these substances enter the soil or water, they will pollute the environment. The consequences can be imagined.
3.How to look at the front and back of button batteries?
There are words on the positive pole, and the entire surface and the surroundings are connected together. The negative pole is only one side, and the edge is separated from the positive pole by a circle, which is obvious.
Power Converter with Inbuilt Charging technology using WBG DevicesSaumitra Jagdale18 January 20242755Although plug-in electric vehicles (PEVs) have gained traction globally, reducing cost, weight, and volume, while enhancing power conversion efficiency in chargers remains crucial. PEVs, recognized by governments for curbing fossil fuel consumption and emissions, rely on sizable battery packs for substantial all-electric range coverage.
Read More
SR626SW Battery Equivalent: Technical Specs, Chemistries, and Selection GuideUTMEL26 May 20261908This comprehensive technical guide details the SR626SW battery, a widely used 1.55V silver oxide cell. It explains regional naming conventions, cross-referencing equivalents like the 377 and LR626, and highlights the performance differences between silver oxide and alkaline chemistries. Additionally, it offers product engineers and technicians essential handling best practices to avoid voltage drops and ensure device longevity.
Read More
How to Choose the Best Deep Cycle Battery in 2024 | Reviews and Buying GuideUTMEL21 July 20253052You will learn about deep-cycle batteries in this post, including their main characteristics, things to think about while selecting one, and more.
Read More
CR123A vs 123A Batteries Explained for 2025UTMEL27 May 20255822CR123A and 123A batteries differ in capacity, lifespan, and compatibility. Learn how these differences affect your device's performance and safety.
Read More
A Guide to the Best AG13 Battery SubstitutesUTMEL27 May 20253298Discover the top AG13 battery equivalents for 2025, including LR44, SR44, 357, and A76. Compare performance, compatibility, and cost for your devices.
Read More
Subscribe to Utmel !
P5916G6-BKAnderson Power Products, Inc.
52045-3045Molex
M22-1900005Harwin Inc.
R191455000Radiall USA, Inc.
R280222000Radiall USA, Inc.
SNT-100-BK-G-HSamtec Inc.
E6341G2Anderson Power Products, Inc.
83614-9016Molex
S1621-46RHarwin Inc.
52030-0629Molex


Product
Brand
Articles
Tools