What’s the relationship between CR2032 and CR2016?

Sophie

Published: 16 June 2022 | Last Updated: 16 June 2022

12482

CR2016

CR2016

Murata Electronics

CR STANDARD

Purchase Guide

CR STANDARD

Just like other batteries in the CR series, CR2016 and CR2032 are button batteries that seem very similar in many respects. By comparing the CR2032 and CR2016, we’ll see if the two are interchangeable, and what their differences are. The CR2016 and CR2032 are both small single-cell batteries with a squat cylinder shape. Here we will compare the main specs, voltage, thickness, chemistry, and other features of CR2032 and CR2016 batteries. These two button cells are very similar. For instance, they have the same diameter of 20 mm, so they can fit in the same device battery compartment. Nevertheless, some differences exist between the two.

This video is about the differences between CR2032 and CR2016.

CR2032 vs CR2016 – What is the Difference Between These Batteries

CR2016 Overview

The CR2016 lithium coin cell is a primary lithium battery with a voltage of 3V. The CR2016 lithium coin cell is a 3V Lithium battery with a long shelf life for back up energy, great temperature resistance, and superior storage capacity. This lithium coin cell battery has a high energy density, durability, and stability, as well as long battery life in a variety of applications.

cr2016.jpg

CR2032 Overview

The CR2032 battery is a non-rechargeable (primary) battery that is very common today. It is a coin-cell battery that utilizes lithium chemistry. These batteries are used in a wide range of applications and are available from many retailers.

cr2032.jpg

CR2016 VS CR2032: Diameter

The duo of CR2016 and CR2032 batteries have the same diameter of 20mm. The first two numbers of the battery name ‘20’ stand for the diameter. 


CR2016 VS CR2032: Depth

Depth is the only visual difference between these 2016 and 2032 batteries. The CR2016 battery has 1.6mm and the CR2032 battery has 3.2mm. The last two numbers of the battery names such as ‘16’ and ‘32’ stand for their respective depth.


CR2016 VS CR2032: Application

CR2016 Application

CR2016 power supplies have demonstrated their worth and are used more frequently than other power supplies with similar dimensions. The CR2016 battery is used in a wide variety of devices and applications including Watches, Calculators, PC notebooks, Electronic keys, Card-type radios, IC cards, Memory cards, Medical equipment, and CMOS memory backups.

 

CR2032 Application

The CR2032 battery is used in a wide variety of devices and applications including computer motherboards, car key fobs, watches, calculators, PDAs, electronic organizers, garage door openers, toys, games, door chimes, pet collars, LED lights, sporting goods, pedometers, calorie counters, stopwatches, and medical devices.


CR2016 VS CR2032: Operating Temperature

Each of the CR2016 and 2032 CMOS batteries works properly under the temperature range of 0°C to 60°C. But the range varies from battery to battery of different brands. If the operating temperature goes beyond the standard range, the battery will lose its capacity and the device will start malfunctioning or not work at all.


CR2016 VS CR2032: Weight

The weight of the CMOS batteries also varies with their depth. For CR2016, the weight is 2.3gram and for CR2032, the weight is 3.1gram.


CR2016 VS CR2032: Voltage

The nominal voltage for both the 2032 and 2016 CMOS batteries is the same, which is 3V. Because of this shared feature, both of the batteries can act as a replacement for another one.


CR2016 VS CR2032: Capacity

Capacity is one of the main differences between the CR2025 and CR2032 batteries. The 2032 CMOS battery offers more capacity which is 225 mAh. On the other hand, the 2016 CMOS battery capacity is only 90 mAh.


CR2016 VS CR2032: Comparison Table


CR2032CR2016
Nominal Voltage3 Volts3 Volts
Capacity 225 mAh90 mAh
Operating Temperature0°C ~ 60°C0°C ~ 60°C
Height:3.2mm1.6mm
Width (Diameter)20mm20mm
ChemistryLithium CoinLithium Coin
Weight3.1g1.7g


CR2016 VS CR2032: Rechargeability 

None of the 2032 and 2016 CMOS batteries are separately rechargeable. They only get charged via laptop while it is plugged in. 


The relationship between CR2016 and CR2032

CR2016 and CR2032 may vary in thickness, but they are identical in several ways.

They're both 3-volt versions, and none of them is rechargeable. However, it is important to remember that there are variations in ability. CR 2032 has a capacity of 240 mAh, while CR2016 has a capacity of just 90mAh. The CR2032 can provide 10 hours of use, while you only get about six hours from the CR2016, depending on the power you're using, of course.

Due to their equivalent voltage, there are several cases where CR2016 and CR2032 can be interchanged. However, the fact that they have different capacities and therefore different run times can cause problems. You will not get the power from the CR2016 that you will get from the CR2032, and some devices won't function at all.


CR2016 Safety Issues

Modern CR2016, BR2016, and LiR2016 batteries are made using no lead, cadmium, and similar heavy metals, but, they are nonetheless dangerous when swallowed.

With 20mm diameter, they are not easy to swallow, but just in case, keep them away from kids and pets. And if something like that happens, call emergency services right away.

Although they don't contain heavy elements, they can cause electrolytic reactions in the body that may be very harmful.

Fortunately, most CR2016 and similar batteries come in 'children safe' packages, making them generally inaccessible to children. IMHO, a very determined kid with scissors can open even such packages...


CR2016 VS CR2032: Datasheet

Frequently Asked Questions

Are all CR2016 batteries the same?

Although all CR2016 batteries feature the same chemistry and physical dimensions, they may differ in actual capacity, discharge features, self-discharge rate, operating temperature range, and similar.

What is the difference between a CR2032 and a CR2016 battery?

The main difference is the height (3.2 vs 1.6 mm), capacity, and drain currents.

What battery can replace CR2016?

Lithium 3.0V batteries that are labeled as ECR2016, DL2016, E-CR2016, SB-T11, 5000LC and similar can replace CR2016 batteries since they are different labels for the same battery - CR2016 battery.

What are CR2016 batteries used for?

CR2016 batteries are used for digital watches, credit-card size devices, remote controls, calculators, thermometers, Bluetooth sets, wearable electronics, CMOS memory, key chain LED flashlights, etc.

What Uses a CR2032 Battery?

The CR2032 battery is used in a wide variety of devices and applications including computer motherboards, car key fobs, watches, calculators, PDAs, electronic organizers, garage door openers, toys, games, door chimes, pet collars, LED lights, sporting goods, pedometers, calorie counters, stopwatches, and medical devices.
CR2016

Murata Electronics

In Stock

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe

Related Parts More