web counter

ULN2003A Seven Darlington Array: Pinout, Features and Datasheet

Sophie

Published: 18 May 2021 | Last Updated: 18 May 2021

22762

ULN2003A

ULN2003A

STMicroelectronics

STMICROELECTRONICS - ULN2003A - Bipolares Transistor-Array, Darlington, NPN, 50 V, 2.25 W, 500 mA, 1000 hFE, DIP

Purchase Guide

STMICROELECTRONICS - ULN2003A - Bipolares Transistor-Array, Darlington, NPN, 50 V, 2.25 W, 500 mA, 1000 hFE, DIP

ULN2003A is a stepper motor driver IC. This article mainly introduces pinout, specifications, features, and other detailed information about STMicroelectronics ULN2003A.

A Tutorial using the ULN2003A Transistor Array with Arduino.

Using the ULN2003A Transistor Array with Arduino

ULN2003A Description

The ULN2003 are high voltage, high current Darlington arrays containing seven open collectors Darlington pairs with common emitters. Each channel rated at 500 mA and can withstand peak currents of 600 mA. Suppression diodes are included for inductive load driving and the inputs are pinned opposite the outputs to simplify board layout.

The versions interface to all common logic families:

– ULN2001 (general purpose, DTL, TTL, PMOS, CMOS)

– ULN2002 (14 - 25 V PMOS)

– ULN2003 (5 V TTL, CMOS)

– ULN2004 (6 - 15 V CMOS, PMOS)

These versatile devices are useful for driving a wide range of loads including solenoids, relays

DC motors, LED displays filament lamps, thermal printheads, and high power buffers.

The ULN2003A are supplied in 16 pin plastic DIP packages with a copper lead frame to reduce thermal resistance. They are available also in small outline package (SO-16) as ULN2003D1.

ULN2003A Pinout

Pin configuration.jpg


Pin Number

Pin Name

Description

1 to 7

Input 1 to Input 7

Seven Input pins of Darlington pair, each pin is connected to the base of the transistor and can be triggered by using +5V

8

Ground

Ground Reference Voltage 0V

9

COM

Used as test pin or Voltage suppresser pin (optional to use)

10 to 16

Output 1 to Output 7

Respective outputs of seven input pins. Each output pin will be connected to the ground only when its respective input pin is high(+5V)


ULN2003A CAD model

PCB Symbol - STMicroelectronics ULN2003A.png

PCB Symbol - STMicroelectronics ULN2003A

PCB Footprint - STMicroelectronics ULN2003A.png

PCB Footprint - STMicroelectronics ULN2003A

3D Model - STMicroelectronics ULN2003A.jpg

3D Model - STMicroelectronics ULN2003A

ULN2003A Features

■ Seven Darlingtons per package

■ Output current 500 mA per driver (600 mA peak)

■ Output voltage 50 V

■ Integrated suppression diodes for inductive loads

■ Outputs can be paralleled for higher current

■ TTL/CMOS/PMOS/DTL compatible inputs

■ Inputs pinned opposite outputs to simplify layout

Specifications

STMicroelectronics ULN2003A technical specifications, attributes, parameters and parts with similar specifications to STMicroelectronics ULN2003A.
  • Type
    Parameter
  • Factory Lead Time
    15 Weeks
  • Contact Plating

    Contact plating (finish) provides corrosion protection for base metals and optimizes the mechanical and electrical properties of the contact interfaces.

    Gold
  • Mount

    In electronic components, the term "Mount" typically refers to the method or process of physically attaching or fixing a component onto a circuit board or other electronic device. This can involve soldering, adhesive bonding, or other techniques to secure the component in place. The mounting process is crucial for ensuring proper electrical connections and mechanical stability within the electronic system. Different components may have specific mounting requirements based on their size, shape, and function, and manufacturers provide guidelines for proper mounting procedures to ensure optimal performance and reliability of the electronic device.

    Through Hole
  • Mounting Type

    The "Mounting Type" in electronic components refers to the method used to attach or connect a component to a circuit board or other substrate, such as through-hole, surface-mount, or panel mount.

    Through Hole
  • Package / Case

    refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.

    16-DIP (0.300, 7.62mm)
  • Number of Pins
    16
  • Weight
    1.627801g
  • Transistor Element Material

    The "Transistor Element Material" parameter in electronic components refers to the material used to construct the transistor within the component. Transistors are semiconductor devices that amplify or switch electronic signals and are a fundamental building block in electronic circuits. The material used for the transistor element can significantly impact the performance and characteristics of the component. Common materials used for transistor elements include silicon, germanium, and gallium arsenide, each with its own unique properties and suitability for different applications. The choice of transistor element material is crucial in designing electronic components to meet specific performance requirements such as speed, power efficiency, and temperature tolerance.

    SILICON
  • Collector-Emitter Breakdown Voltage
    50V
  • Collector-Emitter Saturation Voltage
    1.1V
  • Number of Elements
    7
  • Operating Temperature

    The operating temperature is the range of ambient temperature within which a power supply, or any other electrical equipment, operate in. This ranges from a minimum operating temperature, to a peak or maximum operating temperature, outside which, the power supply may fail.

    -40°C~85°C TA
  • Packaging

    Semiconductor package is a carrier / shell used to contain and cover one or more semiconductor components or integrated circuits. The material of the shell can be metal, plastic, glass or ceramic.

    Tube
  • JESD-609 Code

    The "JESD-609 Code" in electronic components refers to a standardized marking code that indicates the lead-free solder composition and finish of electronic components for compliance with environmental regulations.

    e3
  • Part Status

    Parts can have many statuses as they progress through the configuration, analysis, review, and approval stages.

    Active
  • Moisture Sensitivity Level (MSL)

    Moisture Sensitivity Level (MSL) is a standardized rating that indicates the susceptibility of electronic components, particularly semiconductors, to moisture-induced damage during storage and the soldering process, defining the allowable exposure time to ambient conditions before they require special handling or baking to prevent failures

    1 (Unlimited)
  • Number of Terminations
    16
  • ECCN Code

    An ECCN (Export Control Classification Number) is an alphanumeric code used by the U.S. Bureau of Industry and Security to identify and categorize electronic components and other dual-use items that may require an export license based on their technical characteristics and potential for military use.

    EAR99
  • Terminal Finish

    Terminal Finish refers to the surface treatment applied to the terminals or leads of electronic components to enhance their performance and longevity. It can improve solderability, corrosion resistance, and overall reliability of the connection in electronic assemblies. Common finishes include nickel, gold, and tin, each possessing distinct properties suitable for various applications. The choice of terminal finish can significantly impact the durability and effectiveness of electronic devices.

    Matte Tin (Sn)
  • Additional Feature

    Any Feature, including a modified Existing Feature, that is not an Existing Feature.

    LOGIC LEVEL COMPATIBLE
  • Voltage - Rated DC

    Voltage - Rated DC is a parameter that specifies the maximum direct current (DC) voltage that an electronic component can safely handle without being damaged. This rating is crucial for ensuring the proper functioning and longevity of the component in a circuit. Exceeding the rated DC voltage can lead to overheating, breakdown, or even permanent damage to the component. It is important to carefully consider this parameter when designing or selecting components for a circuit to prevent any potential issues related to voltage overload.

    50V
  • Max Power Dissipation

    The maximum power that the MOSFET can dissipate continuously under the specified thermal conditions.

    2.25W
  • Terminal Position

    In electronic components, the term "Terminal Position" refers to the physical location of the connection points on the component where external electrical connections can be made. These connection points, known as terminals, are typically used to attach wires, leads, or other components to the main body of the electronic component. The terminal position is important for ensuring proper connectivity and functionality of the component within a circuit. It is often specified in technical datasheets or component specifications to help designers and engineers understand how to properly integrate the component into their circuit designs.

    DUAL
  • Current Rating

    Current rating is the maximum current that a fuse will carry for an indefinite period without too much deterioration of the fuse element.

    500mA
  • Base Part Number

    The "Base Part Number" (BPN) in electronic components serves a similar purpose to the "Base Product Number." It refers to the primary identifier for a component that captures the essential characteristics shared by a group of similar components. The BPN provides a fundamental way to reference a family or series of components without specifying all the variations and specific details.

    ULN2003
  • Pin Count

    a count of all of the component leads (or pins)

    16
  • Output Voltage

    Output voltage is a crucial parameter in electronic components that refers to the voltage level produced by the component as a result of its operation. It represents the electrical potential difference between the output terminal of the component and a reference point, typically ground. The output voltage is a key factor in determining the performance and functionality of the component, as it dictates the level of voltage that will be delivered to the connected circuit or load. It is often specified in datasheets and technical specifications to ensure compatibility and proper functioning within a given system.

    50V
  • Polarity

    In electronic components, polarity refers to the orientation or direction in which the component must be connected in a circuit to function properly. Components such as diodes, capacitors, and LEDs have polarity markings to indicate which terminal should be connected to the positive or negative side of the circuit. Connecting a component with incorrect polarity can lead to malfunction or damage. It is important to pay attention to polarity markings and follow the manufacturer's instructions to ensure proper operation of electronic components.

    NPN
  • Configuration

    The parameter "Configuration" in electronic components refers to the specific arrangement or setup of the components within a circuit or system. It encompasses how individual elements are interconnected and their physical layout. Configuration can affect the functionality, performance, and efficiency of the electronic system, and may influence factors such as signal flow, impedance, and power distribution. Understanding the configuration is essential for design, troubleshooting, and optimizing electronic devices.

    COMPLEX
  • Number of Channels
    7
  • Output Current

    The rated output current is the maximum load current that a power supply can provide at a specified ambient temperature. A power supply can never provide more current that it's rated output current unless there is a fault, such as short circuit at the load.

    500mA
  • Transistor Application

    In the context of electronic components, the parameter "Transistor Application" refers to the specific purpose or function for which a transistor is designed and used. Transistors are semiconductor devices that can amplify or switch electronic signals and are commonly used in various electronic circuits. The application of a transistor can vary widely depending on its design and characteristics, such as whether it is intended for audio amplification, digital logic, power control, or radio frequency applications. Understanding the transistor application is important for selecting the right type of transistor for a particular circuit or system to ensure optimal performance and functionality.

    SWITCHING
  • Transistor Type

    Transistor type refers to the classification of transistors based on their operation and construction. The two primary types are bipolar junction transistors (BJTs) and field-effect transistors (FETs). BJTs use current to control the flow of current, while FETs utilize voltage to control current flow. Each type has its own subtypes, such as NPN and PNP for BJTs, and MOSFETs and JFETs for FETs, impacting their applications and characteristics in electronic circuits.

    7 NPN Darlington
  • Collector Emitter Voltage (VCEO)

    Collector-Emitter Voltage (VCEO) is a key parameter in electronic components, particularly in transistors. It refers to the maximum voltage that can be applied between the collector and emitter terminals of a transistor while the base terminal is open or not conducting. Exceeding this voltage limit can lead to breakdown and potential damage to the transistor. VCEO is crucial for ensuring the safe and reliable operation of the transistor within its specified limits. Designers must carefully consider VCEO when selecting transistors for a circuit to prevent overvoltage conditions that could compromise the performance and longevity of the component.

    50V
  • Max Collector Current

    Max Collector Current is a parameter used to specify the maximum amount of current that can safely flow through the collector terminal of a transistor or other electronic component without causing damage. It is typically expressed in units of amperes (A) and is an important consideration when designing circuits to ensure that the component operates within its safe operating limits. Exceeding the specified max collector current can lead to overheating, degradation of performance, or even permanent damage to the component. Designers must carefully consider this parameter when selecting components and designing circuits to ensure reliable and safe operation.

    500mA
  • DC Current Gain (hFE) (Min) @ Ic, Vce

    The parameter "DC Current Gain (hFE) (Min) @ Ic, Vce" in electronic components refers to the minimum value of the DC current gain, denoted as hFE, under specific operating conditions of collector current (Ic) and collector-emitter voltage (Vce). The DC current gain hFE represents the ratio of the collector current to the base current in a bipolar junction transistor (BJT), indicating the amplification capability of the transistor. The minimum hFE value at a given Ic and Vce helps determine the transistor's performance and efficiency in amplifying signals within a circuit. Designers use this parameter to ensure proper transistor selection and performance in various electronic applications.

    1000 @ 350mA 2V
  • Current - Collector Cutoff (Max)

    The parameter "Current - Collector Cutoff (Max)" refers to the maximum current at which a transistor or other electronic component will cease to conduct current between the collector and emitter terminals. This parameter is important in determining the maximum current that can flow through the component when it is in the cutoff state. Exceeding this maximum cutoff current can lead to malfunction or damage of the component. It is typically specified in the component's datasheet and is crucial for proper circuit design and operation.

    50μA
  • Vce Saturation (Max) @ Ib, Ic

    The parameter "Vce Saturation (Max) @ Ib, Ic" in electronic components refers to the maximum voltage drop across the collector-emitter junction when the transistor is in saturation mode. This parameter is specified at a certain base current (Ib) and collector current (Ic) levels. It indicates the minimum voltage required to keep the transistor fully conducting in saturation mode, ensuring that the transistor operates efficiently and does not enter the cutoff region. Designers use this parameter to ensure proper transistor operation and to prevent overheating or damage to the component.

    1.6V @ 500μA, 350mA
  • VCEsat-Max

    VCEsat-Max refers to the maximum collector-emitter saturation voltage of a bipolar junction transistor (BJT) or an insulated gate bipolar transistor (IGBT). It is a crucial parameter that indicates the minimum voltage drop across the collector-emitter junction when the transistor is in saturation mode. This parameter is important for determining the efficiency and performance of the transistor in switching applications. A lower VCEsat-Max value indicates better performance and reduced power losses in the transistor during operation. Designers often consider this parameter when selecting transistors for applications where minimizing power dissipation is critical.

    1.6 V
  • Height
    4.59mm
  • Length
    20mm
  • Width
    7.1mm
  • REACH SVHC

    The parameter "REACH SVHC" in electronic components refers to the compliance with the Registration, Evaluation, Authorization, and Restriction of Chemicals (REACH) regulation regarding Substances of Very High Concern (SVHC). SVHCs are substances that may have serious effects on human health or the environment, and their use is regulated under REACH to ensure their safe handling and minimize their impact.Manufacturers of electronic components need to declare if their products contain any SVHCs above a certain threshold concentration and provide information on the safe use of these substances. This information allows customers to make informed decisions about the potential risks associated with using the components and take appropriate measures to mitigate any hazards.Ensuring compliance with REACH SVHC requirements is essential for electronics manufacturers to meet regulatory standards, protect human health and the environment, and maintain transparency in their supply chain. It also demonstrates a commitment to sustainability and responsible manufacturing practices in the electronics industry.

    No SVHC
  • Radiation Hardening

    Radiation hardening is the process of making electronic components and circuits resistant to damage or malfunction caused by high levels of ionizing radiation, especially for environments in outer space (especially beyond the low Earth orbit), around nuclear reactors and particle accelerators, or during nuclear accidents or nuclear warfare.

    No
  • RoHS Status

    RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.

    ROHS3 Compliant
  • Lead Free

    Lead Free is a term used to describe electronic components that do not contain lead as part of their composition. Lead is a toxic material that can have harmful effects on human health and the environment, so the electronics industry has been moving towards lead-free components to reduce these risks. Lead-free components are typically made using alternative materials such as silver, copper, and tin. Manufacturers must comply with regulations such as the Restriction of Hazardous Substances (RoHS) directive to ensure that their products are lead-free and environmentally friendly.

    Lead Free
0 Similar Products Remaining

ULN2003A Diagram

ULN2003 Schematic diagram.png

ULN2003 Schematic diagram

Parts with Similar Specs

The three parts on the right have similar specifications to STMicroelectronics & ULN2003A.
  • Image
    Part Number
    Manufacturer
    Mount
    Package / Case
    Collector Emitter Breakdown Voltage
    Max Collector Current
    Transistor Type
    Moisture Sensitivity Level (MSL)
    Configuration
    Current - Collector Cutoff (Max)
    View Compare
  • ULN2003A

    ULN2003A

    Through Hole

    16-DIP (0.300, 7.62mm)

    50 V

    500 mA

    7 NPN Darlington

    1 (Unlimited)

    COMPLEX

    50μA

  • ULN2004AD16-U

    Through Hole

    16-DIP (0.300, 7.62mm)

    50 V

    500 mA

    7 NPN Darlington

    1 (Unlimited)

    COMPLEX

    50μA

ULN2003A Alternatives


Part Number

Description

Manufacturer

ULN2003AIDRG4

50-V, 7-ch darlington transistor array, -40 to 105C 16-SOIC -40 to 105

Texas Instruments

ULN2003AIDR

50-V, 7-ch darlington transistor array, -40 to 105C 16-SOIC -40 to 105

Texas Instruments

BA12003BF

Small Signal Bipolar Transistor, 0.00035A I(C), 55V V(BR)CEO, 7-Element, NPN, Silicon, SOP-16

ROHM Semiconductor

TD62003AFG

TRANSISTOR 500 mA, 50 V, 7 CHANNEL, NPN, Si, SMALL SIGNAL TRANSISTOR, 0.225 INCH, LEAD FREE, PLASTIC, SOP-16, BIP General Purpose Small Signal

Toshiba America Electronic Components

ULN2003ANSE4

50V, 7 CHANNEL, NPN, Si, SMALL SIGNAL TRANSISTOR, PLASTIC, SO-16

Texas Instruments

ULN2003AIDRE4

50-V, 7-ch darlington transistor array, -40 to 105C 16-SOIC -40 to 105

Texas Instruments

DS2003TMX

TRANSISTOR 500 mA, 55 V, 7 CHANNEL, NPN, Si, SMALL SIGNAL TRANSISTOR, SURFACE MOUNT, DIP-16, BIP General Purpose Small Signal

National Semiconductor Corporation

DS2003CMX/NOPB

TRANSISTOR 500 mA, 55 V, 7 CHANNEL, NPN, Si, SMALL SIGNAL TRANSISTOR, SOIC-16, BIP General Purpose Small Signal

National Semiconductor Corporation

ULQ2003ADRG4

50-V, 7-ch darlington transistor array 16-SOIC

Texas Instruments

DS2003TMX/NOPB

High Current/Voltage Darlington Driver 16-SOIC -40 to 125

Texas Instruments

ULN2003ANTRANSISTOR ARRAY, NPN, 2003, DIP16Texas Instruments


Where to use ULN2003

One of the most widely used motor driver ICs is the ULN2003. When using digital logic circuits such as Op-maps, Timers, Gates, Arduino, PIC, ARM, and others to move high current loads, this IC comes in handy. For example, an Arduino I/O cannot power a motor that needs 9V and 300mA to operate, so we use this IC to provide enough current and voltage for the load. Relay modules, motors, high-current LEDs, and even stepper motors are all powered by this IC. So, if you need to deal with something that needs more than 5V 80mA, this IC is the one for you.

How to use a ULN2003

The ULN2003 is a 16-pin integrated circuit. It contains seven Darlington Pairs, each capable of driving loads up to 50V and 500mA. We have seven Input and Output Pins for these seven Darlington Pairs. We may also add a ground and a common pin to the mix. The ground pin is grounded as is customary, and the use of the Common pin is optional. It can come as a surprise that this IC lacks a Vcc (power) pin; this is due to the fact that the power needed for the transistors to function will be drawn from the input pin itself. The circuit below is a basic circuit that can be used to evaluate the ULN2003 IC's functionality.

working of ULN2003 IC.png

Consider the LEDs to be the loads in the circuit, and the logic pins (blue color) to be the pins attached to the digital circuit or microcontroller like the Arduino. The LED's positive pin is connected to the positive load voltage, while the negative pin is connected to the IC's output pin. This is because when the IC's input pin goes heavy, the corresponding output pin goes to earth. When the LED's negative terminal is grounded, the circuit is completed, and the LED glows. Each load connected to the output pin must be no more than 50C and 500mA. However, by combining two or more output pins to gather, you can run higher current loads.

The COM pin is connected to ground through a switch, this connection is optional. It can be used a test switch, meaning when this pin is grounded all the output pins will be grounded.


ULN2003A Applications

  • Used to drive high current loads using Digital Circuits

  • Can be used to drive Stepper motors

  • High current LED’s can be driven

  • Relay Driver module (can drive 7 relays)

  • Logic Buffers in digital electronics

  • Used as a Touch sensor for Arduino

ULN2003A Dimension

DIP-16L package dimensions.png

DIP-16L package dimensions

DIP-16L mechanical data.png

DIP-16L mechanical data

ULN2003A Manufacturer

STMicroelectronics is a global independent semiconductor company and is a leader in developing and delivering semiconductor solutions across the spectrum of microelectronics applications. An unrivaled combination of silicon and system expertise, manufacturing strength, Intellectual Property (IP) portfolio, and strategic partners positions the Company at the forefront of System-on-Chip (SoC) technology, and its products play a key role in enabling today's convergence trends.

Trend Analysis

Frequently Asked Questions

1.What is the use of ULN2003A?

Typical usage of the ULN2003A is in driver circuits for relays, lamp and LED displays, stepper motors, logic buffers and line drivers.

2.How do you test ULN2003A?

Use a 1K series resistor and a 5V supply. Apply 5V to the input (or 3V). You can also damage the ULN2003A by leaving out the resistor. It is fairly unlikely you have damaged the chip by soldering to it, however you have a good chance of damaging it by leaving out the series resistor.

3.Why do we need a ULN2003 in driving a motor?

Known for its high current and high voltage capacity, the ULN2003 gives a higher current gain than a single transistor and enables the low voltage and low current output of a microcontroller to drive a higher current stepper motor. Hence, we connect this IC to source for enough current and voltage for the motor.

4.What is a Darlington array?

Darlington devices are high-voltage, high-current switch arrays containing multiple open-collector Darlington pairs or multiple Darlington transistors with common emitters, and integral suppression diodes for inductive loads.

5.What is ULN2001A?

The ULN2001A is a general-purpose array and can be used with TTL and CMOS technologies. The ULN2003A and ULQ2003A have a 2.7-kΩ series base resistor for each Darlington pair for operation directly with TTL or 5-V CMOS devices.
ULN2003A

STMicroelectronics

In Stock: 10000

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe

Related Parts More