Basic Knowledge of Various Types of Mixers

Published: 13 December 2022 | Last Updated: 03 January 20236321
Welcome to the new post today. Today I will introduce the basic knowledge of mixer.
This video will show you different examples of mixer.

Basic concept of RF mixer with examples. mixers in radio frequency. Mixer tutorials #14

Topics covered in this article:
Ⅰ. Single/Double/Triple Balanced Passive Mixer
Ⅱ. I/Q Image Reject (IRM) Mixer
Ⅲ. Active mixer
Ⅳ. Integrated Frequency Conversion Mixer


A mixer, as the name suggests, combines two input signals to generate their frequency sum or difference. It is known as up-conversion when a mixer is used to produce an output frequency greater than the input signal (the two frequencies are added), and it is known as down-conversion when a mixer is used to produce an output frequency lower than the input signal.


Ⅰ. Single/Double/Triple Balanced Passive Mixer

In general, passive mixers are noted for their simplicity and lack of need for additional setup or external DC power. Wide bandwidth performance, strong dynamic range, low noise figure (NF), and good port isolation are further noteworthy characteristics of this type of mixer. Due to the design of this type of mixer and its benefit of not requiring an external DC power supply, the mixer output has a very low noise figure. A good generalization is that a passive mixer's noise figure should be equal to its conversion loss. These mixers are perfect for situations that require a low noise figure but cannot be satisfied by active mixers. This type of mixer also performs exceptionally well in systems with high frequencies and broad bandwidths. From RF to mmWave frequencies, they offer good performance. The isolation between the various ports is another crucial feature of a mixer. This feature frequently dictates which mixer can be utilized for a specific application. Double-balanced passive mixers have strong port-to-port isolation and a simpler architecture than triple-balanced passive mixers, which often have the best isolation performance but a complex architecture and perhaps insufficient other qualities (such as linearity, etc.). Double-balanced mixers offer the finest isolation, linearity, and noise figure for the majority of applications.

In terms of the entire signal chain, linearity, which is frequently quantified by the third-order intercept point IIP3, is one of the most crucial properties of RF and microwave devices. Generally speaking, passive mixers are noted for their strong linearity performance. Unfortunately, significant LO input power is necessary for passive mixers to work at their best. It takes between 13 and 20 dBm of LO drive, which is relatively strong for some applications, to operate the majority of passive mixers, which use diodes or FET transistors. Passive mixers' greatest flaw is their high LO drive needs. The conversion loss at the mixer output is another flaw in passive mixers. Since these mixers are passive components without gain blocks, the output of the mixer frequently experiences significant signal loss. For instance, if the mixer's conversion loss is 9 dB and its input power is 0 dBm, the mixer's output will be -9 dBm. Overall, these mixers are excellent for the military and test measurement applications.


Advantages of Passive Mixers

 

wide bandwidth

 

high dynamic range

 

low noise figure

 

High port-to-port isolation

 Figure. 1 IQ Mixer Block Diagram and Image Rejection Frequency Domain Diagram.png

Figure 1. I/Q Mixer Block Diagram and Image Rejection Frequency Domain Diagram

 

Ⅱ. I/Q Image Reject (IRM) Mixer

I/Q mixers are a subclass of passive mixers that provide the benefits of traditional passive mixers as well as the added advantage of filtering out undesirable image signals internally. When used as downconverters, these mixers are also known as IRMs (Image Reject Mixers), and when used as upconverters, they are known as SSBs (Single Sideband Mixers). The LO signal is split in half and then phase-shifted by 90° (0° for one mixer and 90° for the other) in the I/Q mixer, which consists of two double balanced mixers. With the help of this phase shift, the mixer is able to generate only the desired sideband signal while filtering out undesired signals.

On the same spectrogram, Figure 2 displays the performance of the I/Q mixer (purple trace) and double-balanced mixer (blue trace). As can be observed, the double balanced mixer generates both high and low sidebands, but the I/Q mixer reduces the undesirable low sidebands by offering 45 dB of rejection.

Figure. 2 Spectrum Plot of HMC773A Passive Mixer and HMC8191 IQ Mixer with 1 GHz IF Input and 16 GHz LO Input.jpg

Figure 2. Spectrum Plot of HMC773A Passive Mixer and HMC8191 I/Q Mixer with 1 GHz IF Input and 16 GHz LO Input

 

I/Q mixers require a high LO input power level, just like double-balanced passive mixers. The I/Q mixer normally needs around 3 dB more LO drive than two double-balanced mixers because of the way it is built. I/Q mixers are delicate to precisely balanced input amplitude and phase matching. The degree of picture rejection will be directly impacted by any deviation from 90° in phase or amplitude of the input signal, mixing structure, system board, or mixer itself. By externally calibrating the mixer to increase performance, the consequences of these inaccuracies can be reduced.

I/Q mixers are frequently employed in applications where sideband removal is required without the use of external filtering because of their sideband suppression capabilities. They also offer very good noise figure and linearity. Microwave point-to-point backhaul communications, test and measurement equipment, and military applications are typical examples of such markets.

 

Advantages of I/Q Mixers

 

Inherent Image Rejection

 

No need for expensive filtering

 

Good Amplitude and Phase Matching

 

Ⅲ. Active mixer

Single balanced and double balanced active mixers, commonly referred to as Gilbert unit mixers, are the two basic varieties. The built-in gain blocks at the RF output and LO port are a benefit of active mixers. Such mixers have minimal input LO power requirements and offer some conversion gain to the output signal. In contrast to the majority of passive mixers, the typical LO input power for active mixers is close to 0 dBm.

An LO frequency multiplier, which is used to multiply the LO frequency to a higher frequency, is frequently integrated into active mixers. The customer will benefit greatly from this frequency doubler's ability to drive the mixer without using a high LO frequency. Port-to-port isolation is often very good in active mixers. High noise figure and, in most situations, low linearity are its drawbacks. The noise figure and linearity of an active mixer are impacted by the demand for an input DC power source. In the communications and defense industries, where having a low LO drive and integrated conversion gain can be crucial, active mixers are frequently utilized. Active mixers are typically utilized in low-end instrumentation or as the third or final stage mixer in the IF portion of the test and measurement industry (integration and cost-effective design are more important than noise figure).

 

Advantages of Active Mixers

 

High integration, small size

 

LO drive requirements are low

 

Integrated LO doubler

 

Good isolation, but poor linearity and noise figure

 

Ⅳ. Integrated Frequency Conversion Mixer

Due to growing customer need for more comprehensive signal chain solutions, integrated frequency converters have gained popularity. These devices are made up of various functional components that are linked together to form a subsystem, simplifying the final system design for the customer. In one package or chip, these devices combine many blocks including mixers, phase-locked loops (PLLs), voltage-controlled oscillators (VCOs), frequency multipliers, gain blocks, detectors, etc. Such devices can be produced as a single die that contains all the design blocks or as a SIP (system in package), where many die are combined into a single package.

Frequency converters can provide designers many advantages by combining many devices onto a single chip or package, including: lower size, fewer components, a simpler design architecture, and—most importantly—a quicker time to market. quick.

 Figure. 3 Functional block diagram of the HMC6147A integrated frequency translation mixer.png

Figure 3. Functional block diagram of the HMC6147A integrated frequency translation mixer


UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1. What is a mixer?

The mixer is also called the frequency converter (Variable-frequency Drive, VFD), which is a power control device that uses frequency conversion technology and microelectronics technology to control the AC motor by changing the frequency of the motor's operating power supply.

2. How is the noise of a mixer defined?

The noise of the mixer is defined as: NF=Pno/Pso Pno is the total noise resource power transmitted to the output port when the noise temperature at the input port is the standard temperature at all frequencies, ie T0=290K.

3. What are the similarities and differences between a mixer and a frequency converter?

The same thing: the frequency has changed.  The difference:  1. Different frequencies: The mixer requires two sets of signals with different frequencies to be mixed, and frequency conversion means that the frequency of a signal is changing.  2. Different fields of application: mixers are used in communication circuits, and frequency converters are used in power circuits.  3.Different properties: A mixer is a circuit whose output signal frequency is equal to the sum, difference, or other combination of the two input signal frequencies. The frequency converter is a power control device that uses frequency conversion technology and microelectronics technology to control the AC motor by changing the frequency of the motor's working power supply.
Related Articles

  • HDMI RF Modulators: Architecture, Setup, Types, and Commercial Applications
    HDMI RF Modulators: Architecture, Setup, Types, and Commercial Applications
    UTMEL18 May 202667

    An HDMI RF modulator is a specialized hardware device designed to encode and modulate baseband digital audio and video signals into radio frequency (RF) formats. By converting an HDMI source into an RF signal, these devices allow high-definition content to be distributed over standard coaxial cable infrastructure.

    Read More
  •  Explain in Detail the Three Sharp Weapons to Eliminate EMC: Capacitors/Inductors/Magnetic Beads
    Explain in Detail the Three Sharp Weapons to Eliminate EMC: Capacitors/Inductors/Magnetic Beads
    UTMEL24 December 20214774

    Filter capacitors, common mode inductors, and magnetic beads are all typical components in EMC design circuits, and they're the three main tools for reducing electromagnetic interference.The notion of removing the three principal EMC weapons from the design is examined in-depth in this article.

    Read More
  • Everything You Need to Know about RF Chip
    Everything You Need to Know about RF Chip
    UTMEL14 January 202619933

    RF chip is one of the most important cores of cell phone terminals. The RF chip is responsible for RF transceiver, frequency synthesis, and power amplification.

    Read More
  • What are Electromagnetic Waves?
    What are Electromagnetic Waves?
    UTMEL07 December 20215438

    Hello everyone, I am Rose. Today I will introduce Electromagnetic waves to you. Electromagnetic waves are a type of electromagnetic energy.It can be considered the most perfect signal carrier because it can be carried without restriction in open space, as well as through metal transmission lines and controlled freely.

    Read More
  • Is Electromagnetic Radiation from Base Stations Terrible?
    Is Electromagnetic Radiation from Base Stations Terrible?
    UTMEL06 December 20214804

    Hello everyone, I am Rose. Today I will introduce electromagnetic radiation to you. Through this article, I hope that everyone can better understand electromagnetic radiation and protect themselves better.

    Read More