Introduction to Photonic Integrated Circuits and PIC Technology

Silicon photonic integrated circuits and lasers
Originally published in 2020, this article has been updated to reflect the latest technological advancements, market trends, and breakthroughs in the rapidly evolving field of photonic integration as of October 2025.
With the relentless demand for higher bandwidth and energy efficiency, driven by the rise of artificial intelligence (AI), 5G networks, and large-scale data centers, the need to upgrade network infrastructure at lower costs and with reduced energy consumption has never been more critical. Similar to the revolution sparked by electronic integrated circuits, the maturation of photonic integrated circuit (PIC) technology is catalyzing another profound transformation in optical information technology. PICs promise to deliver unprecedented performance, scalability, and efficiency by manipulating light on a microchip.
Catalog
I. Classification of Photonic Integrated Circuit Platforms
The choice of substrate material is fundamental to a PIC's performance, cost, and application range. Each platform offers a unique set of advantages and challenges. The industry has moved beyond monolithic classifications to a platform-based approach.

| Platform | Key Characteristics & Advantages | Limitations & Challenges | Primary Applications |
|---|---|---|---|
| Silicon (Si) | Leverages mature CMOS manufacturing for low-cost, high-volume production. High refractive index contrast allows for dense integration and small device footprints. | Indirect bandgap makes it inefficient for light generation, requiring hybrid integration of III-V materials for lasers. | Data center transceivers, co-packaged optics, LiDAR, quantum computing. |
| Indium Phosphide (InP) | Direct bandgap material allows for monolithic integration of active components like lasers, amplifiers, modulators, and detectors. Enables true "all-in-one" chips. | More expensive and complex fabrication compared to silicon. Wafers are smaller, limiting scalability. | High-performance telecommunications, 5G networks, high-speed data links. |
| Silicon Nitride (SiN) | Extremely low propagation loss across a broad transparency window (visible to mid-IR). Excellent for high-Q resonators and passive components. | Lacks native light generation and high-speed modulation capabilities, often used in hybrid approaches with other materials. | Biosensing, LiDAR, nonlinear photonics, AR/VR, quantum networks. |
| Lithium Niobate (LiNbO₃) | Superior electro-optic properties for high-speed, high-linearity modulators. Strong nonlinearity for frequency conversion. | Historically difficult to process, but thin-film lithium niobate (TFLN) is changing the game. Birefringence can be a challenge. | High-bandwidth modulators, quantum photonics, RF-over-fiber. |
| Silicon-Germanium-Tin (SiGeSn) | A 2024-2025 breakthrough. Enables the first Group IV electrically pumped lasers directly on silicon, solving a major challenge for silicon photonics. | Emerging technology, requires cryogenic temperatures for operation currently. Still in the research and development phase. | Future on-chip light sources for fully integrated silicon PICs. |
II. Industry Demands & Market Growth for PICs (2025)
The demand for PICs has exploded since 2020, driven by exponential data growth and the need for faster, more efficient processing. The global PIC market was valued at approximately $17.93 billion in 2025 and is projected to soar to $97.62 billion by 2034. The silicon photonics segment alone is expected to maintain a compound annual growth rate (CAGR) of 20% over the next decade.
Key drivers include:
AI and Machine Learning: The insatiable data transfer requirements of AI training and inference workloads are pushing data centers towards optical interconnects. Collaborations like the one between STMicroelectronics and Amazon Web Services (AWS) to produce silicon-germanium PICs for AI infrastructure highlight this trend.
Telecommunications and 5G: The rollout of 5G and the upcoming 6G standards require massive upgrades to backhaul and fronthaul networks, where high-speed, low-latency PIC-based transceivers are essential.
Emerging Applications: Significant growth is also anticipated in applications like automotive LiDAR, advanced biosensors for point-of-care diagnostics, and quantum computing, where PICs provide the only viable path to scaling complex optical systems.
III. Development Status & Recent Breakthroughs in PIC Technology
The period between 2020 and 2025 has been marked by significant breakthroughs that are solving long-standing challenges in the field.
The "Last Missing Piece" for Silicon Photonics
In a landmark achievement published in late 2024, an international research team developed the first electrically pumped continuous-wave semiconductor laser made entirely from Group IV elements (silicon-germanium-tin). This laser, grown directly on a standard silicon wafer, is compatible with CMOS manufacturing processes. While it currently operates at cryogenic temperatures, it represents a critical step towards creating a fully integrated, low-cost light source for silicon PICs, a challenge that has been pursued for decades.
Maturation of Hybrid Integration and Co-Packaged Optics
Hybrid integration, which combines the strengths of different material platforms (e.g., bonding InP lasers onto silicon PICs), has become a mainstream, commercially viable solution. This has led to the rise of co-packaged optics (CPO), where optical I/O is integrated directly with the main processing chip (like a CPU or GPU) in the same package. This approach drastically reduces power consumption and latency by shortening the electrical path, a critical factor for high-performance computing and AI clusters. Companies like Ayar Labs, which secured $155 million in funding, are at the forefront of this transition.
IV. Future Development Directions for PIC Technology
Continued Research on Silicon-Based Large-Scale PICs
The industry is pushing towards higher levels of integration and performance. Research is focused on achieving room-temperature operation for Group IV lasers and scaling production to 300mm wafers. The goal is to create complex systems-on-a-chip that combine logic, memory, and photonics, enabling ultra-high-bandwidth communication at the chip level. This is seen as essential for next-generation AI accelerators and processors.
Expansion into New Wavelengths and Applications
While data communications primarily use near-infrared wavelengths, there is growing interest in using PICs for a wider range of the electromagnetic spectrum. Silicon nitride, with its broad transparency, is enabling applications in the visible spectrum for AR/VR displays and biosensors, and extending into the mid-infrared for environmental sensing and medical diagnostics.
The Role of PICs in Optical Transport Networks (OTN)
High-speed transmission and dense integration are core strengths of PICs. In the context of Optical Transport Networks (OTN), PICs are enabling a new generation of hardware that combines high-speed interfaces with advanced networking and scheduling capabilities. The OTN market is robust, valued at over $25 billion in 2024 and projected to grow steadily. PIC-enabled OTN devices achieve high-quality, high-speed link grooming while improving network transparency and simplifying end-to-end management.

V. 2025 Update Summary
This article was originally published in 2020. This 2025 update incorporates significant industry developments:
Market Growth: Updated market data reflects the explosive growth driven by AI, with projections now reaching nearly $100 billion by 2034.
Technological Breakthroughs: The creation of the first Group IV electrically pumped laser on silicon is a major addition, solving a long-standing problem.
Material Platforms: The classification has been updated to a platform-based view, including modern materials like Silicon Nitride, TFLN, and the new SiGeSn alloys.
Industry Drivers: The role of AI and co-packaged optics as primary market drivers has been emphasized.
Recommended Articles:
Introduction to Voltage Stabilizer
LED Driver: Function, Types, and Application
1.What are photonic integrated circuits used for?
It is used in fibre-optic communication to make Externally Modulated Lasers (EML) which has a combination of a distributed feedback laser diode and an electro-absorption modulator on a single Indium-Phosphide [InP] chip.
2.What photonic IC contains?
In an electronic chip, electron flux passes through electrical components such as resistors, inductors, transistors, and capacitors; in a photonic chip, photons pass through optical components such as waveguides (equivalent to a resistor or electrical wire), lasers (equivalent to transistors), polarizers, and phase.
3.What is photonic semiconductor?
Introduction Optoelectronics is a branch of Photonics Science concerns with devices and systems that combine both electronic devices where information is carried among electrons and holes (generation and recombination) and photonic devices.
4.What are photonic devices?
Photonic devices are components for creating, manipulating, or detecting light. This can include laser diodes, light-emitting diodes, solar and photovoltaic cells, displays, and optical amplifiers.
5.Why are integrated circuits important?
The advent of the integrated circuit revolutionized the electronics industry and paved the way for devices such as mobile phones, computers, CD players, televisions, and many appliances found around the home. In addition, the spread of the chips helped to bring advanced electronic devices to all parts of the world.
Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap DevicesSaumitra Jagdale15 March 20242938For a long era, silicon has stood out as the primary material for fabricating electronic devices due to its affordability, moderate efficiency, and performance capabilities. Despite its widespread use, silicon faces several limitations that render it unsuitable for applications involving high power and elevated temperatures. As technological advancements continue and the industry demands enhanced efficiency from devices, these limitations become increasingly vivid. In the quest for electronic devices that are more potent, efficient, and compact, wide bandgap materials are emerging as a dominant player. Their superiority over silicon in crucial aspects such as efficiency, higher junction temperatures, power density, thinner drift regions, and faster switching speeds positions them as the preferred materials for the future of power electronics.
Read More
Applications of FPGAs in Artificial Intelligence: A Comprehensive GuideUTMEL29 August 20255759This comprehensive guide explores FPGAs as powerful AI accelerators that offer distinct advantages over traditional GPUs and CPUs. FPGAs provide reconfigurable hardware that can be customized for specific AI workloads, delivering superior energy efficiency, ultra-low latency, and deterministic performance—particularly valuable for edge AI applications. While GPUs excel at parallel processing for training, FPGAs shine in inference tasks through their adaptability and power optimization. The document covers practical implementation challenges, including development complexity and resource constraints, while highlighting solutions like High-Level Synthesis tools and vendor-specific AI development suites from Intel and AMD/Xilinx. Real-world applications span telecommunications, healthcare, autonomous vehicles, and financial services, demonstrating FPGAs' versatility in mission-critical systems requiring real-time processing and minimal power consumption.
Read More
The 2026 Engineer’s Guide: Choosing the Right MCU for Your Next IoT & New Energy ProjectUTMEL30 April 20262212A comprehensive comparison of 2026's leading MCUs from ST, NXP, and Microchip across power efficiency, processing performance, connectivity, and ecosystems to help engineers select the optimal chip for next-gen IoT and new energy projects.
Read More
AI Server Components: Engineering Next-Gen Data Center Hardware for 100kW RacksUTMEL15 May 20261169The transition from traditional enterprise IT to AI-driven workloads has rendered legacy data center hardware obsolete, forcing infrastructure planners to re-engineer server components for extreme thermal environments.
Read More
The Practical Engineer’s Guide to the NE555N Timer: Pinout, Setup, and TroubleshootingUTMEL29 May 20261021This comprehensive guide explores the NE555N timer, detailing its 8-pin layout, internal architecture, and key datasheet specifications. It compares the bipolar IC to CMOS variants and details setup configurations for astable, monostable, and bistable modes. Additionally, the guide offers practical troubleshooting advice to prevent common breadboard failures, such as floating reset pins and electrical noise issues.
Read More
Subscribe to Utmel !
FOD3180SDVON Semiconductor
ADUM4135BRWZAnalog Devices Inc.
ISO5452DWRTexas Instruments
ISO5452DWTexas Instruments
ATECC608A-SSHDA-TMicrochip Technology
HCS500-I/SMMicrochip Technology
AT88SC0404CA-SHMicrochip Technology
FSSD06BQXON Semiconductor
HCNW3120-500EBroadcom Limited
FOD8342TR2ON Semiconductor


Product
Brand
Articles
Tools