What is Field Programmable Gate Array(FPGA)?

Introduction to FPGA Part 1 - What is an FPGA? | Digi-Key Electronics
| Topics covered in this article: |
| Ⅰ. What is an FPGA |
| Ⅱ. Where we use FPGA? |
| Ⅲ. FPGA manufacturer |
Ⅰ. What is an FPGA
A semi-custom digital integrated circuit called an FPGA (Field Programmable Gate Array). Due to their great flexibility, short development cycle, and high processing performance, FPGAs are widely utilized in communication, image processing, medical, and other industries (parallel). FPGA s are becoming more common in sectors like artificial intelligence, 5G, and autonomous driving as technology improves.
FPGA is a product that was developed from programmable devices like the PAL, GAL, and CPLD. In the field of application-specific integrated circuits (ASIC), it appears as a semi-custom circuit that not only solves the drawbacks of bespoke circuits but also overcomes the limitations of the restricted number of original programmable devices gate circuits.
Breadboard to build digital clock circuit

Figure. 1
The circuit is a digital clock with a crystal oscillator, buzzer, digital tube, and different 74 series tiny chips, as shown in the diagram. These little devices can perform functions that are comparable to multiple logic gates. If you make it yourself, you'll quickly discover that it's a difficult circuit to construct. Connect one line at a time, and review the schematic design frequently for fear of constructing the incorrect line, or your mentality collapsing.
That's all there is to it when it comes to making a simple digital clock. If we want to implement more complex functions, we will have difficulty because we will need to use dozens or hundreds of such dedicated small chips to complete, which will complicate the layout and wiring of the circuit board. It will also have a significant impact on the overall system's performance, and the built circuit is bulky, unsightly, and impractical, so this method is clearly unacceptable.
To change this predicament, everyone devised a solution: using application-specific integrated circuits (ASICs), we can hand over the particular needs to be implemented to ASIC makers, who would then create an application-specific integrated circuit chip to solve the problem.
For example, we can give the ASIC manufacturer the digital clock's functional requirements, and the ASIC manufacturer will develop an application-specific integrated circuit chip based on the digital clock's functional needs. The function of our digital clock circuit is actually completed by this little device. Although this strategy is effective, it also has a number of drawbacks. The generation cycle, for example, is long, the chip is difficult to test, and the chip's internal circuit cannot be altered. As a result, individuals began to search continually to see whether there was any way for me to not only realize the function well, but also to fix the custom circuit's insufficiency.
As a result, FPGA was born. It was created in 1985 by Ross Freeman , one of Xilinx's founders. It's a type of PLD (programmable logic device) (Programmable Logic Device).
Xilinx A7 series FPGA chips

Figure. 2
Xilinx invented the first FPGA chip, the XC2064, in the genuine sense, roughly 20 years after Moore's Law, however, once FPGA was released, the ensuing development speed was faster than most people expected.
Before leaving the manufacturer, we need to know that the function of a specific ASIC custom integrated circuit chip has been fixed. As an example, consider the digital clock shown above. If I get a brand new digital clock chip right now, all I have to do now is look at it. The manufacturer handed me the data sheet so I could look at it and see how it works. I figured I'd just power it up and set up it to function.
It has a fixed function; it can only run a digital clock, and I have no idea what its internal circuit is. The FPGA. on the other hand is distinct since it is straightforward to use but lacks versatility. It serves no purpose at the time, hence it can be described as a blank piece of paper. This piece of white paper is yours to do whatever you want with. If you want it to perform the function of a digital clock, that is not an issue. The logic of the digital clock can be written in a specific editing language, such as Verilog, VHDL, or other hardware description languages, and then downloaded to the FPGA's internal memory. To complete the function of the digital clock, it will generate a digital clock circuit. You can delete the internal software at any moment or use a new design to overwrite the original design if you don't want this function. In theory, we should be able to produce whatever function we want using FPGA, FPGA has been increasingly recognized by the market in recent years as a result of its powerful editability, and its scope of use will continue to expand in the future.
Ⅱ. Where we use FPGA?
The fields in which FPGAs can be applied can be roughly divided into six categories:
1) Communication field
The omnipotent application of FPGA in the sphere of communication can be asserted. Due to the internal structure of the FPGA. it is very easy to realize the distributed algorithm structure, which is particularly useful for realizing high-speed digital signal processing in wireless communication. Because many functional modules in a wireless communication system require a significant number of filtering operations, these filtering functions frequently necessitate a large number of multiplying and accumulating operations. An FPGA can efficiently implement these multiply and accumulate operations by developing a distributed arithmetic structure. Xilinx's FPGA. in particular, integrates a large number of communication-related resources, including baseband processing (channel card), interface and connection operations, and RF (radio frequency card) in three categories:
(1) Baseband processing resources
Channel codec (LDPC, Turbo, convolutional code, and RS code codec techniques) and synchronization algorithm implementation are the major components of baseband processing (WCDMA system cell search, etc.).
(2) Interface and connection resources
The exterior high-speed communication interface (PCI Express, Ethernet MAC, high-speed AD/DA interface) of the wireless base station, as well as the related internal backplane protocols, are primarily realized via the interface and connection functions (OBSAI, CPRI, EMIF, LinkPort).
(3)RF Application Resources
Modulation/demodulation, up/down conversion (WiMAX, WCDMA, TD-SCDMA, single-channel, multi-channel DDC/DUC for CDMA2000 systems), peak clipping (PC-CFR), and distortion (Predistortion) are the most common RF applications.
Overall, as long as you master FPGA. you will be able to demonstrate your communication abilities.
2) The field of digital signal processing
FPGA is also unbeatable in the field of digital signal processing, owing to its high-speed parallel processing capability. The most significant advantage of FPGA is its parallel processing mechanism, which employs parallel architecture to accomplish digital signal processing functions. Because of this parallel mechanism, FPGA is particularly well suited to performing repetitive digital signal processing tasks such as FIR digital filtering. FPGA performance greatly outperforms the serial execution architecture of general-purpose DSP processors for high-speed parallel digital signal processing workloads. One is that, unlike traditional DSP, the voltage and driving capability of its interface can be programmable and configured. This is in contrast to traditional DSP, which is controlled by the instruction set because the instruction set's clock cycle is limited and cannot handle very high-speed signals. It's difficult to deal with class signals. As a result, FPGA has a wide range of applications in the field of digital signal processing.
3) Video image processing field
With the passage of time, people's expectations for visual stability, clarity, brightness, and color have risen steadily, similar to how standard definition (SD) gradually evolved into high definition (HD) and now Blu-ray quality. Image. This increases the amount of data that the processing chip must process in real time, while simultaneously increasing the complexity of the picture compression method, to the point where the simple use of ASSP or DSP can no longer handle such a significant volume of data processing. The benefits of FPGA are being emphasized at this moment. It has the ability to digest data more quickly. As a result, in the field of image processing, FPGA is becoming increasingly popular in the market after taking into account all costs.
4) High-speed interface design field
In reality, after seeing FPGA's capabilities in communication and digital signal processing, I believe everyone should have realized that FPGA must also have a place in high-speed interface design. Its distinctive benefits in the field of high-speed interface design are determined by its high-speed processing capability and hundreds or thousands of IOs.
For example, I may need to interact with data on a computer, send collected data to a computer for processing, or send processed results to a computer for display. ISA, PCI, PCI Express, PS/2, USB, and more interfaces exist between the PC and the external system. The typical way is to use the matching interface chip, such as a PCI interface chip, for the corresponding interface. I require numerous such interface chips when I need a lot of interfaces, which will surely complicate our hardware peripherals and raise the volume. It is large and inconvenient, but if you use FPGA, the benefit will be immediately apparent, because different interface logic can be implemented inside FPGA, so there is no need for as many interface chips as before. This, combined with the use of DDR memory, will make our interface Data processing more convenient.
5) Artificial intelligence field
If you prefer to keep up with technology news, you've probably heard a lot about 5G communication and artificial intelligence recently. Without realizing it, the twenty-first century has slipped into the year 2020. Artificial intelligence has advanced rapidly over the last 20 years, and the smooth growth of 5G has made it even more powerful. It is clear that the world of artificial intelligence will be the world of the future.
FPGAs are also widely used in the front-end part of artificial intelligence systems, such as autonomous driving, which necessitates the collection of a variety of traffic signals, such as driving routes, traffic lights, roadblocks, and driving speeds, and the use of multiple sensors to synthesize these signals. For driver and fusion processing, FPGAs can be employed. FPGAs are also useful for the front-end information processing of artificial intelligence systems, as some intelligent robots require to gather and process photos or interpret sound inputs, which can be done using FPGAs.
6) IC verification field
When you hear the word IC, you might think it is something incredibly advanced that is beyond reach for ordinary people, and that IC design is something only gods can do. Although the bar for IC design is unquestionably high, we don't need to go too far. To put it another way, we can relate it to PCB design. Building components one by one on a printed circuit board is known as PCB. One MOS tube and PN section are used to produce a circuit combined with a specific function on the silicon substrate, one macro, and one micro, and IC design is to use one MOS tube and PN section to build a circuit combined with a specific function on the silicon substrate. If the PCB design is abandoned and then revised, the loss will be little, but if the IC design is abandoned and then redesigned, the loss will be significant. Gold is not blown when the machine is turned on. The photoresist is costly, and opening molds using photolithography is costly. Hundreds of thousands of other processes, such as people, material resources, machine loss, and machine maintenance, are also involved. Absolutely It's a heartbreaking loss, thus IC design must accentuate the first edition's success. To assure the success of the IC version, significant simulation testing and FPGA verification are required. Simulation verification, comparable to ModelSim /VCS software, entails running simulation software on a server for testing; FPGA verification entails transplanting IC code to the FPGA and using FPGA synthesis. The tool is synthesized, put, and routed to generate a bit file, which is then downloaded and verified on the FPGA verification board. We can also partition complex ICs into numerous partial functions to verify separately, and each functional module is installed on an FPGA, FPGA-generated circuits are remarkably similar to real IC chips. This makes it much easier for our IC creators to check their own designs.
Ⅲ. FPGA manufacturer
Two giants: Xilinx and Altera.
Ziguang Tongchuang, Jingwei Yager, Gowin Semiconductor, Shanghai Anlu, Xi'an Zhiduoji, and others are a group of younger brothers. In terms of product performance, power consumption, and functionality, domestic FPGA manufacturers lag behind global top manufacturers.
ZYNQ
ZYNQ = FPGA + ARM core, you can customize the circuit yourself, and you can also do ordinary embedded development.
Xilinx introduced the Zynq-7000 series, an all-programmable system-on-chip that consists of two parts: PS (Processing System, processor system) and PL (Programmable Logic, programmable logic). The Zynq SoC combines an ARM dual-core cortex-A9 processor with a Xilinx 7 series FPGA fabric, providing it not only the power, performance, and compatibility of an ASIC, but also the flexibility and programmability of FPGA hardware.
PYNQ: Python Productivity for Zynq (Python + ZYNQ) is an open-source framework created by Xilinx that uses the Python language and libraries to allow designers to quickly build high-performance Embedded applications using programmable logic and microprocessors in Zynq.
Replenish
PLD: Programmable Logic Device, programmable logic device.

Figure. 3
What is the difference between ARM and FPGA?
ARM is like a well-designed office building, which department is responsible for everything is determined, all you have to do is to reasonably allocate department resources to achieve your goals. An FPGA is all about giving you a bunch of building materials and people, and it's what you want it to be built as.
What are the advantages and disadvantages of FPGA?
The advantages of FPGA are as follows: (1) FPGA is composed of hardware resources such as logic unit, RAM, multiplier, etc. By rationally organizing these hardware resources, hardware circuits such as multiplier, register, and address generator can be realized. (2) FPGA can be designed by using block diagram or Verilog HDL, from simple gate circuit to FIR or FFT circuit. (3) The FPGA can be reprogrammed infinitely, and it only takes a few hundred milliseconds to load a new design scheme, and the hardware overhead can be reduced by reconfiguration. (4) The operating frequency of the FPGA is determined by the FPGA chip and design, and some harsh requirements can be met by modifying the design or replacing a faster chip. The disadvantages of FPGA are as follows: (1) All functions of FPGA are realized by hardware, and operations such as branch conditional jump cannot be realized. (2) FPGA can only implement fixed-point operations.
What is the difference between FPGA and CPLD?
①CPLD is more suitable for completing various algorithms and combinational logic, and FPGA is more suitable for completing sequential logic. In other words, FPGAs are more suitable for flip-flop-rich structures, while CPLDs are more suitable for flip-flop-limited and product-rich structures. ②The continuous wiring structure of CPLD determines that its timing delay is uniform and predictable, while the segmented wiring structure of FPGA determines the unpredictability of its delay. ③ FPGA has greater flexibility than CPLD in programming. CPLDs are programmed by modifying the logic function with fixed interconnected circuits, while FPGAs are programmed mainly by changing the wiring of the interconnections; FPGAs can be programmed under logic gates, while CPLDs are programmed under logic blocks. ④ FPGA has a higher integration level than CPLD, and has more complex wiring structure and logic implementation. ⑤ CPLD is more convenient to use than FPGA. The programming of CPLD adopts E2PROM or FASTFLASH technology, no external memory chip is required, and it is easy to use. The programming information of the FPGA needs to be stored in the external memory, and the usage method is complicated.
Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap DevicesSaumitra Jagdale15 March 20242876For a long era, silicon has stood out as the primary material for fabricating electronic devices due to its affordability, moderate efficiency, and performance capabilities. Despite its widespread use, silicon faces several limitations that render it unsuitable for applications involving high power and elevated temperatures. As technological advancements continue and the industry demands enhanced efficiency from devices, these limitations become increasingly vivid. In the quest for electronic devices that are more potent, efficient, and compact, wide bandgap materials are emerging as a dominant player. Their superiority over silicon in crucial aspects such as efficiency, higher junction temperatures, power density, thinner drift regions, and faster switching speeds positions them as the preferred materials for the future of power electronics.
Read More
Applications of FPGAs in Artificial Intelligence: A Comprehensive GuideUTMEL29 August 20255581This comprehensive guide explores FPGAs as powerful AI accelerators that offer distinct advantages over traditional GPUs and CPUs. FPGAs provide reconfigurable hardware that can be customized for specific AI workloads, delivering superior energy efficiency, ultra-low latency, and deterministic performance—particularly valuable for edge AI applications. While GPUs excel at parallel processing for training, FPGAs shine in inference tasks through their adaptability and power optimization. The document covers practical implementation challenges, including development complexity and resource constraints, while highlighting solutions like High-Level Synthesis tools and vendor-specific AI development suites from Intel and AMD/Xilinx. Real-world applications span telecommunications, healthcare, autonomous vehicles, and financial services, demonstrating FPGAs' versatility in mission-critical systems requiring real-time processing and minimal power consumption.
Read More
The 2026 Engineer’s Guide: Choosing the Right MCU for Your Next IoT & New Energy ProjectUTMEL30 April 20261862A comprehensive comparison of 2026's leading MCUs from ST, NXP, and Microchip across power efficiency, processing performance, connectivity, and ecosystems to help engineers select the optimal chip for next-gen IoT and new energy projects.
Read More
AI Server Components: Engineering Next-Gen Data Center Hardware for 100kW RacksUTMEL15 May 20261004The transition from traditional enterprise IT to AI-driven workloads has rendered legacy data center hardware obsolete, forcing infrastructure planners to re-engineer server components for extreme thermal environments.
Read More
The Practical Engineer’s Guide to the NE555N Timer: Pinout, Setup, and TroubleshootingUTMEL29 May 2026799This comprehensive guide explores the NE555N timer, detailing its 8-pin layout, internal architecture, and key datasheet specifications. It compares the bipolar IC to CMOS variants and details setup configurations for astable, monostable, and bistable modes. Additionally, the guide offers practical troubleshooting advice to prevent common breadboard failures, such as floating reset pins and electrical noise issues.
Read More
Subscribe to Utmel !
UCC5310MCDRTexas Instruments
1EDI20H12AHXUMA1Infineon Technologies
1EDI60H12AHXUMA1Infineon Technologies
1EDI30I12MFXUMA1Infineon Technologies
UCC21220DRTexas Instruments
HCS201T-I/SNMicrochip Technology
ADATE305BSVZAnalog Devices Inc.
AD9172BBPZAnalog Devices Inc.
ADUM4223CRWZAnalog Devices Inc.
FM33256B-GCypress Semiconductor Corp


Product
Brand
Articles
Tools