web counter

Bluetooth Explained: Characteristics and Applications

Published: 02 June 2021 | Last Updated: 02 June 202121879
Bluetooth is a global specification of wireless data and voice communication, which is a special close-range wireless technology for setting communication environments for fixed and mobile devices. Bluetooth allows some of the current portable mobile devices and computer devices to connect to the Internet without a cable and can be wirelessly accessing the Internet.
This video explains how Bluetooth works and why Bluetooth has this outlandish name.

Bluetooth Explained | All you need to know

Catalog

Ⅰ Overview
Ⅱ Characteristics
Ⅲ System composition
Ⅳ Bluetooth applications

 

Ⅰ Overview

Bluetooth is a radio technology that supports device short-range communication (generally 10m), which can be exchanged between many devices including mobile phones, PDAs, wireless bluetooth headphones, laptops, and related peripherals. With the Bluetooth technique, communication between mobile communication terminals can effectively simplify communication between mobile communication terminals, and can successfully simplify communication between the device and the Internet Internet, so that data transmission becomes more rapid and efficient, and broaden the road for wireless communication.

Wireless Bluetooth headset.jpg

Wireless Bluetooth headset

Bluetooth can achieve convenience, flexibility, safety, low cost, low power data communication, and voice communication, so it is one of the mainstream technology of wireless domain network communication. Connected to other networks can bring a wider range of applications. It is an open-ended wireless communication that allows all digital devices wireless communication, one of the wireless network transmission technology, which is originally used to replace infrared.

Bluetooth technology is an open global specification for wireless data and voice communication. It establishes a special connection for the communication environment of the mobile device. The actual content is to establish a universal radio empty interface for the communication environment between the fixed equipment or mobile device, and the communication technology is further combined with computer technology so that various 3C devices are connected to each other without wires or cables. In this case, mutual communication or operation can be implemented within the short distance range. Simply put, Bluetooth technology is a technique that utilizes a low-power radio to transmit data between various 3C devices. Bluetooth works in a global 2.4GHz ISM (ie, industrial, scientific, medical) band, using IEEE802.15 protocol. As an emerging short-range wireless communication technology, it is powerful to promote the development of low-rate wireless personal regional networks.

Bluetooth technology is wireless communication with Ericsson, Nokia, Toshiba, International Commercial Machine (IBM) and Intel (Intel) jointly announced. Bluetooth devices are the main carriers for Bluetooth technology applications. Bluetooth products accommodate the Bluetooth module, support Bluetooth radio connection, and software applications. The Bluetooth device connection must be paired within a certain range. This pairing search is called the short-range temporary network mode that can accommodate up to 8 units. Bluetooth technology has RF characteristics. The TDMA structure and network multi-level structure are used, and the frequency of frequency hopping technology, wireless technology, etc. are technically applied, and the transmission efficiency is high, so it is applied by various industries.

Ⅱ Characteristics

The characteristics of Bluetooth technology and Bluetooth products are:

1. Bluetooth technology communicates with telecommunications networks via wireless. The Bluetooth applicable equipment is very wide and there is no cable connection.

2. Bluetooth technology's working frequency band is globally universal, suitable for use in users in the world, solves the "national" obstacle of cellular mobile phones. Bluetooth products are easy to use, and the Bluetooth device can search for another Bluetooth product, quickly establish contact between two devices, automatically transfer data automatically under the scope of control software.

Bluetooth new standard support mesh network protocol.jpg

Bluetooth new standard support mesh network protocol

3. Good security and strong anti-interference ability. Due to the function of fluduming technology with frequency hopping, it effectively avoiding the ISM band encountered an interference source. Bluetooth technology has better compatibility and has been capable of developing a technology independent of the operating system, achieving good compatibility in various operating systems.

4. Short transmission distance: At this stage, the main operating range of Bluetooth technology is around 10 meters. The Bluetooth technology after increasing RF power can be operated in the range of 100 meters, and only this can ensure the quality of work when Bluetooth is propagating. In addition, the interference between the technology and other electronic products can also be effectively reduced during the Bluetooth technology connection, thereby ensuring that Bluetooth technology can operate normally. Bluetooth technology not only has high communication quality and efficiency but also has a high propagation safety feature.

Ⅲ System composition

1. The underlying hardware module

The underlying hardware module in the Bluetooth technology system is managed by baseband, frequency hopping, and link management. Among them, the baseband is the transfer of Bluetooth data and frequency hopping. The wireless FM layer is not required to authorize microwaves, data streaming, and filtering are implemented in wireless fax, which is mainly defined by the Condition of the Bluetooth transceiver to meet the conditions of this frequency band. Link management implements security control of link establishment, connection, and demolition.

2. The intermediate protocol layer

The intermediate protocol layer in the Bluetooth technology system consists mainly of the service discovery protocol, the logical link control, and the adaptation protocol, the telephone communication protocol, and the serial simulation protocol. The role of the service discovery protocol layer is to provide a mechanism for the upper layer application to use services in the network. Logical link control and adaptation protocols are responsible for data disassembly, multiplexing protocols, and control quality, which are the foundation of other protocol layers.

3. High-level application

In the system consisting of Bluetooth technology, the high-level application is located in the uppermost frame portion of the protocol layer. The high-level application of Bluetooth technology mainly has documentation, network, and local area network access. Different kinds of high-level applications are wireless communication implemented by a certain application mode through a corresponding application.

Ⅳ Bluetooth applications

1. Automotive field

1) Bluetooth hands-free communication

The Bluetooth technology is applied to the car hands-free system, which is the most typical car Bluetooth application technology. Using the mobile phone as a gateway, open the mobile phone Bluetooth function and the car hands-free system. As long as the phone is within 10 meters away from the car's hands-free system, it can be automatically connected. The phone can control the microphone and sound system in the car, thereby achieving full-duplex-free calls.

2) Car Bluetooth entertainment system

Car Bluetooth Entertainment System, mainly including USB technology, audio decoding technology, Bluetooth technology, etc... Combined with the above technology, using automotive internal microphones, audio, etc., it will play various audio and phone books stored in the U disk. Connect the network in the in-vehicle system in CAN, so that the operation of the in-vehicle information entertainment system can be realized. It also retains scalability for the system.

3) Bluetooth vehicle remote condition diagnosis

The in-vehicle diagnostic system mainly relies on Bluetooth remote technology to check vehicle maintenance, especially for real-time monitoring of automobile engines. It helps the vehicle master the specific operation of different functional modules. Once the system is not working properly, the setup calculation will accurately judge the cause of the fault. The fault diagnostic code is uploaded to the in-vehicle running system memory.

4) Car Bluetooth anti-theft

As technology has gradually matured, Bluetooth will have further improvements in terms of application of wide range of applications, safety, transmission accuracy, transmission efficiency, etc. In particular, the Bluetooth anti-theft device is applied. If the car is in a state, the Bluetooth sensing function will automatically connect the car owner's mobile phone. Once the vehicle state changes or theft, it will automatically alarm.

2. Bluetooth technology is used in industrial production

1) Technicians' wireless monitoring of CNC machine tools

The application of Bluetooth technology in CNC machine tools is mainly reflected in wireless monitoring, using Bluetooth technology to install the corresponding monitoring facilities, providing convenience for user production of CNC machine tools, and also maintaining the safety of CNC machine tools. According to the carrier, the technical personnel monitor and manage the machine tools at any time, and discover the production problem of CNC machine tools. In particular, the automatic monitoring capabilities implemented under the wireless data link can be properly intervened, such as stopping the spindle or system shutdown.

2) Detection of partial wear

The Bluetooth detection function is also reflected in industrial parts wear, using Bluetooth detection software combined with wear testing materials to conduct experimental studies. Wear detection data is transmitted to related equipment by Bluetooth wireless transmission, and the relevant equipment is intelligently analyzed, and the results are notified to personnel.

3) Power output standardization

Bluetooth technology is also very important in industrial power output. Adjusting equipment uses Bluetooth technology to transmit production power changes and compare it with standard run power. If there is a power change abnormality, it will be adjusted in time and will be uploaded.

4) Real-time and complete records of the operating state of CNC systems

The Bluetooth transmission device is mainly composed of monitoring systems, records the operating state of the CNC system, and transmits any fluctuations during the operating period of the CNC system to the storage device. Using communication port upload information provides more reference materials for numerical control management managers.

3. Bluetooth audio products-Bluetooth wireless speakers

Bluetooth speakers are mainly portable speakers, which are generally small and portable. Bluetooth speaker technology has gradually been valued and accepted by consumers due to its convenient features. Common Bluetooth speakers on the market are mostly mono speakers (single speaker units). At the same time, some multi-channel speakers (two or more speaker units) with excellent sound quality have emerged.

bluetooth speaker.jpg

Bluetooth speaker

Since the advent of Bluetooth speakers, with the development of smart terminals, it has attracted widespread attention from users such as mobile phones and tablets. Bluetooth technology (Bluetooth) makes it possible to make speakers wireless. Various well-known brands have launched many "Bluetooth speakers" with a variety of shapes. Consumers can buy them for a price ranging from tens of yuan to more than 3,000 yuan. Super stylish and convenient Bluetooth speaker.

Recommended Bluetooth wireless speakers:

UE Megaboom 3.

Anker Soundcore 2.

Sonos Roam.

UE Wonderboom 2.

JBL Go 3.

JBL Charge 5.

UE Hyperboom.

LG XBoom Go PL7.

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1.How can I add Bluetooth to my computer?

Connect a Device to the Bluetooth Adapter

For Windows 10, go to Settings > Devices > Add Bluetooth or other devices> Bluetooth. Windows 8 and Windows 7 users should go into Control Panel to find Hardware and Sound > Devices and Printers > Add a device.

2.How do I give Bluetooth permission on Android?

Use of the Bluetooth APIs requires declaring several permissions in your manifest file.
If Bluetooth is available, there are three steps to make a connection:
1.Find nearby Bluetooth devices, either devices that are already paired or new ones.
2.Connect to a Bluetooth device.
3.Transfer data with the connected device.

3.How do I know if my PC has Bluetooth?

Check Bluetooth capability
1.Right-click the Windows icon, then click Device Manager.
2.Look for the Bluetooth heading. If an item is under the Bluetooth heading, your Lenovo PC or laptop has built-in Bluetooth capabilities.

4.Why is my Bluetooth not pairing?

For Android phones, go to Settings > System > Advanced> Reset Options > Reset Wi-fi, mobile & Bluetooth. For iOS and iPadOS devices, you'll have to unpair all of your devices (go to Setting > Bluetooth, select the info icon and choose to Forget This Device for each device) then restart your phone or tablet.

5.Why is Bluetooth pairing rejected?

Please skip pairing/bonding on Bluetooth phone settings level entirely. Turn Bluetooth ON and make sure to check all of the Bluetooth requirements for Android phones like Location ON for Android 6+, etc. Then open Swimmo mobile app directly and simply allow it to connect itself.
Related Articles

  • Why are TWS Earbuds so Popular?
    Why are TWS Earbuds so Popular?
    UTMEL17 July 20217676

    TWS (True Wireless Stereo) is a Bluetooth chip-based audio technology. TWS technology was applied to the field of Bluetooth earphones, resulting in the creation of TWS earbuds.

    Read More
  • What is a Wireless Network Adapter?
    What is a Wireless Network Adapter?
    UTMEL01 June 20217214

    The wireless network adapter is actually a terminal wireless network device, which needs to be used for Internet access through the wireless connection network under the wireless coverage of the wireless local area network. With a wireless network adapter, it also needs a wireless network that can be connected, so it needs to be used with a wireless router or wireless AP.

    Read More
  • Wireless Charging Explained: Working and Standards
    Wireless Charging Explained: Working and Standards
    UTMEL26 May 202111165

    Wireless charging technology originates from wireless power transmission technology, which can be divided into low-power wireless charging and high-power wireless charging. Low-power wireless charging often uses electromagnetic induction, such as the Qi method for charging mobile phones. High-power wireless charging often uses resonance (most electric vehicle charging uses this method) from the power supply equipment (charger) to transfer energy to the device that uses electricity.

    Read More
  • What is Wi-Fi 7?
    What is Wi-Fi 7?
    UTMEL20 August 20216105

    Following the release of Wi-Fi 6 (802.11ax), new 802.11be (EXTREMELY High Throughput) standards have been proposed. The WiFi Union will name the 802.11be standard Wi-Fi 7.

    Read More
  • What is 4G Router?
    What is 4G Router?
    UTMEL27 September 20217860

    Hello, I am Rose. Welcome to the new post today. The 4G Router is a high-speed industrial Internet of Things router, which is fully compatible with 4G/3.5G/3G networks, supports VPN links, industrial-grade protection, and a wide-temperature design. This article will introduce 4G Router in 6 aspects.

    Read More

Subscribe to Utmel !

Featured Parts More