web counter

5 Easy Ways to Choose Sample-and-Hold Amplifiers

Published: 06 June 2025 | Last Updated: 06 June 20253738
Learn how to choose the right sample-and-hold amplifiers by evaluating signal type, bandwidth, accuracy, and cost to ensure optimal performance for your application.

Choosing the correct sample-and-hold amplifiers can significantly improve how your system processes a signal. These amplifiers play a crucial role in maintaining accuracy during high-speed sampling. For instance, a track-and-hold amplifier can achieve a spurious-free dynamic range (SFDR) of over 72 dB when sampling a 0.9 Vpp signal at 925 MHz with a 0.5 GS/s rate. It also supports input frequencies up to 2.5 GHz, maintaining an SFDR above 50 dB. These capabilities ensure precise signal capture, even in demanding conditions. Understanding these benefits helps you select the right amplifier for your needs.

Understand Your Application Requirements

Define the signal type and range

The first step in selecting sample-and-hold amplifiers is understanding the type of signal your application will process. Signals can vary widely, from low-frequency analog signals to high-speed digital ones. For instance, if your input signal has a wide voltage swing, you need an amplifier that can handle it without distortion. A good example is a circuit with a differential peak-to-peak output swing of more than 2.4V, which ensures accurate signal capture.

You should also consider the signal's amplitude and frequency range. High-frequency signals require amplifiers with sufficient bandwidth to avoid performance degradation. For analog signals, maintaining linearity and minimizing distortion is critical.

Consider the operating environment (e.g., temperature, noise levels)

Environmental factors play a significant role in the performance of your sample and hold circuit. Temperature variations can affect the stability of analog components, leading to errors in signal processing. Noise levels in the environment can also interfere with the input signal, reducing the accuracy of your circuit.

Choose amplifiers designed to operate within your application's temperature range. For example, amplifiers with a total harmonic distortion (THD) of less than -60 dB and a signal-to-noise ratio (SNR) that meets your requirements can help maintain signal integrity in noisy environments.

Identify the required sampling rate and resolution

Sampling rate and resolution are critical parameters for any sample-and-hold circuit. The sampling rate determines how often the input signal is captured, while resolution defines the precision of the analog-to-digital conversion. Applications like ADCs require amplifiers capable of high-speed sampling, such as those operating at up to 200 MSample/s.

Additionally, ensure the amplifier's resolution matches your application's needs. For high-precision applications, look for amplifiers with a signal-to-noise and distortion ratio (SNDR) larger than 59 dB, even in worst-case scenarios. This ensures accurate signal representation and optimal circuit performance.

FeatureDescription
Gain149MHz unity-gain bandwidth, 76.7dB gain
Voltage SwingMore than 2.4V differential peak-to-peak output swing
SNR SpecificationsMeets requirements for SNR
Operation SpeedUp to 200-MSample/s
Power Consumption3.6mW with 1.8V supply voltage
THDLess than -60 dB
SNDRLarger than 59 dB in worst-case simulation

By understanding these requirements, you can select a sample-and-hold amplifier that aligns with your application's needs and ensures reliable performance.

Evaluate Key Performance Specifications of Sample-and-Hold Amplifiers

Evaluate     

Bandwidth and acquisition time

When choosing sample-and-hold amplifiers, bandwidth and acquisition time are two critical performance parameters. Bandwidth determines how well the amplifier can handle high-frequency signals. A higher bandwidth ensures that the amplifier can process fast-changing analog signals without distortion. For example, if your input signal operates at high frequencies, you need an amplifier with sufficient bandwidth to maintain signal integrity.

Acquisition time refers to how quickly the amplifier can capture and stabilize the input signal. Faster acquisition times are essential for applications requiring high-speed sampling, such as analog-to-digital converters (ADCs). If your sample and hold circuit operates in a high-speed environment, prioritize amplifiers with low acquisition times to ensure accurate signal capture.

Accuracy, linearity, and input offset voltage

Accuracy and linearity are vital for maintaining the quality of your analog signal. Accuracy ensures that the output signal closely matches the input signal, while linearity minimizes distortion across the signal range. For applications requiring precise analog-to-digital conversion, look for amplifiers with high linearity and low distortion.

Input offset voltage is another important factor. It represents the small voltage difference that may exist between the amplifier's input terminals. A lower input offset voltage improves the accuracy of your sample and hold circuit, especially when dealing with low-amplitude signals.

Hold mode droop rate, settling time, and charge injection

The hold mode droop rate measures how much the output voltage changes while the amplifier is in hold mode. A lower droop rate ensures that the signal remains stable during this phase. This is particularly important for circuits that require precise signal retention.

Settling time refers to how quickly the amplifier stabilizes after a change in the input signal. Faster settling times improve the overall performance of your sample-and-hold circuit, especially in high-speed sampling applications.

Charge injection occurs when switching between the sample and hold modes. Excessive charge injection can distort the signal, reducing the accuracy of your circuit. To minimize this effect, choose amplifiers designed to handle charge injection efficiently.

StandardDescription
IEC 61260Specifies performance requirements for analog, sampled data, and digital implementations of band-pass filters.
IEC 61672Provides specifications for sound level meters, including time-weighting and integrating-averaging types.
ANSI S1 4Sets minimum requirements for three basic types of sound level meters.
IEC 60942Specifies performance requirements for sound calibrators across three classes.
IEC 61094-4Details specifications for working standard microphones used in measuring systems.
The Big Six MeasurementsKey benchmarks for evaluating audio devices, including Level, Frequency Response, THD+N, Phase, Crosstalk, and SNR.

By evaluating these key performance specifications, you can ensure that your sample and hold circuit delivers reliable and accurate results for your applications.

Ensure Compatibility with Your Sample-and-Hold Circuit

Input and output voltage ranges

To ensure your sample-and-hold circuit works effectively, you must verify that the input and output voltage ranges of the amplifier align with your circuit's requirements. The input signal should fall within the amplifier's acceptable range to avoid distortion or clipping. Similarly, the output voltage range must match the needs of the connected components to maintain signal integrity.

For example, consider the following parameters when evaluating voltage ranges:

Parameter NameData TypeRangeUnitsDescription
ICNumber0 to 1noneInitial condition of the output at time=0
T_ACQNumbermin: 1fsFilter acquisition time in seconds

By ensuring compatibility in voltage ranges, you can prevent performance issues in your sample and hold circuit.

Interface compatibility with other components

Your sample-and-hold amplifiers must interface seamlessly with other components in your circuit. Check the input and output impedance to ensure proper signal transfer. Mismatched impedance can lead to signal loss or reflection, which reduces the accuracy of your analog signals.

Additionally, confirm that the amplifier supports the communication protocols used in your circuit. For instance, if your application involves analog-to-digital converters (ADCs), the amplifier must provide a clean and stable signal for accurate conversion.

Power supply requirements and noise immunity

Power supply compatibility is another critical factor. Verify that the amplifier operates within the voltage and current limits of your circuit's power supply. Overloading the power supply can damage the amplifier or other components.

Noise immunity is equally important, especially in environments with high electromagnetic interference (EMI). Choose amplifiers with built-in noise rejection features to maintain the integrity of your input signal. This ensures that your sample and hold circuit delivers reliable performance, even in challenging conditions.

By addressing these compatibility factors, you can optimize the performance of your sample-and-hold circuit and ensure it meets the demands of your applications.

Consider Practical Design Factors for Your Sample and Hold Circuit    

Package type and size constraints

The physical design of your sample and hold circuit depends heavily on the package type and size of the sample-and-hold amplifiers. You need to ensure that the amplifier fits within the available space on your printed circuit board (PCB). Compact designs are often necessary for portable or space-constrained applications. For example, surface-mount packages like SOIC or QFN are ideal for minimizing space usage while maintaining excellent performance.

Additionally, consider the thermal properties of the package. Amplifiers in smaller packages may face heat dissipation challenges, which can affect their performance. Choose a package type that balances size and thermal management to ensure reliable operation in your circuit.

Ease of integration into your circuit

Integrating the amplifier into your sample and hold circuit should be straightforward. Look for amplifiers with clear pin configurations and minimal external components. This simplifies the design process and reduces the risk of errors during assembly.

You should also evaluate the amplifier's compatibility with your circuit's layout. For instance, amplifiers with low input and output impedance are easier to integrate with other components, ensuring smooth signal transfer. Proper integration minimizes signal loss and enhances the overall performance of your analog signals.

Availability of technical support and documentation

Reliable technical support and comprehensive documentation are essential when working with sample-and-hold amplifiers. These resources help you troubleshoot issues and optimize your circuit's performance. Manufacturers that provide detailed datasheets, application notes, and design guides make it easier for you to implement their products effectively.

The circuitry involved is demanding, and unexpected properties of commonplace components such as capacitors and printed circuit boards may degrade SHA performance. When the SHA is used with an ADC, the SHA performance is critical to the overall dynamic performance of the combination, and plays a major role in determining the SFDR, SNR, etc., of the system.

When selecting an amplifier, prioritize brands known for their robust technical support. This ensures you have access to expert guidance when designing your sample and hold circuit. Comprehensive documentation also helps you understand the amplifier's parameters and how to optimize its use in your applications.

Balance Performance and Cost

Prioritize essential features over optional ones

When selecting sample-and-hold components, focus on the features that directly impact your circuit's performance. Essential features like bandwidth, acquisition time, and input voltage range should take precedence. These factors ensure your circuit can handle high frequency sampling and maintain signal integrity. For example, if your application involves data acquisition systems, prioritize amplifiers with low noise and high linearity to capture accurate analog signals.

Avoid spending on optional features that do not align with your circuit's requirements. For instance, advanced temperature compensation might not be necessary for indoor applications with stable conditions. By narrowing your focus to essential features, you can optimize both performance and cost.

Compare options within your budget

Comparing amplifiers within your budget helps you find the best value without compromising on quality. Start by listing your circuit's requirements, such as sampling rate, resolution, and power supply compatibility. Then, evaluate amplifiers that meet these criteria.

To simplify your decision, consider the following table showcasing reliable brands and their products:

BrandProduct ExampleTID RatingApplications
Texas InstrumentsRH1024Up to 300 kradSatellite systems, high-reliability defense
Analog Devices, Inc.AD963450-100 kradNuclear power plants, Mars rover instrumentation
Infineon TechnologiesAQEC-V grade components> 1×10¹² particles/cm²Geostationary satellites, Galileo navigation
Renesas ElectronicsR5F series microcontrollers> 200 kradInterplanetary probes, Mars 2020 Perseverance Rover

This comparison highlights products suited for various applications, from analog circuits to advanced ADC systems. Choose an amplifier that balances cost and performance while meeting your circuit's needs.

Look for reliable brands and suppliers

Reliable brands and suppliers ensure consistent quality and robust technical support. Companies like Texas Instruments, Analog Devices, and Infineon Technologies have a proven track record in producing high-performance sample-and-hold architecture components. Their products are widely used in critical applications, including satellite systems and nuclear power plants.

When evaluating suppliers, check for detailed documentation and customer reviews. Reliable brands often provide comprehensive datasheets and application notes, making it easier to integrate their amplifiers into your circuit. Partnering with trusted suppliers reduces the risk of performance issues and ensures long-term reliability for your analog systems.


Choosing the right sample-and-hold amplifier becomes easier when you follow a structured approach. Start by understanding your application’s requirements, such as signal type and sampling rate. Evaluate critical performance specifications like bandwidth and accuracy. Ensure the amplifier is compatible with your circuit’s voltage ranges and power supply. Consider practical design factors, including size and ease of integration. Finally, balance performance with cost to stay within your budget.

Tip: Consult manufacturers or industry experts for additional guidance. Their insights can help you make an informed decision and optimize your circuit’s performance.

By following these steps, you can confidently select an amplifier that meets your needs.

FAQ

What is a sample-and-hold amplifier used for?

A sample-and-hold amplifier captures and holds an analog signal's voltage for a specific time. It ensures the signal remains stable during processes like analog-to-digital conversion, where precise voltage levels are critical for accurate data representation.


How do you choose the right sampling rate?

You should select a sampling rate at least twice the highest frequency of your input signal. This follows the Nyquist theorem, ensuring accurate signal reconstruction without aliasing or distortion.


Why is bandwidth important in sample-and-hold amplifiers?

Bandwidth determines how well the amplifier handles high-frequency signals. A higher bandwidth ensures the amplifier can process fast-changing signals without losing accuracy or introducing distortion.


What is the hold mode droop rate?

The hold mode droop rate measures how much the output voltage changes while the amplifier holds the signal. A lower droop rate ensures better signal stability, which is crucial for high-precision applications.


Can environmental factors affect amplifier performance?

Yes, factors like temperature and electromagnetic interference can impact performance. Choose amplifiers designed for your operating environment to maintain accuracy and reliability.

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Related Articles

  • Introduction to MD8002A Audio Amplifier
    Introduction to MD8002A Audio Amplifier
    UTMEL27 March 20259704

    The MD8002A is an audio power amplifier that uses a 5V DC power supply to provide 2.0 watts of continuous power to a BTL load with less than 10% distortion. It was created with the aim of providing high-quality o/p control with fewer components. It doesn't use any output coupling capacitors or bootstrap capacitors.

    Read More
  • Understanding the Low Noise Amplifier (LNA)
    Understanding the Low Noise Amplifier (LNA)
    UTMEL20 March 202526398

    A low noise amplifier is an amplifier with a very low noise figure. It is generally used as a high-frequency or intermediate-frequency preamplifier for various types of radio receivers, as well as amplifying circuits for high-sensitivity electronic detection equipment.

    Read More
  • Introduction to Optical Amplifier
    Introduction to Optical Amplifier
    UTMEL27 March 202510372

    An optical amplifier is a subsystem product that can amplify optical signals in optical fiber communication systems. The principle of the optical amplifier is basically based on the stimulated radiation of the laser, which realizes the amplification effect by converting the energy of the pump light into the energy of the signal light.

    Read More
  • What is an Inverting Amplifier?
    What is an Inverting Amplifier?
    UTMEL25 April 202512285

    An inverting amplifier is a fundamental configuration of operational amplifiers where the output signal has opposite polarity to the input signal. This configuration uses an operational amplifier with its inverting input terminal receiving the input signal, while the non-inverting terminal is typically connected to ground. The primary function of this circuit is to amplify the input signal while inverting its phase by 180 degrees.

    Read More
  • Low-Power Design of Operational Amplifiers
    Low-Power Design of Operational Amplifiers
    UTMEL27 March 20257628

    Hello, this is Candy. With the rise in popularity of battery-powered electronics in recent years, analog circuit designers have been increasingly concerned about power usage. This article will cover how to use low-power op amps in system design, as well as low-power op amps with low supply voltage capabilities and their applications, as well as how to read and understand op amp data sheets appropriately. Circuit design with energy-saving technologies for more efficient device choices.

    Read More

Subscribe to Utmel !

Featured Parts More