cr2450 vs cr2032 what to know before replacing
You might wonder if you can swap a CR2450 for a CR2032 battery in your device. Both are lithium types and look similar, but they have key differences. CR2450 vs cr2032 batteries do not match in size or capacity. Using the wrong battery can cause poor performance, device malfunctions, or even damage. For example, a smaller button battery may not fit securely or deliver enough power, while a larger one could damage your device. Always check your device’s battery requirements before replacing any lithium battery. CR2450 vs cr2032 swaps can lead to more issues than solutions.
cr2450 vs cr2032 overview
Key Differences
When you compare cr2450 vs cr2032, you will notice several important differences. The most obvious difference is size. The cr2450 battery has a diameter of 24.5 mm and a thickness of 5.0 mm. The cr2032 battery is smaller, with a diameter of 20 mm and a thickness of 3.2 mm. This means the cr2450 is both wider and thicker than the cr2032. You can see these differences in the table below:
| Attribute | CR2450 | CR2032 |
|---|---|---|
| Diameter (mm) | 24.5 | 20 |
| Thickness (mm) | 5.0 | 3.2 |
| Weight (grams) | 6.3 | 3.1 |
| Capacity (mAh) | 620 | 240 |
| Voltage | 3V | 3V |
| Chemistry | Lithium | Lithium |
| Shelf Life (years) | >20 | 10-15 |
The cr2450 also has a much higher capacity. It stores about 620 mAh, while the cr2032 holds only 240 mAh. This means the cr2450 can power devices for a longer time. The cr2450 is heavier, too. You will find that the cr2450 works best in devices that need more power or longer battery life, such as smart door locks, LED lights, and medical tools. The cr2032 fits smaller devices like watches, calculators, and car key remotes.
You can see a visual comparison in the chart below:
Tip: Always check the size and capacity before choosing a replacement. Using the wrong battery can affect device performance and safety.
Similarities
Both cr2450 and cr2032 batteries share some key features. Each uses lithium chemistry, which gives them a stable 3V output. Both are non-rechargeable and have a long shelf life. You will find that both batteries follow the same industry labeling system. The "CR" stands for lithium manganese dioxide, and the numbers show the diameter and thickness in millimeters. This makes it easy to identify the right button battery for your device.
Both batteries work well in many electronic devices. They deliver steady voltage and reliable performance. You can trust either battery to power your device if you use the correct size. Both cr2450 and cr2032 batteries are safe when you use them as directed. However, you should always keep them away from children because of ingestion risks.
Note: Even though both batteries use lithium and have the same voltage, their size and capacity lead to performance differences. Always match the battery to your device’s needs for the best results.
cr2450 battery vs cr2032 battery specifications
Size Comparison
When you look at the cr2450 battery and the cr2032 battery, you will see clear differences in size. The cr2450 battery is larger and thicker than the cr2032 battery. This difference in size makes them fit different devices. You can check the table below to see the exact measurements:
| Feature | CR2450 Size | CR2032 Size |
|---|---|---|
| Diameter | 24.5 mm | 20 mm |
| Thickness | 5.0 mm | 3.2 mm |
The cr2450 battery has a diameter of 24.5 mm and a thickness of 5.0 mm. The cr2032 battery has a diameter of 20 mm and a thickness of 3.2 mm. Because the cr2450 battery is both wider and thicker, it will not fit in a device made for a cr2032 battery. Always check the size and thickness before you replace a button battery.
Tip: Using the wrong size can damage your device or cause it to stop working.
Capacity Comparison
The cr2450 battery and the cr2032 battery also have big differences in capacity. Capacity means how much energy the battery can store. The cr2450 battery usually has a capacity between 600 and 620 mAh. The cr2032 battery has a capacity between 210 and 230 mAh. This means the cr2450 battery can last almost three times longer than the cr2032 battery. If your device needs more power or longer battery life, you should use a cr2450 battery. Devices like smart door locks, LED lights, and medical tools often use the cr2450 battery for better performance. The cr2032 battery works well in smaller devices like watches, calculators, and car key remotes.
Voltage and Chemistry
Both the cr2450 battery and the cr2032 battery have a nominal voltage of 3 volts. This means they both deliver the same amount of electrical power. Both batteries use lithium manganese dioxide chemistry. The "CR" in their names shows they are lithium batteries. This chemistry gives them a long shelf life and stable voltage. Even though the cr2450 battery and the cr2032 battery have the same voltage and chemistry, their size and capacity make them suitable for different devices. You should always use the correct battery to get the best performance and safety.
cr2450 and cr2032 compatibility
Device Fit
You cannot swap a cr2450 battery for a cr2032 battery in your device. The cr2450 battery is larger in both diameter and thickness than the cr2032 battery. If you try to fit a cr2450 battery into a compartment made for a cr2032 battery, it simply will not fit. Forcing a larger battery can damage the compartment or the device itself. On the other hand, if you use a cr2032 battery in a slot designed for a cr2450 battery, the smaller size means the battery will not stay in place. This loose fit can cause the battery to move around, lose contact, or even fall out.
Tip: Always check the battery compartment label or your device manual before replacing a battery. The correct size ensures a secure fit and reliable operation.
Common problems from using the wrong battery size include:
The battery does not fit or sits loosely.
The device will not power on or works only sometimes.
The battery compartment or terminals get damaged.
Performance Impact
The cr2450 battery and the cr2032 battery have different capacities and are designed for different power needs. The cr2450 battery stores much more energy than the cr2032 battery. If your device needs a cr2450 battery and you use a cr2032 battery instead, you will notice shorter battery life and poor performance. The device may shut down unexpectedly or fail to work at all. Using a cr2450 battery in a device made for a cr2032 battery can also cause problems. The device may not handle the higher capacity or thicker size, leading to unpredictable performance differences.
You should always match the battery to your device’s requirements. Devices that need more power, such as smart locks or medical tools, require the higher capacity of a cr2450 battery. Smaller devices like watches or remotes work best with a cr2032 battery. Using the wrong battery can cause:
Reduced battery life
Unstable voltage or power loss
Device malfunction or failure
Note: The cr2450 vs cr2032 comparison shows that each battery serves a specific purpose. Using the correct battery ensures the best performance and protects your device.
Safety Issues
Using the wrong battery size can create serious safety risks. If you force a cr2450 battery into a cr2032 battery compartment, you may damage the compartment or the battery itself. This damage can lead to poor electrical contact or mechanical stress. When a battery does not fit properly, it can move around and scrape against metal parts. This movement increases the risk of short circuits, overheating, or even fire.
Lithium batteries, like the cr2450 battery and the cr2032 battery, are sensitive to physical damage and electrical abuse. Poor contact or mechanical stress can cause internal damage, leading to heat buildup, leakage, or thermal runaway. In extreme cases, the battery can vent with flame or explode. Always handle lithium batteries with care and use the correct size for your device.
| Regulatory Requirement | Description |
|---|---|
| Secure Battery Compartments | Devices must prevent child access to reduce ingestion risk. |
| Child-Resistant Packaging | Packaging must be child-resistant to prevent accidental ingestion. |
| Warning Labels | Labels must warn about ingestion hazards and provide medical instructions. |
| Safety Standards | Compliance with UL 4200A, EN IEC 60086, and other safety standards. |
| Substance Restrictions | Limits on hazardous substances like mercury and nickel. |
| Documentation & Testing | Technical documentation and safety testing are required. |
Alert: Always follow safety guidelines and use only the battery size specified by the manufacturer. This protects you, your device, and those around you.
You should never try to modify the battery compartment or force a battery to fit. If you are unsure, check the device manual or the label inside the battery compartment. Using the correct cr2450 battery or cr2032 battery keeps your device safe and working as intended.
correct battery replacement tips
Checking Device Requirements
You should always check your device’s manual or the label inside the battery compartment before replacing a cr2450 or cr2032 battery. Manufacturers design each device to work with a specific battery size. Using the wrong battery can cause your device to malfunction or even stop working. Many users report problems like error messages, short battery life, or sudden shutdowns when they do not match the correct battery to their device. Some devices may even warn you if the battery is not genuine or compatible. You can avoid these issues by confirming the exact battery type your device needs.
Follow these steps for safe battery replacement:
Power down your device and unplug it from any power source.
Open the battery compartment carefully.
Remove the old cr2450 or cr2032 battery.
Insert the new battery of the same type, making sure it fits securely.
Close the compartment and reconnect power.
Set up your device if needed.
Tip: Never try to force a cr2450 battery into a slot made for a cr2032 battery or the other way around. This can damage your device and create safety risks.
Equivalent Battery Options
When you need to replace a cr2450 or cr2032 battery, you may see different model numbers from various brands. These numbers often mean the same size and type. For the cr2450 battery, common equivalents include DL2450, EC2450, KL2450, LM2450, and BR2450. The BR2450 is a mercury-free option with similar capacity. For the cr2032 battery, DL2032 and BR2032 are popular substitutes. Major brands like Panasonic, Sony, Duracell, Energizer, and Varta make reliable cr2450 and cr2032 batteries. These brands offer high-quality batteries with long shelf life and safe performance.
| Battery Type | Common Equivalents | Popular Brands |
|---|---|---|
| cr2450 | DL2450, EC2450, KL2450, LM2450, BR2450 | Panasonic, Sony, Duracell, Energizer, Varta |
| cr2032 | DL2032, BR2032 | Panasonic, Sony, Duracell, Energizer, Varta |
⚠️ Alert: Never substitute a cr2450 for a cr2032 or vice versa. Even though both have the same voltage, their size and capacity are different. Always use the battery size listed by your device’s manufacturer.
To avoid counterfeit batteries, buy only from trusted sellers and check the packaging for signs of tampering. Counterfeit cr2450 and cr2032 batteries may have lower capacity, shorter life, or even leak. Dispose of used batteries at certified recycling centers to protect the environment and prevent fire hazards.
cr2450 vs cr2032 quick reference
Comparison Table
You can use this table to quickly compare the main features of the cr2450 and cr2032 batteries. This side-by-side view helps you choose the right battery for your device. Notice the differences in size, capacity, and typical applications.
| Specification | cr2450 | cr2032 |
|---|---|---|
| Chemical Composition | LiMnO2 | LiMnO2 |
| Nominal Voltage | 3 V | 3 V |
| Size (Diameter x Height) | 24.5 mm x 5.0 mm | 20 mm x 3.2 mm |
| Capacity | 600-700 mAh | 200-250 mAh |
| Weight | 6.9 grams | 3 grams |
| Operating Temperature | -20°C to +50°C | -20°C to +85°C |
| Typical Applications | Calculator, remote control, Bluetooth devices | Watch, electronic scale, car key |
You see that the cr2450 offers a larger size and higher capacity. This makes it better for devices that need more power or longer battery life. The cr2032 fits smaller devices and works well in items like watches and car keys. Both batteries use the same chemistry and voltage, but their size and capacity set them apart.
Tip: Always check your device’s manual or battery compartment before choosing between cr2450 vs cr2032. The right fit ensures safe and reliable performance.
Replacement Checklist
Follow this checklist to replace your cr2450 or cr2032 battery safely:
Make sure the device cover closes tightly. Use screws or tape for extra security.
Remove old batteries with care. Tape the terminals to prevent short circuits.
Store used batteries in a safe container, away from children.
Choose lithium coin batteries with child-safe packaging or bitter coatings.
Check your devices often to confirm covers stay secure.
Teach family and caregivers about battery safety.
If a child swallows a battery, get medical help right away.
⚠️ Alert: Never leave batteries where children can reach them. Proper handling keeps everyone safe.
You should never swap a cr2450 for a cr2032 in your device. The cr2450 has a different size and capacity, so using the wrong battery can cause device failure or safety risks. Always choose the cr2450 if your device manual lists it. Following the correct cr2450 guidelines helps you avoid overheating, damage, or short battery life. Research shows that using the right cr2450 extends device life and reduces costs. Manufacturer advice also points to better performance and safety with the proper cr2450. Check the quick reference table and checklist before you replace your cr2450. Always follow the cr2450 instructions for best results.
FAQ
Can you use a CR2450 battery in place of a CR2032?
You cannot use a CR2450 in a device that needs a CR2032. The CR2450 is larger and will not fit. Always check your device’s manual for the correct battery size.
What happens if you put the wrong battery in your device?
If you use the wrong battery, your device may not work. You could damage the battery compartment or cause the device to malfunction. Always match the battery type to your device.
How do you know which battery your device needs?
You can find the correct battery type in your device’s manual or on the label inside the battery compartment. Look for the battery code, such as CR2450 or CR2032, before buying a replacement.
Are CR2450 and CR2032 batteries safe for children?
Both batteries can be dangerous if swallowed. Keep them away from children. Choose batteries with child-safe packaging and always secure the battery compartment.
Tip: If a child swallows a battery, seek medical help right away.
Power Converter with Inbuilt Charging technology using WBG DevicesSaumitra Jagdale18 January 20242224Although plug-in electric vehicles (PEVs) have gained traction globally, reducing cost, weight, and volume, while enhancing power conversion efficiency in chargers remains crucial. PEVs, recognized by governments for curbing fossil fuel consumption and emissions, rely on sizable battery packs for substantial all-electric range coverage.
Read More
How to Choose the Best Deep Cycle Battery in 2024 | Reviews and Buying GuideUTMEL21 July 20252483You will learn about deep-cycle batteries in this post, including their main characteristics, things to think about while selecting one, and more.
Read More
CR123A vs 123A Batteries Explained for 2025UTMEL27 May 20252917CR123A and 123A batteries differ in capacity, lifespan, and compatibility. Learn how these differences affect your device's performance and safety.
Read More
A Guide to the Best AG13 Battery SubstitutesUTMEL27 May 20251795Discover the top AG13 battery equivalents for 2025, including LR44, SR44, 357, and A76. Compare performance, compatibility, and cost for your devices.
Read More
CR2450 vs CR2032 BatteriesUTMEL18 June 20252010CR2450 vs CR2032: CR2450 offers higher capacity and is larger, ideal for high-drain devices, while CR2032 suits compact, low-power gadgets. Learn more.
Read More
Subscribe to Utmel !
MS27484E16B8PCCorsair
934815330TE Connectivity
098371-0000ITT
D38999/24JC8PB-LCTE Connectivity
881545-1TE Connectivity AMP Connectors
5745781-4TE Connectivity AMP Connectors
65474-001LFAmphenol ICC (FCI)
![8225-6000]()
SNT-100-BK-T-HSamtec Inc.
S1731-46RHarwin Inc.


Product
Brand
Articles
Tools