An Overview of Fiber Optic Cable

Optical fiber cables, how do they work?
Topics Covered in this Article:
What is a fiber optic cable?
Fiber optic cables are designed to meet certain optical, mechanical, and environmental requirements. It is a communication cable assembly that uses one or more optical fibers placed in a sheath as a transmission medium and can be used individually or in groups. It has the advantages of large capacity, long relay distance, good confidentiality, immunity to electromagnetic interference, and saving copper. Optical fiber communication is one of the important ways of modern information transmission.

fiber optic cable
Optical fiber is a kind of fiber composed of two layers of transparent media in concentric circles. Quartz glass is the most extensively used dielectric substance (SiO2). The inner medium is known as the core, and it has a greater refractive index than the outer media (called the cladding). Doping impurities in the quartz glass, such as germanium, phosphorus, fluorine, boron, and others, change the refractive index of the core or cladding. The wavelength of light transmitted by optical fiber for communication is primarily near-infrared light with a wavelength of 0.8 to 1.7 microns. The core diameter of the optical fiber varies with the type, usually a few microns to 100 microns, and the outer diameter is mostly about 125 microns.
What is the structure of fiber optic cable?
A multi-layer coaxial cylinder, consisting primarily of a core, cladding, and coating layer, is the usual structure of an optical fiber.

Typical structure of the optical fiber
Fiber core
The fiber core is at the center of the optical fiber. The material is made up mostly of high-purity silica with a tiny quantity of dopant. The core has a little higher refractive index than the cladding, and it has a smaller loss than the cladding. The core is where the majority of the light energy is conveyed.
Cladding
The cladding is located around the core. It also contains a minor amount of dopants and is made out of high-purity silica. The cladding acts as a reflector and light isolator for light transmission, as well as providing some mechanical protection.
Coating
The optical fiber's outermost layer is made up of acrylate, silicone rubber, and nylon. The coating protects the optical fiber from water vapor erosion and mechanical abrasion.
How do fiber optic cables work?
Optical fiber transmission is based on the principle of total reflection of available light at the interface of two media. n1 is the refractive index of the core medium. n2 is the refractive index of the cladding medium. n1 is greater than n2. The light entering the core has an incident angle when it reaches the interface between the core and the cladding. When the incident angle is greater than the critical angle of total reflection θc, total reflection can occur without light energy passing through the core. And the incident light can be transmitted forward through countless total reflections at the interface.

When the optical fiber is bent, the normal line of the interface turns, and the incident angle is small. Therefore, the incident angle of a part of the light becomes smaller than θc and cannot be totally reflected. However, those rays with a larger incident angle can still be totally reflected, so the light can still be transmitted when the optical fiber is bent, but it will cause energy loss. Generally, when the bending radius is greater than 50 to 100 mm, the loss is negligible. Small bending will cause serious "micro bending loss".

Total reflection path
People often use electromagnetic wave theory to further study the mechanism of optical fiber transmission. They the boundary conditions of the optical fiber dielectric waveguide to solve the wave equation. The light propagating in the optical fiber contains many modes, and each mode represents an electromagnetic field distribution and corresponds to a certain light described in geometric optics. The conduction mode existing in the fiber depends on the normalized frequency ν value of the fiber.

Where NA is the numerical aperture, which is related to the refractive index of the core and cladding medium. ɑ is the core radius, and λ is the wavelength of the transmitted light. When the fiber is bent, mode coupling occurs. A part of the energy is transferred from the conduction mode to the radiating mode and is lost outside the core of the fiber.
What is the difference between fiber optic cable and network cable?
Fiber optic cable and network cable look similar in appearance, and they are both used in network communication. What are the specific differences?
1. Different materials: Most optical fibers are made of glass fiber, which is used as a light transmission tool. The transmission principle is "total reflection of light". The network cable is a copper core. There are mainly three types of lines: coaxial cable, optical cable, and twisted pair. The difference in materials also led to the difference in technical indicators between the two.
2. Transmission distance: Theoretically, the transmission distance of the network cable is within 100 meters. The single-mode fiber optic cable can realize the transmission of 10-20km, and the multi-mode fiber optic cable can realize the information transmission of 2km and 3km, which is much higher than that of the network cable.
3. Role: The optical fiber is to accelerate the transmission speed of network information, and exists as an information transmission tool. The network cable is used to connect the equipment to ensure intercommunication between the equipment.
4. Application scenarios: The network cable is used for communication transmission, which can provide users with interactive multimedia information of communication, data, and views, such as network interactive games, remote video monitoring, work conference videos, etc. The network cable is to connect the equipment, engineering wiring, network connection, equipment port connection, etc...
5. Product nature: Network cable is the carrier of information transmission and a kind of physical medium. The optical fiber is an abstract concept, which is the transmission rate of dynamic information.
6. Existence mode: Optical fiber exists in a virtual manner, and optical fiber cable is the carrier of its existence. The network cable is a real cable with concrete objects.
What is the fastest fiber optic cable?
Modern people's lives are inseparable from the Internet. It can even be said to be a very important part of life. Recently, a lecturer from University College London (UCL) has researched the fastest data transmission speed in the world. Using 16.8 THz bandwidth reached 178 Tbps, which is 178,000,000 Mbps, setting a world record. The speed of data transmission is really unimaginable. If you take a practical example, 178 Tbps can download all Netflix videos in less than 1 second.
Fiber optic cables are divided into single-mode and multi-mode. Single-mode refers to an optical fiber that can only transmit one mode, and multi-mode refers to an optical fiber that can transmit multiple modes. How to see whether the fiber optic cable is single-mode or multi-mode:
1. Look at the color, usually orange is multi-mode, and yellow is single-mode.
2. Look at the model. The single-mode fiber optic cables are usually GYTS and GYXTW, while the multi-mode models are GYFTZY and GYFTY.
3. It is distinguished by basic identification, SM is single-mode, and MM is multi-mode.
4. It can also be distinguished according to the transmission mode of light in the optical fiber.
What are the commonly used fiber optic cable models?
Common types of optical cables: G.651, G.652, G.653, G.654, G.655, and G.656.
(1) The G.651 category is a multimode fiber. IEC and GB/T are further subdivided into four subcategories A1a, A1b, A1c, and A1d according to their core diameter, cladding diameter, and numerical aperture parameters.
(2) G.652 category is a conventional single-mode fiber, currently divided into four sub-categories G.652A, G.652B, G.652C, and G.652D, IEC and GB/T named G.652C as B1.3. And the rest are named B1.1.
(3) G.653 fiber is a dispersion-shifted single-mode fiber. IEC and GB/T classify G.653 fiber as type B2 fiber. G.653 fiber is suitable for point-to-point long-distance, high-speed single-channel systems.
(4) G.654 fiber is a cut-off wavelength shifted single-mode fiber, also known as 1550nm best performance fiber. IEC and GB/T classify G.654 fiber as type B1.2 fiber. It is mainly used for non-relay submarine optical cable communication systems that have long transmission distances and cannot be inserted into active devices that require particularly high attenuation.
(5) G.655 fiber is a non-zero dispersion shift single-mode fiber, currently divided into three sub-categories G.655A, G.655B, and G.655C. IEC and GB/T classify G.655 fiber as B4 Class fiber.
(6) Non-zero dispersion single-mode fiber for wideband optical transmission of G.656 fiber, currently not named by IEC and GB/T. G.656 fiber can be used in the wide band of S+C+L (1460~1625nm).
How will fiber optic cable evolve in the future?
The structure of fiber optic cables evolves with the development of optical networks and the requirements of the environment in which they are used. The new generation of all-optical networks requires fiber optic cables to provide wider bandwidth, accommodate more wavelengths, transmit higher rates, facilitate installation and maintenance, and have a longer service life. The emergence of new materials for fiber optic cables has, in turn, promoted the improvement of the structure of fiber optic cables, such as the use of dry water-blocking materials, nano-materials, flame retardant materials, etc., so that the performance of fiber optic cables has improved significantly. In recent years, the emergence of ecological fiber optic cable, nanotechnology fiber optic cable, micro fiber optic cable and other emerging fiber optic cable.
Ecological fiber optic cable: mainly from the perspective of environmental protection, to solve the problem of fiber optic cable containing environmentally unfriendly materials, such as PVC burning will release toxic gases, optical cable stabilizers contain lead. This kind of fiber optic cable is mainly used in indoor, building and home. At present, some companies have produced some new materials for such cables, such as halogen-free flame retardant plastic.
Nanotechnology fiber optic cable: the use of nanomaterials (such as nano fiber coating, nano fiber optic grease, nano sheath with polyethylene, fiber optic sheath nano PBT) fiber optic cable, the use of nanomaterials have many excellent properties, such as improving the mechanical impact resistance of fiber optic cable.
Micro fiber optic cable: micro fiber optic cable is mainly used in order to cooperate with the use of pneumatic or hydraulic installation construction system, a variety of micro fiber optic cable structure has been designed and used, requiring a certain coefficient between the fiber optic cable and the pipe, the weight of the cable to be accurate and have a certain degree of hardness, etc... Micro fiber optic cable and automatic installation in order to adapt to the future needs of access networks, especially in the user premises network-integrated cabling system, in intelligent buildings in the intelligent pipeline wiring.
In summary, fiber optic cable with the development of higher technology in optical networks, continue to improve in structure, new materials, and performance improvements to meet the diverse needs of future communications, such as the 5G era of massive data-bearing, massive connectivity needs.
How Big is the DV/DT and DI/DT of the Power Device?UTMEL24 April 202211820Hello everyone, I am Rose. Welcome to the new post today. This article describes how big the dv/dt and di/dt of high-speed power devices are?
Read More
Why is 50 ohms?UTMEL13 June 202211763Hello everyone, I am Rose.Welcome to the new post today. Today We will discuss why impedance is 50ohm, not 30ohm, 75ohm or 100ohm?
Read More
What is Cat 7 Cable?UTMEL04 January 20228680Cat 7 cable is the latest twisted pair in the ISO/IEC 11801 Cat 7 / Class F standard, which is designed to accommodate the application and development of 10 Gigabit Ethernet technology.
Read More
What is a USB Data Cable?UTMEL27 August 202115413The USB data cable is used for the connection and communication of the computer and external devices. It can also be used for the charging of the phone and the external connection. It is popular for transmitting data and charging.
Read More
Understanding of Coaxial CableUTMEL06 August 202140073Coaxial cable is a broadband transmission line with low loss and high isolation characteristics. This blog introduces the classification, structure, working principle, parameters, and characteristics of coaxial cables.
Read More
Subscribe to Utmel !
ABM3-19.6608MHZ-D2Y-TAbracon LLC
ABLS-16.000MHZ-K4TAbracon LLC
AB308-4.9152MHZAbracon LLC
AB308-12.288MHZAbracon LLC
ECS-120-18-18-TRECS Inc.
ABLS-14.7456MHZ-B4H-TAbracon LLC
ABLS-11.0592MHZ-TAbracon LLC
ABM10-26.000MHZ-7-A15-TAbracon LLC
7B-27.120MEEQ-TTXC Corporation
ABL-30.000MHZ-B4Y-TAbracon LLC


Product
Brand
Articles
Tools