web counter

Understanding of Coaxial Cable

Published: 06 August 2021 | Last Updated: 06 August 202140138
Coaxial cable is a broadband transmission line with low loss and high isolation characteristics. This blog introduces the classification, structure, working principle, parameters, and characteristics of coaxial cables.
In this video, coaxial cables types, applications are to be discussed.

Coaxial Cables | Types | What is coaxial cable used for?

Catalog

What is Coaxial Cable?
What are the main types of Coaxial Cable?
What does a Coaxial Cable look like?
How do Coaxial Cables work?
Coaxial cable advantages and disadvantages
What is the difference between the coaxial cable and ordinary cable?
Parameter Index of coaxial cable
What are the characteristics of different dielectric materials of coaxial cable?

 

What is Coaxial Cable?

A coaxial cable is a type of wire that transmits signals. Four layers of materials form a coaxial cable: the innermost line is a conductive copper wire, and the outside of the line is surrounded by a layer of plastic (for insulator and dielectric). There is a thin layer of net-like conductors outside the insulator (usually copper or alloy). Outside the conductor is the outermost insulating material as the outer skin.

Coaxial Cable.jpg

Coaxial Cable

Analog and digital communications can both be transmitted using coaxial lines. They can be used for a variety of purposes, the most common of which are television broadcasting, long-distance phone transmission, short-distance computer system connections, and local area networks. Coaxial cable has grown in popularity as a means of distributing television signals to thousands of homes. A coaxial cable for TV system can carry dozens, if not hundreds, of TV channels, with a transmission range of tens of kilometers. Long-distance telephone networks have relied on coaxial cable for years. Fiber optics, terrestrial microwaves, and satellites are all posing rising rivalry today.

What are the main types of Coaxial Cable?

Baseband coaxial cables and broadband coaxial cables are the two primary coaxial cable types.

Baseband coaxial cable

The baseband coaxial cable's shielding layer is commonly a copper mesh structure with a characteristic impedance of 50. The most common versions are RG-8 (thick cable) and RG-58 (thin cable) for transmitting digital signals (thin cable). The diameter of a thick cable vs a thin cable is the most obvious distinction. Thick cable is ideal for medium-sized local networks. It has a vast standard range and a high level of dependability. However, the thick cable network requires transceivers and transceiver cables, which are both difficult to install, resulting in a high overall cost. The skinny cable, on the other hand, is simpler and less expensive. During the installation, however, the cable must be cut. As a result, when there are a lot of joints, it's easy to make bad contact.

Broadband coaxial cable

In most cases, the shielding layer of broadband coaxial cable is made of aluminum. It has a 75-ohm characteristic impedance. Analog communications are typically sent using this type of connection. The RG-59 is the most widely used model. It's a type of transmission cable that's commonly used in cable television networks. It may simultaneously broadcast numerous channels of TV signals over a single cable. Some computer networks can also use broadband coaxial cable as a transmission method.

What does a Coaxial Cable look like?

There are two coaxial conductors in a coaxial cable, one is the inner conductor and the other is the outer conductor. And their role can be imagined: one is the data transmission path, and the other is the data transmission loop. As shown below:

Coaxial Cable structure.png

Coaxial cable cross section.png

Inner and outer conductors make up the coaxial wire. The two conductors are arranged coaxially, and the transmission signal is completely confined in the outer conductor. The grounding of the outer conductor is a shielded transmission line to ensure good shielding performance, low transmission loss, and strong anti-interference. It is often used for the transmission of higher frequency signals. For common coaxial cables with copper conductors, the insulating material is usually Teflon or polyvinyl chloride.

How do Coaxial Cables work?

Four layers from the inside to the outside form the coaxial cable: the central copper wire (single-strand solid wire or multi-stranded wire), plastic insulator, mesh conductive layer, and wire sheath. A current loop is formed by the central copper wire and the mesh conductive layer. The coaxial interaction between the center copper wire and the meshed conductive layer gives it its name.

Coaxial cable material 2.jpg

Coaxial cable material

Instead of conducting direct current, coaxial cables conduct alternating current, which means the current's direction is reversed multiple times every second.

If a normal wire is used to transmit a high-frequency current, this wire will be equivalent to an antenna that emits radio outwards. The signal's power is lost, and the received signal's strength is reduced as a result of this consequence.

The coaxial cable can solve this problem. The radio emitted by the central wire is isolated by the mesh conductive layer, which can be grounded to control the emitted radio.

There is also a problem with coaxial cables. If a certain section of the cable is squeezed or twisted, the distance between the center wire and the mesh conductive layer is not consistent, which will cause the internal radio waves to be affected. In this case, the internal radio waves will be reflected back to the source of the signal. This effect reduces the receivable signal power. In order to overcome this problem, a layer of the plastic insulator is added between the center wire and the mesh conductive layer to ensure that the distance between them is consistent. This also causes the cable to be relatively stiff and not easy to bend.

The outside conductor of a coaxial cable is substantially improved by the shielding material. It has progressed from a tubular outer conductor to a single-layer braided and double-layered metal. Although the tubular outer conductor has excellent shielding properties, it is difficult to bend and utilize. The shielding efficiency of single-layer braiding is the worst, and the transfer impedance of double-layer braiding is 3 times lower than that of one-layer braiding. It can be seen that the shielding effect of double-layer braiding has been greatly improved than that of single-layer braiding. Major coaxial cable manufacturers are constantly improving the outer conductor structure of the cable to maintain its performance.

Coaxial cable advantages and disadvantages

The advantage of coaxial cable is that it can enable high-bandwidth communication over a long distance without the use of a repeater, but it also has drawbacks. For starters, it's big, and a thin cable's diameter is 3/8 inch thick, so it takes up a lot of space. In the pipeline, there is plenty of room. The second disadvantage is that it is unable to endure tangles, pressures, or abrupt bends, all of which can destroy the cable structure and inhibit signal transmission. Last but not least, there is the expensive expense, but twisted pair can overcome all of these drawbacks.

What is the difference between the coaxial cable and ordinary cable?

Different materials:

Coaxial cables are made of copper conductors separated by insulating materials.

The constituent materials of ordinary cables are several wires or groups of wires.

Different categories:

Baseband and broadband coaxial cables are the two types of coaxial cables.

DC and AC cables are the two types of ordinary cables.

Different types:

Coaxial cables are divided into thin cable RG-58 and thick cable RG-11.

Ordinary cables are divided into flame-retardant rubber sheathed cables, nuclear-grade cables, bare wires, and bare conductor products, power cables, communication cables, and optical fibers, electromagnetic wires, and flexible fire-resistant cables.

Parameter Index of coaxial cable

Coaxial cable 2.jpg

Electrical parameters

(1) The characteristic impedance of the coaxial cable: the average characteristic impedance of the coaxial cable is 50±2Ω. The periodic change of the impedance along a single coaxial cable is a sine wave. The center average value is ±3Ω, and its length is less than 2 meters.

(2) Coaxial cable attenuation: It refers to the attenuation value of a 500-meter cable length in general. Its value does not exceed 8.5db (17db/km) when measured with a 10MHz sine wave, and it does not exceed 6.0db (12db/km) when measured with a 5MHz sine wave.

(3) The propagation speed of the coaxial cable: The minimum propagation speed required is 0.77C (C is the speed of light).

(4) Coaxial cable DC loop resistance: the sum of the resistance of the center conductor of the cable and the resistance of the shielding layer does not exceed 10 milliohms/m (measured at 20°C)

Physical parameter

A coaxial cable is composed of a central conductor, an insulating material layer, a shielding layer composed of mesh fabric, and an outer isolation material layer.

The coaxial cable is flexible enough to support a bending radius of 254mm (10 inches). The center conductor is a solid copper wire with a diameter of 2.17mm±0.013mm. The insulating material must meet the coaxial cable's electrical characteristics. A metal strip or sheet that meets the transmission impedance and ECM criteria serve as the shielding layer. The inner diameter of the shielding layer is 6.15mm and the outer diameter is 8.28mm. Polyvinyl chloride (PVC) or related polymers are commonly used for external insulation.

What are the characteristics of different dielectric materials of coaxial cable?

Like other cables, coaxial cables have different wire diameters and core diameters, conductor and insulation materials, and structures, and cable sheath materials. The combination of these parameters determines the electrical performance, mechanical performance, and environmental adaptability of the coaxial cable.

Impact on cable delay and propagation speed

The dielectric insulator (dielectric) in the cable is the main factor that affects the delay and propagation speed of the cable. The dielectric materials mainly include solid polyethylene (PE), polyethylene foam (FE/PF), air-insulated polyethylene (ASP), foamed polystyrene (FS), solid Teflon/solid polytetrafluoroethylene (ST /SPTFE), air-insulated Teflon (AST), and so on. The following table mainly summarizes the influence of various materials on cable delay and propagation speed.

The influence of various materials on cable time delay and propagation speed.png

The applicable working temperature of the insulating medium and outer skin

This determines the applicable environment of the selected cable, you can directly look at the following table.

Applicable working temperature of insulating medium and outer skin.png

Cable sheath material

1)If you need to wrap a certain cable around the object that needs to be connected, the cable sheath is preferably a highly flexible thermoplastic rubber (TPR). But, remember that it is best not to always move the cable with this cable sheath. That will affect performance.

2) For cables that are used in elevators and have flame-retardant requirements, special upright cables (CMR) must be used instead of polyethylene materials. The cable sheath can prevent the spread of flames to unfired areas.

3)For the cables in the hidden space of the horizontal path in the building, the mezzanine cable (CMP) bundled by Teflon outside can be used to prevent the cables from kinking together and only produce low toxicity when on fire.

4)If you need to route cables outside the building or along with the ceiling of the office, you can use PVC or TPR cable skins to increase flexibility without increasing insertion loss.

5)The sandwich cable with fluorinated ethylene propylene (FEP) material has the characteristics of low loss and high-temperature resistance.

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1.What is a coaxial cable used for?

Coaxial cable is commonly used by cable operators, telephone companies, and internet providers around the world to convey data, video, and voice communications to customers. It has also been used extensively within homes.

2.Are there different types of coaxial cable?

There are two main types of coaxial cables – ones with an impedance of 75 Ohm (Ω) and ones with an impedance of 50 Ohm. Cables with 75 Ohm are mostly used for video signals, while 50 Ohm cables tend to be used for data and wireless communications.

3.Is a coax cable the same as a TV cable?

Cable internet service uses the same coaxial cable network as cable television to provide your home with internet. First, your internet service provider sends a data signal through the coaxial cable, or coax cable, into your home—specifically, to your modem.

4.Which coaxial cable is best for digital TV?

RG6 coaxial cable

An RG6 coaxial cable is best used for connecting a TV set or set top box to a TV aerial, satellite dish, or satellite receiver. It is also used for the internet and digital video. RG-6 cables are made with a different kind of shielding and have a 75-ohm impedance, making them more effective for carrying GHz signals.

5.Is coax cable good for the Internet?

While you might not want to spend much money on a good coaxial cable. A high-quality coaxial cable boosts your internet connection speed by blocking radio frequency interference and minimizing signal loss.
Related Articles

  • How Big is the DV/DT and DI/DT of the Power Device?
    How Big is the DV/DT and DI/DT of the Power Device?
    UTMEL24 April 202211890

    Hello everyone, I am Rose. Welcome to the new post today. This article describes how big the dv/dt and di/dt of high-speed power devices are?

    Read More
  • Why is 50 ohms?
    Why is 50 ohms?
    UTMEL13 June 202211826

    Hello everyone, I am Rose.Welcome to the new post today. Today We will discuss why impedance is 50ohm, not 30ohm, 75ohm or 100ohm?

    Read More
  • What is Cat 7 Cable?
    What is Cat 7 Cable?
    UTMEL04 January 20228750

    Cat 7 cable is the latest twisted pair in the ISO/IEC 11801 Cat 7 / Class F standard, which is designed to accommodate the application and development of 10 Gigabit Ethernet technology.

    Read More
  • What is a USB Data Cable?
    What is a USB Data Cable?
    UTMEL27 August 202115460

    The USB data cable is used for the connection and communication of the computer and external devices. It can also be used for the charging of the phone and the external connection. It is popular for transmitting data and charging.

    Read More
  • Understanding of Coaxial Cable
    Understanding of Coaxial Cable
    UTMEL06 August 202140138

    Coaxial cable is a broadband transmission line with low loss and high isolation characteristics. This blog introduces the classification, structure, working principle, parameters, and characteristics of coaxial cables.

    Read More

Subscribe to Utmel !