RG6 VS RG59: Who is the winner?

Sophie

Published: 28 March 2022 | Last Updated: 28 March 2022

26383

RG6 versus RG59 appears to be a popular comparison among coaxial cable buyers. That is correct. The two most widely used coax wires are RG6 and RG59. Which one do you think you should pick? It depends on how you intend to use it. As a result, understanding the differences between RG6 and RG59 cables is critical for making the best decision. What's the difference between an RG6 cable and an RG59 cable? Allow Magi to educate you on the differences between RG6 and RG59 coax.

This video is about the difference between RG59 & RG6 coax cables.

The difference between RG59 & RG6 coax cables

Introduction

Coaxial cables, sometimes known as 'coax,' are the most common cables used in video and satellite installations. The RG59  and RG6  cables are two types of cables that can be used for various applications. The biggest difference between the two is the size of the RG6, which is larger than the RG59. The RG6  cable's inner conductor core is thicker, as is the shielding within the rubber sheath.

What is a Coaxial Cable?

It's a form of copper wire with a metal shield or other such components. This cable's purpose is to keep interference out of the cable. This cable is mostly used to connect a satellite antenna to a television set. There are several variants of this cable, but we'll focus on the RG6 and RG59 coaxial cables in this post.


What is RG?

RG ratings are used to differentiate between different types of coaxial cables. The acronym   RG  stands for "radio guide," a long-forgotten military word. The number identifies the various cable specifications, however, it is assigned at random, so don't expect any sort of order in the numbers. There have been dozens of coaxial cables developed throughout the years, but the only ones that most people need to worry about are RG  6 and RG  59 cables, so we'll focus on those two types here.

Overview of RG6

RG6-1.jpg

The RG6   cable was created with higher data frequency needs in mind. Because of its bigger conductor, this cable provides greater signal quality. It has a copper center conductor of 18 AWGSatellite and internet transmissions are compatible with this connection. The thicker dielectric insulation on RG6  coaxial is also present. It has a particular type of shielding that can tolerate signals at Gigahertz frequencies. Both foil and braided shielding  are used in RG6

Overview of RG59

RG591.jpg

RG59 has been around for a long time. This wire was used to connect televisions. This cable can still be found in most older homes and commercial structures. The copper wire conductor of the RG59  coax cable is 20   AWG. Because this cable has a smaller conductor, it cannot provide the same signal quality as RG6. Its shielding also fails to keep Gigahertz-level signals contained within the cables. This cable became practically obsolete as a result of all of these issues.

 

The insulation of the RG59  cable is braided. It's made for megahertz interference with lengthy waveforms. Because of this, it's ideal for low-frequency communications. It's suitable for anything with a frequency of less than 50MHz.


Properties of RG6 cables:

1. RG6 cables are made of foil shields and braided aluminum shields.

2. They have better insulation properties.

3. The inner conductor is thicker at the 18 AWG copper center. This helps RG6 cables provide more extended distance proficiency and better bandwidth.

4. The frequency range is better, which means if you are looking for a cable to serve the purpose of a higher frequency range, RG6 is your answer.

5. RG6 cables have low attenuation even though the cables are long.

6. Problems with RG6 come when you need them to work below 50 Mhz. They are not efficient in this case and you will need to use RG59. But these cables work better with frequencies over 50Mhz.

7. Fewer signal loss problems are reported with RG6.


Properties of RG59 cables:

1. RG59 cables are made of 95% copper shields, which helps them block RFI inclusion.

2. Insulation is not as good as RG6 cables.

3. The inner conductor of RG59 cables is a thin – 20 AWG copper center. This makes its diameter smaller than RG6.

4. The frequency range is lower. RG6 can work even with 3Ghz, but RG59 may start showing inefficiency upon touching 2 GHz.

5. If you need to work below 50 Mhz, RG59 is the way to go.

6. RG6 provides lower attenuation when compared to RG59. This is a significant drawback for RG59 cables.


Different applications of RG6 vs RG59

According to the description above, we know that RG6 and RG59 are used for different purposes. Let’s make it in detail.

1.RG6: Satellite DSS applications, CATV

2. RG59: Plasma TV, component video, video projectors, and other baseband video applications, CCTV. One cannot use these cables for satellite feeds because they do not have foil shields.


RG59 vs RG6: Signal Loss

What is the difference in signal loss between RG6 and RG59 coax cable? The shielding has something to do with signal loss. A cable's shielding can help to ensure optimum signal quality. The better the signal shielding, the less signal interference. Braided Mesh and Foil shielding are the most common types of shielding found in coaxial cables.

Both forms of shielding are used in RG6 cables to prevent signal interference. However, some RG59 cables are only shielded on one side. As a result, RG6 cables often have lesser signal loss than RG59 cables.


Furthermore, signal loss is proportional to transmission distance. The farther the cables are run, the greater signal loss occurs. In comparison to RG59 cables, RG6 cables can transport signals over longer distances while maintaining superior signal quality. As a result, RG6 cables are typically used for high-frequency applications such as television connections, whereas RG59 cables are better suited to low-frequency and short-distance transmission.

As a result, the graphic below might help you better comprehend the topic of coax RG6 versus RG59 on signal loss. It compares the signal loss of RG6 and RG59 at various frequencies.

Frequency50Mhz100Mhz400Mhz900Mhz1000Mhz
RG61.5dB2.0dB4.3dB6.8dB7.0dB
RG592.4dB3.4dB7.0dB11.1dB12.0dB


RG6 vs RG59 Cable: How To Tell?

What is the difference between RG6 and RG59 coax cables? There are messages on the PVC jacket of each coaxial cable if you look closely. It aids in determining whether this is an RG6, RG11, or RG59 coax cable. However, if the type names are overlooked, the cables may not be qualified or professional. These coaxial wires should not be purchased.

Another technique to distinguish between RG6 and RG59 coax cables is to compare their diameters. RG6 has a 6.90mm outer diameter, while RG59 has a 6.15mm outer diameter. Because it has a thicker center conductor, RG6 wire is thicker than RG59 cable. You'll see the difference when you separate the two cords.


Conclusion

RG6 cable has stronger insulation and greater shielding than RG5 cable. It's best for high-bandwidth or high-frequency communications like the Internet, Cable TV, and Satellite TV. If you're not sure which cable to choose, RG6 is the best option.

 

RG59 cable is thinner and less shielded than RG6 cable. Only low bandwidth and low-frequency applications, such as CCTV installations, are recommended.


Frequently Asked Questions

Is RG6 superior to RG59?

In comparison to RG59 cables, RG6 cables can transport signals over longer distances while maintaining superior signal quality. As a result, RG6 cables are typically used for high-frequency applications such as television connections, whereas RG59 cables are better suited to low-frequency and short-distance transmission.

What does the abbreviation RG59 mean?

In the Joint Electronics Type Designation System of the United States military, RG (for radio guide) was initially a unit indicator for bulk radio frequency (RF) cable. The suffix /U denotes that the item is intended for general utility use. The number 59 was assigned in a certain order.

Is it possible to utilize RG6 for CCTV?

RG6 can be utilized for video surveillance. It's also available with a solid copper core / inner conductor and copper braiding that's 95 percent copper. RG6 can be run longer distances without losing visual quality than RG59, but it is a thicker, more stiff cable that is less practical to deal with (especially around corners).

Which coaxial cable has the least amount of signal loss?

For long cable lines (more than 100 feet), Cable Type 400 or even better Cable Type 600 Low Loss Coaxial Cable is the best option for minimizing signal loss due to cabling.

Is it possible to utilize RG59 cable for satellite?

A crimped-on or twisted-on connector is frequently an indicator of an RG59 cable, simply because this type of connector isn't common anymore, and RG59 cable isn't either. Crimp and twist-on connections can be used on RG6 cables, however, they are not suitable for satellite television.
RG6WRO,TW

Belden Inc.

In Stock

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe

Related Parts More