Fiber Optic Connectors Explained: LC, SC, ST, FC and How to Choose

Fiber Optic Connector Types Explained in Details
A fiber optic connector is the small, precise fitting that joins two optical fibers, or a fiber to a piece of equipment, so light can pass across the junction with as little loss and reflection as possible. To the eye it looks like a simple plug, but most of the engineering hides inside a ceramic sleeve no wider than a pencil lead. Get the type, the polish, and the cleanliness right and a link runs quietly for years. Get them wrong and you chase intermittent faults that never show up on a quick visual check.
What a fiber optic connector does
The core of a single-mode fiber is only a few microns across, so the real job of a connector is alignment. Each fiber is bonded into a ferrule, usually a precision ceramic cylinder, with the fiber end polished flush to the ferrule tip. When two connectors mate, their ferrules slide into a split alignment sleeve that holds the two endfaces centered and pressed lightly together under spring load. That physical contact lets light cross the boundary with minimal scatter.

Figure 1. Inside a mated connector pair: each fiber is bonded into a ceramic ferrule, and a split alignment sleeve holds the two endfaces in spring-loaded physical contact so light crosses with minimal scatter.
Two things go wrong at that boundary. Light can be lost as it crosses (insertion loss), and light can bounce back toward the source where the glass meets air or another surface (return loss, sometimes called back-reflection). A good connector keeps both small and, just as important, keeps them consistent every time the link is unplugged and reconnected. Repeatability matters as much as a single good reading, because patch panels are mated and unmated throughout their service life.
The main connector types at a glance
Most installed fiber today uses a handful of connector families. They differ in size, in how they latch, and in the density they allow on a panel.

Figure 2. The five connector families you will meet in the field, shown at relative scale: compact duplex LC, square push-pull SC, bayonet-locking ST, threaded FC, and the multi-fiber MPO/MTP.
LC is a small-form-factor connector with a push-pull latch, the workhorse of high-density patch panels, single-mode runs, and transceiver ports. Its compact body lets two LC ferrules sit in the footprint of one older connector, which is why duplex LC dominates modern data and telecom equipment.
SC is a larger square-bodied push-pull connector. It is robust, easy to handle, and still common on older equipment, FTTH terminations, and anywhere a simple positive click is preferred over density.
ST uses a round body with a spring-loaded bayonet that you push and twist a quarter turn to lock. It appears widely in legacy multimode building cabling and some industrial settings.
FC is a round threaded connector that screws down onto the adapter. The metal coupling nut makes it stable under vibration, which is why it lingers in test equipment and measurement setups.
MPO/MTP is a multi-fiber connector that carries many fibers in a single rectangular ferrule, the backbone of parallel optics and high-speed trunk cabling in data centers. MTP is a branded, performance-enhanced version of the MPO design.
You may still encounter MU as a compact single-fiber connector and MT-RJ as a small two-fiber design; both are best treated as legacy or specialty parts rather than first choices for new work.
| Connector | Form / latch | Fiber count | Typical use today |
|---|---|---|---|
| LC | Small body, push-pull latch | One or two (duplex) | High-density panels, transceivers, single-mode and multimode links |
| SC | Square body, push-pull | One or two (duplex) | Older equipment, FTTH, simple field terminations |
| ST | Round body, bayonet twist-lock | One | Legacy multimode building cabling, some industrial |
| FC | Round body, threaded nut | One | Test and measurement, vibration-prone setups |
| MPO/MTP | Rectangular multi-fiber ferrule | Many (e.g. 8, 12, 16, 24) | Parallel optics, data-center trunks and breakouts |
Endface polish: PC, UPC, and APC
How the ferrule tip is polished changes how much light reflects back, so polish is a real selection decision, not a cosmetic one.
PC (Physical Contact) rounds the endface into a slight dome so the fiber cores touch under spring pressure rather than trapping an air gap. This is the baseline that makes low-loss mating possible.
UPC (Ultra Physical Contact) is a finer, more tightly controlled version of the same flat-domed geometry. It improves return loss over a basic PC finish and is the common choice for most data and Ethernet single-mode work.
APC (Angled Physical Contact) polishes the endface at a slight angle so any reflected light is directed out into the cladding instead of straight back down the core. That angle gives APC the best return-loss behavior, which is why it is favored for sensitive, high-power, or analog services such as RF-over-glass video and many passive optical network deployments.

Figure 3. UPC vs APC endface geometry: the flat-domed UPC face reflects light straight back down the core, while the 8-degree APC face steers reflections into the cladding — never mate the two together.
By long-standing convention, APC connectors are housed in green, while UPC single-mode parts are usually blue; multimode hardware tends to follow its own color family. A critical field rule follows from the geometry: never mate an APC connector to a UPC one. The angled and flat faces cannot make proper contact, and forcing them damages the endfaces and wrecks performance.
| Polish | Endface geometry | Reflection behavior | Common housing color | Where it fits |
|---|---|---|---|---|
| PC | Domed, flat finish | Baseline | Varies | Older or general-purpose links |
| UPC | Domed, finer polish | Better than PC | Blue (single-mode) | Most single-mode data and Ethernet |
| APC | Angled (typically 8 degrees) | Best back-reflection control | Green | PON, RF video, high-sensitivity links |
How to identify connectors quickly
In a crowded patch panel the fastest tells are shape and latch:
SC versus LC comes down to size and footprint. SC is the larger square plug with a sliding push-pull body; LC is roughly half the size with a small lever latch like a tiny network cable clip, almost always seen as a side-by-side duplex pair.
ST versus FC are both round, so check the coupling. ST has a bayonet that you push and twist a quarter turn until it clicks, while FC has a knurled threaded nut you spin to tighten.
Color is a useful hint but not proof: a green boot strongly suggests APC, but always confirm the polish and connector type before mating into live equipment.
MPO/MTP is unmistakable, a wide flat rectangular ferrule with a guide-pin arrangement and a key that fixes its orientation.
Insertion loss, return loss, and what really hurts performance
The two numbers most people quote are insertion loss and return loss. Insertion loss measures how much signal is given up crossing the connection; return loss measures how strongly light reflects back toward the transmitter. Lower insertion loss and higher return loss are better, and the exact figures that count as "passing" depend on the application and on the standard or product specification you are working to, so confirm the target values in the relevant manufacturer datasheet or industry standard rather than assuming a universal number.
In day-to-day work, though, the dominant cause of poor performance is rarely the connector design at all. It is contamination. A single speck of dust, a fingerprint, or a trace of oil on a ferrule endface can scatter and block light, and pressing that contamination between two ferrules can scratch the glass permanently. The professional habit is simple and non-negotiable: inspect before you connect. Use a fiber inspection scope to check the endface, clean with proper dry or wet cleaning tools when needed, re-inspect, and only then mate. Treat every unmated connector as dirty until you have confirmed otherwise, and keep dust caps on whenever a connector is not in use.
How to choose a connector for your link
Choosing is mostly a matter of matching the connector and polish to the fiber type, the density you need, and the environment.
Fiber type: match single-mode or multimode hardware to the fiber you are running; the connector and adapter should suit the same class of fiber as the link.
Polish: UPC suits most single-mode data and Ethernet links, while APC is the right call for PON, analog RF video, and other reflection-sensitive or higher-power services. Multimode work generally uses a PC-class flat polish.
Density: when panel space and port count matter, LC and MPO/MTP win; SC and ST trade density for simple handling and legacy compatibility.
Environment: for vibration or frequent handling, a threaded FC or a securely latched design is reassuring; for routine patching, push-pull LC or SC is faster.
Consistency: standardize on as few connector and polish combinations as the network allows, so spares, patch cords, and cleaning tools stay interchangeable across the site.
Always verify the specific performance grade against a named standard or the product documentation before you commit to a build, and confirm that both ends of every mated pair share the same connector type and polish.
| Decision point | Ask yourself | Practical lean |
|---|---|---|
| Fiber class | Single-mode or multimode? | Match connector and adapter to the fiber class |
| Polish | Reflection-sensitive service? | UPC for general single-mode; APC for PON / RF video |
| Density | How many ports in the space? | LC or MPO/MTP for high density |
| Handling | Vibration or frequent moves? | FC threaded or firmly latched designs |
| Field discipline | Inspection tools on hand? | Plan cleaning and inspection before any mating |
FAQ
What are the most common fiber optic connector types?
LC and SC dominate current installations, with MPO/MTP carrying many fibers in data-center trunks. ST and FC remain common in legacy and test environments, while MU and MT-RJ are best treated as specialty or legacy parts.
What is the difference between FC and SC connectors?
FC is a round connector that screws down with a threaded nut, which keeps it stable under vibration and makes it popular in test equipment. SC is a larger square connector that mates with a simple push-pull motion, favored for quick, positive connections on older gear and FTTH.
How do I tell ST and LC connectors apart?
ST is round and locks with a push-and-twist bayonet, taking a single fiber. LC is a much smaller rectangular plug with a small lever latch, usually arranged as a duplex pair, and is built for high-density panels and transceivers.
When should I use APC instead of UPC?
Reach for APC when back-reflection must be tightly controlled, such as passive optical networks and RF-over-glass video. UPC is fine for most single-mode data and Ethernet links. Never mate APC to UPC, because the angled and flat faces cannot make proper contact.
Why does my fiber link lose signal even with the right connector?
Contamination is the usual culprit. Dust, oils, or fingerprints on the ferrule endface scatter light and can scratch the glass when mated. Inspecting and cleaning before every connection fixes far more problems than swapping connector types does.
Can I mix single-mode and multimode connectors?
The connector body may physically fit, but the fiber types are not interchangeable for performance. Keep single-mode and multimode hardware aligned with their matching fiber throughout the link, and confirm the class at both ends.
What insertion-loss or return-loss figure should I aim for?
The target depends on the application and the standard or product you are building to, so read the figure from the relevant manufacturer datasheet or industry standard rather than relying on a single universal value.
Sources and references
The Fiber Optic Association reference library explains connector construction, ferrule alignment, and the role of polish and cleaning in plain technical language, which is useful for grounding definitions. It is an educational body rather than a product source, so confirm any specific performance grade against the hardware you actually buy.
TIA (Telecommunications Industry Association) develops the structured-cabling standards that define how connector performance is specified and tested. The detailed numeric thresholds live in paid standards documents, so treat the public site as a pointer to the relevant standard rather than the figures themselves.
Corning's fiber and connectivity resources document real connector and polish options with manufacturer datasheets, which helps when you need to confirm a spec for a specific part. As a vendor library it naturally centers on Corning's own catalog, so cross-check when comparing across brands.
CommScope's fiber connectivity pages describe LC, SC, MPO and related systems with installation and selection guidance. The material is tied to their product lines, so use it for concepts and confirm exact values on the datasheet for your chosen item.
Senko's connector resources cover a broad range of connector and polish designs from a specialist connector maker, useful for understanding form factors and endface options. Being a manufacturer site, it reflects their portfolio, so verify any figure against the specific part number you intend to use.
High-speed Connectors Shortage Outlook 2026: Supply, Lead Times, and Sourcing OptionsUTMEL16 July 2026906Entering 2026, the electronics supply chain faces a bifurcated market. While standard connectors remain stable, high-speed interconnects, RF modules, and optical transceivers experience severe shortages driven by rapid AI infrastructure growth. To mitigate these bottlenecks, engineering and procurement teams must adopt proactive design-for-availability strategies, utilize multi-footprint layouts, and leverage alternative global sourcing channels like UTMEL to secure critical BOM components.
Read More
The Introduction to USB Type-C Pin Signal and PCB LayoutUTMEL03 December 202127540Hello everyone. Welcome to the new post today. USB Type-C is a smaller-volume USB interface standard than Type-A and Type-B. It can be used on a PC (master device) as well as external devices (slave devices, such as mobile phones).
Read More
Everything You Need to Know about ConnectorsUTMEL07 September 20218758Electrical connectors, as key components for current or signal connections, are also an important part of the industrial system. Connectors can be as huge as airplanes and rockets or as small as mobile phones and televisions, forming bridges between circuits or other components and serving as electric current or signal links.
Read More
Network Interface Card: Types, Functions and Buying GuideUTMEL17 August 202111035Network Interface Card (NIC, also known as a network interface controller) is one of the most basic components in the local area network. It is the hardware device connecting the computer and the network. Whether it is a twisted pair connection, a coaxial cable connection, or an optical fiber connection, data communication must be realized with the help of a network interface card.
Read More
What is Universal Serial Bus (USB)?UTMEL12 June 202613247Universal Serial Bus (USB) is a serial bus standard and a technical specification for input and output interfaces. It is widely used in information communication devices. The latest generation is USB4, and its transmission speed is 40Gbit/s, the three-stage voltage is 5V/12V/20V, the maximum power supply is 100W.
Read More
Subscribe to Utmel !
TH30Teledyne LeCroy
RHT35Teledyne LeCroy
989KL61T00EAdvantech
ACP-4010MB-00XEAdvantech
AMO-R002EAdvantech
DMB54D0UV-13Diodes
ION219-AAMB-BRLantronix
ION106-AAB-UKLantronix
ION106-AAMB-LALantronix
ION106-AAB-ARLantronix


Product
Brand
Articles
Tools