web counter

Exploring the Strengths and Hurdles of Wide Bandgap Devices in Alternating Current Electric Drives

Published: 19 January 2024 | Last Updated: 19 January 20243783
Wide-bandgap materials have emerged as pioneers in the era of power devices, altering the performance and efficiency of electronic systems. Silicon, the traditional semiconductor material, has limitations that become apparent as power requirements escalate. WBG materials, such as silicon carbide and gallium nitride, possess high switching frequency, low losses and high-temperature operating capability making them an ideal choice in power devices.

This characteristic translates into reduced energy losses and enhanced power density, making WBG devices ideal for applications like power converters and inverters in electric vehicles and renewable energy systems. The unique electrical properties of WBG materials pave the way for more compact, lightweight, and efficient power electronics, fostering the transition towards a greener and more sustainable energy landscape. 

Furthermore, the deployment of WBG materials in power devices has profound implications for the aerospace and telecommunications industries. The high-frequency capabilities of WBG semiconductors allow for the design of more efficient and compact power electronics in satellite systems and communication devices. 

With the relentless demand for miniaturization and increased performance, WBG materials serve as catalysts for technological advancements, advancing industries into a new era of energy-efficient and high-speed electronic solutions. As research and development in WBG materials continue to flourish, the integration of these materials into power devices is poised to redefine the possibilities and efficiencies of electronic systems across diverse sectors.

Examining the Superiority and Role of WBG Devices in Motor Drives


Motor drives, the basic building block of electromechanical systems, are the beating heart behind the seamless connection of machinery and devices. Motor drives regulate the speed, torque, and direction of electric motors, translating electrical energy into precise mechanical motion, therefore it is important for these drives to have the maximum efficiency and precision. As a result, WBG devices are being integrated into motor drives for numerous applications such as the operation of high-speed motors, low-inductance motors and electric drives operating in high temperatures. Low inductance motors for instance can utilize Si MOSFETs as they have the capability to switch up to 50 kHz and provide the desired current ripple which ultimately enhances reliability and efficiency. Traditional materials like Si lack the required critical electric field as shown in Figure 1, which makes WBG devices an ideal choice for electric drives.


Comparison of key electrical parameters in Wide bandgap materials and Silicon.png

Figure 1: Comparison of key electrical parameters in Wide bandgap materials and Silicon


On the other hand, the popularity of high-speed electric machines has been on the rise mainly due to their superior power density, which is made possible by integrating the motor with a compressor via the gearbox. Therefore, the high-frequency ability of SiC Mosfets was taken into consideration which ultimately enabled the motor to run at the same speed as the compressor, thereby eliminating the gearbox. This innovation alone increased the reliability and the efficiency of GaN-based by around 4 percent when compared to traditional Si-based motor drives. 

Semiconductors with a wider bandgap can operate at high temperatures when compared to conventional silicon. Integrated motor drives have been gaining a lot of popularity as they directly replace the inefficient online direct motors however, as the converter and the motor are in proximity, the temperature is at an all-time high. Therefore, the development of WBG power modules with high frequency and reverse voltage blocking has proven to be an ideal choice for high-temperature applications like IMD.

Overcoming Hurdles to Unlocking the Maximum Potential of Wide Bandgap Devices in Motor Drive Systems


Wide bandgap devices have proven to be a boon for high-temperature, high speed, and low-inductance motors however these devices generate a significant EMI which increases with an increase in switching frequency. A comparison of conducted EMI performance for different wide bandgap devices is shown in Figure 2. This clearly shows that during switching transients the excited parasitic oscillations are high in the SiC JFET inverter which is the main culprit behind noise performance and low efficiency. 


Comparison Between CM EMI of SiC MOSFET and Si IGBT-based Motor Drives.png

Figure 2: Comparison Between CM EMI of SiC MOSFET and Si IGBT-based Motor Drives


To tackle this issue, several innovative CM voltage cancellation and filter topologies are adopted for WBG devices which significantly reduce the generation of EMI, moreover, an integration of dual winding stator configuration and inverter topology is adopted as shown in Figure 3. This method especially configured for PWM motor drives with symmetrical circuits cancels out the complimentary CM voltage, thereby decreasing the overall EMI in the system.


Newly Designed CM Voltage Cancellation Inverter Topology with Dual Winding Stator.png

Figure 3: Newly Designed CM Voltage Cancellation Inverter Topology with Dual Winding Stator

Conclusion


WBG devices serve as crucial enablers for a wide spectrum of motor drive applications, proving particularly advantageous for low-inductance motors, high-speed motors, and operations in high-temperature environments. Electric drive applications stand to gain significantly from the incorporation of WBG devices, showcasing improvements in power density, dynamic response, and overall energy efficiency. However, realizing the maximum potential of WBG devices requires intricate converter design. Specifically, the inclusion of appropriately designed gate drivers is vital, ensuring rapid switching with minimal overshoot and losses. 

Furthermore, the converter design should address challenges such as minimizing parasitic inductance in the commutation loop and implementing fast short-circuit protection for the WBG switches. These considerations are critical for optimizing the performance and reaping the full benefits of WBG devices in motor drive systems.

To make the higher cost of Wide Bandgap devices worth it and utilize them fully, they need to be switched fast. However, these high speeds lead to more Electromagnetic Interference being produced. This high voltage change in the motor also causes a type of current called Common Mode that can harm the motor's insulation. If we choose to switch WBG devices at much slower speeds, it keeps things compatible with the insulation standards used in motors today. This way, we can use methods to control EMI similar to what we use in the current drives based on Insulated Gate Bipolar Transistors. However, the trade-off is that slower speeds mean we don't fully utilize the power and efficiency advantages that WBG devices offer, which are crucial in balancing out the higher cost of these devices. Therefore, newer and innovative technologies such as the integration of inverter topology and dual winding stator are being introduced to reduce the generation of EMI at higher speed and voltage.

Saumitra Jagdale

Saumitra Jagdale is a Backend Developer, Freelance Technical Author, Global AI Ambassador (SwissCognitive), Open-source Contributor in Python projects, Leader of Tensorflow Community India, and Passionate AI/ML Enthusiast

Related Articles

Subscribe to Utmel !

Featured Parts More