web counter

The Introduction of Car Fuse

Published: 09 October 2021 | Last Updated: 09 October 20217099
A small tubular fuse, which consists of two major parts: a tube body with metal connection terminals on both ends and a metal melt in the tube, is the most widely used in circuit overcurrent safety components. This article introduce its relevant knowledge in car.
In this video we show you how to tap into your fuse box.

How to tap into your cars fuse box safely and cleanly

Topics covered in this article:
Ⅰ. What is fuse?
Ⅱ. Where is the car fuse in the car?
Ⅲ. Daily maintenance of car fuse
Ⅳ. How to replace the fuse yourself
Ⅴ. Why does the fuse break?
Ⅵ. Precautions for fuse replacement


Ⅰ. What is fuse?

FUSE.png

Types of fuse

1. Structure: A small tubular fuse, which consists of two major parts: a tube body with metal connection terminals on both ends and a metal melt in the tube, is the most widely used in circuit overcurrent safety components. The purpose of its part of the shell is to connect and support. Most fuses have a cylindrical form, which is known as tubular, and the internal melt determines the main function.

 

2.Function: When the circuit is working normally, the fuse is only equivalent to a wire that can be used stably for a long time; due to power supply or external interference, the fuse is connected in series in the circuit, and its resistance is generally required to be small (low power consumption), so when the circuit is working normally, the fuse is only equivalent to a wire that can be used stably for a long time. The fuse can sustain a specific range of overload when the current fluctuates; only when there is a substantial overload current-fault or short circuit in the circuit will the fuse respond and preserve the circuit's safety by breaking the current.

 

3.Principle: When the fuse is energized, the heat converted by the current raises the temperature of the melt. The heat generated by the current is radiated and convective via the melt, the shell, and the surrounding environment when the load is normal working current or permitted overload current. The heat dispersed via conduction and conduction can gradually approach equilibrium; if the pace of heat dissipation cannot keep up with the rate of heat generation, the heat will gradually accumulate in the melt, causing the temperature of the melt to rise. When the temperature reaches and exceeds the melting point of the melt material, it will melt, cutting off the current and posing a safety hazard.

 

Ⅱ. Where is the car fuse in the car?

Because there are numerous parts and electronic devices on a car, each of which will be equipped with a fuse, the designer places the automobile fuses in one place at the start of the design process, which is known as a fuse box, to make future maintenance easier.

 

Ⅲ. Daily maintenance of car fuse

Under normal conditions, there is no need for special maintenance because the automobile fuse is located in the fuse box, but it should be remembered that if the fuse box lid that protects the fuse is destroyed, the fuse must not be exposed to avoid a short circuit. Furthermore, other materials cannot be substituted at will when covering the fuse, because the fuse box's material is completely considered for insulation and high-temperature resistance, and covering the fuse with other materials at will result in a fire hazard.

 

Ⅳ. How to replace the fuse yourself

How do you discover the damaged fuse when you have a basic understanding of the fuse and the car fails due to the fuse?

Step 1: Find the location of the fuse box

In the cab, the fuse box is usually found on the side of the center console near the door or beneath the steering wheel; in the engine compartment, the fuse box is usually found on the vehicle's engine compartment's edge.

Step 2: Look up the fuse table to find the location of the fuse

We can locate the location of the fuse we're looking for using the fuse comparison table on the fuse box's cover.

Step 3: Find the actual position of the fuse according to the legend

We may compare the legend to the precise position map of the fuse we're looking for to identify the fuse's actual placement in the car.

The last step is to pull out the damaged fuse with the special tool that came with the automobile and replace it with a new spare fuse. There is no longer a distinction between the positive and negative poles of the blade fuse used in vehicles, therefore when replacing the fuse, all that matters is the size and amperage.

Through the fuse, you can assess the basic state of vehicle-related issues.

When we go to a 4S shop, the maintenance fee for a little fuse might cost more than 1,000 yuan, while the small fuse costs only a few pennies. This also reveals something: if the vehicle's electrical system is malfunctioning, we can check to see if the fuse is blown first. For the most common example, if your vehicle's cigarette lighter stops working, you should first check the cigarette lighter's matching fuse to see whether it is blown. If the fuse is not blown, the cigarette lighter may be problematic for other reasons, in which case you should take it to a 4S shop for repair.

 

Ⅴ. Why does the fuse break?

CAR FUSE.png

Car fuse

Car manufacture now has a pretty high level of craftsmanship. It is claimed that the car's circuit was thoroughly tested before leaving the factory or even at the design stage. It shouldn't be an issue, but why does the car's fuse keep blowing? When a current vehicle fuse blows, one of two things can happen: the load on the electrical appliance is too high, or there is a short circuit in the automobile circuit.

Changing headlights, automotive audio equipment, using an inferior cigarette lighter adapters, and high-power electrical appliances connected to the cigarette lighter are the main causes of increased electrical appliance load. As a result, before altering the automobile circuit, all car owners should be aware of the power and maximum load of the original car's electrical equipment. For example, if the modified headlight's power is higher than the original factory setting, the lamp fuse may be blown.

Whether the car's electrical appliances haven't been changed and the fuse has blown, check to see if the wiring has been short-circuited. It is a good habit to flush the engine compartment without using water pipes to avoid short circuits in the fuse box and wiring; additionally, you can visually inspect whether there is a short circuit caused by the aging of the wire rubber and exposed metal wires; and finally, when cleaning the car, you should avoid touching the wiring harness burs.

 

Ⅵ. Precautions for fuse replacement

As previously said, if there is an electrical problem, you should first check to see if the fuse is the source of the problem. If the fuse is truly broken, we can repair it ourselves; but, when doing so, keep the following in mind:

★ The ampere value must be correct

If you need to replace a fuse, make sure you get the right amperage fuse. Increase the fuse's current specification as needed, but don't replace it with iron wire.

It's obvious that you can't use iron wire in place of high-current insurance, so why can't you use high-current insurance instead? It is, of course, for the safety of electrical appliances. When the current is less than 1A, the electrical appliances perform smoothly, but when the current is larger than 1A, the electrical appliances may not work properly. As a result, the fuse must be replaced using the "lower than high" method.

★ Purchase channels should be formal

Fuses can be purchased almost anywhere, however, we recommend that car owners get them from a regular 4S or repair shop. The protection of the circuit cannot be guaranteed because the unqualified fuse is likely to be made of other metals, and the inferior plastic shell is apt to burn when the fuse is overloaded and create a fire.

Without a spare fuse, how do you replace it?

In the event that you don't have a replacement fuse, you can change the fuse on other equipment that won't affect your driving or safety. If a fuse with the same current load is unavailable, a fuse with a lower rated current than the original fuse can be substituted.


UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1.Is the car fuse positive or negative? ? Why is it not negative?

The car fuse has a positive charge. The negative pole is connected to the frame by the ground. If the positive pole is grounded, the entire frame will be charged. Running the battery will cause the battery to lose power and damage the battery. When it rains, it will leak.

2.What do the numbers on car fuse mean?

The number on the top of the car fuse is the rated current value of the fuse.

3.How to remove the car's fuse?

You need to use a fuse clip to remove the fuse of the car. This clip is located in the same fuse box as the fuse. Use this clip to clamp the fuse and pull up to pull out the fuse.
Related Articles

  • eFuse Capacitive Load Startup: Calculate Inrush Current and Prevent Hiccup Trips
    eFuse Capacitive Load Startup: Calculate Inrush Current and Prevent Hiccup Trips
    UTMEL14 September 2026247

    An eFuse that repeatedly restarts while charging a capacitor bank needs three checks: how much current reaches the capacitor, how long the pass transistor can sustain the resulting dissipation, and which protection function actually ends the attempt. Reducing the programmed slew rate often helps, but the result also depends on the active load, supply behavior, and the device's startup state machine.

    Read More
  • Fuse Design and Selection Points
    Fuse Design and Selection Points
    UTMEL01 July 20227895

    Hello, this is Candy. Today I would like to have a discussion about Fuse Design and Selection Points.

    Read More
  • The Introduction of Car Fuse
    The Introduction of Car Fuse
    UTMEL09 October 20217099

    A small tubular fuse, which consists of two major parts: a tube body with metal connection terminals on both ends and a metal melt in the tube, is the most widely used in circuit overcurrent safety components. This article introduce its relevant knowledge in car.

    Read More
  • How does a Resettable Fuse Work?
    How does a Resettable Fuse Work?
    UTMEL26 August 202037825

    A resettable fuse is a kind of over-current electronic protection component. It is made of a high-molecular organic polymer under high pressure, high temperature, and sulfidation reaction. It's mixed with conductive particle materials, and processed by special technology.

    Read More
  • How Electric Fuses Work: Types, Ratings, and Selection Guide
    How Electric Fuses Work: Types, Ratings, and Selection Guide
    UTMEL14 July 202618420

    This guide walks through how a fuse actually interrupts a fault, the difference between fast and slow elements, the main fuse families and where each one belongs, the ratings that genuinely matter, and a repeatable method for choosing a fuse for your own circuit. It closes with the mistakes that most often cause either nuisance opening or unsafe under-protection, a clear comparison with circuit breakers, and a frequently asked questions section.

    Read More

Subscribe to Utmel !

Featured Parts More