Neural Processing Unit (NPU) Explained

Neural Processing Unit NPU, Artificial Intelligence AI and Machine Learning ML explained

What is an NPU?
Neural Processing Unit (NPU) is a dedicated processor optimized for neural network and AI workloads. With the explosive growth of deep learning and AI applications, traditional CPUs and GPUs, while capable of performing similar tasks, have a significant disadvantage in terms of efficiency and power consumption. the NPU has been architecturally designed specifically for neural network computation through hardware-level optimization, and is able to deliver higher AI computation performance with lower power consumption.
It is just at the beginning of the explosion of demand for neural networks and machine learning processing. Traditional CPUs/GPUs can do similar tasks, but NPU specifically optimized for neural networks can perform much better than CPUs/GPUs. Gradually, similar neural network tasks will be done by dedicated NPU units.
NPU (neural processing unit) is a specialized processor for network application packets, using a "data-driven parallel computing" architecture, especially good at processing massive multimedia data such as video and images.
NPU is also a kind of integrated circuit, but different from the single function of special-purpose integrated circuit (ASIC), network processing is more complex, more flexible. Generally, we can use software or hardware in accordance with the characteristics of network computing special programming to achieve the special purpose of the network.

NPU
Core Advantages of NPU
The main advantage of NPU is its specialized parallel computing architecture, which is manifested in the following ways:
| Advantages | Specific Descriptions |
|---|---|
| High Parallelism | The capability to run multiple parallel threads simultaneously to handle large-scale matrix operations. |
| Dedicated Optimization | Hardware-level optimization, including efficient caching systems and simplified processing cores. |
| Low-precision Computing | Focus on low-precision algorithms, increasing throughput instead of focusing on latency. |
| High Power Efficiency | 10-100 times more efficient than general-purpose processors for AI tasks. |
| Storage-computing Integration | The convergence of storage and computation at the circuit level by simulating neurons and synapses. |
The highlight of the NPU is the ability to run multiple parallel threads -- The NPU is taken to another level with some special hardware-level optimizations, such as providing some easily accessible caching systems for some really different processing cores. These high-capacity cores are simpler than typical "regular" processors because they don't need to perform multiple types of tasks. This set of "optimizations" makes NPUs more efficient, which is why so much R&D is being put into ASICs.
One of the advantages of NPUs is that they spend most of their time focusing on low-precision algorithms, new data flow architectures, or in-memory computing capabilities. Unlike GPUs, they are more concerned with throughput than latency.
Processor modules of NPU
NPU is specially designed for IoT AI to accelerate neural network operations and solve the problem of inefficiency of traditional chips in neural network operations. The NPU processor includes modules for multiplication and addition, activation functions, 2D data operations, decompression, etc.
The multiplication and addition module is used to calculate matrix multiplication and addition, convolution, dot product, and other functions. There are 64 MACs inside the NPU and 32 in the SNPU.

The activation function module is used to implement the activation function in the neural network by using the highest 12th order parameter fitting, with 6 MACs inside the NPU and 3 in the SNPU.
The 2D data operation module is used to implement operations on a plane, such as downsampling and plane data copying, etc. There are 1 MAC and 1 SNPU inside the NPU.
The decompression module is used to decompress the weighted data. In order to solve the characteristics of small memory bandwidth in IoT devices, the weights in the neural network are compressed in the NPU compiler, which can achieve a 6-10 times compression effect with almost no impact on accuracy.
Modern NPUs typically contain the following core processing modules that work together to accomplish efficient computation in neural networks:
| Core Processing Modules | Descriptions |
|---|---|
| Multiply-Accumulate Module | It is the core computational unit of NPU, used to perform basic operations such as matrix multiplication, addition, convolution, and dot product. High-end NPUs usually integrate hundreds or even thousands of MAC units to achieve massively parallel computing. |
| Activation Function Module | This module is responsible for realizing the nonlinear transformations in neural networks. Modern NPUs usually adopt higher-order parameter fitting methods to implement various activation functions (e.g., ReLU, Sigmoid, Tanh, etc.), which improves computational efficiency while ensuring accuracy. |
| 2D Data Manipulation Module | This module specializes in planar data operations such as downsampling and planar data replication. These operations are particularly important in image processing and computer vision tasks. |
| Data Compression and Decompression Module | To address the issue of limited memory bandwidth in mobile devices, modern NPUs usually integrate dedicated weighted data compression/decompression modules. Advanced compression algorithms can achieve a compression ratio of 6-10 times with little or no impact on computational accuracy. |
| Tensor Acceleration Unit | A unit specifically designed to accelerate tensor operations, which can efficiently process multi-dimensional data structures and is a key component of deep learning model inference. |
Neural Processing Unit (NPU) architecture Diagram:

NPU: the core carrier of cell phone AI
As we all know, the normal operation of cell phones is inseparable from the SoC chip, which is only the size of a fingernail cover but has all the "guts". Its integrated modules work together to support the implementation of cell phone functions. The CPU is responsible for smooth switching of mobile applications, the GPU supports fast loading of game screens, and the NPU is specifically responsible for the implementation of AI computing and AI applications.
It is also necessary to start with Huawei, which is the first company to use NPU (neural-network processing units) on cell phones, and the first company to integrate NPU into cell phone CPUs.
Evolution of NPUs in mobile devices
The evolution of mobile NPUs:
The application of NPU in smartphones began in 2017, when Huawei first integrated NPU in a commercial cell phone.Since then, major chip vendors have launched their own NPU solutions:
2017: Huawei first integrated NPU in the Kirin 970 processor
2018: Apple introduces a neural network engine in the A12 Bionic chip
2019-2020: Qualcomm, Samsung, MediaTek and other vendors have launched mobile SoCs with integrated NPUs
2021-2023: NPU performance becomes a key competitive point for flagship mobile chips
2024-2025: the performance of mobile NPU is greatly improved to support the operation of large AI models on the device side
Comparison of Current Mainstream Mobile NPUs
NPU has become standard in the latest mobile processors, and the performance difference is significant:
Apple A17 Pro: 26-core neural network engine, AI performance increased by about 40% compared to A16
Qualcomm Snapdragon 8 Gen 3: new Hexagon processor, AI performance increased by about 45% over the previous generation
MediaTek Tiangui 9300: 6th generation APU, AI performance increased by more than 100 percent
Samsung Exynos 2400: new generation NPU, AI performance increase of about 14.7 times
NPU vs. GPU
Although GPU has the advantage in parallel computing capability, it does not work alone and needs the CPU's co-processing. The construction of neural network models and data streams are still carried out on the CPU. There is also the problem of high power consumption and large size. The higher the performance, the larger the GPU, the higher the power consumption, and the more expensive it is, which will not be available for some small devices and mobile devices. Therefore, a small size, low power consumption, high computational performance, and high computational efficiency of a dedicated chip NPU was born.
NPU works by simulating human neurons and synapses at the circuit layer and directly processing large-scale neurons and synapses with a deep learning instruction set, where one instruction completes the processing of a set of neurons. Compared with CPUs and GPUs, NPUs integrate storage and computation through synaptic weights, thus improving operational efficiency.
CPU and GPU processors need to use thousands of instructions to complete the neuron processing. NPU can be completed with just one or a few instructions, so it has obvious advantages in the processing efficiency of deep learning. Experimental results show that the performance of NPU is 118 times that of GPU with the same power consumption.
| Comparison Items | GPU | NPU |
|---|---|---|
| Architectural Differences | General-purpose parallel computing architecture, which requires the CPU to handle tasks in cooperation. Building neural network models and data streams are still carried out on the CPU. | By simulating human neurons and synapses at the circuit layer, it can directly process a large number of neurons and synapses, and uses a deep learning instruction set. |
| Computational Efficiency Comparison - Instruction Efficiency | The CPU and GPU need thousands of instructions to complete neuron processing. | Only one or a few instructions are required for the NPU to complete neuron processing. |
| Computational Efficiency Comparison - Energy Efficiency Ratio | Under the same power consumption, the AI computing performance of a general-purpose GPU is far lower than that of a dedicated NPU. | The AI computing performance of a dedicated NPU can reach 10-50 times that of an equivalent GPU under the same power consumption. |
| Computational Efficiency Comparison - Memory Access | There is a large memory access overhead as it does not have a special integration mechanism for storage and computation. | The NPU realizes the integration of storage and computation through synaptic weights, greatly reducing the memory access overhead. |
| Differences in Application Scenarios | Advantages in scenarios: General computing, graphics rendering, large-scale training. | Advantages in scenarios: Inference on edge devices, low-power consumption scenarios, real-time AI applications. |
CPU, GPU, and NPU Architecture Comparison

The characteristics of different processing units
CPU -- 70% of the transistors are used to build Cache, and part of the control unit. Few computational units, suitable for logic control operations.
GPU -- Transistors are mostly used to build computational units, with low computational complexity, suitable for large-scale parallel computing. Mainly used in big data, backend server, image processing.
NPU -- simulate neurons in circuit layer, realize storage and computation integration by synaptic weights. One instruction completes the processing of a group of neurons, improve operation efficiency. Mainly used in the communication field, big data, image processing.
FPGA -- programmable logic, high computational efficiency, closer to the underlying IO. Logic editable through redundant transistors and linkages. Essentially instructionless, no shared memory required, and more computationally efficient than CPU and GPU. Mainly used in smartphones, portable mobile devices, and automobiles.
| Type | Characteristics | Applications |
|---|---|---|
| CPU | Approximately 70% of the transistors are used to build the cache and control unit. There are fewer computing units, making it suitable for logical control operations. It has strong versatility but low AI computing efficiency. | N/A (Not specifically mentioned in the original text for this part) |
| GPU | Transistors are mainly used to build computing units. It has low computational complexity and is suitable for large-scale parallel computing. | Big data, backend servers, image processing |
| NPU | Simulates neurons at the circuit layer and realizes the integration of storage and computation through synaptic weights. One instruction can complete the processing of a group of neurons, improving operation efficiency. | Communication field, big data, image processing, edge AI |
| FPGA | Programmable logic, high computing efficiency, and closer to the underlying IO. Realizes logical editability through redundant transistors and connections. Essentially has no instructions, does not require shared memory, and has higher computing efficiency than CPU and GPU. | Smartphones, portable mobile devices, and automobiles |
Practical applications of NPU
AI scene recognition by NPU when taking photos, and retouching pictures with NPU computing.
NPU judges light source and dark light details to synthesize super night scenes.
Realize voice assistant operation by NPU.
NPU with GPU Turbo pre-determine the next frame to achieve early rendering to improve the smoothness of the game.
NPU pre-determines the touch to improve the following hand and sensitivity.
NPU judges the difference of front and back-end network speed demand with Link Turbo.
NPU judge the game rendering load to adjust the resolution intelligently.
Give the NPU the power saving by reducing the computing load of AI during the game.
NPU realizes the dynamic scheduling of CPU and GPU.
NPU assists in big data advertising push.
Implement AI intelligent word association function of input method through NPU.
Explanation of each type of processing unit
APU: Accelerated Processing Unit, AMD product for accelerated image processing
BPU: Brain Processing Unit, Horizon's embedded processor architecture
CPU: Central Processing Unit, a mainstream product for PC cores
DPU: Data Stream Processing Unit, the AI architecture proposed by Wave Computing.
FPU: Floating Point Processing Unit, floating point module in general-purpose processors
GPU: Graphics Processing Unit, multi-threaded SIMD architecture, designed for graphics processing
HPU: Holographic Processing Unit, Microsoft's holographic computing chip and device
IPU: Intelligent Processing Unit, the AI processor product of Graphcore, a DeepMind investment
MPU/MCU: Microprocessor/Microcontroller Unit, typically used for low-computing applications in RISC computer architecture products
NPU: Neural Network Processing Unit, a new type of processor based on neural network algorithms and acceleration
TPU: Tensor Processing Unit, Google's processor dedicated to accelerating artificial intelligence algorithms
VPU: Vector Processing Unit, a chip introduced by Movidius, acquired by Intel, dedicated to accelerating image processing and artificial intelligence.
Future development trend of NPU
With the rapid development of AI technology and the continuous expansion of application scenarios, NPU, as the core hardware of AI computing, is experiencing unprecedented innovation and change. The following is an in-depth analysis of the future development trend of NPU:
Architecture Innovation
Further Convergence of Heterogeneous Computing Architectures
Deep integration of NPU with other computing units: future SoC designs will realize tighter integration of computing units such as NPU, CPU, GPU and DSP, and seamless switching and collaborative work between different computing tasks through unified memory architecture and intelligent scheduling system.
Reconfigurable Computing Architecture: The new generation NPU will adopt a dynamic reconfigurable architecture, which can adaptively adjust hardware resource allocation according to the characteristics of different AI tasks, and strike a better balance between generality and specialization.
Mixed-precision computing: Supporting mixed-precision computing modes ranging from INT4 to FP16, the NPU will automatically select the most suitable computing precision according to different parts of the model, balancing performance and precision requirements.
Mature In-Memory Computing Technology
Non-volatile memory computing: Utilizing new non-volatile memories such as ReRAM, MRAM, etc. to realize in-memory computing will significantly reduce the data handling overhead and increase the energy efficiency ratio by 10-100 times.
Analog in-store computing: By executing analog computation directly in the storage array, energy efficiency and computational density can be further improved, which is especially suitable for computationally intensive tasks such as convolutional neural networks.
3D Integrated In-Store Computing: Adopting 3D stacking technology, vertically integrating computing units with storage units, significantly increasing bandwidth and reducing latency, providing more efficient hardware support for large-scale neural networks.
Commercialization of brain-like computing architectures
Specialized Hardware for Stimulated Neural Networks (SNN): Specialized NPUs designed for biologically-inspired stimulated neural networks, capable of achieving computational efficiencies close to those of biological neural systems with very low power consumption.
Neuromorphic chips: Neuromorphic computing architectures that mimic the working mechanism of neurons and synapses in the human brain will move from research to commercialization, showing unique advantages in scenarios such as time series prediction and anomaly detection.
Adaptive Learning Hardware: NPU architecture that supports online learning and self-adaptation can continuously optimize models based on new data without relying on the cloud, realizing true edge intelligence.
Performance Enhancement
Specialized Operators Further Optimized
Domain-specific operators: Highly optimized dedicated operators are developed for different AI application areas, such as computer vision, natural language processing, recommendation systems, etc., providing 10-100 times performance improvement.
Sparse Computing Acceleration: Hardware acceleration units specifically designed for sparsity in neural networks, capable of skipping zero-value computation and significantly improving computational efficiency.
Dynamic operator fusion: Intelligent compiler works with NPU to realize dynamic fusion of multiple operators, reducing intermediate result storage and access, and improving computational throughput.
Wide Application of Quantization Technology
Extremely low-bitwidth quantization: 2-bit or even 1-bit extremely low-bitwidth quantization techniques will be widely used in NPUs to achieve several to dozens of times performance improvement with acceptable accuracy loss.
Adaptive quantization: Automatically adjust the quantization strategy according to the sensitivity of different layers of the model to maximize the performance improvement under the premise of guaranteeing accuracy.
Hardware support for quantization-aware training: NPU will directly support quantization-aware training so that the model can better adapt to the low-precision hardware characteristics and reduce the loss of precision caused by quantization.
Continuous Advancement of Chip Processes
Advanced process nodes: with the application of 2nm or even more advanced processes, the transistor density of NPUs will continue to increase, and the computing power per unit area will be significantly enhanced.
Advanced Packaging Technology: Advanced packaging technologies such as chiplet design and 3D stacking will enable NPUs to break through single-chip area limitations and realize larger-scale integration of parallel computing units.
New semiconductor materials: the application of carbon nanotubes, graphene and other new semiconductor materials will bring NPU higher energy efficiency and lower operating temperature.
Application Expansion
Dramatic increase in edge AI capability
End-side training: future NPUs will support lightweight end-side training, enabling devices to perform personalized model tuning based on user data while protecting privacy.
Multi-device co-computing: Multiple smart devices in a home or office environment will realize distributed co-computing through NPUs, working together to complete complex AI tasks.
All-weather low-power AI: The new generation of NPUs will support ultra-low-power modes to realize all-weather AI sensing and analysis while controlling power consumption at the milliwatt level.
Device-side large model reasoning becomes standardized
Mobile-side large language model (LLM): optimized large language models with 10-100B parameter scales will be able to run smoothly on mobile devices, providing a local interaction experience similar to ChatGPT.
Multi-Round Dialogue Understanding: The NPU will be specifically optimized for multi-round dialogue understanding to support more natural and coherent human-computer interactions.
Knowledge Base Integration: The device-side NPU will support efficient integration with the local knowledge base, enabling the AI assistant to access and understand the user's personal data and provide more relevant services.
Popularization of multimodal AI applications
Audio-visual fusion understanding: the NPU will support real-time fusion analysis of multimodal data such as video, audio, and text to achieve more comprehensive scene understanding.
Generative AI acceleration: Generative AI applications such as text generation image, video editing, music creation, etc. will realize real-time response under the acceleration of NPU.
Immersive experience: combined with AR/VR devices, NPU will support real-time environment understanding and virtual content generation to create a more natural and immersive mixed reality experience.
AI Security and Privacy Protection
Federated Learning Hardware Acceleration: the NPU will provide a specialized federated learning acceleration unit, enabling devices to participate in model training without sharing raw data.
Differential Privacy Computing: NPUs with built-in differential privacy mechanisms will ensure data privacy protection during AI computation, balancing utility and privacy protection needs.
Model anti-tampering mechanism: the NPU will integrate a secure computing unit to prevent the model from being maliciously tampered with or extracted, protecting AI intellectual property.
Vertical Industry Application Deepening
Medical health monitoring: Dedicated NPUs will enable wearable devices to monitor health indicators in real time and perform complex analysis, warning potential health risks in advance.
Intelligent Manufacturing Optimization: Industrial-grade NPUs will support real-time production line optimization and predictive maintenance to improve manufacturing efficiency and product quality.
Automated Driving Decision Making: Vehicle-grade NPUs will process multi-sensor fusion data to realize millisecond-level environment sensing and decision making, promoting the development of automated driving technology.
Ecosystem Evolution
Development tool chain maturity
Unified programming model: cross-platform and cross-device NPU unified programming model will significantly reduce the difficulty of AI application development and accelerate application innovation.
Automated model optimization: AI-assisted compilers will automatically optimize models for different NPU architectures, realizing the vision of “train once, deploy everywhere”.
Visual debugging and analysis tools: Professional NPU performance analysis and debugging tools will help developers pinpoint performance bottlenecks and optimize resource utilization.
Standardization and Open Ecology
Standardization of hardware interface: Standardization of NPU hardware interface will promote the prosperity of hardware and software ecosystem and reduce development and adaptation costs.
Open-source NPU design: open-source NPU architecture will lower the threshold of AI hardware innovation and promote the rapid development of NPUs in specific fields.
NPU-as-a-Service (NPUaaS): the cloud will provide customizable NPU services, enabling developers to customize virtual NPU resources according to application requirements.
References
Sze, V., Chen, Y. H., Yang, T. J., & Emer, J. S. (2020). Efficient processing of deep neural networks. Synthetic Lectures on Computer Architecture, 15(2), 1-341.
Dally, W. J., Turakhia, Y., & Han, S. (2022). Domain-specific hardware gas pedals. communications of the ACM, 65(9), 48-57.
Technical White Papers and Product Specification Notes from Major Chip Vendors (2023-2025)
AI Chip Market Research Report (2024)
Mobile Computing Platform Performance Review Report (2025)
Last updated: 2025-04-22
1. What is NPU and how does it work?
An NPU (Neural Processing Unit) is a processor specifically designed to handle AI tasks.NPUs are equipped with dedicated compute units that focus on key operations of neural networks, such as matrix multiplication and convolution, and these specific designs enable NPUs to perform better in AI inference tasks.NPUs are capable of performing AI tasks such as speech recognition, image processing, and natural language processing natively on the device, Image processing and natural language processing locally on the device, providing a smoother user experience.The primary role of the NPU is to enable efficient device-side AI processing for fast and private computation.
2. Who makes NPU?
Arm today announced two new processors (or one and a half, depending on how you look at it). The company, which designs the chips that power the majority of the world's cell phones and smart devices, launched both the newest Cortex-M processor (the M55) and the Arm Ethos-U55 micro neural processing unit (NPU).
3. Are NPUs better than GPUs?
NPUs and GPUs each have their own advantages, and it's not easy to say which one is better: NPUs are more efficient than GPUs for deep learning and compute-intensive tasks, especially in areas such as natural language processing, speech recognition, and computer vision. While GPUs are more general purpose, NPUs are more efficient when dealing with large language models or edge computing applications4. There are significant differences between NPUs and GPUs in terms of execution efficiency and energy consumption, with NPUs typically consuming less energy for AI task processing. With the rise of edge computing, NPUs enable devices to run AI locally, reducing reliance on the cloud while also better protecting privacy.
4. How is an NPU different from a CPU?
NPUs and CPUs have significant differences in design purpose and function: A CPU is responsible for managing the operation and task allocation of the entire system, and is the general-purpose processor of a computer system. NPUs, on the other hand, are designed to efficiently process AI tasks on the device, focusing on fast and private computations. The architecture of the NPU is optimized to handle neural network operations, while the CPU is a general-purpose processor designed for a wide range of computing tasks. As AI technology has evolved, new types of computer chips have emerged, including CPUs, GPUs, and the newer NPUs, each with different computational units and uses.
Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap DevicesSaumitra Jagdale15 March 20242456For a long era, silicon has stood out as the primary material for fabricating electronic devices due to its affordability, moderate efficiency, and performance capabilities. Despite its widespread use, silicon faces several limitations that render it unsuitable for applications involving high power and elevated temperatures. As technological advancements continue and the industry demands enhanced efficiency from devices, these limitations become increasingly vivid. In the quest for electronic devices that are more potent, efficient, and compact, wide bandgap materials are emerging as a dominant player. Their superiority over silicon in crucial aspects such as efficiency, higher junction temperatures, power density, thinner drift regions, and faster switching speeds positions them as the preferred materials for the future of power electronics.
Read More
A Comprehensive Guide to FPGA Development BoardsUTMEL11 September 202514087This comprehensive guide will take you on a journey through the fascinating world of FPGA development boards. We’ll explore what they are, how they differ from microcontrollers, and most importantly, how to choose the perfect board for your needs. Whether you’re a seasoned engineer or a curious hobbyist, prepare to unlock new possibilities in hardware design and accelerate your projects. We’ll cover everything from budget-friendly options to specialized boards for image processing, delve into popular learning paths, and even provide insights into essential software like Vivado. By the end of this article, you’ll have a clear roadmap to navigate the FPGA landscape and make informed decisions for your next groundbreaking endeavor.
Read More
Applications of FPGAs in Artificial Intelligence: A Comprehensive GuideUTMEL29 August 20253488This comprehensive guide explores FPGAs as powerful AI accelerators that offer distinct advantages over traditional GPUs and CPUs. FPGAs provide reconfigurable hardware that can be customized for specific AI workloads, delivering superior energy efficiency, ultra-low latency, and deterministic performance—particularly valuable for edge AI applications. While GPUs excel at parallel processing for training, FPGAs shine in inference tasks through their adaptability and power optimization. The document covers practical implementation challenges, including development complexity and resource constraints, while highlighting solutions like High-Level Synthesis tools and vendor-specific AI development suites from Intel and AMD/Xilinx. Real-world applications span telecommunications, healthcare, autonomous vehicles, and financial services, demonstrating FPGAs' versatility in mission-critical systems requiring real-time processing and minimal power consumption.
Read More
800G Optical Transceivers: The Guide for AI Data CentersUTMEL24 December 20253525The complete guide to 800G Optical Transceiver standards (QSFP-DD vs. OSFP). Overcome supply shortages and scale your AI data center with Utmel Electronic.
Read More
Xilinx FPGAs: From Getting Started to Advanced Application DevelopmentUTMEL09 September 20254199This guide is your comprehensive roadmap to understanding and mastering the world of Xilinx FPGA technology. From selecting your first board to deploying advanced AI applications, we'll cover everything you need to know to unlock the potential of these remarkable devices. The global FPGA market is on a significant growth trajectory, expected to expand from USD 8.37 billion in 2025 to USD 17.53 billion by 2035. This surge is fueled by the relentless demand for high-performance, adaptable computing in everything from 5G networks and data centers to autonomous vehicles and the Internet of Things (IoT). This guide will walk you through the key concepts, tools, and products in the Xilinx ecosystem, ensuring you're well-equipped to be a part of this technological revolution.
Read More
Subscribe to Utmel !
HCPL-3120-500EBroadcom Limited
HCS200-I/SNMicrochip Technology
FOD3150ON Semiconductor
HCPL-314J-500EBroadcom Limited
UCC21520DWRTexas Instruments
AT88SC0404CA-PUMicrochip Technology
KSZ8999Microchip Technology
KSZ8993MLMicrochip Technology
AT88SC0404CA-SH-TMicrochip Technology
ATECC508A-MAHDA-TMicrochip Technology


Product
Brand
Articles
Tools