Introduction to Optical Zoom and Digital Zoom

Optical Zoom Vs. Digital Zoom
Catalog
| Ⅰ Optical zoom |
| Ⅱ Digital zoom |
| Ⅲ Hybrid zoom |
Ⅰ Optical zoom
Optical zoom is produced by changes in the positions of the lens, object, and focus. When the imaging surface moves in the horizontal direction, the angle of view and focal length will change, and the farther scene becomes clearer.
Obviously, there must be two ways to change the angle of view. One is to change the focal length of the lens. In photography terms, this is optical zoom. The focal length of the lens is changed by changing the relative position of each lens in the zoom lens. The other is the digital zoom. Digital zoom is actually an electronic enlargement of the screen, which uses "interpolation" to enlarge a part of the pixels on the original CCD image sensor. Through the digital zoom, the shooting scene is enlarged, but the quality of the image will inevitably be lost. In fact, digital zoom does not change the focal length of the lens, but only changes the angle of view by changing the angle of the imaging face, which produces an effect that is "equivalent" to the focal length of the lens.
Therefore, we see that some digital cameras with longer lenses have more room for movement of the internal lenses and photoreceptors, so the zoom factor is also larger. We see that some ultra-thin digital cameras on the market generally do not have an optical zoom function, because the movement of the photosensitive device is not allowed inside the body, while the "long lens" digital cameras such as Sony F828 and Fuji S7000 have an optical zoom function.

Wide, 5x and 100x zoom
The optical zoom factor of today's digital cameras is mostly between 2x and 5x, which can bring objects 10 meters away to close to 5-3 meters. There are also some digital cameras that have a 10x optical zoom effect. The optical zoom of a home camcorder is between 10x and 22x, which can clearly capture things up to 70 meters away. The use of an extender can increase the optical zoom of the camcorder. If the optical zoom is not enough, we can add an extender in front of the lens. The calculation method is: A 2x teleconverter is attached to a digital camera with 4x optical zoom. Then this digital camera's optical zoom multiples have changed from 1x, 2x, 3x, and 4x to 2x, 4x, 6x, and 8x, which is obtained by multiplying the magnification of the teleconverter and the optical zoom magnification.
The working of optical zoom
The principle of camera imaging is that the light on the subject passes through the lens and is projected onto the rear photosensitive element. The point where the light converges is called the focal point. The distance from the focal point to the plane behind the image is called the focal length.

optical zoom principle
From the above figure, we can see that there are three planes behind the lens, and there are three focal lengths respectively "focal length 1", "focal length 2", and "focal length 3". As can be seen from the figure, the distance between the two orange lines is the size of the image. In "focal length 1", because the focal length is relatively small, the light passing through the lens is projected onto the plane before it "diverges", so the image will be smaller. "focal length 2" is slightly longer, and the image will be "larger". By analogy, the larger the focal length, the "larger" the image. The principle of optical zoom is to change the size of the image by changing the size of the focal length. Inside the optical zoom camera lens, there are lenses that can move. The photosensitive element behind the camera is fixed, and the lens moves, which is equivalent to the focus moving. When the focus moves, the distance to the rear photosensitive element also changes, and the focal length also changes. After the focal length is changed, the size of the image also changes.
So we can understand that the optical zoom only changes the distance of light transmission, the light itself does not change. Since the light has not changed, the image presented remains the same after the focal length has been changed. So the biggest feature of optical zoom is that the pixels of the image will not change after zooming in, that is, the picture will not be affected.
The focal length of the digital camera optical zoom that we usually contact is actually the length of the focal length in the above picture. For example, the 3x optical zoom lens of Canon A95 has a focal length of 7.8-23.4mm, which refers to the range in which the focal length can be changed, which is actually the range in which the subject can be enlarged.
Ⅱ Digital zoom
Different from optical zoom, digital zoom is a change in the vertical direction of the photosensitive device, which gives people a zoom effect. The smaller the area on the photosensitive device, the visually will allow the user to see only a part of the scene. Digital zoom is actually a kind of electronic magnification of the picture, which magnifies a part of the pixels on the original image sensor to the entire picture. Through the digital zoom, the shooting scene is enlarged, but its sharpness is reduced. There is no movable or retractable part of the digital zoom. It uses the processor in the digital camera, and it only zooms in what it can observe, which is actually an electronic zoom of the picture. That is to say, a part of the pixels on the original CCD image sensor is enlarged by means of "interpolation" processing, so as to achieve the purpose of enlargement. This method is like using image processing software to increase the area of the picture, but the program is carried out in a digital camera. A part of the pixels on the original CCD image sensor is enlarged using "interpolation" processing methods, and the CCD image sensor is enlarged. It uses the interpolation algorithm to enlarge the picture to the whole picture. In fact, digital zoom does not change the focal length of the lens.

The imaging difference between optical zoom and digital zoom
Although the shooting scene becomes larger, its sharpness will be reduced to a certain extent. The larger the zoom factor, the lower the sharpness. The digital zoom is generally about 3 times, and the digital zoom of the camera is 44 Times ~ 600 times. When using digital zoom, the degree of pixelation is more serious than when using optical zoom. This is because the camera uses "interpolation" processing methods. When zooming in, it can only estimate the shape of the photo.
Ⅲ Hybrid zoom
Hybrid zoom is a fairly new concept introduced on smartphones. It combines the optical zoom, digital zoom, and software algorithms mentioned above together. When the zoom requirement exceeds the physical limit of the lens, it can switch from optical zoom to digital zoom to achieve better results.
Currently, any mobile phone with optical zoom function generally supports 3x or 5x optical zoom. But if your shooting scene requirements exceed the focal length of the optical zoom, then it will cause the picture effect to be distorted. Because in theory, to continue zooming after exceeding the optical zoom range is to use digital zoom. And this combination of optical zoom and digital zoom is the so-called hybrid zoom.
Although the algorithms and technologies used by each smartphone manufacturer are different, the overall concepts and principles are similar. Hybrid zoom uses software enhancements and algorithms to synthesize shots from multiple photos to create a better image. The principle is somewhat similar to night mode and HDR effects, but the focus is on the focal length instead of exposure.
Smartphone manufacturers can make use of the different sensors and focal lengths of the mobile phone, and use the details captured by multiple cameras at the same time. All of this information can be used to improve the magnification of photos through smart algorithms. Of course, this is not a true optical zoom, but it is better than ordinary digital zoom, and it can keep the details within a certain distance without missing too many details.
1.What is the difference between optical zoom and digital zoom?
With optical zoom, you first get the subject close before you capture it. With digital zoom, your camera uses part of the image and later brings it to the correct size. With digital zoom, you have more chance of quality loss.
2.What does 3X optical zoom mean?
A “3X zoom” doesn't mean the subject is actually magnified 3X. It just means the lens can zoom to three times that widest focal length number. So, a 3x zoom that starts at 28mm would zoom in to 84mm, but a 3X zoom that starts at 24mm would only zoom in to 72mm.
3.What is optical zoom and how does it work?
Optical zoom is when the physical properties of a lens genuinely magnify distant objects. For example, a telescope is all-optical zoom. If you view the moon through one, it looks bigger. There's no loss in quality—objects just appear closer.
4.Which is better optical or digital zoom?
This is digital zoom: The camera's processor crops into the center of the photo. Optical zoom is ultimately better, as it magnifies an image to fill the entire image sensor — say 10 megapixels worth. Digital zoom takes just the center portion of what the lens threw on the sensor, capturing fewer pixels, say 6MP.
5.Is digital zoom better than cropping?
Cropping is the better option than zooming in. Cropping a photo on your iPhone is better than zooming in before capturing it. That is because your iPhone, especially if it's one of the models before the iPhone 7 Plus, uses digital zoom. This produces a lesser quality output compared to optical zoom.
Optical Transceiver Guide: How It Works, Types, Form Factors, and SelectionUTMEL24 June 2026687An optical transceiver is the replaceable interface between electronic network equipment and an optical fiber link. It converts electrical data from a switch, router, server, storage system, or transport platform into modulated light, then converts received light back into electrical data.
Read More
Transceivers Shortage Outlook 2026: Supply, Lead Times, and Sourcing OptionsUTMEL09 July 20262330The 2026 transceiver market is defined not by a broad, systemic silicon crisis, but by a highly targeted, structural constraint driven by AI data center build-outs. Figure 3: Power connectors on server racks designed for intense workloads.
Read More
The Introduction to Common Tools and Using Methods of Fiber OpticUTMEL07 January 20227502The building and maintenance of optical cables in the intelligent industry has gradually expanded with the rapid expansion of the Internet of Things and 5G technologies, resulting in an increase in demand for various optical fiber tools. Cutting shears, for example, come in a variety of shapes and sizes, and each tool serves a different purpose. Do you have any experience with them? When should you utilize certain fiber optic tools?
Read More
What are Fiber Optic Patch Cables?UTMEL11 February 20228494Hello everyone, I am Rose. Today I will introduce fiber optic patch cables to you. Optical fiber communication, as an emerging technology, has become one of the main pillars of modern communication and plays a critical role in modern telecommunication networks, thanks to the rapid growth of traffic data.
Read More
Basis of Fiber Optic and Fiber Optic CommunicationUTMEL22 October 20215472Hello everyone, I am Rose. Today I will introduce fiber optic to you. Fiber Optic is a type of glass or plastic fiber that can be utilized to transmit light. It is mostly used for communication. This article will show you the basic knowledge of fiber optic and fiber optic communication.
Read More
Subscribe to Utmel !
16-219A/T2D-AR2T1QY/3TEverlight Electronics Co Ltd
SIM-030STROHM Semiconductor
SML-D12D1WT86ROHM Semiconductor
HFBR-2505AZBroadcom Limited
HFBR-2526ZBroadcom Limited
SFH 4725SOSRAM Opto Semiconductors Inc.
HSMG-A100-H01J1Broadcom Limited
IR204C-AEverlight Electronics Co Ltd
HSMM-A100-U4PJ1Broadcom Limited
204-10SURD/S530-A3Everlight Electronics Co Ltd


Product
Brand
Articles
Tools