web counter

Car Sensors: Classification and Application

Published: 21 July 2020 | Last Updated: 27 October 202514372
The car sensor is the input device of the automotive computer-controlled system. The earliest car sensors are oil pressure sensors, oil quantity sensors, and water temperature sensors connected to instruments or indicator lights in the 1960s. There are many kinds of car sensors like temperature sensors, pressure sensors, flow sensors, etc., and they are applied in different applications according to their specific properties.
This video describes the common types of automobile sensors.

Common Sensor Types

Catalog

I Development History
II Classification and Application1. Temperature Sensors
2. Pressure Sensors
3. Flow Sensors
4. Position and Speed Sensors
5. Gas Sensors
6. Knock Sensors
7. Radar Sensors
8. Vehicle Body Control Sensors
9. Car Sensors for Chassis Application
III Detection of Car Sensors1. Detection of the Throttle Switch
2. Detection of Throttle Valve with Linear Variable Resistance Output
IV Development Trend of Car Sensors

I Development History

In the 1960s, automobiles featured only basic sensors including oil pressure sensors, fuel quantity sensors, and water temperature sensors, which were connected to simple instruments or indicator lights.

After entering the 1970s, to control emissions and meet environmental regulations, catalytic converters, electronic ignition systems, and fuel injection devices were introduced, requiring precise air-fuel ratio maintenance. This necessitated additional sensors to help control the car's powertrain system. The 1980s saw significant safety improvements with the introduction of anti-lock braking systems (ABS) and airbags.

Today, modern vehicles utilize sophisticated sensor networks for:

(1) Measuring temperature and pressure of various fluids (intake air temperature, manifold pressure, coolant temperature, fuel injection pressure, etc.)

(2) Determining wheel speed and position of various components (vehicle speed, throttle position percentage, camshaft and crankshaft positions, transmission angles and speeds, exhaust gas recirculation (EGR) valve positions, etc.)

(3) Measuring engine load, knock detection, misfire detection, and oxygen content in exhaust gases

(4) Determining seat positions and occupancy

(5) Measuring wheel speed, road surface variations, and tire pressure in anti-lock braking systems and suspension control devices

Airbags for protecting passengers require multiple impact sensors and acceleration sensors. Modern anti-collision systems use radar, lidar, or camera-based sensors to determine and control lateral acceleration, instantaneous speed of each wheel, and required torque, making the braking system an integral part of vehicle stability control systems.

Modern airbag system with multiple sensors

Modern airbag system with multiple sensors

Traditional oil pressure and water temperature sensors operated independently with clear maximum or minimum limits. As sensors evolve toward electronic and digital systems, their output values are utilized more comprehensively, with many modern automotive sensors functioning as intelligent switches with variable output capabilities.

II Classification and Application

Types of Sensors in Modern Cars

Sensors for engine control systems form the core of automotive sensor networks, including temperature sensors, pressure sensors, position and speed sensors, flow sensors, gas sensors, and knock sensors. These automotive sensors provide precise control of engine operating conditions for the Electronic Control Unit (ECU) to optimize dynamic performance, reduce fuel consumption and exhaust emissions, and perform comprehensive fault detection.

Modern automotive ECU with sensor connections

Modern automotive ECU with sensor connections

1. Temperature Sensors

Automotive temperature sensors are primarily used to detect engine temperature, intake air temperature, coolant temperature, fuel temperature, and catalytic converter temperature. There are three main types of vehicle temperature sensors: wire-wound resistor type, thermistor type, and thermocouple type. Each type has distinct characteristics and specific applications.

(1) Wire-wound resistor temperature sensors offer high accuracy but have poor response characteristics.

(2) Thermistor temperature sensors provide high sensitivity and good response characteristics but have poor linearity and are better adapted to lower temperatures.

(3) Thermocouple temperature sensors offer high accuracy and wide temperature measurement ranges but require amplifiers and cold-junction compensation.

Car coolant temperature sensor

Car coolant temperature sensor

2. Pressure Sensors

Automotive pressure sensors are primarily used to detect cylinder vacuum, atmospheric pressure, turbocharger boost pressure, cylinder internal pressure, and oil pressure. Intake manifold pressure sensors are mainly used for detecting intake air pressure, vacuum levels, and oil pressure. There are numerous types of pressure sensors used in automobiles: capacitive, piezoresistive, linear variable differential transformer (LVDT), and surface acoustic wave (SAW) types.

(1) Capacitive pressure sensors are primarily used to detect vacuum, hydraulic pressure, and air pressure, measuring ranges from 20-100kPa, with high input energy, excellent dynamic response characteristics, and good environmental adaptability.

(2) Piezoresistive pressure sensors are significantly affected by temperature, often requiring separate temperature compensation circuits, but are suitable for mass production.

(3) LVDT pressure sensors have large output signals and are easy to digitize, but have poor interference resistance.

(4) SAW pressure sensors feature small size, lightweight construction, low power consumption, high reliability, sensitivity, and resolution, used to detect intake manifold pressure and capable of stable operation at high temperatures.

Automotive pressure sensor applications

Automotive pressure sensor applications

3. Flow Sensors

Flow sensors are primarily used for measuring engine airflow and fuel flow. Airflow measurement is used by engine control systems to determine combustion conditions, control air-fuel ratios, startup procedures, ignition timing, etc. There are four types of airflow sensors: rotary vane type, Karman vortex type, hot wire type, and hot-film type.

(1) Rotary vane airflow sensors have simple structures and lower measurement accuracy. The measured flow requires temperature compensation.

(2) Karman vortex airflow sensors have no moving parts, are sensitive, and require high accuracy with temperature compensation.

(3) Hot-wire airflow sensors have high measurement accuracy with no temperature compensation required, but are easily affected by gas pulsation and prone to breakage.

(4) Hot-film airflow sensors use the same measuring principle as hot-wire sensors but are smaller in volume and suitable for mass production at lower cost.

Main technical specifications of airflow sensors:

  • Working range: 0.11-103 m³/min

  • Operating temperature: -40°C to 120°C

  • Accuracy: ≤ 1%

(5) Fuel flow sensors are used to detect fuel flow, mainly divided into turbine wheel type and circulating ball type.

Technical specifications:

  • Dynamic range: 0-60kg/h

  • Operating temperature: -40°C to 120°C

  • Accuracy: 1%

  • Response time:<10ms

Mass airflow sensor

Mass airflow sensor

4. Position and Speed Sensors

Position and speed sensors are primarily used to detect crank angle, engine speed, throttle position percentage, vehicle speed, etc. Automotive position sensors and speed sensors include generator type, magnetoresistive type, Hall effect type, reed switch type, optical type, semiconductor magnetic transistor type, etc. The measurement range is 0-360°, with accuracy better than 0.5°, and measured angle resolution of 0.1°.

There are many types of vehicle speed sensors, including those sensitive to wheel rotation, transmission rotation, and differential drive shaft rotation. When vehicle speed exceeds 100km/h, conventional measurement methods have significant errors, requiring non-contact photoelectric speed sensors.

Technical specifications:

  • Speed range: 0.5-250km/h

  • Repeat accuracy: 0.1%

  • Distance measurement error:<0.3%

Hall effect sensors in automotive applications

Hall effect sensors in automotive applications

5. Gas Sensors

Gas sensors are primarily used to detect exhaust gas composition and emissions in vehicles. The most important is the automotive oxygen sensor. Practical types include zirconia sensors (operating temperature -40°C to 900°C, accuracy 1%), zirconia concentration cell gas sensors (operating temperature 300°C to 800°C), solid electrolyte zirconia gas sensors (operating temperature 0°C to 400°C, accuracy 0.5%), and titanium dioxide automotive O₂ sensors. Compared to zirconia sensors, titanium dioxide oxygen sensors have simpler structures, are lightweight, cost-effective, and have strong resistance to lead contamination.

Automotive gas sensor

Automotive gas sensor

6. Knock Sensors

Automotive knock sensors, also called vibration sensors, are used to detect engine oscillation by adjusting ignition advance angle to control and prevent engine knock. Knock detection can be achieved by testing cylinder pressure, engine block vibration, and combustion noise.

Knock sensors include magnetostrictive and piezoelectric types. The magnetostrictive knock sensor operates at temperatures from -40°C to 125°C with a frequency range of 5-10kHz. Piezoelectric knock sensors have sensitivity up to 200mV/g at center frequency of 5.417kHz and exhibit good linearity at amplitudes of 0.1g-10g.

Knock sensor

Knock sensor

7. Radar Sensors

Modern automotive radar systems utilize multiple frequency bands: 24GHz, 77GHz, and 79GHz radar sensors are used in collision avoidance systems, adaptive cruise control, and autonomous driving features. These systems emit radar waves to determine object size, distance, and movement speed to prevent collisions using display systems and automated braking. The 77GHz band is now preferred for long-range applications due to better resolution and smaller antenna size requirements.

Automotive radar sensor

Automotive radar sensor

8. Vehicle Body Control Sensors

Vehicle body control sensors are primarily used to improve automotive safety, reliability, and comfort. Since their operating conditions are less harsh than engine sensors and chassis components, general industrial sensors can be applied with minor modifications. These automotive sensors can be categorized into several groups according to their applications:

(1) Automatic climate control systems: temperature sensors, humidity sensors, air volume sensors, and sunlight sensors

(2) Airbag systems: acceleration sensors and impact sensors

(3) Door lock control: vehicle speed sensors

(4) Automatic brightness control: ambient light sensors

(5) Parking assistance: ultrasonic or laser sensors

(6) Safe following distance: distance sensors

(7) Blind spot elimination: camera and image sensors

(8) Navigation systems: compass sensors, gyroscopes, vehicle speed sensors, and steering wheel angle sensors

Additional sensors used in vehicle body applications include: collision acceleration sensors, ultrasonic short-range sensors, infrared sensors, millimeter-wave radar, and ambient gas electrochemical sensors. Advanced sensor types include reverse sensors, lane departure warning systems, and infrared thermal imaging night vision sensors.

9. Car Sensors for Chassis Applications

(1) Transmission control systems: vehicle speed sensors, accelerator pedal position sensors, acceleration sensors, throttle position sensors, engine speed sensors, coolant temperature sensors, transmission fluid temperature sensors, etc.

(2) Suspension control systems: vehicle speed sensors, throttle sensors, acceleration sensors, body height sensors, steering wheel angle sensors, etc.

(3) Power steering systems: vehicle speed sensors, engine speed sensors, torque sensors, hydraulic pressure sensors, etc.

Digital chassis acceleration sensors

Digital chassis acceleration sensors

III Detection of Car Sensors

(Using throttle position sensor as the discussion example)

The driver operates the vehicle throttle with the accelerator pedal to change engine air intake, thereby controlling engine operation. Different throttle positions indicate various engine operating conditions.

1. Detection of the Throttle Switch

(1) Structure and Circuit

The throttle switch, also called switch output type throttle position sensor, has two pairs of contacts: idle contact (IDL) and full load contact (PSW). A cam coaxial with the throttle valve controls the opening and closing of these switch contacts.

Throttle position sensor structure

Throttle position sensor structure

When the throttle valve is fully closed, the idle contact closes, and the ECU determines that the engine is in idle mode according to the idle switch closing signal, controlling fuel injection quantity according to idle mode requirements.

When the throttle valve opens, the idle contact opens, and the ECU performs fuel injection control during the transition from idle to light load based on this signal. The full load contact remains open from fully closed to small and medium throttle openings.

When the throttle opens to a certain angle, the full-load contact closes, sending a signal to the ECU that the engine is in full-load operation, and the ECU performs full-load enrichment control based on this signal.

(2) Check and Adjustment

  • Check conductivity between terminals in the vehicle

Step 1: Set the ignition switch to "OFF" position, remove the throttle position sensor connector, and insert an appropriate thickness gauge between the throttle stop screw and limit rod.

Step 2: Connect a multimeter to the connector to test the conduction mode of idle contacts and full load contacts.

When the throttle is fully closed, the idle contact should be conducting; when the throttle is fully opened or nearly fully opened, the full load contact should be conducting; at other opening angles, neither contact should be conducting. The specific conditions are shown in Table 1. Otherwise, the throttle position sensor should be adjusted or replaced.


Fully-closedFully-opened/Close to fully openedOpened at other angles
Idle contactTurned onXX
Full load contactXTurned onX

Table 1. Throttle switch contact states

2. Detection of Throttle Valve with Linear Variable Resistance Output

(1) Structure and Circuit

The throttle position sensor with linear variable resistance output is a type of linear potentiometer whose sliding contact is driven by the throttle shaft. Under different throttle positions, the potentiometer resistance varies, converting throttle position into voltage signals sent to the ECU. Through the throttle position sensor, the ECU obtains continuously changing voltage signals representing all throttle valve opening angles and the rate of throttle position change, enabling more accurate determination of engine operating conditions. Generally, this type of throttle position sensor also includes an idle contact (IDL) to determine engine idle operating conditions.

(2) Inspection and Adjustment

  • Conductivity Detection of Idle Contact

  • Set the ignition switch to "OFF" position, remove the throttle position sensor wire connector, and use a multimeter to measure idle contact conductivity on the connector. When the throttle is fully closed, resistance between terminal IDL and E2 should be 0Ω. When the throttle is open, resistance between the two terminals should be ∞. Otherwise, replace the throttle position sensor.

  • Measure the resistance

Set the ignition switch to OFF position, unplug the throttle position sensor wire connector, and measure the linear potentiometer resistance with the multimeter's Ω setting. The resistance should increase linearly with increasing throttle position.

IV Development Trend of Car Sensors

The development trend of automotive sensor technology is toward miniaturization, multi-functionality, integration, and intelligentization.

Currently, advancements in design technology, materials technology, especially MEMS (Microelectromechanical Systems) technology, have brought micro-sensors to new levels. Using microelectronic mechanical processing technology, micron-level sensitive components, signal processors, and data processing devices can be packaged on a single chip, featuring small size, low cost, high reliability, and significantly improved system test accuracy. Additionally, MEMS technology enables manufacturing of miniature sensors that detect mechanical, magnetic, thermal, chemical, and biological quantities. Because MEMS miniature sensors can greatly reduce automotive electronic system costs while improving performance, they are gradually replacing sensors based on traditional electromechanical technology and becoming an important component of global automotive electronics.

MEMS automotive sensors offer low cost, excellent reliability, and small size. They can be integrated into new systems and operate for millions of hours. The earliest MEMS devices were absolute pressure sensors and airbag acceleration sensors. Currently, MEMS/MST products under development and in small-batch production include wheel speed rotation sensors, tire pressure sensors, refrigeration pressure sensors, engine oil pressure sensors, brake sensors, and yaw rate sensors. In the next 5-7 years, MEMS devices will be widely adopted in automotive systems.

With microelectronic technology development and rapid increase in automotive electronic control system applications, market demand for automotive sensors will maintain rapid growth. Miniaturized, multifunctional, integrated, and intelligent sensors based on MEMS technology will gradually replace traditional sensors and become mainstream automotive sensors.

  • Multifunctionality means one sensor can detect two or more physical or chemical parameters, reducing the number of vehicle sensors and improving automotive sensor system reliability.

  • Integration refers to using IC manufacturing technology and precision processing technology to create IC-type sensors.

  • Intelligentization refers to combining sensors with large-scale integrated circuits containing CPUs, providing intelligent functions to reduce ECU complexity, volume, and costs.

MEMS automotive sensors

MEMS automotive sensors

Article Update Information

Last Updated: October 2025

Key Updates Made:

  • Updated radar sensor frequencies to include modern 77GHz and 79GHz systems

  • Enhanced mobile-responsive design with modern CSS styling

  • Corrected technical specifications and temperature ranges

  • Added information about autonomous driving sensor technologies

  • Updated MEMS technology applications and market trends

  • Expanded coverage of advanced driver assistance systems (ADAS)

  • Added current automotive sensor integration examples

  • Improved technical accuracy of sensor detection procedures

  • Updated recommended articles section

Technology Evolution Since 2020: Automotive sensors have significantly advanced with AI integration, enhanced ADAS capabilities, electric vehicle-specific sensors, and improved connectivity for autonomous driving applications. The market has expanded dramatically with the rise of electric vehicles and autonomous driving technologies.

Recommended Articles:

What are Types and Application of Gas Sensors?            Working Principle and Application of Infrared Sensors            All You Need to Know about Ultrasonic Sensors            Introduction to Temperature Sensors

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1.What are all the sensors in a car?

5 Car Sensors and Their Functions
Mass Air Flow (MAF) Sensor.
Manifold Absolute Pressure (MAP) Sensor.
Engine Speed Sensor.
Coolant Temperature (CTS) Sensor.

2.How many sensors does a car have?

Currently, each vehicle has from 60 to 100 sensors on board and we can expect that number to rise as cars get 'smarter'.” In fact, recent industry figures suggest the number of sensors is projected to reach as many as 200 per car based on current trends.

3.What are the different types of sensors?

List of Sensors
Vision and Imaging Sensors.
Temperature Sensors.
Radiation Sensors.
Proximity Sensors.
Pressure Sensors.
Position Sensors.
Photoelectric Sensors.
Particle Sensors.

4.Is it OK to drive a car with a bad O2 sensor?

In summary, yes, you can drive with a faulty O2 sensor. But you'll want to change it immediately because otherwise, you'll be spending more money on fuel and you risk having to spend more on a new catalytic converter as well.

5.How much are car engine sensors?

A brand new replacement oxygen sensor can cost you from $20 to $100, depending on the make and year of your car. Taking your car to a mechanic to fix the issue can cost up to $200. Though, this depends on the type of car and the rates of the mechanic.
Related Articles

  • The Key Role of Electronic Components in IoT Devices
    The Key Role of Electronic Components in IoT Devices
    UTMEL01 September 20236370

    The article discusses the pivotal role of electronic components in Internet of Things (IoT) devices. IoT devices work by capturing real-world data using sensors, processing it through a microcontroller, and then sending it to the cloud for further analysis.

    Read More
  • Accelerometer Sensors Guide: Working Principle, Circuit Design, Specifications, and Applications
    Accelerometer Sensors Guide: Working Principle, Circuit Design, Specifications, and Applications
    UTMEL25 June 20261262

    A practical accelerometer sensor guide covering working principles, MEMS and piezoelectric types, datasheet specifications, circuit design, mounting, applications, and selection.

    Read More
  • 2026 ADAS Sensors: Supply Outlook and Alternative Sourcing
    2026 ADAS Sensors: Supply Outlook and Alternative Sourcing
    UTMEL18 July 20261399

    Automotive cleanroom assembly integrating advanced driver assistance systems. The automotive industry faces a structural semiconductor deficit in 2026, driven not by pandemic-era demand shocks but by AI data centers absorbing global foundry capacity on legacy nodes (40nm-90nm) where 95% of automotive-grade components are manufactured. Video demonstrations of these systems show a "machine view" overlay with red crosshairs tracking pedestrian movement and sudden cut-ins before traditional collision thresholds are triggered.

    Read More
  • Magnetic Sensors for Position Detection: Hall Effect vs. AMR vs. TMR Engineering Guide
    Magnetic Sensors for Position Detection: Hall Effect vs. AMR vs. TMR Engineering Guide
    UTMEL21 August 2026764

    This guide compares Hall effect, AMR, and TMR magnetic sensors for position detection in motor control and robotics. It explains their physical principles, key performance metrics, and selection criteria. Hall effect suits low-cost commutation, AMR offers high-speed angle sensing, and TMR provides maximum precision and low power, with practical integration advice.

    Read More
  • Temperature Sensor Types Comparison: Thermocouple, RTD, and Semiconductor IC Selection Guide
    Temperature Sensor Types Comparison: Thermocouple, RTD, and Semiconductor IC Selection Guide
    UTMEL17 August 2026647

    This comprehensive selection guide compares thermocouples, platinum RTDs, and semiconductor ICs across measurement range, accuracy limits, and signal conditioning complexity. It covers fundamental operating physics, mathematical transfer functions, lead-wire compensation topologies, and power budgets. Engineers will find practical design checklists, benchtop multimeter diagnostic techniques, and an architectural decision workflow to optimize system performance and bill-of-materials cost.

    Read More

Subscribe to Utmel !

Featured Parts More