web counter

AD5420 16-Bit DAC Design Notes: Managing Thermal Limits, HART Slew Rates, and 4-20mA Loops

UTMEL

Published: 06 May 2026 | Last Updated: 06 May 2026

270

AD5420AREZ-REEL7

AD5420AREZ-REEL7

Analog Devices Inc.

5V V DAC Current - Buffered Surface Mount R-2R R 2 B B

Purchase Guide

5V V DAC Current - Buffered Surface Mount R-2R R 2 B B

Discover integration notes for the AD5420 16-bit DAC. Learn how to manage 4-20mA loops, solve HART network disruptions, and handle thermal limits in PLC designs.

The AD5420 is a 16-bit digital-to-analog converter (DAC) designed for programmable current source outputs in industrial process control applications. Because industrial environments demand high reliability over long cable runs, designing with a precision current-source DAC requires more than just connecting SPI lines. Engineers must account for loop compliance, harsh factory transients, and thermal dissipation limits when driving high currents from high-voltage rails.

  • Market Position: A low-cost, fully integrated solution specifically tailored for programmable logic controllers (PLCs), actuator control, and process automation.

  • Core Selection Factor: Integrates an on-chip reference and fault detection, reducing the external bill of materials (BOM) for standard 4–20 mA, 0–20 mA, and 0–24 mA loops.

  • Integration Risk: High power dissipation when sourcing maximum current from a 60V supply requires strict thermal derating and careful PCB layout.

AD5420 product photo

Key Electrical Characteristics for Process Control

When evaluating the AD5420 for an industrial module, the primary focus is on accuracy over temperature and power supply flexibility. The device guarantees 16-bit resolution and monotonicity, which is critical for smooth actuator positioning without hunting or oscillation.

  • Output Current Ranges: The device supports the standard 4-20 mA range for traditional industrial loops, as well as 0-20 mA and an over-range 0-24 mA setting. The 24 mA range is particularly useful for signaling out-of-band alarm conditions to a central controller.

  • Total Unadjusted Error (TUE): Rated at a typical ±0.01% of Full Scale Range (FSR). This minimizes the need for extensive multi-point factory calibration in standard applications.

  • Output Drift: At ±3 ppm/°C typical, the DAC maintains highly stable output across its -40°C to +85°C operating range. The on-chip reference itself is rated for a maximum of 10 ppm/°C, which is sufficient for most standard PLC analog output modules without requiring an external precision reference.

  • Supply Voltage (AVDD): The part is split into two distinct voltage ratings based on the ordering code. The AREZ variant supports 10.8 V to 40 V, while the ACPZ variant can handle up to 60 V.

Managing Thermal Dissipation in High-Voltage Loops

One of the most critical engineering compromises when designing with the AD5420 is managing the thermal load. While the device can source 24 mA and can operate from a 60 V supply (in the ACPZ version), doing both simultaneously forces the silicon to dissipate an immense amount of power.

If your AVDD is 60V and the load resistance is very low (e.g., a short circuit or a low-impedance receiver), the internal output transistor drops the majority of that voltage. Sourcing 24 mA across a 60 V drop results in nearly 1.44 W of localized power dissipation on the chip. Without mitigation, this will rapidly cause the junction temperature to exceed the 125°C maximum absolute rating, triggering thermal shutdown or permanent silicon degradation.

To fix this, you must de-rate the power dissipated directly on the chip. This is typically achieved by transferring the heat burden to the PCB or an external component. Using the LFCSP package is highly recommended for these high-power scenarios, as it provides a much lower thermal impedance (28°C/W) compared to standard TSSOPs, provided the exposed thermal pad is soldered to a substantial copper ground plane. In extreme cases, adding a series drop resistor outside the feedback loop can help absorb some of the voltage drop, keeping the DAC's internal dissipation within safe operating limits. Exact thermal derating will depend heavily on your PCB copper area, copper thickness, and ambient enclosure temperature, so running a thermal model during the layout phase is strictly required here.

Solving HART Communication Disruption

For environments utilizing the Highway Addressable Remote Transducer (HART) protocol, the AD5420 presents a specific integration challenge. The DAC's natural, unconstrained slew rate from 4 mA to 20 mA is approximately 10 µs. This extremely fast current transition generates high-frequency harmonics that can cause major disruption to a HART network, drowning out the 1.2 kHz and 2.2 kHz FSK signals used by the protocol.

To maintain HART compliance and prevent communication dropouts, the slew rate must be artificially slowed down. The AD5420 provides two mechanisms to achieve this:

  1. Hardware Slew Rate Control: You must add external capacitors at the CAP1 and CAP2 pins. These capacitors directly limit the rate of change of the output current.

  2. Digital Slew Rate Control: The device includes an internal digital slew rate control function accessible via the SPI interface. Enabling this allows the DAC to step through the output codes gradually rather than making a single massive jump.

Using a combination of both the external capacitors and the internal digital stepping is the most robust way to guarantee the output transitions smoothly without corrupting the HART network layer.

AD5420 application circuit schematic

Surviving Hi-Pot Testing: Output Range Shifts

Industrial equipment must frequently undergo High Potential (Hi-Pot) testing to verify isolation barriers. A known pain point with the AD5420 is that the high voltage transients generated during aggressive Hi-Pot testing can couple into the device and corrupt the internal calibration registers.

When these registers are corrupted, the microprocessor loses its calibration framing, causing the output to shift abnormally high—sometimes driving the loop up to 134 mA, completely saturating the receiver and potentially damaging downstream equipment.

If your module must survive repeated Hi-Pot testing, you cannot rely on the bare DAC. You must design external protection. Adding external protection diodes (such as TVS arrays) and surge current limiting resistors on the output lines is mandatory. If a transient does manage to lock up the device, you can execute a hard hardware reset by briefly shorting the R3sense output to ground; this collapses the AVDD supply locally and forces the internal microprocessor to reset and reload its default states.

Troubleshooting Unexpected /FAULT Line Activations

The AD5420 includes an active-low /FAULT pin designed to alert the host microcontroller of over-temperature conditions or broken output loops (IOut faults). However, during prototyping, engineers often encounter unexpected /FAULT line activations even when the ambient temperature is normal and the loop appears connected.

If this occurs, investigate the output loop compliance voltage. The AD5420 requires a compliance headroom of AVDD − 2.5 V. This means if your AVDD is 24 V, the maximum voltage that can be developed across your load resistor is 21.5 V. If your load resistance is too high (e.g., 1 kΩ) and you attempt to drive 24 mA, the required voltage (24 V) exceeds the compliance limit (21.5 V). The internal driver starves for voltage, fails to reach the target current, and correctly flags an IOut fault.

Always verify your maximum load resistor against your minimum expected AVDD supply, and double-check your slew-rate settings, as overly aggressive capacitive loads can momentarily trigger the fault comparator during fast transitions.

AD5420 functional block diagram manufacturer datasheet

Alternatives, Equivalents, and Replacement Considerations

When navigating supply chain constraints or looking for feature upgrades, several direct competitors and sister parts exist. Be aware that "equivalents" in precision analog are rarely drop-in replacements without some firmware or layout adjustments.

  • Analog Devices AD5422: The most direct upgrade path. The AD5422 is essentially the same core architecture but adds a programmable voltage output alongside the current output. If you are migrating from an AD5420 to an AD5422 due to stock shortages, the footprint is often compatible, but you must ensure your firmware does not accidentally enable the voltage output stage into a pure current loop.

  • Analog Devices AD5421: This is a loop-powered, 16-bit, 4-20 mA DAC. Unlike the AD5420, which is locally powered by a separate AVDD supply, the AD5421 extracts its operating power directly from the 4-20 mA loop itself. It is not a drop-in replacement, but it is the correct architectural choice if you are designing a 2-wire transmitter rather than a 3-wire/4-wire PLC output module.

  • Texas Instruments DAC8750: A strong competitor in the industrial 4-20 mA space. It offers similar 16-bit resolution and programmable current ranges. Switching to the DAC8750 requires a complete PCB footprint redesign and a rewrite of the SPI driver, as the register maps and internal fault handling differ significantly.

  • Analog Devices AD420: An older generation, legacy 16-bit current-output DAC. It lacks the advanced fault detection and flexible digital slew rate control of the AD5420. It should generally not be considered for new designs, but you may see it in legacy BOMs being upgraded to the AD5420.

Datasheet, Package, and Ordering Verification

Before finalizing your schematic symbol and footprint library, pay close attention to the ordering suffix, as it dictates both package type and absolute maximum ratings.

  • Voltage Limits: As noted, the AREZ suffix indicates a lower maximum supply voltage (40 V), while the ACPZ suffix handles up to 60 V. Do not mix these up in your BOM, or a 48 V industrial rail will instantly destroy an AREZ-rated part.

  • Package Types: The ACPZ variant utilizes the LFCSP (Lead Frame Chip Scale Package). When verifying your EDA footprint, you must ensure the center thermal pad is present, correctly sized, and stitched with vias to a large internal ground plane. The device relies entirely on this pad to achieve its 28°C/W thermal resistance.

  • Digital Interface: Verify your microcontroller's SPI mode. The AD5420 features a flexible serial digital interface compatible with standard SPI, MICROWIRE, QSPI, and DSP protocols, but ensuring your clock polarity (CPOL) and phase (CPHA) match the datasheet timing diagrams will save hours of firmware debugging. An asynchronous clear function is also provided—ensure this pin is tied off correctly if unused to prevent spurious output resets in noisy environments.

Hyper-Specific FAQs

Why does my AD5420 output jump to 134mA after factory isolation testing?High voltage transients during Hi-Pot testing can couple into the device and corrupt the internal calibration registers. This loss of calibration causes the output to shift abnormally high. You must add external protection diodes and surge resistors to the output path, or briefly short the R3sense pin to ground to collapse AVDD and force a hard reset.

Why is the /FAULT pin triggering when I output 20mA, even though the loop is closed?You are likely violating the output loop compliance voltage. The maximum voltage you can drive across your load is AVDD − 2.5 V. If your AVDD drops due to supply sag, or if your load resistance is too high, the DAC cannot physically push 20 mA through the loop. The driver saturates and triggers the fault line.

Can I use the AD5420 on a HART network without external capacitors?No. The natural slew rate of the AD5420 is 10 µs, which is far too fast and will generate harmonics that disrupt HART communications. You must use external capacitors on the CAP1 and CAP2 pins, combined with the internal digital slew rate control, to smooth the transitions.

Why is my AD5420 overheating when running off a 48V supply?Power dissipation is calculated as the voltage dropped across the DAC multiplied by the current. Sourcing 24 mA from a 48 V supply into a low-impedance load forces the DAC to dissipate over 1 Watt. You must de-rate the power, ensure you are using the LFCSP package with a proper thermal ground plane, or add a series drop resistor to share the thermal load.

Watch Tutorial: AD5420

Specifications

Parts with Similar Specs

The three parts on the right have similar specifications to Analog Devices Inc. & AD5420AREZ-REEL7.

Datasheet PDF

Download datasheets and manufacturer documentation for Analog Devices Inc. AD5420AREZ-REEL7.
AD5420AREZ-REEL7

Analog Devices Inc.

In Stock: 1000

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe

Related Parts More