What is a Variable Resistor?

Published: 19 February 2020 | Last Updated: 16 March 202630156
With a variable resistor, you can readily adjust the resistance, and therefore the current, of a circuit for functions such as dimming lights, controlling the speed of a motor, or adjusting a signal generator. This article will explain the symbols, construction and types of variable resistors and how potentiometers (three-terminal variable resistors) can be used as adjustable voltage dividers.
In this video, basics of variable resistor are introduced.

Variable Resistors Explained

Executive Summary: A variable resistor is a crucial electromechanical component used to dynamically adjust circuit resistance, controlling current (as a rheostat) or dividing voltage (as a potentiometer). In 2026, these components remain foundational in everything from precision industrial robotics to smart home IoT devices, offering reliable, manual control over electrical parameters.

A variable resistor is an electromechanical component whose resistance can be adjusted by moving a wiper across its resistive element. They serve two main functions: as a rheostat (two-terminal configuration) to control current, or as a potentiometer (three-terminal configuration) to divide voltage.

Contents

  1. 1. What Are the Circuit Symbols of Variable Resistors?

  2. 2. How Does a Variable Resistor Work?

  3. 3. What Are the Different Types of Variable Resistors?

  4. 4. What Are the Physical Characteristics of Variable Resistors?

  5. 5. What Are the Main Functions and Applications in 2026?

  6. 6. What Is a Potentiometer and How Does It Differ?

1. What Are the Circuit Symbols of Variable Resistors?

Variable resistors are represented in circuit diagrams using specific symbols that indicate their adjustability and terminal configuration, typically featuring a standard resistor zigzag line with a diagonal or perpendicular arrow.


Standard Variable Resistor and Potentiometer Symbols in 2026 Circuit Diagrams

Figure 1: Standard variable resistor (two-terminal) and potentiometer (three-terminal) symbols

Traditional Variable Resistor Symbol for Rheostat Configuration

Figure 2: Traditional variable resistor symbol (two-terminal configuration)

Potentiometer Symbol Showing Three Terminals for Voltage Division

Figure 3: Potentiometer symbol (three-terminal configuration)

Variable resistors are represented in circuit diagrams using specific symbols:

  • Standard symbol (Figure 1): A resistor with an arrow through it, indicating adjustability. The letter "R" denotes a resistor, and "W" indicates the wiper terminal.

  • Traditional symbol (Figure 2): Often found in older circuit diagrams, showing a rheostat configuration where the wiper is connected to one fixed terminal.

  • Potentiometer symbol (Figure 3): Shows all three terminals as independent connections, functioning as a voltage divider.

Note: Modern circuit diagrams typically use the standard symbol (Figure 1), while older diagrams may use the traditional representation (Figure 2).

2. How Does a Variable Resistor Work?

A variable resistor works by sliding a conductive wiper across a resistive track, which dynamically changes the effective electrical length and alters the resistance between the terminals.


Internal Structure of a Variable Resistor Showing Wiper and Resistive Track

Figure 4: Structure of a small-signal variable resistor

A typical small-signal variable resistor consists of:

  • Resistive track: Made of carbon film, metal film, or other resistive material

  • Wiper (moving contact): Slides across the resistive track

  • Terminals: Two fixed terminals at track ends and one wiper terminal

  • Adjustment mechanism: Usually a shaft or screw slot

Working Principle

When you rotate the adjustment shaft using a screwdriver:

  1. The wiper (moving contact) slides along the resistive track

  2. This changes the effective length of the resistive material between the wiper and each fixed terminal

  3. As the wiper moves closer to one fixed terminal, resistance decreases between them while increasing between the wiper and the other terminal

  4. The total resistance between the two fixed terminals remains constant

Example: When the wiper is at the extreme left position, resistance between the left terminal and wiper is zero, while resistance between the wiper and right terminal equals the component's full nominal resistance.

3. What Are the Different Types of Variable Resistors?

Variable resistors are primarily classified by their resistive materials—such as carbon film, metal film, or wire-wound—and their enclosure designs, which dictate their power handling and environmental durability.

With the global passive electronic components market expanding rapidly, advanced cermet and conductive plastic variable resistors are increasingly dominating high-cycle applications in 2026. However, traditional types remain highly relevant.

3.1 Film-type Variable Resistors

Carbon Film Variable Resistor for Small Signal Applications

Figure 5: Carbon film variable resistor

Film-type variable resistors use a synthetic carbon or metal film as the resistive element. They typically employ a rotary adjustment mechanism and are designed for small-signal applications.

Components:

  • Resistor body (synthetic carbon film)

  • Movable contact (metal reed or carbon contact)

  • Adjustment mechanism

  • Three terminals (two fixed, one moving)

Based on their enclosure design, film-type variable resistors are categorized into:

Full-sealed (Solid)
  • Made from carbon black, quartz powder, and organic binders

  • Sealed with metal casing

  • Excellent dust protection

  • Reliable contact performance

Semi-sealed
  • Similar resistor body to fully-sealed type

  • Uses metal reed for movable contact

  • Sealed with plastic outer cover

  • Easier to adjust but less dust-resistant

Non-sealed (Chip Adjustable)
  • Suspension liquid coated on glass fiberboard or bakelite

  • Limited dust protection

  • Contacts prone to oxidation

  • Higher failure rate

3.2 Wire-Wound Variable Resistors

Wire Wound Variable Resistor for High Power Applications

Figure 9: Wire-wound variable resistor

Wire-wound variable resistors use resistance wire wrapped around an insulating core. They are designed for power applications and offer:

  • Low noise characteristics

  • High temperature resistance

  • Ability to handle large currents

  • Suitable for voltage/current adjustment in low-frequency circuits

Wire-wound variable resistors are further classified as:

High-power (Sliding Wire) Types
  • Axial porcelain tube wire-wound

  • Porcelain disc wire-wound

  • Designed for high current applications

Low-power Types
  • Round vertical wire-wound

  • Round horizontal wire-wound

  • Square wire-wound

  • All feature fully sealed package structures

Application Guideline: For general-purpose applications with moderate current, metal variable resistors are recommended. For small currents, carbon film types are optimal. For high current applications, electrolytic variable resistors (with electrodes immersed in conductive liquid) offer the best performance.

4. What Are the Physical Characteristics of Variable Resistors?

The physical characteristics of variable resistors include a larger footprint than fixed resistors, a three-terminal configuration, and a mechanical adjustment shaft or slot for tuning.


Terminal Configuration and Pins of a Variable Resistor

Figure 10: Terminal configuration of a variable resistor

Variable resistors have distinct physical characteristics that set them apart from fixed resistors:

  • Size: Larger than standard resistors, making them easy to identify on circuit boards

  • Terminal configuration: Three terminals (one moving and two fixed)

  • Adjustment mechanism: Slot or shaft for screwdriver adjustment

  • Resistance marking: Shows the nominal (maximum) resistance value

Vertical Variable Resistors

  • Used in small-signal circuits

  • Three pins vertically downward

  • Mounted vertically on the circuit board

  • Horizontal adjustment port

Horizontal Variable Resistors

  • Used in small-signal circuits

  • Pins at 90° angle to the resistor body

  • Mounted vertically on the circuit board

  • Upward-facing adjustment port

Important Note: Variable resistors typically have higher failure rates than fixed resistors due to their mechanical components and adjustment mechanisms. This should be considered when designing circuits that require long-term reliability.

5. What Are the Main Functions and Applications in 2026?

In 2026, variable resistors function primarily to adjust circuit current, divide voltage, and calibrate sensitive electronic instruments across automotive, audio, and IoT applications.

Variable resistors serve several critical functions in electronic circuits:

Primary Functions

  • Adjusting circuit current by varying resistance

  • Dividing voltage (in potentiometer configuration)

  • Protecting sensitive components by limiting current

  • Calibrating electronic instruments

Common Applications

  • Audio equipment (volume, tone controls)

  • Light dimmers and smart home lighting systems

  • Motor speed controllers in industrial robotics

  • Signal generator characteristics adjustment

  • Sensor calibration for IoT edge devices

Selection Guide

Application TypeRecommended Variable Resistor
General current applicationsMetal-type variable resistors
Small current applicationsCarbon film type
Large current applicationsElectrolytic type
Audio controlPotentiometers (exponential for volume)
Precision applicationsMulti-turn potentiometers

6. What Is a Potentiometer and How Does It Differ?

A potentiometer is a specific three-terminal variable resistor configured to act as an adjustable voltage divider, whereas a standard variable resistor (rheostat) uses only two terminals to control current.


Potentiometer Symbols Showing Voltage Divider Configuration

Figure 11: Potentiometer symbols

A potentiometer is a special type of variable resistor that functions as a voltage divider. It divides the voltage applied to its fixed terminals according to the position of the wiper, providing adjustable output voltage.

The potentiometer concept can be compared to a water valve that controls flow, but for electrical signals instead of water. This makes it a crucial component in many electronic devices requiring manual adjustment.

6.1 Types of Potentiometers

Various Types of Potentiometers Including Rotary and Slider

Figure 12: Various types of potentiometers

Potentiometers can be categorized based on their construction materials and mechanical design:

By Material:
  • Carbon film potentiometers

  • Wire-wound potentiometers

  • Conductive plastic potentiometers

  • Cermet (ceramic-metal) potentiometers

By Design:
  • Rotary potentiometers

  • Linear sliding potentiometers

  • Multi-turn potentiometers

  • Digital/stepper potentiometers

  • Motorized potentiometers

Advanced Types: With increasing demand for precision audio equipment, specialized potentiometers have been developed:

  • Stepping potentiometers: Use series and parallel resistor networks to maintain synchronized resistance values in dual-track configurations, critical for stereo audio applications

  • Electric potentiometers: Incorporate motors that drive the potentiometer through gears, enabling remote control while maintaining the frequency characteristics of traditional potentiometers

6.2 Using Potentiometers

Identifying Potentiometers in Circuits

When working with potentiometers, the first step is to recognize their symbol in circuit diagrams, as illustrated in Figure 13. The second critical step is understanding the relationship between the circuit symbol and the physical potentiometer, particularly the position of the center tap (wiper).

Potentiometer Representation in Circuit Diagrams

Figure 13: Potentiometer representation in circuit diagrams

Since potentiometers are variable resistors, it's essential to consider both their resistance value and power rating when incorporating them into circuits. While their application principles align with regular resistors, potentiometers are uniquely designated in circuit diagrams with the symbol "RP" (or "W" in older circuit diagrams).

Understanding Resistance Values

The resistance value marked on a potentiometer represents its total resistance. For example, in Figure 13, if the resistance between terminals A and B is 10kΩ, then the resistance values between terminals AC and BC will vary from 0 to 10kΩ as you rotate the wiper.

Pro Tip: Finding the Center Tap

New users often struggle to identify the center tap (wiper terminal) on a potentiometer. To solve this issue, follow these three steps:

  1. Set your multimeter to the resistance (Ohms) mode.

  2. Measure the resistance between different pairs of terminals while rotating the shaft; the pair with constant resistance are the outer terminals (A and B).

  3. Identify the remaining terminal as the center tap (wiper, C), which will show varying resistance when measured against A or B during rotation.

Referring to Figure 13, when the wiper (C) moves closer to terminal A, the resistance between A and C decreases while the resistance between B and C increases. Conversely, when the wiper moves toward B, the AC resistance increases while the BC resistance decreases.

Resistance Changing Curves for Exponential, Logarithmic, and Linear Potentiometers

Figure 14: Resistance changing curves for different potentiometer types

Types of Potentiometers by Taper

Potentiometers come in three primary taper types, each with different resistance variation patterns as shown in Figure 14:

  • Exponential (Z): Resistance changes exponentially with rotation, making fine adjustments possible at one end of the range

  • Logarithmic (D): Resistance follows a logarithmic curve, ideal for audio applications

  • Linear (X): Resistance changes uniformly throughout the rotation range

These different taper types make potentiometers suitable for specific applications. For instance, logarithmic potentiometers are preferred for volume control in audio circuits because they match human hearing perception, while linear potentiometers are better suited for balance controls or applications requiring proportional adjustment.

Common Applications

  • Volume controls (logarithmic)

  • Light dimmers (linear)

  • Sensor calibration

  • Voltage dividers

  • Motor speed controls


Selection Criteria

  • Total resistance value

  • Power rating

  • Taper type (linear/log/exponential)

  • Mechanical design (rotary/slider)

  • Environmental considerations

Conclusion

This article has introduced the fundamental aspects of potentiometers, including their circuit symbols, structure, and functionality. We've explored the different taper types—exponential, logarithmic, and linear—and their specific applications. Understanding these characteristics enables you to select the appropriate potentiometer for your electronic projects, whether you're working with audio circuits, lighting controls, or precision measurement systems.

Recommended Articles


Frequently Asked Questions

What is the difference between a variable resistor and a potentiometer?

A variable resistor (rheostat) uses two terminals to control current flow in a circuit. A potentiometer uses all three terminals to act as a voltage divider. While all potentiometers can be wired as variable resistors, not all variable resistors can function as potentiometers.

How do you test a variable resistor with a multimeter?

To test a variable resistor, set your multimeter to the ohms (Ω) setting. Connect the probes to the two outer terminals to verify the total resistance. Then, move one probe to the center wiper terminal and turn the shaft; the resistance should change smoothly without sudden drops.

Can I use a potentiometer as a rheostat?

Yes, you can use a potentiometer as a rheostat by connecting only two of its terminals: the center wiper and one of the outer fixed terminals. It is recommended to tie the unused outer terminal to the wiper to prevent circuit interruption if the wiper loses contact.

Why do variable resistors fail?

Variable resistors typically fail due to mechanical wear, dirt accumulation on the resistive track, or thermal overload. In 2026, environmental sealing has improved, but repeated friction from the wiper eventually degrades the carbon or metal film, leading to "scratchy" outputs or dead spots.

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1.What is a variable resistor?

A variable resistor is a resistor of which the electric resistance value can be adjusted. When a variable resistor is used as a potential divider by using 3 terminals it is called a potentiometer. When only two terminals are used, it functions as a variable resistance and is called a rheostat.

2.What is a variable resistor used for?

A resistor limits the passage of electrical current. A fixed resistor has a resistance that does not change. The resistance of this resistor is changed by moving the position of a slider. A variable resistor is used in some dimmer switches and volume controls.

3.What is an example of a variable resistor?

Variable Resistors are resistors whose resistance values can vary according to some factor applied to them. For example, potentiometers are variable resistors that change when a user adjusts the knob. Photoresistors are variable resistors that change according to the light that strikes their surface.

4.How do variable resistors work?

A variable resistor works by adjusting the path that the current has to flow. Inside the resistor is a strip of metal or conducting ceramic that is connected to one part of the circuit. The dial you turn will move another piece of wire inside the resistor.

5.What are three common types of variable resistors?

The different types of variable resistors include:
Potentiometer.
Rheostat.
Thermistor.
Magneto resistor.
Photoresistor.
Humistor.
Force-sensitive resistor.
Related Articles

  • What are the Differences Between Pull up and Pull down Resistors?
    What are the Differences Between Pull up and Pull down Resistors?
    UTMEL22 October 202538073

    Pull up is to clamp an uncertain signal to a high level with a resistor, and the resistor also acts as a current limiter. In the same way, pull down means to clamp the uncertain signal to a low level through a resistor. To pull up is to input current to the device, and the pull-down is to output the current.

    Read More
  • Rheostat Basics: Types, Principle and Functions
    Rheostat Basics: Types, Principle and Functions
    UTMEL25 December 202517815

    A rheostat is a device that can adjust the size of the resistance and can be connected to the circuit to adjust the size of the current. A general rheostat is composed of a wire with a larger resistance and a device that can change the contact point to adjust the effective length of the resistance wire. Rheostat can limit the current and protect the circuit, and change the voltage distribution in the circuit.

    Read More
  • Basic Introduction to Metal Film Resistor
    Basic Introduction to Metal Film Resistor
    UTMEL28 August 202013755

    Metal film resistors are a kind of film resistors. Metal film resistors are resistors in which special metals or alloys are used as resistor materials, and the resistor film layer is basically formed on ceramic or glass by vacuum evaporation or sputtering.

    Read More
  • Varistor: Definition, Function, Working and Testing
    Varistor: Definition, Function, Working and Testing
    UTMEL03 April 202583287

    A varistor is a device with a non-linear volt-ampere characteristic. When the voltage applied to the varistor is lower than its threshold value, the current flowing through it is extremely small, which is equivalent to a resistor with infinite resistance, vice versa. The most common varistor is a metal oxide varistor (MOV).

    Read More
  • Photoresistor Basics: Types, Principles and Applications
    Photoresistor Basics: Types, Principles and Applications
    UTMEL16 October 202545398

    The article introduces the photoresistor’s main characteristics and principles including the working principle and structural principle. There are three types of photoresistor: ultraviolet photoresistors, infrared photoresistors, visible light photoresistors. Dimming circuit and light switch are the two applications of the photoresistor.

    Read More